/** * @file rm_linux_osal.c * * @brief * This is the OS abstraction layer used by the Resource Manager in Linux. * * \par * ============================================================================ * @n (C) Copyright 2012-2013, Texas Instruments, Inc. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * * \par */ /* Standard Includes */ #include #include #include /********************************************************************** ****************************** Defines ******************************* **********************************************************************/ /********************************************************************** ************************** Global Variables ************************** **********************************************************************/ uint32_t rmMallocCounter = 0; uint32_t rmFreeCounter = 0; /********************************************************************** *************************** OSAL Functions ************************** **********************************************************************/ /* FUNCTION PURPOSE: Allocates memory *********************************************************************** * DESCRIPTION: The function is used to allocate a memory block of the * specified size. */ void *Osal_rmMalloc (uint32_t num_bytes) { /* Increment the allocation counter. */ rmMallocCounter++; /* Allocate memory. */ return calloc(1, num_bytes); } /* FUNCTION PURPOSE: Frees memory *********************************************************************** * DESCRIPTION: The function is used to free a memory block of the * specified size. */ void Osal_rmFree (void *ptr, uint32_t size) { /* Increment the free counter. */ rmFreeCounter++; free(ptr); } /* FUNCTION PURPOSE: Critical section enter *********************************************************************** * DESCRIPTION: The function is used to enter a critical section. * Function protects against * * access from multiple cores * and * access from multiple threads on single core */ void *Osal_rmCsEnter(void) { return NULL; } /* FUNCTION PURPOSE: Critical section exit *********************************************************************** * DESCRIPTION: The function is used to exit a critical section * protected using Osal_cppiCsEnter() API. */ void Osal_rmCsExit(void *CsHandle) { } /* FUNCTION PURPOSE: Cache invalidate *********************************************************************** * DESCRIPTION: The function is used to indicate that a block of memory is * about to be accessed. If the memory block is cached then this * indicates that the application would need to ensure that the * cache is updated with the data from the actual memory. */ void Osal_rmBeginMemAccess(void *ptr, uint32_t size) { return; } /* FUNCTION PURPOSE: Cache writeback *********************************************************************** * DESCRIPTION: The function is used to indicate that the block of memory has * finished being accessed. If the memory block is cached then the * application would need to ensure that the contents of the cache * are updated immediately to the actual memory. */ void Osal_rmEndMemAccess(void *ptr, uint32_t size) { return; } /* FUNCTION PURPOSE: Creates a task blocking object *********************************************************************** * DESCRIPTION: The function is used to create a task blocking object * capable of blocking the task a RM instance is running * within */ void *Osal_rmTaskBlockCreate(void) { return(NULL); } /* FUNCTION PURPOSE: Blocks a RM instance *********************************************************************** * DESCRIPTION: The function is used to block a task whose context a * RM instance is running within. */ void Osal_rmTaskBlock(void *handle) { } /* FUNCTION PURPOSE: unBlocks a RM instance *********************************************************************** * DESCRIPTION: The function is used to unblock a task whose context a * RM instance is running within. */ void Osal_rmTaskUnblock(void *handle) { } /* FUNCTION PURPOSE: Deletes a task blocking object *********************************************************************** * DESCRIPTION: The function is used to delete a task blocking object * provided to a RM instance */ void Osal_rmTaskBlockDelete(void *handle) { } /* FUNCTION PURPOSE: Prints a variable list *********************************************************************** * DESCRIPTION: The function is used to print a string to the console */ void Osal_rmLog (char *fmt, ... ) { va_list ap; va_start(ap, fmt); vprintf(fmt, ap); va_end(ap); }