index 03bd89de5e7d8a3888026227ddb8dbf15ecd6485..0745d743ba389e16699f743e00cf6216d8922065 100644 (file)
--- a/rm.h
+++ b/rm.h
#define RM_ERROR_NS_NAME_AND_RES_VAL_CONFLICT RM_ERROR_BASE-36
/** Instance type not recognized */
#define RM_ERROR_INVALID_INST_TYPE RM_ERROR_BASE-37
-/** Linux DTB alias properties specified in GRL but no Linux DTB provided during server instance init */
-#define RM_ERROR_GRL_LINUX_ALIAS_BUT_NO_DTB RM_ERROR_BASE-38
/** RM attempted to allocate a transport packet but the rmAllocPkt callout was not registered */
-#define RM_ERROR_TRANSPORT_ALLOC_PKT_NOT_REGD RM_ERROR_BASE-39
+#define RM_ERROR_TRANSPORT_ALLOC_PKT_NOT_REGD RM_ERROR_BASE-38
/** RM attempted to send a packet but the rmSendPkt callout was not registered */
-#define RM_ERROR_TRANSPORT_SEND_NOT_REGD RM_ERROR_BASE-40
+#define RM_ERROR_TRANSPORT_SEND_NOT_REGD RM_ERROR_BASE-39
/** RM attempted to send a response packet but the transport to the remote instance that sent
* the request packet is not registered */
-#define RM_ERROR_TRANSPORT_REMOTE_HNDL_NOT_REGD RM_ERROR_BASE-41
+#define RM_ERROR_TRANSPORT_REMOTE_HNDL_NOT_REGD RM_ERROR_BASE-40
/** RM instance cannot be deleted with transports still registered */
-#define RM_ERROR_CANT_DELETE_WITH_REGD_TRANSPORT RM_ERROR_BASE-42
+#define RM_ERROR_CANT_DELETE_WITH_REGD_TRANSPORT RM_ERROR_BASE-41
/** RM instance cannot be deleted with open service handle */
-#define RM_ERROR_CANT_DELETE_WITH_OPEN_SERV_HNDL RM_ERROR_BASE-43
+#define RM_ERROR_CANT_DELETE_WITH_OPEN_SERV_HNDL RM_ERROR_BASE-42
/** RM instance cannot be deleted when there are transactions pending and the
* ignorePendingServices parameter is set to false */
-#define RM_ERROR_CANT_DELETE_PENDING_TRANSACTIONS RM_ERROR_BASE-44
+#define RM_ERROR_CANT_DELETE_PENDING_TRANSACTIONS RM_ERROR_BASE-43
/** Only the Server instance can be used to return resource status via the
* Rm_resourceStatus API */
-#define RM_ERROR_INVALID_RES_STATUS_INSTANCE RM_ERROR_BASE-45
+#define RM_ERROR_INVALID_RES_STATUS_INSTANCE RM_ERROR_BASE-44
/** RM Shared Server and Client instances should always return a finished request since
* the instance has access to the resource structures no matter what core the service
* is requested from */
-#define RM_ERROR_SHARED_INSTANCE_UNFINISHED_REQ RM_ERROR_BASE-46
+#define RM_ERROR_SHARED_INSTANCE_UNFINISHED_REQ RM_ERROR_BASE-45
/** RM Shared Server and Client instances cannot register transports */
-#define RM_ERROR_SHARED_INSTANCE_CANNOT_REG_TRANS RM_ERROR_BASE-47
+#define RM_ERROR_SHARED_INSTANCE_CANNOT_REG_TRANS RM_ERROR_BASE-46
/** RM Shared Client handle was provided an invalid Shared Server handle. The shared
* server handle was either NULL or was not an instance of type Rm_instType_SHARED_SERVER */
-#define RM_ERROR_INVALID_SHARED_SERVER_HANDLE RM_ERROR_BASE-48
+#define RM_ERROR_INVALID_SHARED_SERVER_HANDLE RM_ERROR_BASE-47
/**
* @brief Maximum number of characters allowed for RM instance, resource, and