index e41967289eb2bda043899d510cfcdbcc417ec365..4203e0c248c1471ac2b0c706f5dbbb654816d1fd 100644 (file)
--- a/rm.h
+++ b/rm.h
#define RM_ERROR_ALREADY_REGD_SERVER_OR_CD RM_ERROR_BASE-37
/** Transport registration callout function pointers specified as valid but were NULL */
#define RM_ERROR_NULL_CALLOUTS_WHEN_VALID RM_ERROR_BASE-38
-/** Service both a NameServer name and a base, length, or alignment */
+/** Service has both a NameServer name and a base, length, or alignment specified */
#define RM_ERROR_NS_NAME_AND_RES_VAL_CONFLICT RM_ERROR_BASE-39
/** Instance type not recognized */
#define RM_ERROR_INVALID_INST_TYPE RM_ERROR_BASE-40
* must match an instance name defined in the "valid-instances" lists contained
* in the global and static policy DTS files. Resources and privileges to the
* resources will be based on the name assigned to the RM instance*/
- char *instName;
+ const char *instName;
/** The type of RM instance that will be created. */
Rm_InstType instType;
/** Instance-type specific configurations */
* @retval
* Failure - NULL Rm_Handle and result < #RM_OK
*/
-Rm_Handle Rm_init(Rm_InitCfg *initCfg, int32_t *result);
+Rm_Handle Rm_init(const Rm_InitCfg *initCfg, int32_t *result);
/**
* @b Description