index f61840c2904a90428fd6ee5ea41597b06867ca88..91947c78aa9bc74868f6dc3ddef8940075dba594 100644 (file)
--- a/rm.h
+++ b/rm.h
#define RM_ERROR_TRANSPORT_ALLOC_PKT_NOT_REGD RM_ERROR_BASE-37
/** RM attempted to send a packet but the rmSendPkt callout was not registered */
#define RM_ERROR_TRANSPORT_SEND_NOT_REGD RM_ERROR_BASE-38
-/** RM attempted to send a response packet but the transport to the remote instance that sent
- * the request packet is not registered */
-#define RM_ERROR_TRANSPORT_REMOTE_HNDL_NOT_REGD RM_ERROR_BASE-39
/** RM instance cannot be deleted with transports still registered */
-#define RM_ERROR_CANT_DELETE_WITH_REGD_TRANSPORT RM_ERROR_BASE-40
+#define RM_ERROR_CANT_DELETE_WITH_REGD_TRANSPORT RM_ERROR_BASE-39
/** RM instance cannot be deleted with open service handle */
-#define RM_ERROR_CANT_DELETE_WITH_OPEN_SERV_HNDL RM_ERROR_BASE-41
+#define RM_ERROR_CANT_DELETE_WITH_OPEN_SERV_HNDL RM_ERROR_BASE-40
/** RM instance cannot be deleted when there are transactions pending and the
* ignorePendingServices parameter is set to false */
-#define RM_ERROR_CANT_DELETE_PENDING_TRANSACTIONS RM_ERROR_BASE-42
+#define RM_ERROR_CANT_DELETE_PENDING_TRANSACTIONS RM_ERROR_BASE-41
/** Only the Server instance can be used to return resource status via the
* Rm_resourceStatus API */
-#define RM_ERROR_INVALID_RES_STATUS_INSTANCE RM_ERROR_BASE-43
+#define RM_ERROR_INVALID_RES_STATUS_INSTANCE RM_ERROR_BASE-42
/** RM Shared Server and Client instances should always return a finished request since
* the instance has access to the resource structures no matter what core the service
* is requested from */
-#define RM_ERROR_SHARED_INSTANCE_UNFINISHED_REQ RM_ERROR_BASE-44
+#define RM_ERROR_SHARED_INSTANCE_UNFINISHED_REQ RM_ERROR_BASE-43
/** RM Shared Server and Client instances cannot register transports */
-#define RM_ERROR_SHARED_INSTANCE_CANNOT_REG_TRANS RM_ERROR_BASE-45
+#define RM_ERROR_SHARED_INSTANCE_CANNOT_REG_TRANS RM_ERROR_BASE-44
/** RM Shared Client handle was provided an invalid Shared Server handle. The shared
* server handle was either NULL or was not an instance of type Rm_instType_SHARED_SERVER */
-#define RM_ERROR_INVALID_SHARED_SERVER_HANDLE RM_ERROR_BASE-46
+#define RM_ERROR_INVALID_SHARED_SERVER_HANDLE RM_ERROR_BASE-45
/** A RM Client failed to create a new transaction to request data from the Server in order
* to potentially process a transaction on a Client Delegate */
-#define RM_ERROR_TRANS_REQ_TO_SERVER_NOT_CREATED RM_ERROR_BASE-47
+#define RM_ERROR_TRANS_REQ_TO_SERVER_NOT_CREATED RM_ERROR_BASE-46
/** Service request required a policy check but instance was not initialized with a policy */
-#define RM_ERROR_INSTANCE_HAS_NO_POLICY RM_ERROR_BASE-48
+#define RM_ERROR_INSTANCE_HAS_NO_POLICY RM_ERROR_BASE-47
/** RM Client Delegate was not provided a policy at initialization */
-#define RM_ERROR_INVALID_CD_CONFIGURATION RM_ERROR_BASE-49
+#define RM_ERROR_INVALID_CD_CONFIGURATION RM_ERROR_BASE-48
/** RM CD freed local resources which allowed a free request of local request to be sent to
* the Server. The Server free failed so the CD tried to realloc the local resources
* that were originally freed. The re-allocate operation failed causing a resource loss
* on the CD */
-#define RM_ERROR_LOST_RESOURCES_ON_CD RM_ERROR_BASE-50
+#define RM_ERROR_LOST_RESOURCES_ON_CD RM_ERROR_BASE-49
/**
* @brief Maximum number of characters allowed for RM instance, resource, and