index f61840c2904a90428fd6ee5ea41597b06867ca88..d5bd177b329f32915fd4eea81abf36004b52e6ab 100644 (file)
--- a/rm.h
+++ b/rm.h
*
* \par
* ============================================================================
- * @n (C) Copyright 2012-2013, Texas Instruments, Inc.
+ * @n (C) Copyright 2012-2015, Texas Instruments, Inc.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
*
* @section intro Introduction
*
- * The Resource Manager (RM) is designed to provide an easy to use, extensible
- * uinified resource management solution on TI devices. RM can be integrated by
- * a system application to provide resource management services to the system
- * temporally (pre-main/post-main) and spatially (system subcomponents, task,
- * cores).
+ * The Resource Manager (RM) is designed to provide an easy to use,
+ * extensible uinified resource management solution on TI devices. RM can be
+ * integrated by a system application to provide resource management services
+ * to the system temporally (pre-main/post-main) and spatially (system
+ * subcomponents, task, cores).
*
- * The RM architecture is instance based. All RM resource management services
- * must originate from a RM instance. Resource permissions are assigned by a
- * system integrator using RM instance names provided during the initialization
- * of each RM instance in use. There are three types of RM instances, all of
- * which can be used by the system to request resource management services:
+ * The RM architecture is instance based. All RM resource management
+ * services must originate from a RM instance. Resource permissions are
+ * assigned by a system integrator using RM instance names provided during the
+ * initialization of each RM instance in use. There are three types of RM
+ * instances, all of which can be used by the system to request resource
+ * management services:
* - Server - Manages all resource data structures including the resource
* allocators, the permissions policies, and a simple NameServer.
* There can only be one Server per RM ecosystem. If two Servers
* are initialized within a system they must manage mutually
- * exclusive sets of device resources. There is no limit to the
+ * exclusive sets of device resources. There is no limit to the
* number of Client and Client Delegate instances that can connect
* to the Server
- * - Client - Used by system components to request resource services. There is
- * no limit to the number of Clients a system can have. Client
- * names must be unique since resource permissions are assigned based
- * on RM instance names. Clients can connect to at most one Server
- * or Client Delegate, but not both at the same time.
+ * - Client - Used by system components to request resource services. There
+ * is no limit to the number of Clients a system can have. Client
+ * names must be unique since resource permissions are assigned
+ * based on RM instance names. Clients can connect to at most
+ * one Server or Client Delegate, but not both at the same time.
* - Client Delegate (CD) - At the moment the CD is not different from the
- * Client. However, in the future the CD will be able
- * to act as a proxy for the Server. The CD will be
- * able to satisfy some service requests from Clients,
- * offloading some processing from the Server. This
- * feature will be helpful in situations where a
- * slower data path exists between the Server and
- * CD/Client instances. There is no limit to the number
- * of Clients that can connect to a CD. The CD can
- * connect to at most one Server.
+ * Client. However, in the future the CD will be
+ * able to act as a proxy for the Server. The CD
+ * will be able to satisfy some service requests
+ * from Clients, offloading some processing from
+ * the Server. This feature will be helpful in
+ * situations where a slower data path exists
+ * between the Server and CD/Client instances.
+ * There is no limit to the number of Clients that
+ * can connect to a CD. The CD can connect to at
+ * most one Server.
*
- * RM instances communicate via a generic transport interface. The RM transport
- * interface expects the application to configure and manage the transport data paths
- * between RM instances. This allows RM to easily extend to different device
- * configurations and different devices entirely.
+ * RM instances communicate via a generic transport interface. The RM
+ * transport interface expects the application to configure and manage the
+ * transport data paths between RM instances. This allows RM to easily
+ * extend to different device configurations and different devices entirely.
*
- * Shared memory versions of the Server and Client are available for configuration
- * in cases where the DSP applications cannot tolerate blocking operations or long wait
- * times for resources. The Shared Server - Shared Client model assumes all memory
- * allocated via the OSAL layer is within shared memory. RM service requests
- * received from Shared Servers and Shared Clients will be handled via accesses
- * to the resource management data structures existing in shared memory.
- * - Shared Server - Essentially a Server instance that expects to be allocated
- * from shared memory via the application-supplied OSAL functions.
- * Shared Client instances will piggyback on the Shared Server
- * instance to allocate/free resources without the need to setup
- * transports between the instances. Access to the resource
- * management data structures is managed through OSAL implemented
- * cache writeback and invalidate operations.
- * - Shared Client - Must be provided a Shared Server handle at initialization time.
- * The Shared Client will essentially use the resource management
- * data structures, created in shared memory when the Shared Server
- * was initialized, to handle any server requests.
-
- * RM utilizes the BDS-licensed, open source, Flattened Device Tree format to
- * specify what resources are managed by RM as well as the RM instance permissions
- * for managed resources. The Global Resource List or GRL defines all device
- * resources and their ranges that will be tracked by the RM Server. Addition or
- * subtraction of resources from RM requires one modify only the GRL. RM source code
- * changes are not required to add or subtract resources from RM's umbrella of
- * management. RM Policies specify resource permissions for the RM instances. There
- * are two types of Policies:
- * - Global Policy - Provided to the Server at initialization and defines the
- * resource permissions for all RM instances in the system.
- * All service requests will be validated against the Global
- * Policy on the Server. If the RM instance is found to not
- * hold the privileges for the request a denial of the service
- * will be issued back to the requesting instance.
+ * Shared memory versions of the Server and Client are available for
+ * configuration in cases where the DSP applications cannot tolerate blocking
+ * operations or long wait times for resources. The Shared Server - Shared
+ * Client model assumes all memory allocated via the OSAL layer is within
+ * shared memory. RM service requests received from Shared Servers and
+ * Shared Clients will be handled via accesses to the resource management
+ * data structures existing in shared memory.
+ * - Shared Server - Essentially a Server instance that expects to be
+ * allocated from shared memory via the application-supplied
+ * OSAL functions. Shared Client instances will piggyback
+ * on the Shared Server instance to allocate/free resources
+ * without the need to setup transports between the
+ * instances. Access to the resource management data
+ * structures is managed through OSAL implemented cache
+ * writeback and invalidate operations.
+ * - Shared Client - Must be provided a Shared Server handle at initialization
+ * time. The Shared Client will essentially use the
+ * resource management data structures, created in shared
+ * memory when the Shared Server was initialized, to handle
+ * any server requests.
+ *
+ * RM utilizes the BDS-licensed, open source, Flattened Device Tree format to
+ * specify what resources are managed by RM as well as the RM instance
+ * permissions for managed resources. The Global Resource List or GRL defines
+ * all device resources and their ranges that will be tracked by the
+ * RM Server. Addition or subtraction of resources from RM requires one
+ * modify only the GRL. RM source code changes are not required to add or
+ * subtract resources from RM's umbrella of management. RM Policies specify
+ * resource permissions for the RM instances. There are two types of
+ * Policies:
+ * - Global Policy - Provided to the Server at initialization and defines
+ * the resource permissions for all RM instances in the
+ * system. All service requests will be validated against
+ * the Global Policy on the Server. If the RM instance is
+ * found to not hold the privileges for the request a
+ * denial of the service will be issued back to the
+ * requesting instance.
* - Static Policy - Optionally provided to Client and CD instances at
- * initialization. Allows these instances to statically
+ * initialization. Allows these instances to statically
* allocate resources. This feature is typically used
* for RM instances that must allocate resources prior
- * to the transport connection to the Server being established.
- * Resources allocated via any Static Policies will
- * be validated against the Global Policy once the transport
+ * to the transport connection to the Server being
+ * established. Resources allocated via any Static
+ * Policies will be validated against the Global Policy
+ * once the transport
* to the Server has been fully established. If a Static
- * Policy request fails validation with the Global Policy the
- * RM instance that issued the static request will be placed
- * into a locked state. The locked state prevents any further
- * service requests from the instance.
+ * Policy request fails validation with the Global Policy
+ * the RM instance that issued the static request will be
+ * placed into a locked state. The locked state prevents
+ * any further service requests from the instance.
*
- * Combined, the GRL and Policy Device Tree implementations allow RM to easily extend
- * to new resources without the need to recompile the RM source code.
+ * Combined, the GRL and Policy Device Tree implementations allow RM to easily
+ * extend to new resources without the need to recompile the RM source code.
*
* RM instances currently provides the following resource services:
* - Allocate (initialize) - Allocate a resource for initialization
* - Allocate (usage) - Allocate a resource for use
- * - Status - Return the reference count for a specified resource
- * - Free - Free an allocated resource (The free must originate
- * from the RM instance that allocated the resource
+ * - Status - Return the reference count for a specified
+ * resource
+ * - Free - Free an allocated resource (The free must
+ * originate from the RM instance that allocated
+ * the resource
* - Map resource to name - Map a specified resource to a NameServer name
* - Unmap named resource - Unmap a resource from an existing NameServer name
- * - Get resource by name - Returns a resource based on a provided NameServer name
+ * - Get resource by name - Returns a resource based on a provided NameServer
+ * name
*/
-
+
/* Define RM_API as a master group in Doxygen format and add all RM API
definitions to this group. */
/** @defgroup RM_API Resource Manager API
#define RM_SERVICE_PENDING_SERVER_RESPONSE 2
/** RM has approved requested service */
#define RM_SERVICE_APPROVED 3
-/** RM has approved requested service based on static policy. Request will be validated
- * against global policy once all transports have been registered */
+/** RM has approved requested service based on static policy. Request will be
+ * validated against global policy once all transports have been registered */
#define RM_SERVICE_APPROVED_STATIC 4
/** RM service request denial reasons base */
#define RM_SERVICE_DENIED_RES_NOT_ALLOCD_TO_INST RM_SERVICE_DENIED_BASE+3
/** Free request resource range already free */
#define RM_SERVICE_DENIED_RES_ALREADY_FREE RM_SERVICE_DENIED_BASE+4
-/** Allocate request resource range partially allocated (Handling of partial allocations
- * not yet implemented) */
+/** Allocate request resource range partially allocated (Handling of partial
+ * allocations not yet implemented) */
#define RM_SERVICE_DENIED_PARTIAL_ALLOCATION RM_SERVICE_DENIED_BASE+5
-/** Free request resource range partially free (Handling of partial frees not yet implemented) */
+/** Free request resource range partially free (Handling of partial frees not
+ * yet implemented) */
#define RM_SERVICE_DENIED_PARTIAL_FREE RM_SERVICE_DENIED_BASE+6
-/** Requirements of allocate request could not be satisfied (occurs for UNSPECIFIED base
- * and/or alignment requests */
+/** Requirements of allocate request could not be satisfied (occurs for
+ * UNSPECIFIED base and/or alignment requests */
#define RM_SERVICE_DENIED_RES_ALLOC_REQS_NOT_MET RM_SERVICE_DENIED_BASE+7
/** NameServer add request name string already exists in NameServer */
#define RM_SERVICE_DENIED_NAME_EXISTS_IN_NS RM_SERVICE_DENIED_BASE+8
#define RM_SERVICE_DENIED_INIT_PERM_NOT_GIVEN RM_SERVICE_DENIED_BASE+10
/** Use allocate request resource range not given use privileges in policy */
#define RM_SERVICE_DENIED_USE_PERM_NOT_GIVEN RM_SERVICE_DENIED_BASE+11
-/** Allocate request resource range marked as exclusive in policy has already been allocated */
+/** Allocate request resource range marked as exclusive in policy has already
+ * been allocated */
#define RM_SERVICE_DENIED_EXCLUSIVE_RES_ALLOCD RM_SERVICE_DENIED_BASE+12
-/** Allocate request resource range allocated to an instance assigned exclusive privileges in policy */
+/** Allocate request resource range allocated to an instance assigned exclusive
+ * privileges in policy */
#define RM_SERVICE_DENIED_ALLOCD_TO_EXCLUSIVE_INST RM_SERVICE_DENIED_BASE+13
/** Static allocate request was not an allocate-use or allocate-init request */
#define RM_SERVICE_DENIED_INVALID_STATIC_REQUEST RM_SERVICE_DENIED_BASE+14
/** Static allocate request denied by static policy */
#define RM_SERVICE_DENIED_BY_STATIC_POLICY RM_SERVICE_DENIED_BASE+15
-/** RM instance locked from further services since a static allocation failed validation against
- * global policy. RM instance cannot be unlocked. Please make sure static policy and global policy
- * are in sync */
+/** RM instance locked from further services since a static allocation failed
+ * validation against global policy. RM instance cannot be unlocked. Please
+ * make sure static policy and global policy are in sync */
#define RM_SERVICE_DENIED_RM_INSTANCE_LOCKED RM_SERVICE_DENIED_BASE+16
-/** Allocate request denied because the resource is already reserved by Linux and "Shared Linux"
- * privileges are not assigned to the requesting instance */
+/** Allocate request denied because the resource is already reserved by Linux
+ * and "Shared Linux" privileges are not assigned to the requesting instance */
#define RM_SERVICE_DENIED_RES_NOT_SHARED_LINUX RM_SERVICE_DENIED_BASE+17
-/** Status request resource range partially found (Handling of partial status requests not yet implemented) */
+/** Status request resource range partially found (Handling of partial status
+ * requests not yet implemented) */
#define RM_SERVICE_DENIED_PARTIAL_STATUS RM_SERVICE_DENIED_BASE+18
+/** RM Client Delegate instance is not stable. RM system operation cannot be
+ * guarateed if a CD instance is used. At the time please manage resources
+ * using Server and Client instances - tracked by SDOCM00100797 */
+#define RM_WARNING_CD_INSTANCE_NOT_STABLE (-1024)
+
/** Start of libfdt.h error codes */
#define RM_ERROR_LIBFDT_START (-1)
/** End of libfdt.h error codes */
#define RM_ERROR_LIBFDT_END (-13)
-/** RM error base */
+/** RM error base */
#define RM_ERROR_BASE (-64)
/** Instance name provided is NULL or greater than RM_NAME_MAX_CHARS */
#define RM_ERROR_INVALID_INST_NAME RM_ERROR_BASE-1
/** List of "valid-instances" not found in global or static policy */
#define RM_ERROR_NO_VALID_INST_IN_POLICY RM_ERROR_BASE-2
-/** Instance specified in permissions string does not match any instances specified in the
- * "valid-instances" list */
+/** Instance specified in permissions string does not match any instances
+ * specified in the "valid-instances" list */
#define RM_ERROR_PERM_STR_INST_NOT_VALID RM_ERROR_BASE-3
/** Resource specified in global policy does not have an allocator */
#define RM_ERROR_UNKNOWN_RESOURCE_IN_POLICY RM_ERROR_BASE-4
#define RM_ERROR_PERM_STR_TOO_MANY_ASSIGN_CHARS RM_ERROR_BASE-6
/** Permissions string contains invalid character */
#define RM_ERROR_PERM_STR_INVALID_CHAR RM_ERROR_BASE-7
-/** Permissions string contains a permission character without the assignment operator
- * Ex: assignments = <12 1>, "iux (RM_Client_Delegate)"; */
+/** Permissions string contains a permission character without the assignment
+ * operator Ex: assignments = <12 1>, "iux (RM_Client_Delegate)"; */
#define RM_ERROR_PERM_CHAR_WITHOUT_ASSIGN_CHAR RM_ERROR_BASE-8
-/** Permissions string contains a permission character on opposite side of already made assignment
+/** Permissions string contains a permission character on opposite side of
+ * already made assignment
* Ex: assignments = <12 1>, "iux = (RM_Client_Delegate) x"; */
#define RM_ERROR_INVALID_PERMS_CHAR_ON_RIGHT RM_ERROR_BASE-9
/** Policy resource node contains an unknown property */
#define RM_ERROR_UNKNOWN_POLICY_RESOURCE_PROPERTY RM_ERROR_BASE-10
-/** Instance name provided in "valid-instances" list is greater than RM_NAME_MAX_CHARS */
+/** Instance name provided in "valid-instances" list is greater than
+ * RM_NAME_MAX_CHARS */
#define RM_ERROR_VALID_INST_NAME_TOO_LONG RM_ERROR_BASE-11
/** Instance name in permissions assignment is greater than RM_NAME_MAX_CHARS */
#define RM_ERROR_INST_NAME_IN_ASSIGNMENT_TOO_LONG RM_ERROR_BASE-12
-/** NameServer name in global resource list nameServer assignment is greater than RM_NAME_MAX_CHARS */
-#define RM_ERROR_GRL_NS_ASSIGNMENT_NAME_TOO_LONG RM_ERROR_BASE-13
+/** NameServer name in global resource list nameServer assignment and/or
+ * service request is greater than RM_NAME_MAX_CHARS */
+#define RM_ERROR_NAMESERVER_NAME_TOO_LONG RM_ERROR_BASE-13
/** Linux alias assignment in global resource list is invalid */
#define RM_ERROR_GRL_INVALID_LINUX_ALIAS_FORMAT RM_ERROR_BASE-14
/** Error allocating memory for the service handle */
#define RM_ERROR_GRL_UNKNOWN_RESOURCE_PROPERTY RM_ERROR_BASE-17
/** Could not find an allocator for the specified resource */
#define RM_ERROR_RES_ALLOCATOR_DOES_NOT_EXIST RM_ERROR_BASE-18
-/** A resource node is specified more than once in the Global Resource List (GRL) */
-#define RM_ERROR_GRL_RES_SPECIFIED_MORE_THAN_ONCE RM_ERROR_BASE-19
+/** A resource node is specified more than once in either the
+ * Global Resource List (GRL) or policy. GRL for RM Server. Policy for
+ * CD or Client */
+#define RM_ERROR_RES_SPECIFIED_MORE_THAN_ONCE RM_ERROR_BASE-19
/** No data was found at the GRL resource node's specified Linux alias path */
#define RM_ERROR_DATA_NOT_FOUND_AT_LINUX_ALIAS RM_ERROR_BASE-20
-/** RM server was not provided a Global Resource List (GRL) and global policy at initialization */
+/** RM server was not provided a Global Resource List (GRL) and global policy
+ * at initialization */
#define RM_ERROR_INVALID_SERVER_CONFIGURATION RM_ERROR_BASE-21
/** Service request type not recognized */
#define RM_ERROR_INVALID_SERVICE_TYPE RM_ERROR_BASE-22
/** rmAllocPkt transport callout returned NULL for rmPkt */
#define RM_ERROR_TRANSPORT_ALLOC_PKT_ERROR RM_ERROR_BASE-23
-/** rmSendPkt transport callout returned error when attempting to send the rmPkt */
+/** rmSendPkt transport callout returned error when attempting to send the
+ * rmPkt */
#define RM_ERROR_TRANSPORT_SEND_ERROR RM_ERROR_BASE-24
/** A RM service transaction could not be created for the service request */
#define RM_ERROR_SERVICE_TRANS_NOT_CREATED RM_ERROR_BASE-25
/** RM service transaction could not be found in instance's transaction queue */
#define RM_ERROR_SERVICE_TRANS_DOES_NOT_EXIST RM_ERROR_BASE-26
-/** NameServer does not exist in instance, cannot satisfy NameServer service request */
+/** NameServer does not exist in instance, cannot satisfy NameServer service
+ * request */
#define RM_ERROR_NAMESERVER_DOES_NOT_EXIST RM_ERROR_BASE-27
/** Service request to add a name to the NameServer failed */
#define RM_ERROR_NAMESERVER_NAME_ADD_FAILED RM_ERROR_BASE-28
/** Could not find name specified in service request in NameServer */
#define RM_ERROR_NAMESERVER_NAME_DOES_NOT_EXIST RM_ERROR_BASE-29
-/** Service request made on Client or CD when no transport established and no static policy registered */
+/** Service request made on Client or CD when no transport established and no
+ * static policy registered */
#define RM_ERROR_REQ_FAILED_NO_STATIC_POLICY RM_ERROR_BASE-30
/** RM transport handle has not been registered with the RM instance */
#define RM_ERROR_TRANSPORT_HANDLE_DOES_NOT_EXIST RM_ERROR_BASE-31
#define RM_ERROR_RECEIVED_INVALID_PACKET_TYPE RM_ERROR_BASE-32
/** RM response packet does not match any requests sent from instance */
#define RM_ERROR_PKT_RESP_DOES_NOT_MATCH_ANY_REQ RM_ERROR_BASE-33
-/** Server attempted to connect to another server or a CD attempted to connect to another CD or
- * Client attempted to connect to another client */
+/** Server attempted to connect to another server or a CD attempted to connect
+ * to another CD or Client attempted to connect to another client */
#define RM_ERROR_INVALID_REMOTE_INST_TYPE RM_ERROR_BASE-34
-/** RM client attempted to register with more than one Server or CD or a CD attempted to register
- * with more than one Server */
+/** RM client attempted to register with more than one Server or CD or a CD
+ * attempted to register with more than one Server */
#define RM_ERROR_ALREADY_REGD_SERVER_OR_CD RM_ERROR_BASE-35
/** Instance type not recognized */
#define RM_ERROR_INVALID_INST_TYPE RM_ERROR_BASE-36
-/** RM attempted to allocate a transport packet but the rmAllocPkt callout was not registered */
+/** RM attempted to allocate a transport packet but the rmAllocPkt callout was
+ * not registered */
#define RM_ERROR_TRANSPORT_ALLOC_PKT_NOT_REGD RM_ERROR_BASE-37
-/** RM attempted to send a packet but the rmSendPkt callout was not registered */
+/** RM attempted to send a packet but the rmSendPkt callout was not
+ * registered */
#define RM_ERROR_TRANSPORT_SEND_NOT_REGD RM_ERROR_BASE-38
-/** RM attempted to send a response packet but the transport to the remote instance that sent
- * the request packet is not registered */
-#define RM_ERROR_TRANSPORT_REMOTE_HNDL_NOT_REGD RM_ERROR_BASE-39
/** RM instance cannot be deleted with transports still registered */
-#define RM_ERROR_CANT_DELETE_WITH_REGD_TRANSPORT RM_ERROR_BASE-40
+#define RM_ERROR_CANT_DELETE_WITH_REGD_TRANSPORT RM_ERROR_BASE-39
/** RM instance cannot be deleted with open service handle */
-#define RM_ERROR_CANT_DELETE_WITH_OPEN_SERV_HNDL RM_ERROR_BASE-41
-/** RM instance cannot be deleted when there are transactions pending and the
+#define RM_ERROR_CANT_DELETE_WITH_OPEN_SERV_HNDL RM_ERROR_BASE-40
+/** RM instance cannot be deleted when there are transactions pending and the
* ignorePendingServices parameter is set to false */
-#define RM_ERROR_CANT_DELETE_PENDING_TRANSACTIONS RM_ERROR_BASE-42
+#define RM_ERROR_CANT_DELETE_PENDING_TRANSACTIONS RM_ERROR_BASE-41
/** Only the Server instance can be used to return resource status via the
* Rm_resourceStatus API */
-#define RM_ERROR_INVALID_RES_STATUS_INSTANCE RM_ERROR_BASE-43
-/** RM Shared Server and Client instances should always return a finished request since
- * the instance has access to the resource structures no matter what core the service
- * is requested from */
-#define RM_ERROR_SHARED_INSTANCE_UNFINISHED_REQ RM_ERROR_BASE-44
+#define RM_ERROR_INVALID_RES_STATUS_INSTANCE RM_ERROR_BASE-42
+/** RM Shared Server and Client instances should always return a finished
+ * request since the instance has access to the resource structures no matter
+ * what core the service is requested from */
+#define RM_ERROR_SHARED_INSTANCE_UNFINISHED_REQ RM_ERROR_BASE-43
/** RM Shared Server and Client instances cannot register transports */
-#define RM_ERROR_SHARED_INSTANCE_CANNOT_REG_TRANS RM_ERROR_BASE-45
-/** RM Shared Client handle was provided an invalid Shared Server handle. The shared
- * server handle was either NULL or was not an instance of type Rm_instType_SHARED_SERVER */
-#define RM_ERROR_INVALID_SHARED_SERVER_HANDLE RM_ERROR_BASE-46
-/** A RM Client failed to create a new transaction to request data from the Server in order
- * to potentially process a transaction on a Client Delegate */
-#define RM_ERROR_TRANS_REQ_TO_SERVER_NOT_CREATED RM_ERROR_BASE-47
-/** Service request required a policy check but instance was not initialized with a policy */
-#define RM_ERROR_INSTANCE_HAS_NO_POLICY RM_ERROR_BASE-48
+#define RM_ERROR_SHARED_INSTANCE_CANNOT_REG_TRANS RM_ERROR_BASE-44
+/** RM Shared Client handle was provided an invalid Shared Server handle.
+ * The shared server handle was either NULL or was not an instance of type
+ * Rm_instType_SHARED_SERVER */
+#define RM_ERROR_INVALID_SHARED_SERVER_HANDLE RM_ERROR_BASE-45
+/** A RM Client failed to create a new transaction to request data from the
+ * Server in order to potentially process a transaction on a Client Delegate */
+#define RM_ERROR_TRANS_REQ_TO_SERVER_NOT_CREATED RM_ERROR_BASE-46
+/** Service request required a policy check but instance was not initialized
+ * with a policy */
+#define RM_ERROR_INSTANCE_HAS_NO_POLICY RM_ERROR_BASE-47
/** RM Client Delegate was not provided a policy at initialization */
-#define RM_ERROR_INVALID_CD_CONFIGURATION RM_ERROR_BASE-49
-/** RM CD freed local resources which allowed a free request of local request to be sent to
- * the Server. The Server free failed so the CD tried to realloc the local resources
- * that were originally freed. The re-allocate operation failed causing a resource loss
- * on the CD */
-#define RM_ERROR_LOST_RESOURCES_ON_CD RM_ERROR_BASE-50
+#define RM_ERROR_INVALID_CD_CONFIGURATION RM_ERROR_BASE-48
+/** RM CD freed local resources which allowed a free request of local request
+ * to be sent to the Server. The Server free failed so the CD tried to
+ * realloc the local resources that were originally freed. The re-allocate
+ * operation failed causing a resource loss on the CD */
+#define RM_ERROR_LOST_RESOURCES_ON_CD RM_ERROR_BASE-49
+/** The service source inst name and RM packet source instance names are not
+ * available for the given type of RM packet */
+#define RM_ERROR_PKT_AND_SERVICE_SRC_NOT_AVAIL RM_ERROR_BASE-50
+/** The provided character buffer that will contain the service source inst
+ * name or pkt source inst name is not of size RM_NAME_MAX_CHARS */
+#define RM_ERROR_SRC_NAME_BUF_INVALID_SIZE RM_ERROR_BASE-51
+/** A resource name specified in the GRL, policy, and/or service request is
+ * greater than RM_NAME_MAX_CHARS */
+#define RM_ERROR_RESOURCE_NAME_TOO_LONG RM_ERROR_BASE-52
+/** RM failed to create a new allocator - Occurred because an instance that
+ * does not use allocators tried to create one (RM Client) */
+#define RM_ERROR_COULD_NOT_CREATE_NEW_ALLOCATOR RM_ERROR_BASE-53
+/** Could not allocate the memory needed to store the root entry of the
+ * allocator tree */
+#define RM_ERROR_COULD_NOT_INIT_ALLOC_TREE RM_ERROR_BASE-54
+/** The instance's allocator tree could not be populated because of an invalid
+ * combination of instance type, GRL, and policy. The valid combinations are:
+ * Server OR Shared Server --> Requires GRL and Policy. Optional Linux DTB
+ * Client Delegate --> Requires Policy.
+ * Client --> Optional Static Policy. */
+#define RM_ERROR_INVALID_ALLOCATOR_INIT RM_ERROR_BASE-55
+/** A resource node in the GRL does not have at least a resource range or a
+ * NameServer assignment defined. At a minimum, each node in the GRL must
+ * have a resource range or NameServer assignment */
+#define RM_ERROR_GRL_INVALID_NODE_DEF RM_ERROR_BASE-56
+/** OSAL malloc failed when allocating an allocator node's resource tree */
+#define RM_ERROR_MALLOC_FAILED_RES_TREE RM_ERROR_BASE-57
+/** OSAL malloc failed when allocating an allocator node's policy tree */
+#define RM_ERROR_MALLOC_FAILED_POL_TREE RM_ERROR_BASE-58
+/** OSAL malloc failed when allocating a resource tree node */
+#define RM_ERROR_MALLOC_FAILED_RES_NODE RM_ERROR_BASE-59
+/** A resource specified in the GRL could not be found in the policy */
+#define RM_ERROR_RES_DOES_NOT_EXIST_IN_POLICY RM_ERROR_BASE-60
+/** Server's response to CD request has invalid service type */
+#define RM_ERROR_SERVER_RESP_INVALID_SERVICE_TYPE RM_ERROR_BASE-61
-/**
+/**
* @brief Maximum number of characters allowed for RM instance, resource, and
* NameServer names.
*/
#define RM_NAME_MAX_CHARS (32)
-/**
+/**
* @brief RM instance handle. The RM handle is used to register transports
* between RM instances and request resource services from the RM
* instance.
*/
typedef void *Rm_Handle;
-/**
+/**
* @brief RM instance types
*/
typedef enum {
* The Linux DTB will be parsed for all managed resources reserved for use
* by Linux. Parsing will be based on "linux-dtb-alias" resource
* properties found in the GRL. The Linux DTB must be in DTB format. */
- void *linuxDtb;
+ void *linuxDtb;
/** Pointer to the global policy defining the allocation policies for
* RM instances within the system. The global policy must be in DTB
* format. */
- void *globalPolicy;
+ void *globalPolicy;
} Rm_ServerCfg;
/**
* @brief RM client delegate (CD) initialization configurations
*/
typedef struct {
- /** Pointer to a client delegate policy used by the CD to allocate resources
+ /** Pointer to a client delegate policy used by the CD to allocate resources
* without contacting the server. The cdPolicy will be used by the CD to
* determine whether clients connected to the CD can be allocated resources
* provided to the CD by the server.
*
* The cdPolicy will also act as a static policy until the transport to the
- * server has been established. Static allocations can occur before the
- * instance has been attached to a server instance within the RM system.
- * This is useful for allocating resources prior to main(). Resources allocated
- * via the static policy will be verified against the global policy once the
- * CD connects with the server. The static policy must be in DTB format.
+ * server has been established. Static allocations can occur before the
+ * instance has been attached to a server instance within the RM system.
+ * This is useful for allocating resources prior to main(). Resources
+ * allocated via the static policy will be verified against the global
+ * policy once the CD connects with the server. The static policy must be
+ * in DTB format.
*
* To guarantee proper resource permission synchronization between the CD
* and server the cdPolicy must either be an exact copy of the globalPolicy
- * or a exact replica of a subset of the globalPolicy provided to the server
- * at initialization. */
+ * or a exact replica of a subset of the globalPolicy provided to the
+ * server at initialization. */
void *cdPolicy;
} Rm_ClientDelegateCfg;
* @brief RM client initialization configurations
*/
typedef struct {
- /** Pointer to a static policy used by the client to allocate resources statically.
- * Static allocations can occur before the instance has been attached to a server
- * or CD instance within the RM system. This is useful for allocating resources
- * prior to main(). Resources allocated via the static policy will be verified
- * against the global policy once the client connects with the server (directly or
- * indirectly through a CD). The static policy must be in DTB format. */
+ /** Pointer to a static policy used by the client to allocate resources
+ * statically. Static allocations can occur before the instance has been
+ * attached to a server or CD instance within the RM system. This is
+ * useful for allocating resources prior to main(). Resources allocated
+ * via the static policy will be verified against the global policy once
+ * the client connects with the server (directly or indirectly through a
+ * CD). The static policy must be in DTB format. */
void *staticPolicy;
} Rm_ClientCfg;
* @brief RM shared client initialization configurations
*/
typedef struct {
- /** RM Shared Server handle. Typically, the Shared Server handle is created on
- * DSP core designated for system initialization. The application then
- * the Shared Server handle, located in shared memory, to the other DSP cores.
- * These DSP cores can then piggyback onto the shared memory data structures in
- * the Shared Server via the Shared Client */
+ /** RM Shared Server handle. Typically, the Shared Server handle is
+ * created on DSP core designated for system initialization. The
+ * application then the Shared Server handle, located in shared memory, to
+ * the other DSP cores. These DSP cores can then piggyback onto the
+ * shared memory data structures in the Shared Server via the Shared
+ * Client */
Rm_Handle sharedServerHandle;
} Rm_SharedClientCfg;
-/**
+/**
* @brief RM instance initialization structure
*/
typedef struct {
- /** Pointer to a character array containing the instance name. The name of the
- * RM instance can be no greater than #RM_NAME_MAX_CHARS. The instance name
- * must match an instance name defined in the "valid-instances" lists contained
- * in the global and static policy DTS files. Resources and privileges to the
- * resources will be based on the name assigned to the RM instance*/
+ /** Pointer to a character array containing the instance name. The name of
+ * the RM instance can be no greater than #RM_NAME_MAX_CHARS. The instance
+ * name must match an instance name defined in the "valid-instances" lists
+ * contained in the global and static policy DTS files. Resources and
+ * privileges to the resources will be based on the name assigned to the
+ * RM instance*/
const char *instName;
/** The type of RM instance that will be created. */
Rm_InstType instType;
+ /** Instance's multi-threaded semaphore object. Two or more RM instances
+ * can have their service transactions to the Server serialized by
+ * providing a valid multi-threaded semaphore object. The semaphore
+ * object will be used by the Osal_rmMtCsEnter and Osal_rmMtCsExit
+ * functions. The multi-threaded semaphore associated with the provided
+ * object will be taken when a service transaction is requested. The
+ * semaphore will be released when the service response is returned. This
+ * will serialize the transactions of any RM instance initialized with the
+ * same multi-threaded sem object. Multi-threaded semaphores will not be
+ * used if NULL is provided as the object */
+ uint32_t *mtSemObj;
/** Instance-type specific configurations */
union {
/** #Rm_ServerCfg */
/**
* @b Description
- * @n
+ * @n
* This function prints and returns the status for all resources managed by
* the RM instance network. The allocate/free status as well as ownership
* status will be printed for every resource. Also, the NameServer name
*
* @retval
* Success - Total number of allocated resource nodes owners. Effectively
- * returns the number of resource ranges still allocated.
+ * returns the number of resource ranges still allocated.
* @retval
- * Failure - #RM_ERROR_INVALID_RES_STATUS_INSTANCE
+ * Failure - #RM_ERROR_INVALID_RES_STATUS_INSTANCE
*/
int32_t Rm_resourceStatus(Rm_Handle rmHandle, int printResources);
/**
* @b Description
- * @n
+ * @n
* This function prints the current status of a RM instance. The
* following instance properties will be printed:
* a) instance name & type
/**
* @b Description
- * @n
+ * @n
* This function initializes a RM instance. There are no restrictions
* on the amount of times this function can be called. Each call will
* result in a new RM instance. However, a network of RM instances
/**
* @b Description
- * @n
+ * @n
* This function deletes the specified RM instance. All memory
* associated with the instance will be freed.
*
* Instance handle.
*
* @param[in] ignorePendingServices
- * Non-zero - The instance will be deleted despite any services pending <br>
+ * Non-zero - The instance will be deleted despite any services pending<br>
* 0 - The instance will not be deleted due to at least one service
* pending.
*
/**
* @b Description
- * @n
+ * @n
* The function is used to get the version information of RM.
*
* @retval
/**
* @b Description
- * @n
+ * @n
* The function is used to get the version string for RM.
*
* @retval
*/
const char* Rm_getVersionStr(void);
-/**
-@}
+/**
+@}
*/
#ifdef __cplusplus