diff --git a/rm_osal.h b/rm_osal.h
index 6bf8bde7b863857313fecb1e24df7b776daf92df..dec997e6c37ba9bd4cff6bed4fcc2a29d0a7e685 100644 (file)
--- a/rm_osal.h
+++ b/rm_osal.h
* @file rm_osal.h
*
* @brief
- * This is the sample OS Adaptation layer which is used by the RM low level
- * driver. The OSAL layer can be ported in either of the following
+ * This is the sample OS Adaptation layer which is used by the Resource
+ * Manager. The OSAL layer can be ported in either of the following
* manners to a native OS:
*
* <b> Approach 1: </b>
*
* \par
*/
-#ifndef __RM_OSAL_H__
-#define __RM_OSAL_H__
+#ifndef RM_OSAL_H_
+#define RM_OSAL_H_
/** @addtogroup RM_OSAL_API
@{
extern void Osal_rmLog (char *fmt, ... );
/**
- * @brief The macro is used by the RM LLD to allocate memory of specified
- * size
+ * @brief The macro is used by RM to allocate memory of specified
+ * size
*
* <b> Prototype: </b>
* The following is the C prototype for the expected OSAL API.
* <b> Parameter </b>
* @n Number of bytes to be allocated
*
- * <b> Parameter </b>
- * @n If true the memory should could from shared memory
- *
* <b> Return Value </b>
* @n Pointer to the allocated block size
*/
-
#define Rm_osalMalloc Osal_rmMalloc
/**
- * @brief The macro is used by the RM LLD to free a allocated block of
- * memory
+ * @brief The macro is used by RM to free a allocated block of
+ * memory
*
* <b> Prototype: </b>
* The following is the C prototype for the expected OSAL API.
* <b> Return Value </b>
* @n Not applicable.
*/
-
#define Rm_osalFree Osal_rmFree
/**
- * @brief The macro is used by the RM LLD to log various
- * messages.
+ * @brief The macro is used by RM to log various
+ * messages.
*
* <b> Prototype: </b>
* The following is the C prototype for the expected OSAL API.
/**
@}
*/
-#endif /* __RM_OSAL_H__ */
+
+#endif /* RM_OSAL_H_ */