diff --git a/rm_services.h b/rm_services.h
index f9914adbeaad9206c4f98fbf5f9ae2f1eaaefca5..194969189764e56fe7174697263eb4b678872ff2 100644 (file)
--- a/rm_services.h
+++ b/rm_services.h
#define RM_SERVICE_DENIED_RESOURCE_DOES_NOT_EXIST (RM_SERVICE_DENIED_BEGIN)
/** A resource value within the specifed base+range could not be found within the resource's
* allocator. No action was taken on the resources. */
-#define RM_SERVICE_DENIED_RESOURCE_VALUE_IN_RANGE_DOES_NOT_EXIST (RM_SERVICE_DENIED_BEGIN+1)
+#define RM_SERVICE_DENIED_RESOURCE_VALUE_RANGE_DOES_NOT_EXIST (RM_SERVICE_DENIED_BEGIN+1)
/** A resource value within the specifed base+range was not allocated to the RM instance
* that is the source of the request. No action was taken on the resources. */
#define RM_SERVICE_DENIED_RESOURCE_NOT_ALLOCATED_TO_INSTANCE_REQUESTING_THE_SERVICE (RM_SERVICE_DENIED_BEGIN+2)
/** The base value of the returned resource. In the case of a block resource allocation
* response this field will contain the base value of the block. */
int32_t resourceBase;
- /** The range of resources starting from resourceBase allocated in block requests */
- uint32_t resourceRange;
+ /** The number of resources starting from resourceBase allocated in block requests */
+ uint32_t resourceLength;
} Rm_ServiceRespInfo;
/**
#define RM_RESOURCE_BASE_UNSPECIFIED (-1)
/** The resource base value. */
int32_t resourceBase;
- /** The range of the specified resource to be allocated starting from
+ /** The number of the specified resource to be allocated starting from
* resourceBase. Will be greater than one only for block allocate
* and free service requests. */
- uint32_t resourceRange;
+ uint32_t resourceLength;
/** An allocate service can be requested with an unspecified resource alignment.
* WARNING: Only applicapable if resourceBase is unspecified
*