diff --git a/rm_services.h b/rm_services.h
index 15904bc60d13ba09832321fddb7bd031ebfd86c1..f9914adbeaad9206c4f98fbf5f9ae2f1eaaefca5 100644 (file)
--- a/rm_services.h
+++ b/rm_services.h
#define RM_SERVICE_PROCESSING (RM_SERVICE_STATE_BASE+1)
/** RM service was approved. The resource data in the response is valid if
* the service has been approved. */
-#define RM_SERVICE_APPROVED (RM_SERVICE_STATE_BASE+2)
+#define RM_SERVICE_APPROVED_AND_COMPLETED (RM_SERVICE_STATE_BASE+2)
/** Beginning of resource denied reasons */
#define RM_SERVICE_DENIED_BEGIN (RM_SERVICE_STATE_BASE+3)
+/** RM could not find an allocator for the resource specified with the provided name */
+#define RM_SERVICE_DENIED_RESOURCE_DOES_NOT_EXIST (RM_SERVICE_DENIED_BEGIN)
+/** A resource value within the specifed base+range could not be found within the resource's
+ * allocator. No action was taken on the resources. */
+#define RM_SERVICE_DENIED_RESOURCE_VALUE_IN_RANGE_DOES_NOT_EXIST (RM_SERVICE_DENIED_BEGIN+1)
+/** A resource value within the specifed base+range was not allocated to the RM instance
+ * that is the source of the request. No action was taken on the resources. */
+#define RM_SERVICE_DENIED_RESOURCE_NOT_ALLOCATED_TO_INSTANCE_REQUESTING_THE_SERVICE (RM_SERVICE_DENIED_BEGIN+2)
+/** A resource value within the specifed base+range is already free */
+#define RM_SERVICE_DENIED_RESOURCE_ALREADY_FREE (RM_SERVICE_DENIED_BEGIN+3)
+/** A resource value within the specifed base+range is already allocated to another
+ * RM instance. */
+#define RM_SERVICE_DENIED_RESOURCE_ALREADY_ALLOCATED (RM_SERVICE_DENIED_BEGIN+4)
/** End of resource denied reasons */
-#define RM_SERVICE_DENIED_END (RM_SERVICE_STATE_BASE+3)
+#define RM_SERVICE_DENIED_END (RM_SERVICE_DENIED_BEGIN+4)
/** RM Service Request Error Code Base */
#define RM_SERVICE_ERROR_BASE (-64)
/** Invalid NameServer object modification on non-Server instance */
#define RM_SERVICE_ERROR_NAMESERVER_OBJECT_MOD_ON_INVALID_INSTANCE (RM_SERVICE_ERROR_BASE-12)
+
/**
* @brief Maximum number of characters in the resource names
*/