index d3e8a45787d556abc4808523389eb940bff86a73..dee5d53200155a11aa0831aeeb61b7804ed15f04 100644 (file)
--- a/rmver.h
+++ b/rmver.h
* @brief Resource Manager Version Definitions
*
* ============================================================
- * Copyright (c) Texas Instruments Incorporated 2012-2013
+ * Copyright (c) Texas Instruments Incorporated 2012-2018
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
*/
/**
- * @brief This is the RM Version. Versions numbers are encoded in the following
+ * @brief This is the RM Version. Versions numbers are encoded in the
+ * following
* format:
* 0xAABBCCDD -> Arch (AA); API Changes (BB); Major (CC); Minor (DD)
*/
-#define RM_VERSION_ID (0x02000008)
+#define RM_VERSION_ID (0x02020003)
/**
* @brief This is the version string which describes the RM along with the
* date and build information.
*/
-#define RM_VERSION_STR "RM Revision: 02.00.00.08"
+#define RM_VERSION_STR "RM Revision: 02.02.00.03"
#ifdef __cplusplus
}
#endif
-
+
#endif /* _RMVER_H */