]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-rtos/rm-lld.git/blobdiff - test/k2k/c66/bios/rm_osal.c
Cleaned up test directory and added makefile for ARM test project
[keystone-rtos/rm-lld.git] / test / k2k / c66 / bios / rm_osal.c
diff --git a/test/k2k/c66/bios/rm_osal.c b/test/k2k/c66/bios/rm_osal.c
new file mode 100644 (file)
index 0000000..c8bfc3a
--- /dev/null
@@ -0,0 +1,247 @@
+/**
+ *   @file  rm_osal.c
+ *
+ *   @brief
+ *      This is the OS abstraction layer used by the Resource Manager.
+ *
+ *  \par
+ *  ============================================================================
+ *  @n   (C) Copyright 2012-2013, Texas Instruments, Inc.
+ *
+ *  Redistribution and use in source and binary forms, with or without
+ *  modification, are permitted provided that the following conditions
+ *  are met:
+ *
+ *    Redistributions of source code must retain the above copyright
+ *    notice, this list of conditions and the following disclaimer.
+ *
+ *    Redistributions in binary form must reproduce the above copyright
+ *    notice, this list of conditions and the following disclaimer in the
+ *    documentation and/or other materials provided with the
+ *    distribution.
+ *
+ *    Neither the name of Texas Instruments Incorporated nor the names of
+ *    its contributors may be used to endorse or promote products derived
+ *    from this software without specific prior written permission.
+ *
+ *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
+ *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
+ *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
+ *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
+ *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
+ *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
+ *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
+ *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
+ *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
+ *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
+ *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
+ *
+ *  \par
+*/
+
+/* Standard Includes */
+#include <stdarg.h>
+
+/* XDC Includes */
+#include <xdc/std.h>
+#include <xdc/runtime/Memory.h>
+#include <xdc/runtime/Error.h>
+#include <xdc/runtime/System.h>
+
+/* BIOS Includes */
+#include <ti/sysbios/BIOS.h>
+#include <ti/sysbios/hal/Hwi.h>
+#include <ti/sysbios/knl/Semaphore.h>
+
+/* CSL includes */
+#include <ti/csl/csl_cacheAux.h>
+#include <ti/csl/csl_xmcAux.h>
+
+/**********************************************************************
+ ****************************** Defines *******************************
+ **********************************************************************/
+
+/**********************************************************************
+ ************************** Global Variables **************************
+ **********************************************************************/
+uint32_t rmMallocCounter = 0;
+uint32_t rmFreeCounter   = 0;
+
+/**********************************************************************
+ *************************** OSAL Functions **************************
+ **********************************************************************/
+
+/* FUNCTION PURPOSE: Allocates memory
+ ***********************************************************************
+ * DESCRIPTION: The function is used to allocate a memory block of the
+ *              specified size.
+ */
+void *Osal_rmMalloc (uint32_t num_bytes)
+{
+       Error_Block     errorBlock;
+
+    /* Increment the allocation counter. */
+    rmMallocCounter++;
+
+       /* Allocate memory. */
+       return Memory_alloc(NULL, num_bytes, 0, &errorBlock);
+}
+
+/* FUNCTION PURPOSE: Frees memory
+ ***********************************************************************
+ * DESCRIPTION: The function is used to free a memory block of the
+ *              specified size.
+ */ 
+void Osal_rmFree (void *ptr, uint32_t size)
+{
+    /* Increment the free counter. */
+    rmFreeCounter++;
+       Memory_free(NULL, ptr, size);
+}
+
+/* FUNCTION PURPOSE: Critical section enter
+ ***********************************************************************
+ * DESCRIPTION: The function is used to enter a critical section.
+ *              Function protects against 
+ *      
+ *              access from multiple cores 
+ *              and 
+ *              access from multiple threads on single core
+ */  
+void *Osal_rmCsEnter(void)
+{
+
+    return NULL;
+}
+
+/* FUNCTION PURPOSE: Critical section exit
+ ***********************************************************************
+ * DESCRIPTION: The function is used to exit a critical section 
+ *              protected using Osal_cppiCsEnter() API.
+ */  
+void Osal_rmCsExit(void *CsHandle)
+{
+
+}
+
+/* FUNCTION PURPOSE: Cache invalidate
+ ***********************************************************************
+ * DESCRIPTION: The function is used to indicate that a block of memory is 
+ *              about to be accessed. If the memory block is cached then this 
+ *              indicates that the application would need to ensure that the 
+ *              cache is updated with the data from the actual memory.
+ */  
+void Osal_rmBeginMemAccess(void *ptr, uint32_t size)
+{
+    uint32_t    key;
+
+    /* Disable Interrupts */
+    key = Hwi_disable();
+
+    /* Cleanup the prefetch buffer also. */
+    CSL_XMC_invalidatePrefetchBuffer();
+
+#ifdef L2_CACHE
+    /* Invalidate L2 cache. This should invalidate L1D as well. 
+     * Wait until operation is complete. */    
+    CACHE_invL2 (ptr, size, CACHE_FENCE_WAIT);
+#else       
+    /* Invalidate L1D cache and wait until operation is complete. 
+     * Use this approach if L2 cache is not enabled */    
+    CACHE_invL1d (ptr, size, CACHE_FENCE_WAIT);
+#endif
+
+    /* Reenable Interrupts. */
+    Hwi_restore(key);
+
+    return;
+}
+
+/* FUNCTION PURPOSE: Cache writeback
+ ***********************************************************************
+ * DESCRIPTION: The function is used to indicate that the block of memory has 
+ *              finished being accessed. If the memory block is cached then the 
+ *              application would need to ensure that the contents of the cache 
+ *              are updated immediately to the actual memory. 
+ */  
+void Osal_rmEndMemAccess(void *ptr, uint32_t size)
+{
+    uint32_t    key;
+
+    /* Disable Interrupts */
+    key = Hwi_disable();
+
+#ifdef L2_CACHE
+    /* Writeback L2 cache. This should Writeback L1D as well. 
+     * Wait until operation is complete. */ 
+    CACHE_wbL2 (ptr, size, CACHE_FENCE_WAIT);
+
+#else    
+    /* Writeback L1D cache and wait until operation is complete. 
+     * Use this approach if L2 cache is not enabled */    
+    CACHE_wbL1d (ptr, size, CACHE_FENCE_WAIT);
+#endif
+
+    /* Reenable Interrupts. */
+    Hwi_restore(key);
+
+    return;
+}
+
+/* FUNCTION PURPOSE: Creates a task blocking object
+ ***********************************************************************
+ * DESCRIPTION: The function is used to create a task blocking object
+ *              capable of blocking the task a RM instance is running
+ *              within
+ */
+void *Osal_rmTaskBlockCreate(void)
+{
+    Semaphore_Params semParams;    
+
+    Semaphore_Params_init(&semParams);
+    return((void *)Semaphore_create(0, &semParams, NULL));
+}
+
+/* FUNCTION PURPOSE: Blocks a RM instance
+ ***********************************************************************
+ * DESCRIPTION: The function is used to block a task whose context a
+ *              RM instance is running within.
+ */
+void Osal_rmTaskBlock(void *handle)
+{
+    Semaphore_pend((Semaphore_Handle)handle, BIOS_WAIT_FOREVER);
+}
+
+/* FUNCTION PURPOSE: unBlocks a RM instance
+ ***********************************************************************
+ * DESCRIPTION: The function is used to unblock a task whose context a
+ *              RM instance is running within.
+ */
+void Osal_rmTaskUnblock(void *handle)
+{
+    Semaphore_post((Semaphore_Handle)handle);
+}
+
+/* FUNCTION PURPOSE: Deletes a task blocking object
+ ***********************************************************************
+ * DESCRIPTION: The function is used to delete a task blocking object
+ *              provided to a RM instance
+ */
+void Osal_rmTaskBlockDelete(void *handle)
+{
+    Semaphore_delete((Semaphore_Handle *)&handle);
+}
+
+/* FUNCTION PURPOSE: Prints a variable list
+ ***********************************************************************
+ * DESCRIPTION: The function is used to print a string to the console
+ */
+void Osal_rmLog (char *fmt, ... )
+{
+    VaList ap;
+    
+    va_start(ap, fmt);
+    System_vprintf(fmt, ap);
+    va_end(ap);
+}
+