index 0b6326561f39fde0e222450f72bc274cd51f850f..58f636abdf467042abdd3e3837b3983577a055da 100644 (file)
/* FUNCTION PURPOSE: Critical section exit
***********************************************************************
* DESCRIPTION: The function is used to exit a critical section
- * protected using Osal_cppiCsEnter() API.
+ * protected using Osal_rmCsEnter() API.
*/
void Osal_rmCsExit(void *CsHandle)
{
CSL_semReleaseSemaphore (RM_HW_SEM);
}
+/* FUNCTION PURPOSE: Multi-threaded critical section enter
+ ***********************************************************************
+ * DESCRIPTION: The function is used to enter a multi-threaded critical
+ * section. Function protects against
+ *
+ * access from multiple threads on single core
+ */
+void *Osal_rmMtCsEnter(void *mtSemObj)
+{
+
+ return NULL;
+}
+
+/* FUNCTION PURPOSE: Multi-threaded critical section exit
+ ***********************************************************************
+ * DESCRIPTION: The function is used to exit a multi-threaded critical
+ * section protected using Osal_rmMtCsEnter() API.
+ */
+void Osal_rmMtCsExit(void *mtSemObj, void *CsHandle)
+{
+
+}
+
/* FUNCTION PURPOSE: Cache invalidate
***********************************************************************
* DESCRIPTION: The function is used to indicate that a block of memory is