Merge branch 'master' of gtgit01.gt.design.ti.com:git/projects/rm-lld
sdocm00106374: add missing qpend queues for k2l and k2e
Updated release notes
Removed DEVICE from build of ARM test code
Missed addition of test/armv7 makefile
Cleaned up duplicate rmServer test files
added missing files for k2e/l rmServer sync
SDOCM00103974: allow internal/external linking RAM automatic allocation
Synced k2e and k2l with rmServer daemon update
Resolved SDOCM00107840
Merge branch 'releases/mcsdk_03.01.00.00'
Resolved SDOCM00107059
Resolved SDOCM00107027
Revert "Updated netcp CPPI resource ranges and Linux usage"
This reverts commit 779f3c6b36e6cecb38ffed24d6df7409e5681daa.
This reverts commit 779f3c6b36e6cecb38ffed24d6df7409e5681daa.
Updated netcp CPPI resource ranges and Linux usage
Use libdaemon API to remove pid file
Fixed INTC-QUEUE permissions so that they're shared between Linux and DSP
kill command now deletes pid file
Added optional input for max logfile size
Fixed bug in daemon kill and updated k2k RM server source
Added new transport APIs and daemonized the Linux RM Server app
Documentation upates
Updated GRL and policies with latest Linux DTB. Also, corrected regular expression checks in the dsp_client.cfg.xs for the respective device names
Corrected k2e, k2h, and k2l dsp_client.cfg.xs files to properly reflect the number of cores on the device
Added API to get service src and pkt src instance names from the RM packet
Added copy of k2e and k2l device files to ARM install
Update for Yocto
fix permission
.gitignore left out k2e/k2l makefile
sync k2h to k2[el]
Merge remote-tracking branch 'origin' into releases/mcsdk_03.01.00.00
add resources for PA user stats (32bUsrStats 64bUsrStats)
fixed the file modes to non executable
added shared object library support
get rid of multi core test cases on single core device k2e
put pa back into rm grl/policy
use k2h dts files for rmMemK2L because it should
really use the "test" dts files. Fix merge error
in rm_shared_test.cfg
really use the "test" dts files. Fix merge error
in rm_shared_test.cfg
set version and tag to 2.1.0.1
sync k2e and k2l to k2h updates
Merge 2.0.0.6
Conflicts:
device/k2h/global-resource-list-arm-dsp.c
device/k2h/global-resource-list-arm-dsp.dtb
device/k2h/global-resource-list-arm-dsp.dts
device/k2h/global-resource-list.c
device/k2h/global-resource-list.dtb
device/k2h/global-resource-list.dts
device/k2h/policy_dsp-only.c
device/k2h/policy_dsp-only.dtb
device/k2h/policy_dsp-only.dts
device/k2h/policy_dsp_arm.c
device/k2h/policy_dsp_arm.dtb
device/k2h/policy_dsp_arm.dts
device/k2k/global-resource-list-arm-dsp.c
device/k2k/global-resource-list-arm-dsp.dtb
device/k2k/global-resource-list-arm-dsp.dts
device/k2k/global-resource-list.c
device/k2k/global-resource-list.dtb
device/k2k/global-resource-list.dts
device/k2k/policy_dsp-only.c
device/k2k/policy_dsp-only.dtb
device/k2k/policy_dsp-only.dts
device/k2k/policy_dsp_arm.c
device/k2k/policy_dsp_arm.dtb
device/k2k/policy_dsp_arm.dts
docs/ReleaseNotes_RM.doc
docs/ReleaseNotes_RM.pdf
package.xdc
setupenv.bat
Conflicts:
device/k2h/global-resource-list-arm-dsp.c
device/k2h/global-resource-list-arm-dsp.dtb
device/k2h/global-resource-list-arm-dsp.dts
device/k2h/global-resource-list.c
device/k2h/global-resource-list.dtb
device/k2h/global-resource-list.dts
device/k2h/policy_dsp-only.c
device/k2h/policy_dsp-only.dtb
device/k2h/policy_dsp-only.dts
device/k2h/policy_dsp_arm.c
device/k2h/policy_dsp_arm.dtb
device/k2h/policy_dsp_arm.dts
device/k2k/global-resource-list-arm-dsp.c
device/k2k/global-resource-list-arm-dsp.dtb
device/k2k/global-resource-list-arm-dsp.dts
device/k2k/global-resource-list.c
device/k2k/global-resource-list.dtb
device/k2k/global-resource-list.dts
device/k2k/policy_dsp-only.c
device/k2k/policy_dsp-only.dtb
device/k2k/policy_dsp-only.dts
device/k2k/policy_dsp_arm.c
device/k2k/policy_dsp_arm.dtb
device/k2k/policy_dsp_arm.dts
docs/ReleaseNotes_RM.doc
docs/ReleaseNotes_RM.pdf
package.xdc
setupenv.bat
Resolved SDOCM00103027
Resolved SDOCM00101836
Resolved SDOCM00102876
Updated RN
update RN
add back dsp control for PA channel 7
really remove high priorty accumulator channels, since linux doesn't use them
Merge branch 'master' of gtgit01.gt.design.ti.com:git/projects/rm-lld
remove high priority accumulator channels, since linux doesn't actually use them, and syslib does
Resolved SDOCM00101322
set up policy to block pa/sa/netcp/xge cppi channels
update GRL and policy to match current linux
Updated RN
Merge branch 'ksII-rm-dev'
add cppi for iqn
Updated RN
Resolved SDOCM00101835
Add support for Qmss_QueueType_INTC_SET[234]_QUEUE to allow all INTC/CIC queues
Merge branch 'master' into ksII-rm-dev
Merge branch 'master' into ksII-rm-dev
Merge remote-tracking branch 'origin/master'
10gig definitions missing from global-resoruce-list-arm-dsp.dts
Changes to ARM-DSP test project based on IPC update
Made requesting instance's allocation count for resource available via the service response
Updated release notes
Merge branch 'master' of gtgit01.gt.design.ti.com:git/projects/rm-lld
undo partial workaround for SDOCM00101586
Resolved SDOCM00101586. Added test cases to cover resolved issued
update grl for hyperlink queues
fix file perms
working policy for qm multicore example
no longer need 6638 ipc library
migrate to ipc 3.0.0.20 which uses ti/ipc/Std.h instead of Std.h
missing dsp_client_cfg.xs from package
Updated documentation to point to UG for instructions on running ARM+DSP test
Added dts_files directory to install
Added cify script and test dts files to yocto install
Linux makefile updates for DSP Client example using IPC to communicate to Linux RM Server
Updated RN
Return warning when opening CD instance due to instabilities. Fixed policy verification parsing bug.
ignore makefile made by rtsc
Merge remote-tracking branch 'origin/ksII-rm-dev'
sync with linux
Updated Linux Client test to account for multiple alloc/free reference counts
10 years agoAdded owner reference count to account for multiple allocates/frees of the same resou...
Added owner reference count to account for multiple allocates/frees of the same resource from the same RM instance
Fixed bug where unspecified base requests couldn't return a resource value of zero
Return owner count when resource already owned
1. Makefile fix to recompile library on any source change
2. Fixed bug in policy code which could result in strncmp of a invalid
pointer
3. Minor bug fix in Linux client test
4. updated setupenv batch file
2. Fixed bug in policy code which could result in strncmp of a invalid
pointer
3. Minor bug fix in Linux client test
4. updated setupenv batch file
Preallocation routine will now correctly get next tree node during resource search
Update with the fixes for
- build error
- Missing file in package
- Removed install from all since this is only needed for Yocto
- build error
- Missing file in package
- Removed install from all since this is only needed for Yocto
Added arm makefiles to XDC release packages
RN update
Completed testing of CD local allocation feature
10 years agoAdded missing linker options with support for latest Linaro toolchain DEV.RM_LLD.02.00.00.03
Added missing linker options with support for latest Linaro toolchain
fix linker flags
Added linux makefiles for Linux test project
Added rmver.h
Added Linux example and updated release notes
Transport now directly used to send response packets instead of searching based on transport handle remote instance name. Also, added transport reconfiguration API
Cleaned up test directory and added makefile for ARM test project