9 years agofixed utility bug for command label create during data mode DEV.SA_LLD.03.00.00.07_timestampFix
fixed utility bug for command label create during data mode
merge data mode enhancements with 3GPP fixes
saac_fromair.p & saac_toair.p: use ctrlInfo2 instead of ctrlInfo for control flag flagACCountCCopy
sallddminit.c: salld_data_mode_close() should specifies destInfo
merged enhanced CCM support for WiMax kind of protocols
9 years agoSA LLD:version 3.0.0.7: update projects to be compatible with PA LLD 3.0.1.0 DEV.SA_LLD.03.00.00.07
SA LLD:version 3.0.0.7: update projects to be compatible with PA LLD 3.0.1.0
SA LLD test code and project file update to handle three PA classify1 images instead of one
SA_UnitTest*.txt: fix file name case mismatch
ReleaseNotes_SA_LLD: version 3.0.0.6
Firmware image 3.0.0.6
fw/Module.xs: cp v0/saphp1_bin.c, saphp2_bin.c to fw/ for backward compatibility
Need to memset array sizes[] and aligns prior to API call Pa_getBuffReq()
Version 3.0.0.6
Undo the directory name changes at all SA unit test projects since we have changed the directory name from SaUnittest to SaUnitTest
fixed directory name in all project files: SaUnitTest ==> SaUnittest
Fix include file names: bios.h ==> BIOS.h, task.h ==> Task.h
fixed directory name mismatch for linux builds
resolving SDOCM00111718
added a dummy rule for tests to get pass the error from top level makefile
Merge branch 'master' of gtgit01.gt.design.ti.com:git/projects/sa-lld
fixed compilation issues for simulator support
salld.h: Add comments for callout API (*ScAlloc) to describe the buffer alignment requirement in cacheable memory
9 years agoupdated framework not to exit due to CPPI PA Tx/Rx Channel open during non NO BOOT... DEV.SA_LLD.03.00.00.05
updated framework not to exit due to CPPI PA Tx/Rx Channel open during non NO BOOT modes
Merge branch 'master' of gtgit01.gt.design.ti.com:git/projects/sa-lld
updated the modes
fixed issues on Sa Examples due to hardcoded flow Id, multicore framework for using RM
Merge branch 'master' of gtgit01.gt.design.ti.com:git/projects/sa-lld
salldsrtp.c salldsrtcp.c sallddmcmdl.c: fix coverity issues
.gitignore:add /makefile
adding qmss accumulator osal functions in the examples
SaBasic(MultiCore)Example:unittest.h: add include <ti/csl/csl_qm_queue.h>
salld.h: note that nextHdr at Sa_IpsecConfigParams_t is not used
fix coverity issues #1
ReleaseNotes: add resolved IRs
Merge branch 'master' of gtgit01.gt.design.ti.com:git/projects/sa-lld
saac_util.p: fix IV formatting for Snow3G F9 operation
testconn.c: enhance DM verification algorithm
fix Snow3G and ZUC ciphering operations
salld.h: fix typo in several comments
Initialize queueGroup to 0 prior to invoke Cppi_initDescriptor() API
updated comments for IPSec ESP utility functions
updated for RM lib includes for multicore examples
fixed the RM_LIB includes for shared object exectuables
updated examples to use RM, added sa channel data send/receive utility
saac_util.p php2.p: fix TRNG init code (register conflict)
Close SA at function exitTestFramework()
salldcom.c: update Sa_close() to reset and disable SASS
Enhance examples/unit test to demonstrate NSS layout configuration
add debug flags -g -mn
saipsec_esp_tx(2).p removed unused code and general cleanup
test1_1.c: channel range of the third test group is incorrect;test1_6.c: number of channels is incorrect
add SASS v0 firmware image reference at top firmware directory for backward compatibility
update example makefiles for Yocto build #7
update example makefiles for Yocto build #6
update example makefiles for Yocto build #5
update example makefiles for Yocto build #4
update example makefiles for Yocto build #3
update example makefiles for Yocto build #2
update example makefiles for Yocto build
testconn.c: move pkt buffer to MSMCSRAM
package.bld: include ARM library only if BUILD_LINUX = ON
SA Example: update Linux makefiles #1
Update Linux makefiles as other PDK component LLDs
fix typo at makefile_armv7
fix typo at makefile_armv7
add COPYING.txt and saver.h
update Linux makefile to support library and example installation
add PDSP image files
replease \ with / at fw/v1/php1.p
replease \ with / at fw/v1/php1.p
add eclipse/intermediate files to .gitignore
remove intermediate files from eclispe
Rename 2nd generation PDSP images to Sa2_xxx, merged Air ciphering LTE slow path enhancement
initiate new repository from SA 3.0.0.8