1 @REM ******************************************************************************
2 @REM * FILE PURPOSE: Environment Setup for building Serdes Batch File
3 @REM ******************************************************************************
4 @REM * FILE NAME: serdes_dss_eye_k2l.bat
5 @REM *
6 @REM * DESCRIPTION:
7 @REM * Configures and sets up the Build Environment for K2L Eye Test.
8 @REM *
9 @REM * USAGE:
10 @REM * serdes_dss_eye_k2l.bat
11 @REM *
12 @REM * Copyright (C) 2015, Texas Instruments, Inc.
13 @REM *****************************************************************************
14 @echo off
15 @REM *******************************************************************************
16 @REM ********************** GET PARAMETERS PASSED THROUGH ARGUMENT ***************
17 @REM *******************************************************************************
18 @REM Parameter Validation: Check if the argument was passed to the batch file and
19 @REM if so we use that else we default to the working directory where the batch
20 @REM file was invoked from
22 if not defined PDK_INSTALL_PATH set PDK_INSTALL_PATH=..\..\..\
23 @echo PDK BUILD ENVIRONMENT CONFIGURED
24 echo PDK Directory %PDK_INSTALL_PATH%
25 @echo *******************************************************************************
27 C:\ti\ccsv7\ccs_base\scripting\bin\dss.bat serdes_dss_eye_k2l.js
29 GOTO DONE
31 :DONE