1 /******************************************************************************\r
2 * FILE PURPOSE: Build description for the TCP3D Driver\r
3 ******************************************************************************\r
4 * FILE NAME: package.bld\r
5 *\r
6 * DESCRIPTION: \r
7 * This file contains the build specification and description for the TCP3D driver\r
8 * \r
9 * The file takes the following parameters from the command line through the\r
10 * XDCARGS variable.\r
11 * XDCARGS[0] = TCP3D Driver Install Type \r
12 * Valid Values are "TAR" or "SETUP"\r
13 * DEFAULT is "TAR"\r
14 *\r
15 * Example for a valid command:\r
16 * xdc XDCARGS=SETUP release \r
17 *\r
18 * Copyright (C) 2011, Texas Instruments, Inc.\r
19 *****************************************************************************/\r
20 \r
21 /* List of all subdirectories that combine to make the TCP3D Driver Package. */\r
22 var subDirectories = [ "src", "docs", "example", "test" ];\r
23 \r
24 /* Determine if we need to create the InstallJammer Application or not? \r
25 * TCP3D Driver deliverables be either of the following formats:\r
26 * - TAR Ball Package\r
27 * - Setup Executable \r
28 * DEFAULT is a TAR package. */\r
29 if ((arguments[0] != "TAR") && (arguments[0] != "SETUP"))\r
30 tcp3dDriverInstallType = Pkg.attrs.archiver;\r
31 else\r
32 tcp3dDriverInstallType = arguments[0];\r
33 \r
34 /* Irrespective of the InstallType we always create a TAR Ball Package as a part\r
35 * of the RTSC Build. Here we determine the name of the TAR Ball Package\r
36 * Format is as follows:\r
37 * tcp3d_<version> */\r
38 var tcp3dRTSCFileName = "tcp3d" + "_" +\r
39 tcp3dPartNumber + "_" + \r
40 tcp3dDriverReleaseVersion[0] + "_" +\r
41 tcp3dDriverReleaseVersion[1] + "_" + \r
42 tcp3dDriverReleaseVersion[2] + "_" +\r
43 tcp3dDriverReleaseVersion[3];\r
44 \r
45 /******************************************************************\r
46 ************************ Release Banner **************************\r
47 ******************************************************************/\r
48 \r
49 print ("************* TCP3D Driver Build Information *************");\r
50 print ("TCP3D Driver Install : " + tcp3dDriverInstallType);\r
51 print ("TCP3D Driver Version : " + tcp3dDriverReleaseVersion);\r
52 print ("Tools Directory : " + toolsBaseDir);\r
53 print ("RTSC File Name : " + tcp3dRTSCFileName);\r
54 print ("TCP3D Driver Path : " + tcp3dDriverPath);\r
55 print ("Coverity Analysis : " + (coverityAnalysis == "ON" ? "ON" : "OFF"));\r
56 print ("CC LE opts : " + C66LE.ccOpts.prefix);\r
57 print ("CC BE opts : " + C66BE.ccOpts.prefix);\r
58 print ("**********************************************************");\r
59 \r
60 /* Create the release package for the TCP3D Driver */\r
61 Pkg.defaultRelease = Pkg.addRelease (tcp3dRTSCFileName, {prefix: "./packages/"});\r
62 \r
63 /* Cycle through all the sub-directories and build all the files */\r
64 for (var i = 0; i < subDirectories.length; i++) \r
65 {\r
66 /* Load the capsule in the sub directory. */\r
67 var caps = xdc.loadCapsule (subDirectories[i]+"/Module.xs");\r
68 \r
69 print ("Building directory " + subDirectories[i]);\r
70 \r
71 /* Build the capsule. */\r
72 caps.modBuild();\r
73 \r
74 /* Package the module.xs files for building via package */\r
75 Pkg.otherFiles[Pkg.otherFiles.length++] = subDirectories[i]+"/Module.xs";\r
76 }\r
77 \r
78 /* Package the remaining files */\r
79 Pkg.otherFiles[Pkg.otherFiles.length++] = "config.bld";\r
80 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.bld";\r
81 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xdc";\r
82 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xs";\r
83 Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc";\r
84 Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc.xdt";\r
85 Pkg.otherFiles[Pkg.otherFiles.length++] = "tcp3d_drv.h";\r
86 Pkg.otherFiles[Pkg.otherFiles.length++] = "tcp3d_osal.h";\r
87 Pkg.otherFiles[Pkg.otherFiles.length++] = "tcp3d_drv_types.h";\r
88 Pkg.otherFiles[Pkg.otherFiles.length++] = "tcp3dver.h";\r
89 Pkg.otherFiles[Pkg.otherFiles.length++] = "tcp3dver.h.xdt";\r
90 Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/TCP3D_DRV_doxconfig";\r
91 Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/TCP3D_DRV_doxconfig.xdt";\r
92 Pkg.otherFiles[Pkg.otherFiles.length++] = "build/buildlib.xs";\r
93 Pkg.otherFiles[Pkg.otherFiles.length++] = "makefile";\r
94 \r
95 /* Generate Users Manual Doxyfile */\r
96 var tplt = xdc.loadTemplate("./docs/TCP3D_DRV_doxconfig.xdt");\r
97 tplt.genFile("./docs/TCP3D_DRV_doxconfig",tcp3dDriverReleaseVersion); \r
98 \r
99 /* Generate Settings.xdc */\r
100 var tplt = xdc.loadTemplate("./Settings.xdc.xdt");\r
101 tplt.genFile("./Settings.xdc",tcp3dDriverReleaseVersion); \r
102 \r
103 /* Generate paver.h */\r
104 var tplt = xdc.loadTemplate("./tcp3dver.h.xdt");\r
105 tplt.genFile("./tcp3dver.h",tcp3dDriverReleaseVersion); \r
106 \r
107 /* Generate eclipse sample file */\r
108 var tplt = xdc.loadTemplate("./docs/eclipse/sample.xml.xdt");\r
109 tplt.genFile("./docs/eclipse/sample.xml",tcp3dDriverReleaseVersion); \r
110 \r
111 \r
112 /***************************************************************************\r
113 ********************************* MINI Package ****************************\r
114 ***************************************************************************/\r
115 /* Check if we need to create the mini package? */\r
116 var miniBuild = java.lang.System.getenv("MINI_PACKAGE");\r
117 \r
118 if (miniBuild == "ON")\r
119 {\r
120 /* Create the MINI RTSC Package */\r
121 var additionalFiles = [];\r
122 \r
123 var libUtility = xdc.loadCapsule ("build/buildlib.xs");\r
124 libUtility.createMiniPkg(tcp3dRTSCFileName, additionalFiles);\r
125 }\r
126 \r
127 /********************************************************************* \r
128 *********************** INSTALL-JAMMER Support **********************\r
129 * In order to create the InstallJammer Application; we need to UNTAR\r
130 * the package into a temporary directory. This is required because \r
131 * currently the InstallJammer does not support the TAR Files and thus\r
132 * creating an UNTAR of the file. So to work-around the problem we will\r
133 * do the following in the EPILOGUE Section:-\r
134 * (a) Create a temporary directory called 'tmp'\r
135 * (b) UNTAR the package into 'tmp'\r
136 * (c) Run the INSTALL Jammer on 'tmp'\r
137 * (d) Remove the 'tmp' directory.\r
138 *\r
139 * This can be done only after the 'release' package has been created.\r
140 * Thus all of this work is being done in the EPILOGUE.\r
141 *********************************************************************/\r
142 if (tcp3dDriverInstallType == "SETUP")\r
143 {\r
144 /* Create the Install Jammer Version Variable. This is used inside the \r
145 * MPI File to create the Final executable. \r
146 * The format supported is as follows:-\r
147 * - setupwin32_tcp3d_<device>_<version>.exe \r
148 */\r
149 var InstallJammerVersion = "-DVersion " +\r
150 tcp3dPartNumber + "_" + \r
151 tcp3dDriverReleaseVersion[0] + "_" +\r
152 tcp3dDriverReleaseVersion[1] + "_" + \r
153 tcp3dDriverReleaseVersion[2] + "_" +\r
154 tcp3dDriverReleaseVersion[3];\r
155 \r
156 /* This is the location where the tmp directory is located; this is used as \r
157 * the input directory for the Install Jammer. */ \r
158 var PackageBaseDir = " -DPackageBaseDir " + tcp3dDriverPath + "./tmp";\r
159 \r
160 /* This is the location where the TCP3D Driver will be installed by default. */\r
161 var WinInstallDir = " -DWinInstallDir " + \r
162 "C:/ti/tcp3d" + "_" + \r
163 tcp3dPartNumber + "_" + \r
164 tcp3dDriverReleaseVersion[0] + "_" +\r
165 tcp3dDriverReleaseVersion[1] + "_" + \r
166 tcp3dDriverReleaseVersion[2] + "_" +\r
167 tcp3dDriverReleaseVersion[3];\r
168 \r
169 /* Create the actual EPILOGUE Section for the INSTALLER */\r
170 Pkg.makeEpilogue += "release: install_application\n";\r
171 Pkg.makeEpilogue += "install_application:\n";\r
172 Pkg.makeEpilogue += "\t @echo -------------------------------------------------------\n";\r
173 Pkg.makeEpilogue += "\t @echo Creating the Install\n";\r
174 Pkg.makeEpilogue += "\t @echo -------------------------------------------------------\n";\r
175 Pkg.makeEpilogue += "\t -$(MKDIR) tmp\n";\r
176 Pkg.makeEpilogue += "\t -$(MKDIR) tmp/packages\n";\r
177 Pkg.makeEpilogue += "\t -$(MKDIR) tmp/eclipse\n";\r
178 Pkg.makeEpilogue += "\t -$(CP) -R eclipse tmp\n";\r
179 Pkg.makeEpilogue += "\t tar -xf ./packages/" + tcp3dRTSCFileName + ".tar" + " -Ctmp/packages \n";\r
180 Pkg.makeEpilogue += "\t installjammer " + InstallJammerVersion + PackageBaseDir + WinInstallDir + \r
181 " --output-dir packages/ --build install/tcp3d.mpi\n";\r
182 Pkg.makeEpilogue += "\t -$(RMDIR) tmp\n\n";\r
183 }\r
184 \r
185 /* We need to clean after ourselves; extend the 'clean' target to take care of this. */\r
186 Pkg.makeEpilogue += "clean::\n";\r
187 Pkg.makeEpilogue += "\t -$(RM) .xdcenv.mak\n";\r
188 Pkg.makeEpilogue += "\t -$(RM) tcp3dver.h\n";\r
189 Pkg.makeEpilogue += "\t -$(RM) Settings.xdc\n";\r
190 Pkg.makeEpilogue += "\t -$(RM) makefile\n";\r
191 Pkg.makeEpilogue += "\t -$(RM) docs/TCP3D_DRV_APIIF.chm\n";\r
192 Pkg.makeEpilogue += "\t -$(RM) docs/TCP3D_DRV_doxconfig\n";\r
193 Pkg.makeEpilogue += "\t -$(RM) docs/eclipse/sample.xml\n";\r
194 Pkg.makeEpilogue += "\t -$(RMDIR) docs/doxy/rtf\n";\r
195 Pkg.makeEpilogue += "\t -$(RMDIR) docs/doxy/html\n";\r
196 Pkg.makeEpilogue += "\t -$(RMDIR) lib\n";\r
197 // for (var i = 0; i < devices.length; i++)\r
198 // {\r
199 // Pkg.makeEpilogue += "\t -$(RMDIR) lib/" + devices[i].split("/")[0] + "\n";\r
200 // }\r
201 if (tcp3dDriverInstallType == "SETUP")\r
202 {\r
203 Pkg.makeEpilogue += "\t -$(RM) packages/*.exe\n";\r
204 Pkg.makeEpilogue += "\t -$(RM) packages/*.bin\n";\r
205 Pkg.makeEpilogue += "\t -$(RMDIR) eclipse\n";\r
206 Pkg.makeEpilogue += "\t -$(RMDIR) tmp\n";\r
207 }\r
208 if (miniBuild == "ON")\r
209 {\r
210 Pkg.makeEpilogue += "\t -$(RM) simpleC66LE.mak\n";\r
211 Pkg.makeEpilogue += "\t -$(RM) simpleC66BE.mak\n";\r
212 }\r