- Fix for SDOCM00108178 in src/tcp3d_drv.c.
[keystone-rtos/tcp3d-lld.git] / tcp3d_osal.h
1 /**\r
2  *   @file  tcp3d_osal.h\r
3  *\r
4  *   @brief   \r
5  *      This is the sample OS Adaptation layer which is used by the TCP3D\r
6  *      driver. The OSAL layer can be ported in either of the following \r
7  *      manners to a native OS:\r
8  *\r
9  *      <b> Approach 1: </b>\r
10  *      @n  Use Prebuilt Libraries\r
11  *           - Ensure that the provide an implementation of all \r
12  *             Osal_XXX API for their native OS.\r
13  *           - Link the prebuilt libraries with their application.\r
14  *           - Refer to the "example" directory for an example of this\r
15  *       @n <b> Pros: </b>\r
16  *           - Customers can reuse prebuilt TI provided libraries\r
17  *       @n <b> Cons: </b>\r
18  *           - Level of indirection in the API to get to the actual OS call\r
19  *              \r
20  *      <b> Approach 2: </b>\r
21  *      @n  Rebuilt Library \r
22  *           - Create a copy of this file and modify it to directly \r
23  *             inline the native OS calls\r
24  *           - Rebuild the TCP3D Driver library; ensure that the Include \r
25  *             path points to the directory where the copy of this file \r
26  *             has been provided.\r
27  *           - Please refer to the "test" directory for an example of this \r
28  *       @n <b> Pros: </b>\r
29  *           - Optimizations can be done to remove the level of indirection\r
30  *       @n <b> Cons: </b>\r
31  *           - TCP3D Libraries need to be rebuilt by the customer.\r
32  *\r
33  *  \par\r
34  *  NOTE:\r
35  *      (C) Copyright 2009 Texas Instruments, Inc.\r
36  * \r
37  *  Redistribution and use in source and binary forms, with or without \r
38  *  modification, are permitted provided that the following conditions \r
39  *  are met:\r
40  *\r
41  *    Redistributions of source code must retain the above copyright \r
42  *    notice, this list of conditions and the following disclaimer.\r
43  *\r
44  *    Redistributions in binary form must reproduce the above copyright\r
45  *    notice, this list of conditions and the following disclaimer in the \r
46  *    documentation and/or other materials provided with the   \r
47  *    distribution.\r
48  *\r
49  *    Neither the name of Texas Instruments Incorporated nor the names of\r
50  *    its contributors may be used to endorse or promote products derived\r
51  *    from this software without specific prior written permission.\r
52  *\r
53  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS \r
54  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT \r
55  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR\r
56  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT \r
57  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, \r
58  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT \r
59  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,\r
60  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY\r
61  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT \r
62  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE \r
63  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.\r
64  *\r
65 */\r
66 #ifndef __TCP3D_OSAL_H__\r
67 #define __TCP3D_OSAL_H__\r
68 \r
69 /** @addtogroup TCP3D_OSAL_API\r
70  @{ */\r
71 \r
72 /**********************************************************************\r
73  ************************* Extern Declarations ************************\r
74  **********************************************************************/\r
75 \r
76 extern void* Osal_memset(void *_mem, int32_t _ch, size_t _n);\r
77 extern void* Osal_memcpy(void *_s1, const void *_s2, size_t _n);\r
78 \r
79 extern void Osal_tcp3dLog( String fmt, ... );\r
80 extern void Osal_tcp3dBeginMemAccess (void *ptr, uint32_t size);\r
81 extern void Osal_tcp3dEndMemAccess (void *ptr, uint32_t size);\r
82 \r
83 /**\r
84  * @brief   The macro is used by the TCP3D driver to log various messages.\r
85  *\r
86  * <b> Prototype: </b>\r
87  *  The following is the C prototype for the expected OSAL API.\r
88  *\r
89  *  @verbatim\r
90        void Osal_tcp3dLog( String fmt, ... ) \r
91     @endverbatim\r
92  *\r
93  *  <b> Parameter </b>\r
94  *  @n  printf-style format string \r
95  *\r
96  *  <b> Return Value </b>\r
97  *  @n  Not applicable.\r
98  */\r
99 #define Tcp3d_osalLog            Osal_tcp3dLog\r
100 \r
101 /**\r
102  * @brief   The macro is used by the TCP3D driver to do memory copy.\r
103  *\r
104  * <b> Prototype: </b>\r
105  *  The following is the C prototype for the expected OSAL API.\r
106  *\r
107  *  @verbatim\r
108        void* Osal_memcpy(void *_s1, const void *_s2, size_t _n)\r
109     @endverbatim\r
110  *\r
111  *  <b> Parameter </b>\r
112  *  @n  _s1 - destination address\r
113  *  @n  _s2 - source address\r
114  *  @n  _n  - number of bytes\r
115  *\r
116  *  <b> Return Value </b>\r
117  *  @n  destination address\r
118  */\r
119 #define Tcp3d_memcpy            Osal_memcpy\r
120 \r
121 /**\r
122  * @brief   The macro is used by the TCP3D driver to initialize memory.\r
123  *\r
124  * <b> Prototype: </b>\r
125  *  The following is the C prototype for the expected OSAL API.\r
126  *\r
127  *  @verbatim\r
128        void* Osal_memset(void *_mem, int32_t _ch, size_t _n)\r
129     @endverbatim\r
130  *\r
131  *  <b> Parameter </b>\r
132  *  @n  _mem - destination address\r
133  *  @n  _ch  - value to be set with\r
134  *  @n  _n   - number of bytes\r
135  *\r
136  *  <b> Return Value </b>\r
137  *  @n  address value\r
138  */\r
139 #define Tcp3d_memset            Osal_memset\r
140 \r
141 /**\r
142 @}\r
143 */\r
144 \r
145 #endif /* __TCP3D_OSAL_H__ */\r
146 \r