43097a8bf274abfd7c6ce25acbbc7a2d9461cf1f
[keystone-rtos/wdtimer.git] / package.bld
1 /******************************************************************************
2  * FILE PURPOSE: Build description for the Watchdog Timer Module
3  ******************************************************************************
4  * FILE NAME: package.bld
5  *
6  * DESCRIPTION: 
7  *  This file contains the build specification and description for the 
8  *  Watchdog Timer Library
9  *  
10  *  The file takes the following parameters from the command line through the
11  *  XDCARGS variable.
12  *      XDCARGS[0] = WatchdogTimer Install Type 
13  *      Valid Values are "TAR" or "SETUP"
14  *      DEFAULT is "SETUP"
15  *
16  *  Example for a valid command:
17  *      xdc XDCARGS="SETUP" release   
18  *
19  * Copyright (C) 2012-2015, Texas Instruments, Inc.
20  *****************************************************************************/
22 /* List of all subdirectories that combine to make the Watchdog Timer Package. */
23 var subDirectories = [ "src", "docs", "test"];
25 /* Generate WatchdogTimerver.h */
26 var tplt = xdc.loadTemplate("./WatchdogTimerver.h.xdt");
27 tplt.genFile("./WatchdogTimerver.h",lldReleaseVersion);   
29 /* Determine if we need to create the InstallJammer Application or not? 
30  * Watchdog Timer Deliverables be either of the following formats:
31  *  - TAR Ball Package
32  *  - Setup Executable 
33  * DEFAULT is a TAR Executable. */
35 if ((arguments[0] != "TAR") && (arguments[0] != "SETUP"))
36     lldInstallType = "TAR";
37 else
38     lldInstallType = arguments[0];
40 /* Irrespective of the InstallType we always create a TAR Ball Package as a part
41  * of the RTSC Build. Here we determine the name of the TAR Ball Package
42  *  Format is as follows:
43  *      lld_<version> */
44 var lldRTSCFileName = "WatchdogTimer" + "_" + lldPartNumber + "_" +
45                       lldReleaseVersion[0] + "_" +  lldReleaseVersion[1] + "_" + 
46                       lldReleaseVersion[2]  + "_" + lldReleaseVersion[3];
48 /*****************************************************************
49  ************************ Release Banner *************************
50  *****************************************************************/
52 print ("************* Watchdog Timer Module Build Information *************");
53 print ("Watchdog Timer Install : " + lldInstallType);
54 print ("Watchdog Timer Version : " + lldReleaseVersion);
55 print ("C66 Tools Directory    : " + c66ToolsBaseDir);
56 print ("RTSC File Name         : " + lldRTSCFileName);
57 print ("Watchdog Timer Path    : " + lldPath);
58 print ("Coverity Analysis      : " + (coverityAnalysis == "ON" ? "ON" : "OFF"));
59 print ("CC LE opts             : " + C66LE.ccOpts.prefix);
60 print ("CC BE opts             : " + C66BE.ccOpts.prefix);
61 print ("***********************************************************");
63 /* Create the release package for the Watchdog Timer Module */
64 Pkg.defaultRelease = Pkg.addRelease (lldRTSCFileName, {prefix: "./packages/"});
66 /* Moving forward we need to set the Archiver of the package to be ZIP. This is currently
67  * not supported in the XDC tools being used. Currenly builds need to be done with the 
68  * following options:-
69  *   xdc MK_FIXLISTOPTS=-t release 
70  * ZIP is a better option as it works natively with INSTALL Jammer and we can remove the
71  * uncompression into a temporary directory. XDC Tools with xdc-rXX support the ZIP archiver. */
72 //Pkg.attrs = {archiver : "zip"};
74 /* Cycle through all the sub-directories and build all the files */
75 for (var i = 0; i < subDirectories.length; i++) 
76 {
77     /* Load the capsule in the sub directory. */
78     var caps = xdc.loadCapsule (subDirectories[i]+"/Module.xs");
80     print ("Building directory " + subDirectories[i]);
82     /* Build the capsule. */
83     caps.modBuild();
85     /* Package the module.xs files for building via package */
86     Pkg.otherFiles[Pkg.otherFiles.length++] = subDirectories[i]+"/Module.xs";
87 }
89 /* Package the remaining files */
90 Pkg.otherFiles[Pkg.otherFiles.length++] = "config.bld";
91 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.bld";
92 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xdc";
93 Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc";
94 Pkg.otherFiles[Pkg.otherFiles.length++] = "WatchdogTimer.xdc";
95 Pkg.otherFiles[Pkg.otherFiles.length++] = "WatchdogTimer.xs";
96 Pkg.otherFiles[Pkg.otherFiles.length++] = "WatchdogTimer.h";
97 Pkg.otherFiles[Pkg.otherFiles.length++] = "WatchdogTimerver.h";
98 Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/Doxyfile";
99 Pkg.otherFiles[Pkg.otherFiles.length++] = "build/buildlib.xs";
100 Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/ReleaseNotes_WatchdogTimer.pdf";
101 Pkg.otherFiles[Pkg.otherFiles.length++] = "makefile";
103 /* Generate Users Manual Doxyfile */
104 var tplt = xdc.loadTemplate("./docs/doxyfile.xdt");
105 tplt.genFile("./docs/Doxyfile",lldReleaseVersion); 
107 /* Generate Settings.xdc */
108 var tplt = xdc.loadTemplate("./Settings.xdc.xdt");
109 tplt.genFile("./Settings.xdc",lldReleaseVersion); 
111 /* Check if we need to create the mini package? */
112 var miniBuild = java.lang.System.getenv("MINI_PACKAGE");
114 if (miniBuild == "ON")
116     /***************************************************************************
117      ********************************* MINI Package ****************************
118      ***************************************************************************/
119     /* Create the MINI RTSC Package */
120     var libUtility = xdc.loadCapsule ("build/buildlib.xs");
121     libUtility.createMiniPkg(lldRTSCFileName);
124 /********************************************************************* 
125  *********************** INSTALL-JAMMER Support **********************
126  * In order to create the InstallJammer Application; we need to UNTAR
127  * the package into a temporary directory. This is required because 
128  * currently the InstallJammer does not support the TAR Files and thus
129  * creating an UNTAR of the file. So to work-around the problem we will
130  * do the following in the EPILOGUE Section:-
131  *  (a) Create a temporary directory called 'tmp'
132  *  (b) UNTAR the package into 'tmp'
133  *  (c) Run the INSTALL Jammer on 'tmp'
134  *  (d) Remove the 'tmp' directory.
135  *
136  * This can be done only after the 'release' package has been created.
137  * Thus all of this work is being done in the EPILOGUE.
138  *********************************************************************/
139 if (lldInstallType == "SETUP")
141     /* Create the Install Jammer Version Variable. This is used inside the 
142      * MPI File to create the Final executable. 
143      *  The format supported is as follows:-
144      *   - setupwin32_WatchdogTimer-<part_number>-<version>.exe 
145      *      This is for WatchdogTimer libraries and Header files
146      */
147     var InstallJammerVersion = "-DVersion " + lldPartNumber + "_" + lldReleaseVersion[0] + "_" +
148                                lldReleaseVersion[1] + "_" +  lldReleaseVersion[2]  + "_" + lldReleaseVersion[3];
150     /* This is the location where the tmp directory is located; this is used as 
151      * the input directory for the Install Jammer. */ 
152     var PackageBaseDir = " -DPackageBaseDir " + lldPath + "./tmp";
154     /* This is the location where the WatchdogTimer module will be installed by default. */
155     var WinInstallDir = " -DWinInstallDir C:/ti/WatchdogTimer" + "_" + 
156                             lldPartNumber + "_" + 
157                             lldReleaseVersion[0] + "_" +  lldReleaseVersion[1] + "_" +  
158                             lldReleaseVersion[2]  + "_" + lldReleaseVersion[3];
160     /* Create the actual EPILOGUE Section for the INSTALLER */
161     Pkg.makeEpilogue += "release: install_application\n";
162     Pkg.makeEpilogue += "install_application:\n";
163     Pkg.makeEpilogue += "\t @echo -------------------------------------------------------\n";
164     Pkg.makeEpilogue += "\t @echo Creating the Install\n";
165     Pkg.makeEpilogue += "\t @echo -------------------------------------------------------\n";
166     Pkg.makeEpilogue += "\t -$(MKDIR) tmp\n";
167     Pkg.makeEpilogue += "\t -$(MKDIR) tmp/packages\n";
168     Pkg.makeEpilogue += "\t -$(MKDIR) tmp/eclipse\n";
169     Pkg.makeEpilogue += "\t -$(CP) -R eclipse tmp\n";
170     Pkg.makeEpilogue += "\t tar -xf ./packages/" + lldRTSCFileName + ".tar" + " -Ctmp/packages \n";
171     Pkg.makeEpilogue += "\t installjammer " + InstallJammerVersion + PackageBaseDir + WinInstallDir + 
172                         " --output-dir packages/ --build install/WatchdogTimer.mpi\n";
173     Pkg.makeEpilogue += "\t -$(RMDIR) /S /Q tmp\n\n";
176 /* We need to clean after ourselves; extend the 'clean' target to take care of this. */
177 Pkg.makeEpilogue += "clean::\n";
178 Pkg.makeEpilogue += "\t -$(RM) docs/Doxyfile Settings.xdc WatchdogTimerver.h\n";
179 Pkg.makeEpilogue += "\t -$(RM) makefile\n";
180 Pkg.makeEpilogue += "\t -$(RMDIR) docs/doxygen\n";
181 if (lldInstallType == "SETUP")
183     Pkg.makeEpilogue += "\t -$(RM) packages/*.exe\n";
184     Pkg.makeEpilogue += "\t -$(RM) packages/*.bin\n";
185     Pkg.makeEpilogue += "\t -$(RMDIR) eclipse\n\n";
187 if (miniBuild == "ON")
189     Pkg.makeEpilogue += "\t -$(RM) simpleC66LE.mak\n";
190     Pkg.makeEpilogue += "\t -$(RM) simpleC66BE.mak\n";