summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 20f664a)
raw | patch | inline | side by side (parent: 20f664a)
author | Jamie Iles <jamie.iles@oracle.com> | |
Wed, 11 Jan 2017 00:57:54 +0000 (16:57 -0800) | ||
committer | Linus Torvalds <torvalds@linux-foundation.org> | |
Wed, 11 Jan 2017 02:31:55 +0000 (18:31 -0800) |
Since commit 00cd5c37afd5 ("ptrace: permit ptracing of /sbin/init") we
can now trace init processes. init is initially protected with
SIGNAL_UNKILLABLE which will prevent fatal signals such as SIGSTOP, but
there are a number of paths during tracing where SIGNAL_UNKILLABLE can
be implicitly cleared.
This can result in init becoming stoppable/killable after tracing. For
example, running:
while true; do kill -STOP 1; done &
strace -p 1
and then stopping strace and the kill loop will result in init being
left in state TASK_STOPPED. Sending SIGCONT to init will resume it, but
init will now respond to future SIGSTOP signals rather than ignoring
them.
Make sure that when setting SIGNAL_STOP_CONTINUED/SIGNAL_STOP_STOPPED
that we don't clear SIGNAL_UNKILLABLE.
Link: http://lkml.kernel.org/r/20170104122017.25047-1-jamie.iles@oracle.com
Signed-off-by: Jamie Iles <jamie.iles@oracle.com>
Acked-by: Oleg Nesterov <oleg@redhat.com>
Cc: Alexander Viro <viro@zeniv.linux.org.uk>
Cc: Ingo Molnar <mingo@redhat.com>
Cc: Peter Zijlstra <peterz@infradead.org>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
can now trace init processes. init is initially protected with
SIGNAL_UNKILLABLE which will prevent fatal signals such as SIGSTOP, but
there are a number of paths during tracing where SIGNAL_UNKILLABLE can
be implicitly cleared.
This can result in init becoming stoppable/killable after tracing. For
example, running:
while true; do kill -STOP 1; done &
strace -p 1
and then stopping strace and the kill loop will result in init being
left in state TASK_STOPPED. Sending SIGCONT to init will resume it, but
init will now respond to future SIGSTOP signals rather than ignoring
them.
Make sure that when setting SIGNAL_STOP_CONTINUED/SIGNAL_STOP_STOPPED
that we don't clear SIGNAL_UNKILLABLE.
Link: http://lkml.kernel.org/r/20170104122017.25047-1-jamie.iles@oracle.com
Signed-off-by: Jamie Iles <jamie.iles@oracle.com>
Acked-by: Oleg Nesterov <oleg@redhat.com>
Cc: Alexander Viro <viro@zeniv.linux.org.uk>
Cc: Ingo Molnar <mingo@redhat.com>
Cc: Peter Zijlstra <peterz@infradead.org>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
include/linux/sched.h | patch | blob | history | |
kernel/signal.c | patch | blob | history |
diff --git a/include/linux/sched.h b/include/linux/sched.h
index 4d1905245c7aa50df56acf0f77c77f3347c28c04..ad3ec9ec61f7b6de743b5d6de4225defcc18be99 100644 (file)
--- a/include/linux/sched.h
+++ b/include/linux/sched.h
#define SIGNAL_UNKILLABLE 0x00000040 /* for init: ignore fatal signals */
+#define SIGNAL_STOP_MASK (SIGNAL_CLD_MASK | SIGNAL_STOP_STOPPED | \
+ SIGNAL_STOP_CONTINUED)
+
+static inline void signal_set_stop_flags(struct signal_struct *sig,
+ unsigned int flags)
+{
+ WARN_ON(sig->flags & (SIGNAL_GROUP_EXIT|SIGNAL_GROUP_COREDUMP));
+ sig->flags = (sig->flags & ~SIGNAL_STOP_MASK) | flags;
+}
+
/* If true, all threads except ->group_exit_task have pending SIGKILL */
static inline int signal_group_exit(const struct signal_struct *sig)
{
diff --git a/kernel/signal.c b/kernel/signal.c
index ff046b73ff2d309ce00fbd3bd8949a8f6f5fd297..3603d93a19689be7188a004f2b999b27e0ebdf2f 100644 (file)
--- a/kernel/signal.c
+++ b/kernel/signal.c
* fresh group stop. Read comment in do_signal_stop() for details.
*/
if (!sig->group_stop_count && !(sig->flags & SIGNAL_STOP_STOPPED)) {
- sig->flags = SIGNAL_STOP_STOPPED;
+ signal_set_stop_flags(sig, SIGNAL_STOP_STOPPED);
return true;
}
return false;
* will take ->siglock, notice SIGNAL_CLD_MASK, and
* notify its parent. See get_signal_to_deliver().
*/
- signal->flags = why | SIGNAL_STOP_CONTINUED;
+ signal_set_stop_flags(signal, why | SIGNAL_STOP_CONTINUED);
signal->group_stop_count = 0;
signal->group_exit_code = 0;
}