summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: b4536f0)
raw | patch | inline | side by side (parent: b4536f0)
author | Alexander Duyck <alexander.h.duyck@intel.com> | |
Wed, 11 Jan 2017 00:58:06 +0000 (16:58 -0800) | ||
committer | Linus Torvalds <torvalds@linux-foundation.org> | |
Wed, 11 Jan 2017 02:31:55 +0000 (18:31 -0800) |
Patch series "Page fragment updates", v4.
This patch series takes care of a few cleanups for the page fragments
API.
First we do some renames so that things are much more consistent. First
we move the page_frag_ portion of the name to the front of the functions
names. Secondly we split out the cache specific functions from the
other page fragment functions by adding the word "cache" to the name.
Finally I added a bit of documentation that will hopefully help to
explain some of this. I plan to revisit this later as we get things
more ironed out in the near future with the changes planned for the DMA
setup to support eXpress Data Path.
This patch (of 3):
This patch renames the page frag functions to be more consistent with
other APIs. Specifically we place the name page_frag first in the name
and then have either an alloc or free call name that we append as the
suffix. This makes it a bit clearer in terms of naming.
In addition we drop the leading double underscores since we are
technically no longer a backing interface and instead the front end that
is called from the networking APIs.
Link: http://lkml.kernel.org/r/20170104023854.13451.67390.stgit@localhost.localdomain
Signed-off-by: Alexander Duyck <alexander.h.duyck@intel.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
This patch series takes care of a few cleanups for the page fragments
API.
First we do some renames so that things are much more consistent. First
we move the page_frag_ portion of the name to the front of the functions
names. Secondly we split out the cache specific functions from the
other page fragment functions by adding the word "cache" to the name.
Finally I added a bit of documentation that will hopefully help to
explain some of this. I plan to revisit this later as we get things
more ironed out in the near future with the changes planned for the DMA
setup to support eXpress Data Path.
This patch (of 3):
This patch renames the page frag functions to be more consistent with
other APIs. Specifically we place the name page_frag first in the name
and then have either an alloc or free call name that we append as the
suffix. This makes it a bit clearer in terms of naming.
In addition we drop the leading double underscores since we are
technically no longer a backing interface and instead the front end that
is called from the networking APIs.
Link: http://lkml.kernel.org/r/20170104023854.13451.67390.stgit@localhost.localdomain
Signed-off-by: Alexander Duyck <alexander.h.duyck@intel.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
include/linux/gfp.h | patch | blob | history | |
include/linux/skbuff.h | patch | blob | history | |
mm/page_alloc.c | patch | blob | history | |
net/core/skbuff.c | patch | blob | history |
diff --git a/include/linux/gfp.h b/include/linux/gfp.h
index 7806a8f80abc17c5ff31f1c260c46153ea20b7ba..ed77a86fbbb053243f8a8ce6bfd67036170a28d0 100644 (file)
--- a/include/linux/gfp.h
+++ b/include/linux/gfp.h
struct page_frag_cache;
extern void __page_frag_drain(struct page *page, unsigned int order,
unsigned int count);
-extern void *__alloc_page_frag(struct page_frag_cache *nc,
- unsigned int fragsz, gfp_t gfp_mask);
-extern void __free_page_frag(void *addr);
+extern void *page_frag_alloc(struct page_frag_cache *nc,
+ unsigned int fragsz, gfp_t gfp_mask);
+extern void page_frag_free(void *addr);
#define __free_page(page) __free_pages((page), 0)
#define free_page(addr) free_pages((addr), 0)
diff --git a/include/linux/skbuff.h b/include/linux/skbuff.h
index b53c0cfd417e3bec1c5cfab76787901bafa5884c..a410715bbef8889d148a6b3f8dbd6afc4ae6f4d0 100644 (file)
--- a/include/linux/skbuff.h
+++ b/include/linux/skbuff.h
@@ -2480,7 +2480,7 @@ static inline struct sk_buff *netdev_alloc_skb_ip_align(struct net_device *dev,
static inline void skb_free_frag(void *addr)
{
- __free_page_frag(addr);
+ page_frag_free(addr);
}
void *napi_alloc_frag(unsigned int fragsz);
diff --git a/mm/page_alloc.c b/mm/page_alloc.c
index 74afdb4177cbd89987e7221e5a17ada22b09c66b..097893ffe1940a0708874f5eaadddf83f73f74ce 100644 (file)
--- a/mm/page_alloc.c
+++ b/mm/page_alloc.c
}
EXPORT_SYMBOL(__page_frag_drain);
-void *__alloc_page_frag(struct page_frag_cache *nc,
- unsigned int fragsz, gfp_t gfp_mask)
+void *page_frag_alloc(struct page_frag_cache *nc,
+ unsigned int fragsz, gfp_t gfp_mask)
{
unsigned int size = PAGE_SIZE;
struct page *page;
return nc->va + offset;
}
-EXPORT_SYMBOL(__alloc_page_frag);
+EXPORT_SYMBOL(page_frag_alloc);
/*
* Frees a page fragment allocated out of either a compound or order 0 page.
*/
-void __free_page_frag(void *addr)
+void page_frag_free(void *addr)
{
struct page *page = virt_to_head_page(addr);
if (unlikely(put_page_testzero(page)))
__free_pages_ok(page, compound_order(page));
}
-EXPORT_SYMBOL(__free_page_frag);
+EXPORT_SYMBOL(page_frag_free);
static void *make_alloc_exact(unsigned long addr, unsigned int order,
size_t size)
diff --git a/net/core/skbuff.c b/net/core/skbuff.c
index 5a03730fbc1a84376985d4d68d8b80d8f38b0985..734c71468b013838516cfe8c744dcd0e797a6e2b 100644 (file)
--- a/net/core/skbuff.c
+++ b/net/core/skbuff.c
local_irq_save(flags);
nc = this_cpu_ptr(&netdev_alloc_cache);
- data = __alloc_page_frag(nc, fragsz, gfp_mask);
+ data = page_frag_alloc(nc, fragsz, gfp_mask);
local_irq_restore(flags);
return data;
}
{
struct napi_alloc_cache *nc = this_cpu_ptr(&napi_alloc_cache);
- return __alloc_page_frag(&nc->page, fragsz, gfp_mask);
+ return page_frag_alloc(&nc->page, fragsz, gfp_mask);
}
void *napi_alloc_frag(unsigned int fragsz)
local_irq_save(flags);
nc = this_cpu_ptr(&netdev_alloc_cache);
- data = __alloc_page_frag(nc, len, gfp_mask);
+ data = page_frag_alloc(nc, len, gfp_mask);
pfmemalloc = nc->pfmemalloc;
local_irq_restore(flags);
if (sk_memalloc_socks())
gfp_mask |= __GFP_MEMALLOC;
- data = __alloc_page_frag(&nc->page, len, gfp_mask);
+ data = page_frag_alloc(&nc->page, len, gfp_mask);
if (unlikely(!data))
return NULL;