1 #
2 # GPIO infrastructure and drivers
3 #
5 config ARCH_HAVE_CUSTOM_GPIO_H
6 bool
7 help
8 Selecting this config option from the architecture Kconfig allows
9 the architecture to provide a custom asm/gpio.h implementation
10 overriding the default implementations. New uses of this are
11 strongly discouraged.
13 config ARCH_WANT_OPTIONAL_GPIOLIB
14 bool
15 help
16 Select this config option from the architecture Kconfig, if
17 it is possible to use gpiolib on the architecture, but let the
18 user decide whether to actually build it or not.
19 Select this instead of ARCH_REQUIRE_GPIOLIB, if your architecture does
20 not depend on GPIOs being available, but rather let the user
21 decide whether he needs it or not.
23 config ARCH_REQUIRE_GPIOLIB
24 bool
25 select GPIOLIB
26 help
27 Platforms select gpiolib if they use this infrastructure
28 for all their GPIOs, usually starting with ones integrated
29 into SOC processors.
30 Selecting this from the architecture code will cause the gpiolib
31 code to always get built in.
34 menuconfig GPIOLIB
35 bool "GPIO Support"
36 depends on ARCH_WANT_OPTIONAL_GPIOLIB || ARCH_REQUIRE_GPIOLIB
37 help
38 This enables GPIO support through the generic GPIO library.
39 You only need to enable this, if you also want to enable
40 one or more of the GPIO drivers below.
42 If unsure, say N.
44 if GPIOLIB
46 config GPIO_DEVRES
47 def_bool y
48 depends on HAS_IOMEM
50 config OF_GPIO
51 def_bool y
52 depends on OF
54 config GPIO_ACPI
55 def_bool y
56 depends on ACPI
58 config DEBUG_GPIO
59 bool "Debug GPIO calls"
60 depends on DEBUG_KERNEL
61 help
62 Say Y here to add some extra checks and diagnostics to GPIO calls.
63 These checks help ensure that GPIOs have been properly initialized
64 before they are used, and that sleeping calls are not made from
65 non-sleeping contexts. They can make bitbanged serial protocols
66 slower. The diagnostics help catch the type of setup errors
67 that are most common when setting up new platforms or boards.
69 config GPIO_SYSFS
70 bool "/sys/class/gpio/... (sysfs interface)"
71 depends on SYSFS
72 help
73 Say Y here to add a sysfs interface for GPIOs.
75 This is mostly useful to work around omissions in a system's
76 kernel support. Those are common in custom and semicustom
77 hardware assembled using standard kernels with a minimum of
78 custom patches. In those cases, userspace code may import
79 a given GPIO from the kernel, if no kernel driver requested it.
81 Kernel drivers may also request that a particular GPIO be
82 exported to userspace; this can be useful when debugging.
84 config GPIO_GENERIC
85 tristate
87 # put drivers in the right section, in alphabetical order
89 config GPIO_DA9052
90 tristate "Dialog DA9052 GPIO"
91 depends on PMIC_DA9052
92 help
93 Say yes here to enable the GPIO driver for the DA9052 chip.
95 config GPIO_DA9055
96 tristate "Dialog Semiconductor DA9055 GPIO"
97 depends on MFD_DA9055
98 help
99 Say yes here to enable the GPIO driver for the DA9055 chip.
101 The Dialog DA9055 PMIC chip has 3 GPIO pins that can be
102 be controller by this driver.
104 If driver is built as a module it will be called gpio-da9055.
106 config GPIO_MAX730X
107 tristate
109 comment "Memory mapped GPIO drivers:"
111 config GPIO_CLPS711X
112 tristate "CLPS711X GPIO support"
113 depends on ARCH_CLPS711X || COMPILE_TEST
114 select GPIO_GENERIC
115 help
116 Say yes here to support GPIO on CLPS711X SoCs.
118 config GPIO_DAVINCI
119 bool "TI Davinci/Keystone GPIO support"
120 default y if ARCH_DAVINCI
121 depends on ARM && (ARCH_DAVINCI || ARCH_KEYSTONE)
122 help
123 Say yes here to enable GPIO support for TI Davinci/Keystone SoCs.
125 config GPIO_GENERIC_PLATFORM
126 tristate "Generic memory-mapped GPIO controller support (MMIO platform device)"
127 select GPIO_GENERIC
128 help
129 Say yes here to support basic platform_device memory-mapped GPIO controllers.
131 config GPIO_IT8761E
132 tristate "IT8761E GPIO support"
133 depends on X86 # unconditional access to IO space.
134 help
135 Say yes here to support GPIO functionality of IT8761E super I/O chip.
137 config GPIO_EM
138 tristate "Emma Mobile GPIO"
139 depends on ARM && OF_GPIO
140 help
141 Say yes here to support GPIO on Renesas Emma Mobile SoCs.
143 config GPIO_EP93XX
144 def_bool y
145 depends on ARCH_EP93XX
146 select GPIO_GENERIC
148 config GPIO_MM_LANTIQ
149 bool "Lantiq Memory mapped GPIOs"
150 depends on LANTIQ && SOC_XWAY
151 help
152 This enables support for memory mapped GPIOs on the External Bus Unit
153 (EBU) found on Lantiq SoCs. The gpios are output only as they are
154 created by attaching a 16bit latch to the bus.
156 config GPIO_F7188X
157 tristate "F71882FG and F71889F GPIO support"
158 depends on X86
159 help
160 This option enables support for GPIOs found on Fintek Super-I/O
161 chips F71882FG and F71889F.
163 To compile this driver as a module, choose M here: the module will
164 be called f7188x-gpio.
166 config GPIO_MOXART
167 bool "MOXART GPIO support"
168 depends on ARCH_MOXART
169 help
170 Select this option to enable GPIO driver for
171 MOXA ART SoC devices.
173 config GPIO_MPC5200
174 def_bool y
175 depends on PPC_MPC52xx
177 config GPIO_MPC8XXX
178 bool "MPC512x/MPC8xxx GPIO support"
179 depends on PPC_MPC512x || PPC_MPC831x || PPC_MPC834x || PPC_MPC837x || \
180 FSL_SOC_BOOKE || PPC_86xx
181 help
182 Say Y here if you're going to use hardware that connects to the
183 MPC512x/831x/834x/837x/8572/8610 GPIOs.
185 config GPIO_MSM_V1
186 tristate "Qualcomm MSM GPIO v1"
187 depends on GPIOLIB && ARCH_MSM && (ARCH_MSM7X00A || ARCH_MSM7X30 || ARCH_QSD8X50)
188 help
189 Say yes here to support the GPIO interface on ARM v6 based
190 Qualcomm MSM chips. Most of the pins on the MSM can be
191 selected for GPIO, and are controlled by this driver.
193 config GPIO_MSM_V2
194 tristate "Qualcomm MSM GPIO v2"
195 depends on GPIOLIB && OF && ARCH_MSM
196 help
197 Say yes here to support the GPIO interface on ARM v7 based
198 Qualcomm MSM chips. Most of the pins on the MSM can be
199 selected for GPIO, and are controlled by this driver.
201 config GPIO_MVEBU
202 def_bool y
203 depends on PLAT_ORION
204 depends on OF
205 select GPIO_GENERIC
206 select GENERIC_IRQ_CHIP
208 config GPIO_MXC
209 def_bool y
210 depends on ARCH_MXC
211 select GPIO_GENERIC
212 select GENERIC_IRQ_CHIP
214 config GPIO_MXS
215 def_bool y
216 depends on ARCH_MXS
217 select GPIO_GENERIC
218 select GENERIC_IRQ_CHIP
220 config GPIO_OCTEON
221 tristate "Cavium OCTEON GPIO"
222 depends on GPIOLIB && CAVIUM_OCTEON_SOC
223 default y
224 help
225 Say yes here to support the on-chip GPIO lines on the OCTEON
226 family of SOCs.
228 config GPIO_PL061
229 bool "PrimeCell PL061 GPIO support"
230 depends on ARM_AMBA
231 select GENERIC_IRQ_CHIP
232 help
233 Say yes here to support the PrimeCell PL061 GPIO device
235 config GPIO_PXA
236 bool "PXA GPIO support"
237 depends on ARCH_PXA || ARCH_MMP
238 help
239 Say yes here to support the PXA GPIO device
241 config GPIO_RCAR
242 tristate "Renesas R-Car GPIO"
243 depends on ARM
244 help
245 Say yes here to support GPIO on Renesas R-Car SoCs.
247 config GPIO_SAMSUNG
248 bool
249 depends on PLAT_SAMSUNG
250 help
251 Legacy GPIO support. Use only for platforms without support for
252 pinctrl.
254 config GPIO_SCH311X
255 tristate "SMSC SCH311x SuperI/O GPIO"
256 help
257 Driver to enable the GPIOs found on SMSC SMSC SCH3112, SCH3114 and
258 SCH3116 "Super I/O" chipsets.
260 To compile this driver as a module, choose M here: the module will
261 be called gpio-sch311x.
263 config GPIO_SPEAR_SPICS
264 bool "ST SPEAr13xx SPI Chip Select as GPIO support"
265 depends on PLAT_SPEAR
266 select GENERIC_IRQ_CHIP
267 help
268 Say yes here to support ST SPEAr SPI Chip Select as GPIO device
270 config GPIO_STA2X11
271 bool "STA2x11/ConneXt GPIO support"
272 depends on MFD_STA2X11
273 select GENERIC_IRQ_CHIP
274 help
275 Say yes here to support the STA2x11/ConneXt GPIO device.
276 The GPIO module has 128 GPIO pins with alternate functions.
278 config GPIO_TS5500
279 tristate "TS-5500 DIO blocks and compatibles"
280 help
281 This driver supports Digital I/O exposed by pin blocks found on some
282 Technologic Systems platforms. It includes, but is not limited to, 3
283 blocks of the TS-5500: DIO1, DIO2 and the LCD port, and the TS-5600
284 LCD port.
286 config GPIO_TZ1090
287 bool "Toumaz Xenif TZ1090 GPIO support"
288 depends on SOC_TZ1090
289 select GENERIC_IRQ_CHIP
290 default y
291 help
292 Say yes here to support Toumaz Xenif TZ1090 GPIOs.
294 config GPIO_TZ1090_PDC
295 bool "Toumaz Xenif TZ1090 PDC GPIO support"
296 depends on SOC_TZ1090
297 default y
298 help
299 Say yes here to support Toumaz Xenif TZ1090 PDC GPIOs.
301 config GPIO_XILINX
302 bool "Xilinx GPIO support"
303 depends on PPC_OF || MICROBLAZE || ARCH_ZYNQ
304 help
305 Say yes here to support the Xilinx FPGA GPIO device
307 config GPIO_XTENSA
308 bool "Xtensa GPIO32 support"
309 depends on XTENSA
310 depends on HAVE_XTENSA_GPIO32
311 depends on !SMP
312 help
313 Say yes here to support the Xtensa internal GPIO32 IMPWIRE (input)
314 and EXPSTATE (output) ports
316 config GPIO_VR41XX
317 tristate "NEC VR4100 series General-purpose I/O Uint support"
318 depends on CPU_VR41XX
319 help
320 Say yes here to support the NEC VR4100 series General-purpose I/O Uint
322 config GPIO_SCH
323 tristate "Intel SCH/TunnelCreek/Centerton GPIO"
324 depends on PCI && X86
325 select MFD_CORE
326 select LPC_SCH
327 help
328 Say yes here to support GPIO interface on Intel Poulsbo SCH,
329 Intel Tunnel Creek processor or Intel Centerton processor.
330 The Intel SCH contains a total of 14 GPIO pins. Ten GPIOs are
331 powered by the core power rail and are turned off during sleep
332 modes (S3 and higher). The remaining four GPIOs are powered by
333 the Intel SCH suspend power supply. These GPIOs remain
334 active during S3. The suspend powered GPIOs can be used to wake the
335 system from the Suspend-to-RAM state.
336 The Intel Tunnel Creek processor has 5 GPIOs powered by the
337 core power rail and 9 from suspend power supply.
338 The Intel Centerton processor has a total of 30 GPIO pins.
339 Twenty-one are powered by the core power rail and 9 from the
340 suspend power supply.
342 config GPIO_ICH
343 tristate "Intel ICH GPIO"
344 depends on PCI && X86
345 select MFD_CORE
346 select LPC_ICH
347 help
348 Say yes here to support the GPIO functionality of a number of Intel
349 ICH-based chipsets. Currently supported devices: ICH6, ICH7, ICH8
350 ICH9, ICH10, Series 5/3400 (eg Ibex Peak), Series 6/C200 (eg
351 Cougar Point), NM10 (Tiger Point), and 3100 (Whitmore Lake).
353 If unsure, say N.
355 config GPIO_IOP
356 tristate "Intel IOP GPIO"
357 depends on ARM && (ARCH_IOP32X || ARCH_IOP33X)
358 help
359 Say yes here to support the GPIO functionality of a number of Intel
360 IOP32X or IOP33X.
362 If unsure, say N.
364 config GPIO_VX855
365 tristate "VIA VX855/VX875 GPIO"
366 depends on PCI
367 select MFD_CORE
368 select MFD_VX855
369 help
370 Support access to the VX855/VX875 GPIO lines through the gpio library.
372 This driver provides common support for accessing the device,
373 additional drivers must be enabled in order to use the
374 functionality of the device.
376 config GPIO_GE_FPGA
377 bool "GE FPGA based GPIO"
378 depends on GE_FPGA
379 help
380 Support for common GPIO functionality provided on some GE Single Board
381 Computers.
383 This driver provides basic support (configure as input or output, read
384 and write pin state) for GPIO implemented in a number of GE single
385 board computers.
387 config GPIO_LYNXPOINT
388 tristate "Intel Lynxpoint GPIO support"
389 depends on ACPI && X86
390 select IRQ_DOMAIN
391 help
392 driver for GPIO functionality on Intel Lynxpoint PCH chipset
393 Requires ACPI device enumeration code to set up a platform device.
395 config GPIO_GRGPIO
396 tristate "Aeroflex Gaisler GRGPIO support"
397 depends on OF
398 select GPIO_GENERIC
399 select IRQ_DOMAIN
400 help
401 Select this to support Aeroflex Gaisler GRGPIO cores from the GRLIB
402 VHDL IP core library.
404 config GPIO_TB10X
405 bool
406 select GENERIC_IRQ_CHIP
407 select OF_GPIO
409 comment "I2C GPIO expanders:"
411 config GPIO_ARIZONA
412 tristate "Wolfson Microelectronics Arizona class devices"
413 depends on MFD_ARIZONA
414 help
415 Support for GPIOs on Wolfson Arizona class devices.
417 config GPIO_LP3943
418 tristate "TI/National Semiconductor LP3943 GPIO expander"
419 depends on MFD_LP3943
420 help
421 GPIO driver for LP3943 MFD.
422 LP3943 can be used as a GPIO expander which provides up to 16 GPIOs.
423 Open drain outputs are required for this usage.
425 config GPIO_MAX7300
426 tristate "Maxim MAX7300 GPIO expander"
427 depends on I2C
428 select GPIO_MAX730X
429 help
430 GPIO driver for Maxim MAX7300 I2C-based GPIO expander.
432 config GPIO_MAX732X
433 tristate "MAX7319, MAX7320-7327 I2C Port Expanders"
434 depends on I2C
435 help
436 Say yes here to support the MAX7319, MAX7320-7327 series of I2C
437 Port Expanders. Each IO port on these chips has a fixed role of
438 Input (designated by 'I'), Push-Pull Output ('O'), or Open-Drain
439 Input and Output (designed by 'P'). The combinations are listed
440 below:
442 8 bits: max7319 (8I), max7320 (8O), max7321 (8P),
443 max7322 (4I4O), max7323 (4P4O)
445 16 bits: max7324 (8I8O), max7325 (8P8O),
446 max7326 (4I12O), max7327 (4P12O)
448 Board setup code must specify the model to use, and the start
449 number for these GPIOs.
451 config GPIO_MAX732X_IRQ
452 bool "Interrupt controller support for MAX732x"
453 depends on GPIO_MAX732X=y
454 help
455 Say yes here to enable the max732x to be used as an interrupt
456 controller. It requires the driver to be built in the kernel.
458 config GPIO_MC9S08DZ60
459 bool "MX35 3DS BOARD MC9S08DZ60 GPIO functions"
460 depends on I2C=y && MACH_MX35_3DS
461 help
462 Select this to enable the MC9S08DZ60 GPIO driver
464 config GPIO_PCA953X
465 tristate "PCA953x, PCA955x, PCA957x, TCA64xx, and MAX7310 I/O ports"
466 depends on I2C
467 help
468 Say yes here to provide access to several register-oriented
469 SMBus I/O expanders, made mostly by NXP or TI. Compatible
470 models include:
472 4 bits: pca9536, pca9537
474 8 bits: max7310, max7315, pca6107, pca9534, pca9538, pca9554,
475 pca9556, pca9557, pca9574, tca6408
477 16 bits: max7312, max7313, pca9535, pca9539, pca9555, pca9575,
478 tca6416
480 config GPIO_PCA953X_IRQ
481 bool "Interrupt controller support for PCA953x"
482 depends on GPIO_PCA953X=y
483 help
484 Say yes here to enable the pca953x to be used as an interrupt
485 controller. It requires the driver to be built in the kernel.
487 config GPIO_PCF857X
488 tristate "PCF857x, PCA{85,96}7x, and MAX732[89] I2C GPIO expanders"
489 depends on I2C
490 select IRQ_DOMAIN
491 help
492 Say yes here to provide access to most "quasi-bidirectional" I2C
493 GPIO expanders used for additional digital outputs or inputs.
494 Most of these parts are from NXP, though TI is a second source for
495 some of them. Compatible models include:
497 8 bits: pcf8574, pcf8574a, pca8574, pca8574a,
498 pca9670, pca9672, pca9674, pca9674a,
499 max7328, max7329
501 16 bits: pcf8575, pcf8575c, pca8575,
502 pca9671, pca9673, pca9675
504 Your board setup code will need to declare the expanders in
505 use, and assign numbers to the GPIOs they expose. Those GPIOs
506 can then be used from drivers and other kernel code, just like
507 other GPIOs, but only accessible from task contexts.
509 This driver provides an in-kernel interface to those GPIOs using
510 platform-neutral GPIO calls.
512 config GPIO_RC5T583
513 bool "RICOH RC5T583 GPIO"
514 depends on MFD_RC5T583
515 help
516 Select this option to enable GPIO driver for the Ricoh RC5T583
517 chip family.
518 This driver provides the support for driving/reading the gpio pins
519 of RC5T583 device through standard gpio library.
521 config GPIO_SX150X
522 bool "Semtech SX150x I2C GPIO expander"
523 depends on I2C=y
524 default n
525 help
526 Say yes here to provide support for Semtech SX150-series I2C
527 GPIO expanders. Compatible models include:
529 8 bits: sx1508q
530 16 bits: sx1509q
532 config GPIO_STMPE
533 bool "STMPE GPIOs"
534 depends on MFD_STMPE
535 help
536 This enables support for the GPIOs found on the STMPE I/O
537 Expanders.
539 config GPIO_STP_XWAY
540 bool "XWAY STP GPIOs"
541 depends on SOC_XWAY
542 help
543 This enables support for the Serial To Parallel (STP) unit found on
544 XWAY SoC. The STP allows the SoC to drive a shift registers cascade,
545 that can be up to 24 bit. This peripheral is aimed at driving leds.
546 Some of the gpios/leds can be auto updated by the soc with dsl and
547 phy status.
549 config GPIO_TC3589X
550 bool "TC3589X GPIOs"
551 depends on MFD_TC3589X
552 help
553 This enables support for the GPIOs found on the TC3589X
554 I/O Expander.
556 config GPIO_TPS65912
557 tristate "TI TPS65912 GPIO"
558 depends on (MFD_TPS65912_I2C || MFD_TPS65912_SPI)
559 help
560 This driver supports TPS65912 gpio chip
562 config GPIO_TWL4030
563 tristate "TWL4030, TWL5030, and TPS659x0 GPIOs"
564 depends on TWL4030_CORE
565 help
566 Say yes here to access the GPIO signals of various multi-function
567 power management chips from Texas Instruments.
569 config GPIO_TWL6040
570 tristate "TWL6040 GPO"
571 depends on TWL6040_CORE
572 help
573 Say yes here to access the GPO signals of twl6040
574 audio chip from Texas Instruments.
576 config GPIO_WM831X
577 tristate "WM831x GPIOs"
578 depends on MFD_WM831X
579 help
580 Say yes here to access the GPIO signals of WM831x power management
581 chips from Wolfson Microelectronics.
583 config GPIO_WM8350
584 tristate "WM8350 GPIOs"
585 depends on MFD_WM8350
586 help
587 Say yes here to access the GPIO signals of WM8350 power management
588 chips from Wolfson Microelectronics.
590 config GPIO_WM8994
591 tristate "WM8994 GPIOs"
592 depends on MFD_WM8994
593 help
594 Say yes here to access the GPIO signals of WM8994 audio hub
595 CODECs from Wolfson Microelectronics.
597 config GPIO_ADP5520
598 tristate "GPIO Support for ADP5520 PMIC"
599 depends on PMIC_ADP5520
600 help
601 This option enables support for on-chip GPIO found
602 on Analog Devices ADP5520 PMICs.
604 config GPIO_ADP5588
605 tristate "ADP5588 I2C GPIO expander"
606 depends on I2C
607 help
608 This option enables support for 18 GPIOs found
609 on Analog Devices ADP5588 GPIO Expanders.
611 config GPIO_ADP5588_IRQ
612 bool "Interrupt controller support for ADP5588"
613 depends on GPIO_ADP5588=y
614 help
615 Say yes here to enable the adp5588 to be used as an interrupt
616 controller. It requires the driver to be built in the kernel.
618 config GPIO_ADNP
619 tristate "Avionic Design N-bit GPIO expander"
620 depends on I2C && OF_GPIO
621 help
622 This option enables support for N GPIOs found on Avionic Design
623 I2C GPIO expanders. The register space will be extended by powers
624 of two, so the controller will need to accommodate for that. For
625 example: if a controller provides 48 pins, 6 registers will be
626 enough to represent all pins, but the driver will assume a
627 register layout for 64 pins (8 registers).
629 comment "PCI GPIO expanders:"
631 config GPIO_CS5535
632 tristate "AMD CS5535/CS5536 GPIO support"
633 depends on PCI && X86 && MFD_CS5535
634 help
635 The AMD CS5535 and CS5536 southbridges support 28 GPIO pins that
636 can be used for quite a number of things. The CS5535/6 is found on
637 AMD Geode and Lemote Yeeloong devices.
639 If unsure, say N.
641 config GPIO_BT8XX
642 tristate "BT8XX GPIO abuser"
643 depends on PCI && VIDEO_BT848=n
644 help
645 The BT8xx frame grabber chip has 24 GPIO pins than can be abused
646 as a cheap PCI GPIO card.
648 This chip can be found on Miro, Hauppauge and STB TV-cards.
650 The card needs to be physically altered for using it as a
651 GPIO card. For more information on how to build a GPIO card
652 from a BT8xx TV card, see the documentation file at
653 Documentation/bt8xxgpio.txt
655 If unsure, say N.
657 config GPIO_AMD8111
658 tristate "AMD 8111 GPIO driver"
659 depends on PCI
660 help
661 The AMD 8111 south bridge contains 32 GPIO pins which can be used.
663 Note, that usually system firmware/ACPI handles GPIO pins on their
664 own and users might easily break their systems with uncarefull usage
665 of this driver!
667 If unsure, say N
669 config GPIO_INTEL_MID
670 bool "Intel Mid GPIO support"
671 depends on PCI && X86
672 select IRQ_DOMAIN
673 help
674 Say Y here to support Intel Mid GPIO.
676 config GPIO_PCH
677 tristate "Intel EG20T PCH/LAPIS Semiconductor IOH(ML7223/ML7831) GPIO"
678 depends on PCI && X86
679 select GENERIC_IRQ_CHIP
680 help
681 This driver is for PCH(Platform controller Hub) GPIO of Intel Topcliff
682 which is an IOH(Input/Output Hub) for x86 embedded processor.
683 This driver can access PCH GPIO device.
685 This driver also can be used for LAPIS Semiconductor IOH(Input/
686 Output Hub), ML7223 and ML7831.
687 ML7223 IOH is for MP(Media Phone) use.
688 ML7831 IOH is for general purpose use.
689 ML7223/ML7831 is companion chip for Intel Atom E6xx series.
690 ML7223/ML7831 is completely compatible for Intel EG20T PCH.
692 config GPIO_ML_IOH
693 tristate "OKI SEMICONDUCTOR ML7213 IOH GPIO support"
694 depends on PCI
695 select GENERIC_IRQ_CHIP
696 help
697 ML7213 is companion chip for Intel Atom E6xx series.
698 This driver can be used for OKI SEMICONDUCTOR ML7213 IOH(Input/Output
699 Hub) which is for IVI(In-Vehicle Infotainment) use.
700 This driver can access the IOH's GPIO device.
702 config GPIO_SODAVILLE
703 bool "Intel Sodaville GPIO support"
704 depends on X86 && PCI && OF
705 select GPIO_GENERIC
706 select GENERIC_IRQ_CHIP
707 help
708 Say Y here to support Intel Sodaville GPIO.
710 config GPIO_TIMBERDALE
711 bool "Support for timberdale GPIO IP"
712 depends on MFD_TIMBERDALE && HAS_IOMEM
713 ---help---
714 Add support for the GPIO IP in the timberdale FPGA.
716 config GPIO_RDC321X
717 tristate "RDC R-321x GPIO support"
718 depends on PCI
719 select MFD_CORE
720 select MFD_RDC321X
721 help
722 Support for the RDC R321x SoC GPIOs over southbridge
723 PCI configuration space.
725 comment "SPI GPIO expanders:"
727 config GPIO_MAX7301
728 tristate "Maxim MAX7301 GPIO expander"
729 depends on SPI_MASTER
730 select GPIO_MAX730X
731 help
732 GPIO driver for Maxim MAX7301 SPI-based GPIO expander.
734 config GPIO_MCP23S08
735 tristate "Microchip MCP23xxx I/O expander"
736 depends on OF_GPIO
737 depends on (SPI_MASTER && !I2C) || I2C
738 help
739 SPI/I2C driver for Microchip MCP23S08/MCP23S17/MCP23008/MCP23017
740 I/O expanders.
741 This provides a GPIO interface supporting inputs and outputs.
742 The I2C versions of the chips can be used as interrupt-controller.
744 config GPIO_MC33880
745 tristate "Freescale MC33880 high-side/low-side switch"
746 depends on SPI_MASTER
747 help
748 SPI driver for Freescale MC33880 high-side/low-side switch.
749 This provides GPIO interface supporting inputs and outputs.
751 config GPIO_74X164
752 tristate "74x164 serial-in/parallel-out 8-bits shift register"
753 depends on SPI_MASTER && OF
754 help
755 Driver for 74x164 compatible serial-in/parallel-out 8-outputs
756 shift registers. This driver can be used to provide access
757 to more gpio outputs.
759 comment "AC97 GPIO expanders:"
761 config GPIO_UCB1400
762 tristate "Philips UCB1400 GPIO"
763 depends on UCB1400_CORE
764 help
765 This enables support for the Philips UCB1400 GPIO pins.
766 The UCB1400 is an AC97 audio codec.
768 comment "LPC GPIO expanders:"
770 config GPIO_KEMPLD
771 tristate "Kontron ETX / COMexpress GPIO"
772 depends on MFD_KEMPLD
773 help
774 This enables support for the PLD GPIO interface on some Kontron ETX
775 and COMexpress (ETXexpress) modules.
777 This driver can also be built as a module. If so, the module will be
778 called gpio-kempld.
780 comment "MODULbus GPIO expanders:"
782 config GPIO_JANZ_TTL
783 tristate "Janz VMOD-TTL Digital IO Module"
784 depends on MFD_JANZ_CMODIO
785 help
786 This enables support for the Janz VMOD-TTL Digital IO module.
787 This driver provides support for driving the pins in output
788 mode only. Input mode is not supported.
790 config GPIO_PALMAS
791 bool "TI PALMAS series PMICs GPIO"
792 depends on MFD_PALMAS
793 help
794 Select this option to enable GPIO driver for the TI PALMAS
795 series chip family.
797 config GPIO_TPS6586X
798 bool "TPS6586X GPIO"
799 depends on MFD_TPS6586X
800 help
801 Select this option to enable GPIO driver for the TPS6586X
802 chip family.
804 config GPIO_TPS65910
805 bool "TPS65910 GPIO"
806 depends on MFD_TPS65910
807 help
808 Select this option to enable GPIO driver for the TPS65910
809 chip family.
811 config GPIO_MSIC
812 bool "Intel MSIC mixed signal gpio support"
813 depends on MFD_INTEL_MSIC
814 help
815 Enable support for GPIO on intel MSIC controllers found in
816 intel MID devices
818 config GPIO_BCM_KONA
819 bool "Broadcom Kona GPIO"
820 depends on OF_GPIO
821 help
822 Turn on GPIO support for Broadcom "Kona" chips.
824 comment "USB GPIO expanders:"
826 config GPIO_VIPERBOARD
827 tristate "Viperboard GPIO a & b support"
828 depends on MFD_VIPERBOARD && USB
829 help
830 Say yes here to access the GPIO signals of Nano River
831 Technologies Viperboard. There are two GPIO chips on the
832 board: gpioa and gpiob.
833 See viperboard API specification and Nano
834 River Tech's viperboard.h for detailed meaning
835 of the module parameters.
837 endif