/* * drivers/media/i2c/lm3560.c * General device driver for TI lm3560, FLASH LED Driver * * Copyright (C) 2013 Texas Instruments * * Contact: Daniel Jeong * Ldd-Mlp * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License * version 2 as published by the Free Software Foundation. * * This program is distributed in the hope that it will be useful, but * WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 51 Franklin St, Fifth Floor, Boston, MA * 02110-1301 USA * */ #include #include #include #include #include #include #include #include #include #include /* registers definitions */ #define REG_ENABLE 0x10 #define REG_TORCH_BR 0xa0 #define REG_FLASH_BR 0xb0 #define REG_FLASH_TOUT 0xc0 #define REG_FLAG 0xd0 #define REG_CONFIG1 0xe0 /* Fault Mask */ #define FAULT_TIMEOUT (1<<0) #define FAULT_OVERTEMP (1<<1) #define FAULT_SHORT_CIRCUIT (1<<2) enum led_enable { MODE_SHDN = 0x0, MODE_TORCH = 0x2, MODE_FLASH = 0x3, }; /* struct lm3560_flash * * @pdata: platform data * @regmap: reg. map for i2c * @lock: muxtex for serial access. * @led_mode: V4L2 LED mode * @ctrls_led: V4L2 contols * @subdev_led: V4L2 subdev */ struct lm3560_flash { struct device *dev; struct lm3560_platform_data *pdata; struct regmap *regmap; struct mutex lock; enum v4l2_flash_led_mode led_mode; struct v4l2_ctrl_handler ctrls_led[LM3560_LED_MAX]; struct v4l2_subdev subdev_led[LM3560_LED_MAX]; }; #define to_lm3560_flash(_ctrl, _no) \ container_of(_ctrl->handler, struct lm3560_flash, ctrls_led[_no]) /* enable mode control */ static int lm3560_mode_ctrl(struct lm3560_flash *flash) { int rval = -EINVAL; switch (flash->led_mode) { case V4L2_FLASH_LED_MODE_NONE: rval = regmap_update_bits(flash->regmap, REG_ENABLE, 0x03, MODE_SHDN); break; case V4L2_FLASH_LED_MODE_TORCH: rval = regmap_update_bits(flash->regmap, REG_ENABLE, 0x03, MODE_TORCH); break; case V4L2_FLASH_LED_MODE_FLASH: rval = regmap_update_bits(flash->regmap, REG_ENABLE, 0x03, MODE_FLASH); break; } return rval; } /* led1/2 enable/disable */ static int lm3560_enable_ctrl(struct lm3560_flash *flash, enum lm3560_led_id led_no, bool on) { int rval; if (led_no == LM3560_LED0) { if (on == true) rval = regmap_update_bits(flash->regmap, REG_ENABLE, 0x08, 0x08); else rval = regmap_update_bits(flash->regmap, REG_ENABLE, 0x08, 0x00); } else { if (on == true) rval = regmap_update_bits(flash->regmap, REG_ENABLE, 0x10, 0x10); else rval = regmap_update_bits(flash->regmap, REG_ENABLE, 0x10, 0x00); } return rval; } /* torch1/2 brightness control */ static int lm3560_torch_brt_ctrl(struct lm3560_flash *flash, enum lm3560_led_id led_no, unsigned int brt) { int rval; u8 br_bits; if (brt < LM3560_TORCH_BRT_MIN) return lm3560_enable_ctrl(flash, led_no, false); else rval = lm3560_enable_ctrl(flash, led_no, true); br_bits = LM3560_TORCH_BRT_uA_TO_REG(brt); if (led_no == LM3560_LED0) rval = regmap_update_bits(flash->regmap, REG_TORCH_BR, 0x07, br_bits); else rval = regmap_update_bits(flash->regmap, REG_TORCH_BR, 0x38, br_bits << 3); return rval; } /* flash1/2 brightness control */ static int lm3560_flash_brt_ctrl(struct lm3560_flash *flash, enum lm3560_led_id led_no, unsigned int brt) { int rval; u8 br_bits; if (brt < LM3560_FLASH_BRT_MIN) return lm3560_enable_ctrl(flash, led_no, false); else rval = lm3560_enable_ctrl(flash, led_no, true); br_bits = LM3560_FLASH_BRT_uA_TO_REG(brt); if (led_no == LM3560_LED0) rval = regmap_update_bits(flash->regmap, REG_FLASH_BR, 0x0f, br_bits); else rval = regmap_update_bits(flash->regmap, REG_FLASH_BR, 0xf0, br_bits << 4); return rval; } /* V4L2 controls */ static int lm3560_get_ctrl(struct v4l2_ctrl *ctrl, enum lm3560_led_id led_no) { struct lm3560_flash *flash = to_lm3560_flash(ctrl, led_no); int rval = -EINVAL; mutex_lock(&flash->lock); if (ctrl->id == V4L2_CID_FLASH_FAULT) { s32 fault = 0; unsigned int reg_val; rval = regmap_read(flash->regmap, REG_FLAG, ®_val); if (rval < 0) goto out; if (reg_val & FAULT_SHORT_CIRCUIT) fault |= V4L2_FLASH_FAULT_SHORT_CIRCUIT; if (reg_val & FAULT_OVERTEMP) fault |= V4L2_FLASH_FAULT_OVER_TEMPERATURE; if (reg_val & FAULT_TIMEOUT) fault |= V4L2_FLASH_FAULT_TIMEOUT; ctrl->cur.val = fault; } out: mutex_unlock(&flash->lock); return rval; } static int lm3560_set_ctrl(struct v4l2_ctrl *ctrl, enum lm3560_led_id led_no) { struct lm3560_flash *flash = to_lm3560_flash(ctrl, led_no); u8 tout_bits; int rval = -EINVAL; mutex_lock(&flash->lock); switch (ctrl->id) { case V4L2_CID_FLASH_LED_MODE: flash->led_mode = ctrl->val; if (flash->led_mode != V4L2_FLASH_LED_MODE_FLASH) rval = lm3560_mode_ctrl(flash); break; case V4L2_CID_FLASH_STROBE_SOURCE: rval = regmap_update_bits(flash->regmap, REG_CONFIG1, 0x04, (ctrl->val) << 2); if (rval < 0) goto err_out; break; case V4L2_CID_FLASH_STROBE: if (flash->led_mode != V4L2_FLASH_LED_MODE_FLASH) { rval = -EBUSY; goto err_out; } flash->led_mode = V4L2_FLASH_LED_MODE_FLASH; rval = lm3560_mode_ctrl(flash); break; case V4L2_CID_FLASH_STROBE_STOP: if (flash->led_mode != V4L2_FLASH_LED_MODE_FLASH) { rval = -EBUSY; goto err_out; } flash->led_mode = V4L2_FLASH_LED_MODE_NONE; rval = lm3560_mode_ctrl(flash); break; case V4L2_CID_FLASH_TIMEOUT: tout_bits = LM3560_FLASH_TOUT_ms_TO_REG(ctrl->val); rval = regmap_update_bits(flash->regmap, REG_FLASH_TOUT, 0x1f, tout_bits); break; case V4L2_CID_FLASH_INTENSITY: rval = lm3560_flash_brt_ctrl(flash, led_no, ctrl->val); break; case V4L2_CID_FLASH_TORCH_INTENSITY: rval = lm3560_torch_brt_ctrl(flash, led_no, ctrl->val); break; } err_out: mutex_unlock(&flash->lock); return rval; } static int lm3560_led1_get_ctrl(struct v4l2_ctrl *ctrl) { return lm3560_get_ctrl(ctrl, LM3560_LED1); } static int lm3560_led1_set_ctrl(struct v4l2_ctrl *ctrl) { return lm3560_set_ctrl(ctrl, LM3560_LED1); } static int lm3560_led0_get_ctrl(struct v4l2_ctrl *ctrl) { return lm3560_get_ctrl(ctrl, LM3560_LED0); } static int lm3560_led0_set_ctrl(struct v4l2_ctrl *ctrl) { return lm3560_set_ctrl(ctrl, LM3560_LED0); } static const struct v4l2_ctrl_ops lm3560_led_ctrl_ops[LM3560_LED_MAX] = { [LM3560_LED0] = { .g_volatile_ctrl = lm3560_led0_get_ctrl, .s_ctrl = lm3560_led0_set_ctrl, }, [LM3560_LED1] = { .g_volatile_ctrl = lm3560_led1_get_ctrl, .s_ctrl = lm3560_led1_set_ctrl, } }; static int lm3560_init_controls(struct lm3560_flash *flash, enum lm3560_led_id led_no) { struct v4l2_ctrl *fault; u32 max_flash_brt = flash->pdata->max_flash_brt[led_no]; u32 max_torch_brt = flash->pdata->max_torch_brt[led_no]; struct v4l2_ctrl_handler *hdl = &flash->ctrls_led[led_no]; const struct v4l2_ctrl_ops *ops = &lm3560_led_ctrl_ops[led_no]; v4l2_ctrl_handler_init(hdl, 8); /* flash mode */ v4l2_ctrl_new_std_menu(hdl, ops, V4L2_CID_FLASH_LED_MODE, V4L2_FLASH_LED_MODE_TORCH, ~0x7, V4L2_FLASH_LED_MODE_NONE); flash->led_mode = V4L2_FLASH_LED_MODE_NONE; /* flash source */ v4l2_ctrl_new_std_menu(hdl, ops, V4L2_CID_FLASH_STROBE_SOURCE, 0x1, ~0x3, V4L2_FLASH_STROBE_SOURCE_SOFTWARE); /* flash strobe */ v4l2_ctrl_new_std(hdl, ops, V4L2_CID_FLASH_STROBE, 0, 0, 0, 0); /* flash strobe stop */ v4l2_ctrl_new_std(hdl, ops, V4L2_CID_FLASH_STROBE_STOP, 0, 0, 0, 0); /* flash strobe timeout */ v4l2_ctrl_new_std(hdl, ops, V4L2_CID_FLASH_TIMEOUT, LM3560_FLASH_TOUT_MIN, flash->pdata->max_flash_timeout, LM3560_FLASH_TOUT_STEP, flash->pdata->max_flash_timeout); /* flash brt */ v4l2_ctrl_new_std(hdl, ops, V4L2_CID_FLASH_INTENSITY, LM3560_FLASH_BRT_MIN, max_flash_brt, LM3560_FLASH_BRT_STEP, max_flash_brt); /* torch brt */ v4l2_ctrl_new_std(hdl, ops, V4L2_CID_FLASH_TORCH_INTENSITY, LM3560_TORCH_BRT_MIN, max_torch_brt, LM3560_TORCH_BRT_STEP, max_torch_brt); /* fault */ fault = v4l2_ctrl_new_std(hdl, ops, V4L2_CID_FLASH_FAULT, 0, V4L2_FLASH_FAULT_OVER_VOLTAGE | V4L2_FLASH_FAULT_OVER_TEMPERATURE | V4L2_FLASH_FAULT_SHORT_CIRCUIT | V4L2_FLASH_FAULT_TIMEOUT, 0, 0); if (fault != NULL) fault->flags |= V4L2_CTRL_FLAG_VOLATILE; if (hdl->error) return hdl->error; flash->subdev_led[led_no].ctrl_handler = hdl; return 0; } /* initialize device */ static const struct v4l2_subdev_ops lm3560_ops = { .core = NULL, }; static const struct regmap_config lm3560_regmap = { .reg_bits = 8, .val_bits = 8, .max_register = 0xFF, }; static int lm3560_subdev_init(struct lm3560_flash *flash, enum lm3560_led_id led_no, char *led_name) { struct i2c_client *client = to_i2c_client(flash->dev); int rval; v4l2_i2c_subdev_init(&flash->subdev_led[led_no], client, &lm3560_ops); flash->subdev_led[led_no].flags |= V4L2_SUBDEV_FL_HAS_DEVNODE; strcpy(flash->subdev_led[led_no].name, led_name); rval = lm3560_init_controls(flash, led_no); if (rval) goto err_out; rval = media_entity_init(&flash->subdev_led[led_no].entity, 0, NULL, 0); if (rval < 0) goto err_out; flash->subdev_led[led_no].entity.type = MEDIA_ENT_T_V4L2_SUBDEV_FLASH; return rval; err_out: v4l2_ctrl_handler_free(&flash->ctrls_led[led_no]); return rval; } static int lm3560_init_device(struct lm3560_flash *flash) { int rval; unsigned int reg_val; /* set peak current */ rval = regmap_update_bits(flash->regmap, REG_FLASH_TOUT, 0x60, flash->pdata->peak); if (rval < 0) return rval; /* output disable */ flash->led_mode = V4L2_FLASH_LED_MODE_NONE; rval = lm3560_mode_ctrl(flash); if (rval < 0) return rval; /* Reset faults */ rval = regmap_read(flash->regmap, REG_FLAG, ®_val); return rval; } static int lm3560_probe(struct i2c_client *client, const struct i2c_device_id *devid) { struct lm3560_flash *flash; struct lm3560_platform_data *pdata = dev_get_platdata(&client->dev); int rval; flash = devm_kzalloc(&client->dev, sizeof(*flash), GFP_KERNEL); if (flash == NULL) return -ENOMEM; flash->regmap = devm_regmap_init_i2c(client, &lm3560_regmap); if (IS_ERR(flash->regmap)) { rval = PTR_ERR(flash->regmap); return rval; } /* if there is no platform data, use chip default value */ if (pdata == NULL) { pdata = kzalloc(sizeof(struct lm3560_platform_data), GFP_KERNEL); if (pdata == NULL) return -ENODEV; pdata->peak = LM3560_PEAK_3600mA; pdata->max_flash_timeout = LM3560_FLASH_TOUT_MAX; /* led 1 */ pdata->max_flash_brt[LM3560_LED0] = LM3560_FLASH_BRT_MAX; pdata->max_torch_brt[LM3560_LED0] = LM3560_TORCH_BRT_MAX; /* led 2 */ pdata->max_flash_brt[LM3560_LED1] = LM3560_FLASH_BRT_MAX; pdata->max_torch_brt[LM3560_LED1] = LM3560_TORCH_BRT_MAX; } flash->pdata = pdata; flash->dev = &client->dev; mutex_init(&flash->lock); rval = lm3560_subdev_init(flash, LM3560_LED0, "lm3560-led0"); if (rval < 0) return rval; rval = lm3560_subdev_init(flash, LM3560_LED1, "lm3560-led1"); if (rval < 0) return rval; rval = lm3560_init_device(flash); if (rval < 0) return rval; i2c_set_clientdata(client, flash); return 0; } static int lm3560_remove(struct i2c_client *client) { struct lm3560_flash *flash = i2c_get_clientdata(client); unsigned int i; for (i = LM3560_LED0; i < LM3560_LED_MAX; i++) { v4l2_device_unregister_subdev(&flash->subdev_led[i]); v4l2_ctrl_handler_free(&flash->ctrls_led[i]); media_entity_cleanup(&flash->subdev_led[i].entity); } return 0; } static const struct i2c_device_id lm3560_id_table[] = { {LM3560_NAME, 0}, {} }; MODULE_DEVICE_TABLE(i2c, lm3560_id_table); static struct i2c_driver lm3560_i2c_driver = { .driver = { .name = LM3560_NAME, .pm = NULL, }, .probe = lm3560_probe, .remove = lm3560_remove, .id_table = lm3560_id_table, }; module_i2c_driver(lm3560_i2c_driver); MODULE_AUTHOR("Daniel Jeong "); MODULE_AUTHOR("Ldd Mlp "); MODULE_DESCRIPTION("Texas Instruments LM3560 LED flash driver"); MODULE_LICENSE("GPL");