IR: Move MDLocation into place This commit moves `MDLocation`, finishing off PR21433. There's an accompanying clang commit for frontend testcases. I'll attach the testcase upgrade script I used to PR21433 to help out-of-tree frontends/backends. This changes the schema for `DebugLoc` and `DILocation` from: !{i32 3, i32 7, !7, !8} to: !MDLocation(line: 3, column: 7, scope: !7, inlinedAt: !8) Note that empty fields (line/column: 0 and inlinedAt: null) don't get printed by the assembly writer. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@226048 91177308-0d34-0410-b5e6-96231b3b80d8
IR: Make metadata typeless in assembly Now that `Metadata` is typeless, reflect that in the assembly. These are the matching assembly changes for the metadata/value split in r223802. - Only use the `metadata` type when referencing metadata from a call intrinsic -- i.e., only when it's used as a `Value`. - Stop pretending that `ValueAsMetadata` is wrapped in an `MDNode` when referencing it from call intrinsics. So, assembly like this: define @foo(i32 %v) { call void @llvm.foo(metadata !{i32 %v}, metadata !0) call void @llvm.foo(metadata !{i32 7}, metadata !0) call void @llvm.foo(metadata !1, metadata !0) call void @llvm.foo(metadata !3, metadata !0) call void @llvm.foo(metadata !{metadata !3}, metadata !0) ret void, !bar !2 } !0 = metadata !{metadata !2} !1 = metadata !{i32* @global} !2 = metadata !{metadata !3} !3 = metadata !{} turns into this: define @foo(i32 %v) { call void @llvm.foo(metadata i32 %v, metadata !0) call void @llvm.foo(metadata i32 7, metadata !0) call void @llvm.foo(metadata i32* @global, metadata !0) call void @llvm.foo(metadata !3, metadata !0) call void @llvm.foo(metadata !{!3}, metadata !0) ret void, !bar !2 } !0 = !{!2} !1 = !{i32* @global} !2 = !{!3} !3 = !{} I wrote an upgrade script that handled almost all of the tests in llvm and many of the tests in cfe (even handling many `CHECK` lines). I've attached it (or will attach it in a moment if you're speedy) to PR21532 to help everyone update their out-of-tree testcases. This is part of PR21532. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@224257 91177308-0d34-0410-b5e6-96231b3b80d8
Revert "Revert "DI: Fold constant arguments into a single MDString"" This reverts commit r218918, effectively reapplying r218914 after fixing an Ocaml bindings test and an Asan crash. The root cause of the latter was a tightened-up check in `DILexicalBlock::Verify()`, so I'll file a PR to investigate who requires the loose check (and why). Original commit message follows. -- This patch addresses the first stage of PR17891 by folding constant arguments together into a single MDString. Integers are stringified and a `\0` character is used as a separator. Part of PR17891. Note: I've attached my testcases upgrade scripts to the PR. If I've just broken your out-of-tree testcases, they might help. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@219010 91177308-0d34-0410-b5e6-96231b3b80d8
Revert "DI: Fold constant arguments into a single MDString" This reverts commit r218914 while I investigate some bots. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@218918 91177308-0d34-0410-b5e6-96231b3b80d8
DI: Fold constant arguments into a single MDString This patch addresses the first stage of PR17891 by folding constant arguments together into a single MDString. Integers are stringified and a `\0` character is used as a separator. Part of PR17891. Note: I've attached my testcases upgrade scripts to the PR. If I've just broken your out-of-tree testcases, they might help. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@218914 91177308-0d34-0410-b5e6-96231b3b80d8
Move the complex address expression out of DIVariable and into an extra argument of the llvm.dbg.declare/llvm.dbg.value intrinsics. Previously, DIVariable was a variable-length field that has an optional reference to a Metadata array consisting of a variable number of complex address expressions. In the case of OpPiece expressions this is wasting a lot of storage in IR, because when an aggregate type is, e.g., SROA'd into all of its n individual members, the IR will contain n copies of the DIVariable, all alike, only differing in the complex address reference at the end. By making the complex address into an extra argument of the dbg.value/dbg.declare intrinsics, all of the pieces can reference the same variable and the complex address expressions can be uniqued across the CU, too. Down the road, this will allow us to move other flags, such as "indirection" out of the DIVariable, too. The new intrinsics look like this: declare void @llvm.dbg.declare(metadata %storage, metadata %var, metadata %expr) declare void @llvm.dbg.value(metadata %storage, i64 %offset, metadata %var, metadata %expr) This patch adds a new LLVM-local tag to DIExpressions, so we can detect and pretty-print DIExpression metadata nodes. What this patch doesn't do: This patch does not touch the "Indirect" field in DIVariable; but moving that into the expression would be a natural next step. http://reviews.llvm.org/D4919 rdar://problem/17994491 Thanks to dblaikie and dexonsmith for reviewing this patch! Note: I accidentally committed a bogus older version of this patch previously. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@218787 91177308-0d34-0410-b5e6-96231b3b80d8
Revert r218778 while investigating buldbot breakage. "Move the complex address expression out of DIVariable and into an extra" git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@218782 91177308-0d34-0410-b5e6-96231b3b80d8
Move the complex address expression out of DIVariable and into an extra argument of the llvm.dbg.declare/llvm.dbg.value intrinsics. Previously, DIVariable was a variable-length field that has an optional reference to a Metadata array consisting of a variable number of complex address expressions. In the case of OpPiece expressions this is wasting a lot of storage in IR, because when an aggregate type is, e.g., SROA'd into all of its n individual members, the IR will contain n copies of the DIVariable, all alike, only differing in the complex address reference at the end. By making the complex address into an extra argument of the dbg.value/dbg.declare intrinsics, all of the pieces can reference the same variable and the complex address expressions can be uniqued across the CU, too. Down the road, this will allow us to move other flags, such as "indirection" out of the DIVariable, too. The new intrinsics look like this: declare void @llvm.dbg.declare(metadata %storage, metadata %var, metadata %expr) declare void @llvm.dbg.value(metadata %storage, i64 %offset, metadata %var, metadata %expr) This patch adds a new LLVM-local tag to DIExpressions, so we can detect and pretty-print DIExpression metadata nodes. What this patch doesn't do: This patch does not touch the "Indirect" field in DIVariable; but moving that into the expression would be a natural next step. http://reviews.llvm.org/D4919 rdar://problem/17994491 Thanks to dblaikie and dexonsmith for reviewing this patch! git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@218778 91177308-0d34-0410-b5e6-96231b3b80d8
Make these regexes stricter by disallowing any additional characters in the output. Thanks to dblaikie for pointing this out! git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215166 91177308-0d34-0410-b5e6-96231b3b80d8
Reflow this comment. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215160 91177308-0d34-0410-b5e6-96231b3b80d8
DebugInfo: Fix a bunch of tests that, owing to their compile_unit metadata not including a 13th field, had some subtle behavior. Without the 13th field, the "emission kind" field defaults to 0 (which is not equal to either of the values of the emission kind enum (1 == full debug info, 2 == line tables only)). In this particular instance, the comparison with "FullDebugInfo" was done when adding elements to the ranges list - so for these test cases no values were added to the ranges list. This got weirder when emitting debug_loc entries as the addresses should be relative to the range of the CU if the CU has only one range (the reasonable assumption is that if we're emitting debug_loc lists for a CU that CU has at least one range - but due to the above situation, it has zero) so the ranges were emitted relative to the start of the section rather than relative to the start of the CU's singular range. Fix these tests by accounting for the difference in the description of debug_loc entries (in some cases making the test ignorant to these differences, in others adding the extra label difference expression, etc) or the presence/absence of high/low_pc on the CU, and add the 13th field to their CUs to enable proper "full debug info" emission here. In a future commit I'll fix up a bunch of other test cases that are not so rigorously depending on this behavior, but still doing similarly weird things due to the missing 13th field. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214937 91177308-0d34-0410-b5e6-96231b3b80d8
Debug info: Remove ARMAsmPrinter::EmitDwarfRegOp(). AsmPrinter can now scan the register file for sub- and super-registers. No functionality change intended. (Tests are updated because the comments in the assembler output are different.) git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@202416 91177308-0d34-0410-b5e6-96231b3b80d8
Generate the DWARF stack frame decode operations in the function prologue for ARM/Thumb functions. Patch by Keith Walker! git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@201423 91177308-0d34-0410-b5e6-96231b3b80d8
Debug Info: update testing cases to specify the debug info version number. We are going to drop debug info without a version number or with a different version number, to make sure we don't crash when we see bitcode files with different debug info metadata format. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@195504 91177308-0d34-0410-b5e6-96231b3b80d8
Debug Info Testing: updated to use NULL instead of "i32 0" in a few fields. Field 2 of DIType (Context), field 9 of DIDerivedType (TypeDerivedFrom), field 12 of DICompositeType (ContainingType), fields 2, 7, 12 of DISubprogram (Context, Type, ContainingType). git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@190205 91177308-0d34-0410-b5e6-96231b3b80d8
Debug Info: add an identifier field to DICompositeType. DICompositeType will have an identifier field at position 14. For now, the field is set to null in DIBuilder. For DICompositeTypes where the template argument field (the 13th field) was optional, modify DIBuilder to make sure the template argument field is set. Now DICompositeType has 15 fields. Update DIBuilder to use NULL instead of "i32 0" for null value of a MDNode. Update verifier to check that DICompositeType has 15 fields and the last field is null or a MDString. Update testing cases to include an extra field for DICompositeType. The identifier field will be used by type uniquing so a front end can genearte a DICompositeType with a unique identifer. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@189282 91177308-0d34-0410-b5e6-96231b3b80d8
Debug Info Verifier: enable verification of DICompileUnit. We used to call Verify before adding DICompileUnit to the list, and now we remove the check and always add DICompileUnit to the list in DebugInfoFinder, so we can verify them later on. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@187237 91177308-0d34-0410-b5e6-96231b3b80d8
Debug Info: improve the verifier to check field types. Make sure the context and type fields are MDNodes. We will generate verification errors if those fields are non-empty strings. Fix testing cases to make them pass the verifier. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@187106 91177308-0d34-0410-b5e6-96231b3b80d8
Revert "Revert "PR14606: debug info imported_module support"" This reverts commit r179840 with a fix to test/DebugInfo/two-cus-from-same-file.ll I'm not sure why that test only failed on ARM & MIPS and not X86 Linux, even though the debug info was clearly invalid on all of them, but this ought to fix it. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@179996 91177308-0d34-0410-b5e6-96231b3b80d8
Revert "PR14606: debug info imported_module support" This reverts commit r179836 as it seems to have caused test failures. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@179840 91177308-0d34-0410-b5e6-96231b3b80d8