Updates to sync with changes in upstream.
[opencl/llvm.git] / .gitignore
1 #==============================================================================#
2 # This file specifies intentionally untracked files that git should ignore.
3 # See: http://www.kernel.org/pub/software/scm/git/docs/gitignore.html
4 #
5 # This file is intentionally different from the output of `git svn show-ignore`,
6 # as most of those are useless.
7 #==============================================================================#
9 #==============================================================================#
10 # File extensions to be ignored anywhere in the tree.
11 #==============================================================================#
12 # Temp files created by most text editors.
13 *~
14 # Merge files created by git.
15 *.orig
16 # Byte compiled python modules.
17 *.pyc
18 # vim swap files
19 .*.swp
20 .sw?
21 #OS X specific files.
22 .DS_store
24 #==============================================================================#
25 # Explicit files to ignore (only matches one).
26 #==============================================================================#
27 # Various tag programs
28 /tags
29 /TAGS
30 /GPATH
31 /GRTAGS
32 /GSYMS
33 /GTAGS
34 .gitusers
35 autom4te.cache
36 cscope.files
37 cscope.out
38 autoconf/aclocal.m4
39 autoconf/autom4te.cache
40 compile_commands.json
42 #==============================================================================#
43 # Directories to ignore (do not add trailing '/'s, they skip symlinks).
44 #==============================================================================#
45 # External projects that are tracked independently.
46 projects/*
47 !projects/CMakeLists.txt
48 !projects/Makefile
49 # Clang, which is tracked independently.
50 tools/clang
51 # LLDB, which is tracked independently.
52 tools/lldb
53 # lld, which is tracked independently.
54 tools/lld
55 # llgo, which is tracked independently.
56 tools/llgo
57 # Polly, which is tracked independently.
58 tools/polly
59 # Sphinx build tree, if building in-source dir.
60 docs/_build
62 #==============================================================================#
63 # Files created in tree by the Go bindings.
64 #==============================================================================#
65 bindings/go/llvm/llvm_config.go
66 bindings/go/llvm/workdir