]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - .gitignore
Debug Info: Remove unused code. The MInsn of an _abstract_ variable is
[opencl/llvm.git] / .gitignore
1 #==============================================================================#
2 # This file specifies intentionally untracked files that git should ignore.
3 # See: http://www.kernel.org/pub/software/scm/git/docs/gitignore.html
4 #
5 # This file is intentionally different from the output of `git svn show-ignore`,
6 # as most of those are useless.
7 #==============================================================================#
9 #==============================================================================#
10 # File extensions to be ignored anywhere in the tree.
11 #==============================================================================#
12 # Temp files created by most text editors.
13 *~
14 # Merge files created by git.
15 *.orig
16 # Byte compiled python modules.
17 *.pyc
18 # vim swap files
19 .*.swp
20 .sw?
21 #OS X specific files.
22 .DS_store
24 #==============================================================================#
25 # Explicit files to ignore (only matches one).
26 #==============================================================================#
27 .gitusers
28 autom4te.cache
29 cscope.files
30 cscope.out
31 autoconf/aclocal.m4
32 autoconf/autom4te.cache
33 compile_commands.json
35 #==============================================================================#
36 # Directories to ignore (do not add trailing '/'s, they skip symlinks).
37 #==============================================================================#
38 # External projects that are tracked independently.
39 projects/*
40 !projects/CMakeLists.txt
41 !projects/Makefile
42 # Clang, which is tracked independently.
43 tools/clang
44 # LLDB, which is tracked independently.
45 tools/lldb
46 # lld, which is tracked independently.
47 tools/lld
48 # Sphinx build tree, if building in-source dir.
49 docs/_build