1 #===-- Makefile.common - Common make rules for LLVM -------*- makefile -*--====
2 #
3 # This file is included by all of the LLVM makefiles. This file defines common
4 # rules to do things like compile a .cpp file or generate dependancy info.
5 # These are platform dependant, so this is the file used to specify these
6 # system dependant operations.
7 #
8 # The following functionality can be set by setting incoming variables.
9 # The variable $(LEVEL) *must* be set:
10 #
11 # 1. LEVEL - The level of the current subdirectory from the top of the
12 # MagicStats view. This level should be expressed as a path, for
13 # example, ../.. for two levels deep.
14 #
15 # 2. DIRS - A list of subdirectories to be built. Fake targets are set up
16 # so that each of the targets "all", "install", and "clean" each build
17 # the subdirectories before the local target. DIRS are guaranteed to be
18 # built in order.
19 #
20 # 3. PARALLEL_DIRS - A list of subdirectories to be built, but that may be
21 # built in any order. All DIRS are built in order before PARALLEL_DIRS are
22 # built, which are then built in any order.
23 #
24 # 4. Source - If specified, this sets the source code filenames. If this
25 # is not set, it defaults to be all of the .cpp, .c, .y, and .l files
26 # in the current directory. Also, if you want to build files in addition
27 # to the local files, you can use the ExtraSource variable
28 #
29 # 5. SourceDir - If specified, this specifies a directory that the source files
30 # are in, if they are not in the current directory. This should include a
31 # trailing / character.
32 #
33 # 6. LLVM_SRC_ROOT - If specified, points to the top of the LLVM source tree.
34 #
35 # 7. LLVM_OBJ_ROOT - If specified, points to the top directory where LLVM
36 # object files are placed.
37 #
38 # 8. BUILD_SRC_DIR - The directory which contains the current set of Makefiles
39 # and usually the source code too (unless SourceDir is set).
40 #
41 # 9. BUILD_SRC_ROOT - The root directory of the source code being compiled.
42 #
43 # 10. BUILD_OBJ_DIR - The directory where object code should be placed.
44 #
45 # 11. BUILD_OBJ_ROOT - The root directory for where object code should be
46 # placed.
47 #
48 # For building,
49 # LLVM, LLVM_SRC_ROOT = BUILD_SRC_ROOT, and
50 # LLVM_OBJ_ROOT = BUILD_OBJ_ROOT.
51 #
52 #===-----------------------------------------------------------------------====
54 #
55 # Configuration file to set paths specific to local installation of LLVM
56 #
57 include $(LEVEL)/Makefile.config
59 ###########################################################################
60 # Directory Configuration
61 # This section of the Makefile determines what is where. To be
62 # specific, there are several locations that need to be defined:
63 #
64 # o LLVM_SRC_ROOT : The root directory of the LLVM source code.
65 # o LLVM_OBJ_ROOT : The root directory containing the built LLVM code.
66 #
67 # o BUILD_SRC_DIR : The directory containing the code to build.
68 # o BUILD_SRC_ROOT : The root directory of the code to build.
69 #
70 # o BUILD_OBJ_DIR : The directory in which compiled code will be placed.
71 # o BUILD_OBJ_ROOT : The root directory in which compiled code is placed.
72 #
73 ###########################################################################
75 #
76 # Set the source build directory. That is almost always the current directory.
77 #
78 ifndef BUILD_SRC_DIR
79 BUILD_SRC_DIR = $(shell pwd)
80 endif
82 #
83 # Set the source root directory.
84 #
85 ifndef BUILD_SRC_ROOT
86 BUILD_SRC_ROOT = $(shell cd $(BUILD_SRC_DIR)/$(LEVEL); pwd)
87 endif
89 #
90 # Determine the path of the source tree relative from $HOME (the mythical
91 # home directory).
92 #
93 HOME_OBJ_ROOT := $(OBJ_ROOT)$(patsubst $(HOME)%,%,$(BUILD_SRC_ROOT))
95 #
96 # Set the object build directory. Its location depends upon the source path
97 # and where object files should go.
98 #
99 ifndef BUILD_OBJ_DIR
100 ifeq ($(OBJ_ROOT),.)
101 BUILD_OBJ_DIR = $(BUILD_SRC_DIR)
102 else
103 BUILD_OBJ_DIR := $(HOME_OBJ_ROOT)$(patsubst $(BUILD_SRC_ROOT)%,%,$(BUILD_SRC_DIR))
104 endif
105 endif
107 #
108 # Set the root of the object directory.
109 #
110 ifndef BUILD_OBJ_ROOT
111 ifeq ($(OBJ_ROOT),.)
112 BUILD_OBJ_ROOT = $(BUILD_SRC_ROOT)
113 else
114 BUILD_OBJ_ROOT := $(HOME_OBJ_ROOT)
115 endif
116 endif
118 #
119 # Set the LLVM source directory.
120 # It is typically the root directory of what we're compiling now.
121 #
122 ifndef LLVM_SRC_ROOT
123 LLVM_SRC_ROOT := $(BUILD_SRC_ROOT)
124 endif
126 #
127 # Set the LLVM object directory.
128 #
129 ifndef LLVM_OBJ_ROOT
130 LLVM_OBJ_ROOT := $(BUILD_OBJ_ROOT)
131 endif
133 ###########################################################################
134 # Default Targets:
135 # The following targets are the standard top level targets for
136 # building.
137 ###########################################################################
139 ifdef SHARED_LIBRARY
140 # if SHARED_LIBRARY is specified, the default is to build the dynamic lib
141 all:: dynamic
142 endif
144 ifdef BYTECODE_LIBRARY
145 # if BYTECODE_LIBRARY is specified, the default is to build the bytecode lib
146 all:: bytecodelib
147 install:: bytecodelib-install
148 endif
150 # Default Rule: Make sure it's also a :: rule
151 all ::
153 # Default for install is to at least build everything...
154 install ::
156 # Default rule for test. It ensures everything has a test rule
157 test::
159 # Default rule for building only bytecode.
160 bytecode::
162 # Print out the directories used for building
163 prdirs::
164 echo "Home Offset : " $(HOME_OBJ_ROOT)
165 echo "Build Source Root: " $(BUILD_SRC_ROOT)
166 echo "Build Source Dir : " $(BUILD_SRC_DIR)
167 echo "Build Object Root: " $(BUILD_OBJ_ROOT)
168 echo "Build Object Dir : " $(BUILD_OBJ_DIR)
169 echo "LLVM Source Root: " $(LLVM_SRC_ROOT)
170 echo "LLVM Object Root: " $(LLVM_OBJ_ROOT)
172 #
173 # Mark all of these targets as phony. This will hopefully speed up builds
174 # slightly since GNU Make will not try to find implicit rules for targets
175 # which are marked as Phony.
176 #
177 .PHONY: all dynamic bytecodelib bytecodelib-install
178 .PHONY: clean cleandeps distclean install test bytecode prdirs
180 ###########################################################################
181 # Miscellaneous paths and commands:
182 # This section defines various configuration macros, such as where
183 # to find burg, tblgen, and libtool.
184 ###########################################################################
186 #--------------------------------------------------------------------
187 # Variables derived from configuration options...
188 #--------------------------------------------------------------------
190 #BinInstDir=/usr/local/bin
191 #LibInstDir=/usr/local/lib/xxx
192 #DocInstDir=/usr/doc/xxx
194 BURG_OPTS = -I
196 ifdef ENABLE_PROFILING
197 ENABLE_OPTIMIZED = 1
198 CONFIGURATION := Profile
199 else
200 ifdef ENABLE_OPTIMIZED
201 CONFIGURATION := Release
202 else
203 CONFIGURATION := Debug
204 endif
205 endif
207 #
208 # Enable this for profiling support with 'gprof'
209 # This automatically enables optimized builds.
210 #
211 ifdef ENABLE_PROFILING
212 PROFILE = -pg
213 endif
215 #
216 # Suffixes for library compilation rules
217 #
218 .SUFFIXES: .so
220 ###########################################################################
221 # Library Locations:
222 # These variables describe various library locations:
223 #
224 # DEST* = Location of where libraries that are built will be placed.
225 # LLVM* = Location of LLVM libraries used for linking.
226 # PROJ* = Location of previously built libraries used for linking.
227 ###########################################################################
229 # Libraries that are being built
230 DESTLIBDEBUG := $(BUILD_OBJ_ROOT)/lib/Debug
231 DESTLIBRELEASE := $(BUILD_OBJ_ROOT)/lib/Release
232 DESTLIBPROFILE := $(BUILD_OBJ_ROOT)/lib/Profile
233 DESTLIBBYTECODE := $(BUILD_OBJ_ROOT)/lib/Bytecode
234 DESTLIBCURRENT := $(BUILD_OBJ_ROOT)/lib/$(CONFIGURATION)
236 # LLVM libraries used for linking
237 LLVMLIBDEBUGSOURCE := $(LLVM_OBJ_ROOT)/lib/Debug
238 LLVMLIBRELEASESOURCE := $(LLVM_OBJ_ROOT)/lib/Release
239 LLVMLIBPROFILESOURCE := $(LLVM_OBJ_ROOT)/lib/Profile
240 LLVMLIBCURRENTSOURCE := $(LLVM_OBJ_ROOT)/lib/$(CONFIGURATION)
242 # Libraries that were built that will now be used for linking
243 PROJLIBDEBUGSOURCE := $(BUILD_OBJ_ROOT)/lib/Debug
244 PROJLIBRELEASESOURCE := $(BUILD_OBJ_ROOT)/lib/Release
245 PROJLIBPROFILESOURCE := $(BUILD_OBJ_ROOT)/lib/Profile
246 PROJLIBCURRENTSOURCE := $(BUILD_OBJ_ROOT)/lib/$(CONFIGURATION)
248 ###########################################################################
249 # Tool Locations
250 # These variables describe various tool locations:
251 #
252 # DEST* = Location of where tools that are built will be placed.
253 # LLVM* = Location of LLVM tools used for building.
254 # PROJ* = Location of previously built tools used for linking.
255 ###########################################################################
257 DESTTOOLDEBUG := $(BUILD_OBJ_ROOT)/tools/Debug
258 DESTTOOLRELEASE := $(BUILD_OBJ_ROOT)/tools/Release
259 DESTTOOLPROFILE := $(BUILD_OBJ_ROOT)/tools/Profile
260 DESTTOOLCURRENT := $(BUILD_OBJ_ROOT)/tools/$(CONFIGURATION)
262 LLVMTOOLDEBUG := $(LLVM_OBJ_ROOT)/tools/Debug
263 LLVMTOOLRELEASE := $(LLVM_OBJ_ROOT)/tools/Release
264 LLVMTOOLPROFILE := $(LLVM_OBJ_ROOT)/tools/Profile
265 LLVMTOOLCURRENT := $(LLVM_OBJ_ROOT)/tools/$(CONFIGURATION)
267 PROJTOOLDEBUG := $(BUILD_OBJ_ROOT)/tools/Debug
268 PROJTOOLRELEASE := $(BUILD_OBJ_ROOT)/tools/Release
269 PROJTOOLPROFILE := $(BUILD_OBJ_ROOT)/tools/Profile
270 PROJTOOLCURRENT := $(BUILD_OBJ_ROOT)/tools/$(CONFIGURATION)
272 #
273 # Libtool is found in the current directory.
274 #
275 LIBTOOL := $(LLVM_SRC_ROOT)/mklib
277 #
278 # If we're not building a shared library, use the disable-shared tag with
279 # libtool. This will disable the building of objects for shared libraries and
280 # only generate static library objects.
281 #
282 # For dynamic libraries, we'll take the performance hit for now, since we
283 # almost never build them.
284 #
285 # This should speed up compilation and require no modifications to future
286 # versions of libtool.
287 #
288 ifndef SHARED_LIBRARY
289 LIBTOOL += --tag=disable-shared
290 endif
292 #
293 # Verbosity levels
294 #
295 ifndef VERBOSE
296 VERB := @
297 LIBTOOL += --silent
298 endif
300 ###########################################################################
301 # Miscellaneous paths and commands (part deux):
302 # This section defines various configuration macros, such as where
303 # to find burg, tblgen, and libtool.
304 ###########################################################################
306 #--------------------------------------------------------------------------
307 # Utilities used while building the LLVM tree, which live in the utils dir
308 #
309 BURG := $(LLVMTOOLCURRENT)/burg
310 RunBurg := $(BURG) $(BURG_OPTS)
311 TBLGEN := $(LLVMTOOLCURRENT)/tblgen
313 #--------------------------------------------------------------------------
314 # The LLVM GCC front-end in C and C++ flavors
315 #
316 LLVMGCC := PATH=$(LLVMTOOLCURRENT):$(PATH) $(LLVMGCCDIR)/bin/gcc
317 LCC1 := $(LLVMGCCDIR)/lib/gcc-lib/$(LLVMGCCARCH)/cc1
318 LLVMGXX := PATH=$(LLVMTOOLCURRENT):$(PATH) $(LLVMGCCDIR)/bin/g++
319 LCC1XX := $(LLVMGCCDIR)/lib/gcc-lib/$(LLVMGCCARCH)/cc1plus
321 #--------------------------------------------------------------------------
322 # Some of the compiled LLVM tools which are used for compilation of runtime
323 # libraries.
324 #
325 LLVMAS := $(LLVMTOOLCURRENT)/as
328 ###########################################################################
329 # Compile Time Flags
330 ###########################################################################
332 #
333 # Include both the project headers and the LLVM headers for compilation and
334 # dependency computation.
335 #
336 CPPFLAGS += -I$(BUILD_SRC_ROOT)/include -I$(LLVM_SRC_ROOT)/include
338 # By default, strip symbol information from executable
339 ifndef KEEP_SYMBOLS
340 STRIP = $(PLATFORMSTRIPOPTS)
341 STRIP_WARN_MSG = "(without symbols)"
342 endif
344 # Allow gnu extensions...
345 CPPFLAGS += -D_GNU_SOURCE
347 CompileCommonOpts := -Wall -W -Wwrite-strings -Wno-unused -I$(LEVEL)/include
348 CompileOptimizeOpts := -O3 -DNDEBUG -finline-functions -fshort-enums
350 #
351 # Compile commands with libtool.
352 #
353 Compile := $(LIBTOOL) --mode=compile $(CXX) -c $(CPPFLAGS) $(CXXFLAGS) $(CompileCommonOpts)
354 CompileC := $(LIBTOOL) --mode=compile $(CC) -c $(CPPFLAGS) $(CCFLAGS) $(CompileCommonOpts)
356 # Compile a cpp file, don't link...
357 CompileG := $(Compile) -g -D_DEBUG
358 CompileO := $(Compile) $(CompileOptimizeOpts) -felide-constructors -fomit-frame-pointer
359 CompileP := $(Compile) $(CompileOptimizeOpts) -felide-constructors $(PROFILE)
361 # Compile a c file, don't link...
362 CompileCG := $(CompileC) -g -D_DEBUG
363 CompileCO := $(CompileC) $(CompileOptimizeOpts) -fomit-frame-pointer
364 CompileCP := $(CompileC) $(CompileOptimizeOpts) $(PROFILE)
366 ###########################################################################
367 # Link Time Options
368 ###########################################################################
370 #
371 # Link final executable
372 # (Note that we always link with the C++ compiler).
373 #
374 Link := $(LIBTOOL) --mode=link $(CXX)
376 # link both projlib and llvmlib libraries
377 LinkG := $(Link) -g -L$(PROJLIBDEBUGSOURCE) -L$(LLVMLIBDEBUGSOURCE) $(STRIP)
378 LinkO := $(Link) -O3 -L$(PROJLIBRELEASESOURCE) -L$(LLVMLIBRELEASESOURCE)
379 LinkP := $(Link) -O3 -L$(PROJLIBPROFILESOURCE) -L$(LLVMLIBPROFILESOURCE) $(PROFILE)
381 # Create one .o file from a bunch of .o files...
382 Relink := ${LIBTOOL} --mode=link $(CXX)
383 ifndef SHARED_LIBRARY
384 Relink += -only-static
385 endif
387 #
388 # Configure where the item being compiled should go.
389 #
390 ifdef SHARED_LIBRARY
391 Link += -rpath $(DESTLIBCURRENT)
392 endif
394 ifdef TOOLNAME
395 Link += -rpath $(DESTTOOLCURRENT)
396 endif
398 # Create dependancy file from CPP file, send to stdout.
399 Depend := $(CXX) -MM -I$(LEVEL)/include $(CPPFLAGS)
400 DependC := $(CC) -MM -I$(LEVEL)/include $(CPPFLAGS)
402 # Archive a bunch of .o files into a .a file...
403 AR = ${AR_PATH} cq
405 #----------------------------------------------------------
407 # Source includes all of the cpp files, and objects are derived from the
408 # source files...
409 # The local Makefile can list other Source files via ExtraSource = ...
410 #
411 ifndef Source
412 Source := $(ExtraSource) $(wildcard *.cpp *.c *.y *.l)
413 endif
415 #
416 # Libtool Objects
417 #
418 Srcs := $(sort $(notdir $(basename $(Source))))
419 Objs := $(addsuffix .lo, $(Srcs))
420 ObjectsO := $(addprefix $(BUILD_OBJ_DIR)/Release/,$(Objs))
421 ObjectsP := $(addprefix $(BUILD_OBJ_DIR)/Profile/,$(Objs))
422 ObjectsG := $(addprefix $(BUILD_OBJ_DIR)/Debug/,$(Objs))
423 ObjectsBC := $(addprefix $(BUILD_OBJ_DIR)/Bytecode/,$(addsuffix .bc, $(Srcs)))
425 #
426 # The real objects underlying the libtool objects
427 #
428 RObjs := $(sort $(patsubst Debug/%.o, %.o, $(addsuffix .o,$(notdir $(basename $(Source))))))
429 RObjectsO := $(addprefix $(BUILD_OBJ_DIR)/Release/,$(RObjs))
430 RObjectsP := $(addprefix $(BUILD_OBJ_DIR)/Profile/,$(RObjs))
431 RObjectsG := $(addprefix $(BUILD_OBJ_DIR)/Debug/,$(RObjs))
433 #---------------------------------------------------------
434 # Handle the DIRS and PARALLEL_DIRS options
435 #---------------------------------------------------------
437 ifdef DIRS
438 all install clean cleandeps test bytecode ::
439 $(VERB) for dir in ${DIRS}; do \
440 (cd $$dir; $(MAKE) $@) || exit 1; \
441 done
442 endif
444 # Handle PARALLEL_DIRS
445 ifdef PARALLEL_DIRS
446 all :: $(addsuffix /.makeall , $(PARALLEL_DIRS))
447 install :: $(addsuffix /.makeinstall , $(PARALLEL_DIRS))
448 clean :: $(addsuffix /.makeclean , $(PARALLEL_DIRS))
449 cleandeps:: $(addsuffix /.makecleandeps, $(PARALLEL_DIRS))
450 test :: $(addsuffix /.maketest , $(PARALLEL_DIRS))
451 bytecode :: $(addsuffix /.makebytecode, $(PARALLEL_DIRS))
453 %/.makeall %/.makeinstall %/.makeclean %/.makecleandeps %/.maketest \
454 %/.makebytecode:
455 $(VERB) cd $(@D); $(MAKE) $(subst $(@D)/.make,,$@)
456 endif
458 # Handle directories that may or may not exist
459 ifdef OPTIONAL_DIRS
460 all install clean cleandeps test bytecode ::
461 $(VERB) for dir in ${OPTIONAL_DIRS}; do \
462 if [ -d $$dir ]; \
463 then\
464 (cd $$dir; $(MAKE) $@) || exit 1; \
465 fi \
466 done
467 endif
469 ###########################################################################
470 # Library Build Rules:
471 #
472 #---------------------------------------------------------
473 # Handle the LIBRARYNAME option - used when building libs...
474 #---------------------------------------------------------
475 #
476 # When libraries are built, they are allowed to optionally define the
477 # DONT_BUILD_RELINKED make variable, which, when defined, prevents a .o file
478 # from being built for the library. This .o files may then be linked to by a
479 # tool if the tool does not need (or want) the semantics a .a file provides
480 # (linking in only object files that are "needed"). If a library is never to
481 # be used in this way, it is better to define DONT_BUILD_RELINKED, and define
482 # BUILD_ARCHIVE instead.
483 #
484 # Some libraries must be built as .a files (libscalar for example) because if
485 # it's built as a .o file, then all of the constituent .o files in it will be
486 # linked into tools (for example gccas) even if they only use one of the parts
487 # of it. For this reason, sometimes it's useful to use libraries as .a files.
488 ###########################################################################
490 ifdef LIBRARYNAME
492 # Make sure there isn't any extranous whitespace on the LIBRARYNAME option
493 LIBRARYNAME := $(strip $(LIBRARYNAME))
495 LIBNAME_O := $(DESTLIBRELEASE)/lib$(LIBRARYNAME).so
496 LIBNAME_P := $(DESTLIBPROFILE)/lib$(LIBRARYNAME).so
497 LIBNAME_G := $(DESTLIBDEBUG)/lib$(LIBRARYNAME).so
498 LIBNAME_AO := $(DESTLIBRELEASE)/lib$(LIBRARYNAME).a
499 LIBNAME_AP := $(DESTLIBPROFILE)/lib$(LIBRARYNAME).a
500 LIBNAME_AG := $(DESTLIBDEBUG)/lib$(LIBRARYNAME).a
501 LIBNAME_OBJO := $(DESTLIBRELEASE)/$(LIBRARYNAME).o
502 LIBNAME_OBJP := $(DESTLIBPROFILE)/$(LIBRARYNAME).o
503 LIBNAME_OBJG := $(DESTLIBDEBUG)/$(LIBRARYNAME).o
504 LIBNAME_BC := $(DESTLIBBYTECODE)/lib$(LIBRARYNAME).bc
506 #--------------------------------------------------------------------
507 # Library Targets
508 # Modify the top level targets to build the desired libraries.
509 #--------------------------------------------------------------------
511 # dynamic target builds a shared object version of the library...
512 dynamic:: $(DESTLIBCURRENT)/lib$(LIBRARYNAME).so
513 bytecodelib:: $(LIBNAME_BC)
514 bytecodelib-install:: $(LLVMGCCDIR)/bytecode-libs/lib$(LIBRARYNAME).bc
516 $(LLVMGCCDIR)/bytecode-libs/lib$(LIBRARYNAME).bc: $(LIBNAME_BC)
517 @echo ======= Installing $(LIBRARYNAME) bytecode library =======
518 cp $< $@
520 # Does the library want a .o version built?
521 ifndef DONT_BUILD_RELINKED
522 all:: $(DESTLIBCURRENT)/$(LIBRARYNAME).o
523 endif
525 # Does the library want an archive version built?
526 ifdef BUILD_ARCHIVE
527 all:: $(DESTLIBCURRENT)/lib$(LIBRARYNAME).a
528 endif
530 #--------------------------------------------------------------------
531 # Rules for building libraries
532 #--------------------------------------------------------------------
534 LinkBCLib := $(LLVMGCC) -shared
535 ifdef EXPORTED_SYMBOL_LIST
536 LinkBCLib += -Xlinker -internalize-public-api-list=$(EXPORTED_SYMBOL_LIST)
537 else
538 LinkBCLib += -Xlinker -disable-internalize
539 endif
542 # Rule for building bytecode libraries.
543 $(LIBNAME_BC): $(ObjectsBC) $(LibSubDirs) $(DESTLIBBYTECODE)/.dir
544 @echo ======= Linking $(LIBRARYNAME) bytecode library =======
545 $(VERB) $(LinkBCLib) -o $@ $(ObjectsBC) $(LibSubDirs) $(LibLinkOpts)
546 #
547 # Rules for building dynamically linked libraries.
548 #
549 $(LIBNAME_O): $(ObjectsO) $(LibSubDirs) $(DESTLIBRELEASE)/.dir
550 @echo ======= Linking $(LIBRARYNAME) dynamic release library =======
551 $(VERB) $(Link) -o $*.la $(ObjectsO) $(LibSubDirs) $(LibLinkOpts)
552 $(VERB) $(LIBTOOL) --mode=install $(INSTALL) $*.la $(DESTLIBCURRENT)
554 $(LIBNAME_P): $(ObjectsP) $(LibSubDirs) $(DESTLIBPROFILE)/.dir
555 @echo ======= Linking $(LIBRARYNAME) dynamic profile library =======
556 $(VERB) $(Link) -o $*.la $(ObjectsP) $(LibSubDirs) $(LibLinkOpts)
557 $(VERB) $(LIBTOOL) --mode=install $(INSTALL) $*.la $(DESTLIBCURRENT)
559 $(LIBNAME_G): $(ObjectsG) $(LibSubDirs) $(DESTLIBDEBUG)/.dir
560 @echo ======= Linking $(LIBRARYNAME) dynamic debug library =======
561 $(VERB) $(Link) -o $*.la $(ObjectsG) $(LibSubDirs) $(LibLinkOpts)
562 $(VERB) $(LIBTOOL) --mode=install $(INSTALL) $*.la $(DESTLIBCURRENT)
564 #
565 # Rules for building static archive libraries.
566 #
567 $(LIBNAME_AO): $(ObjectsO) $(LibSubDirs) $(DESTLIBRELEASE)/.dir
568 @echo ======= Linking $(LIBRARYNAME) archive release library =======
569 @$(RM) -f $@
570 $(VERB) $(Link) -03 -o $@ $(ObjectsO) $(LibSubDirs) -static
572 $(LIBNAME_AP): $(ObjectsP) $(LibSubDirs) $(DESTLIBPROFILE)/.dir
573 @echo ======= Linking $(LIBRARYNAME) archive profile library =======
574 @$(RM) -f $@
575 $(VERB) $(Link) -03 $(PROFILE) -o $@ $(ObjectsP) $(LibSubDirs) -static
577 $(LIBNAME_AG): $(ObjectsG) $(LibSubDirs) $(DESTLIBDEBUG)/.dir
578 @echo ======= Linking $(LIBRARYNAME) archive debug library =======
579 @$(RM) -f $@
580 $(VERB) $(Link) -g $(STRIP) -o $@ $(ObjectsG) $(LibSubDirs) -static
583 #
584 # Rules for building .o libraries.
585 #
586 # JTC:
587 # Note that for this special case, we specify the actual object files
588 # instead of their libtool counterparts. This is because libtool
589 # doesn't want to generate a reloadable object file unless it is given
590 # .o files explicitly.
591 #
592 # Note that we're making an assumption here: If we build a .lo file,
593 # it's corresponding .o file will be placed in the same directory.
594 #
595 # I think that is safe.
596 #
597 $(LIBNAME_OBJO): $(ObjectsO) $(LibSubDirs) $(DESTLIBRELEASE)/.dir
598 @echo "Linking $@"
599 $(VERB) $(Relink) -o $@ $(RObjectsO) $(LibSubDirs)
601 $(LIBNAME_OBJP): $(ObjectsP) $(LibSubDirs) $(DESTLIBPROFILE)/.dir
602 @echo "Linking $@"
603 $(VERB) $(Relink) -o $@ $(RObjectsP) $(LibSubDirs)
605 $(LIBNAME_OBJG): $(ObjectsG) $(LibSubDirs) $(DESTLIBDEBUG)/.dir
606 @echo "Linking $@"
607 $(VERB) $(Relink) -o $@ $(RObjectsG) $(LibSubDirs)
609 endif
611 #------------------------------------------------------------------------
612 # Create a TAGS database for emacs
613 #------------------------------------------------------------------------
615 ifdef ETAGS
616 ifeq ($(LEVEL), .)
617 tags:
618 $(ETAGS) -l c++ `find include lib tools -name '*.cpp' -o -name '*.h'`
619 all:: tags
620 endif
621 else
622 tags:
623 ${ECHO} "Cannot build $@: The program etags is not installed"
624 endif
626 #------------------------------------------------------------------------
627 # Handle the TOOLNAME option - used when building tool executables...
628 #------------------------------------------------------------------------
629 #
630 # The TOOLNAME option should be used with a USEDLIBS variable that tells the
631 # libraries (and the order of the libs) that should be linked to the
632 # tool. USEDLIBS should contain a list of library names (some with .a extension)
633 # that are automatically linked in as .o files unless the .a suffix is added.
634 #
635 ifdef TOOLNAME
637 # TOOLEXENAME* - These compute the output filenames to generate...
638 TOOLEXENAME_G := $(DESTTOOLDEBUG)/$(TOOLNAME)
639 TOOLEXENAME_O := $(DESTTOOLRELEASE)/$(TOOLNAME)
640 TOOLEXENAME_P := $(DESTTOOLPROFILE)/$(TOOLNAME)
641 TOOLEXENAMES := $(DESTTOOLCURRENT)/$(TOOLNAME)
643 # USED_LIBS_OPTIONS - Compute the options line that add -llib1 -llib2, etc.
644 PROJ_LIBS_OPTIONS := $(patsubst %.a.o, -l%, $(addsuffix .o, $(USEDLIBS)))
645 PROJ_LIBS_OPTIONS_G := $(patsubst %.o, $(PROJLIBDEBUGSOURCE)/%.o, $(PROJ_LIBS_OPTIONS))
646 PROJ_LIBS_OPTIONS_O := $(patsubst %.o, $(PROJLIBRELEASESOURCE)/%.o,$(PROJ_LIBS_OPTIONS))
647 PROJ_LIBS_OPTIONS_P := $(patsubst %.o, $(PROJLIBPROFILESOURCE)/%.o,$(PROJ_LIBS_OPTIONS))
649 LLVM_LIBS_OPTIONS := $(patsubst %.a.o, -l%, $(addsuffix .o, $(LLVMLIBS)))
650 LLVM_LIBS_OPTIONS_G := $(patsubst %.o, $(LLVMLIBDEBUGSOURCE)/%.o, $(LLVM_LIBS_OPTIONS))
651 LLVM_LIBS_OPTIONS_O := $(patsubst %.o, $(LLVMLIBRELEASESOURCE)/%.o,$(LLVM_LIBS_OPTIONS))
652 LLVM_LIBS_OPTIONS_P := $(patsubst %.o, $(LLVMLIBPROFILESOURCE)/%.o,$(LLVM_LIBS_OPTIONS))
654 LIB_OPTS_G := $(LLVM_LIBS_OPTIONS_G) $(PROJ_LIBS_OPTIONS_G)
655 LIB_OPTS_O := $(LLVM_LIBS_OPTIONS_O) $(PROJ_LIBS_OPTIONS_O)
656 LIB_OPTS_P := $(LLVM_LIBS_OPTIONS_P) $(PROJ_LIBS_OPTIONS_P)
658 # USED_LIB_PATHS - Compute the path of the libraries used so that tools are
659 # rebuilt if libraries change. This has to make sure to handle .a/.so and .o
660 # files separately.
661 #
662 STATICUSEDLIBS := $(patsubst %.a.o, lib%.a, $(addsuffix .o, $(USEDLIBS)))
663 USED_LIB_PATHS_G := $(addprefix $(DESTLIBDEBUG)/, $(STATICUSEDLIBS))
664 USED_LIB_PATHS_O := $(addprefix $(DESTLIBRELEASE)/, $(STATICUSEDLIBS))
665 USED_LIB_PATHS_P := $(addprefix $(DESTLIBPROFILE)/, $(STATICUSEDLIBS))
667 #
668 # Libtool link options:
669 # Ensure that all binaries have their symbols exported so that they can
670 # by dlsym'ed.
671 #
672 LINK_OPTS := -export-dynamic $(TOOLLINKOPTS)
678 # Tell make that we need to rebuild subdirectories before we can link the tool.
679 # This affects things like LLI which has library subdirectories.
680 $(USED_LIB_PATHS_G) $(USED_LIB_PATHS_O) $(USED_LIB_PATHS_P): \
681 $(addsuffix /.makeall, $(PARALLEL_DIRS))
683 all:: $(TOOLEXENAMES)
685 clean::
686 $(VERB) $(RM) -f $(TOOLEXENAMES)
688 $(TOOLEXENAME_G): $(ObjectsG) $(USED_LIB_PATHS_G) $(DESTTOOLDEBUG)/.dir
689 @echo ======= Linking $(TOOLNAME) debug executable $(STRIP_WARN_MSG) =======
690 $(VERB) $(LinkG) -o $@ $(ObjectsG) $(LIB_OPTS_G) $(LINK_OPTS) $(LIBS)
692 $(TOOLEXENAME_O): $(ObjectsO) $(USED_LIB_PATHS_O) $(DESTTOOLRELEASE)/.dir
693 @echo ======= Linking $(TOOLNAME) release executable =======
694 $(VERB) $(LinkO) -o $@ $(ObjectsO) $(LIB_OPTS_O) $(LINK_OPTS) $(LIBS)
696 $(TOOLEXENAME_P): $(ObjectsP) $(USED_LIB_PATHS_P) $(DESTTOOLPROFILE)/.dir
697 @echo ======= Linking $(TOOLNAME) profile executable =======
698 $(VERB) $(LinkP) -o $@ $(ObjectsP) $(LIB_OPTS_P) $(LINK_OPTS) $(LIBS)
700 endif
704 #---------------------------------------------------------
705 .PRECIOUS: $(BUILD_OBJ_DIR)/Depend/.dir $(BUILD_OBJ_DIR)/Bytecode/.dir
706 .PRECIOUS: $(BUILD_OBJ_DIR)/Debug/.dir $(BUILD_OBJ_DIR)/Release/.dir
708 # Create .lo files in the ObjectFiles directory from the .cpp and .c files...
709 $(BUILD_OBJ_DIR)/Release/%.lo: $(SourceDir)%.cpp $(BUILD_OBJ_DIR)/Release/.dir
710 @echo "Compiling $<"
711 $(VERB) $(CompileO) $< -o $@
713 $(BUILD_OBJ_DIR)/Release/%.lo: $(SourceDir)%.c $(BUILD_OBJ_DIR)/Release/.dir
714 @echo "Compiling $<"
715 $(VERB) $(CompileCO) $< -o $@
717 $(BUILD_OBJ_DIR)/Profile/%.lo: $(SourceDir)%.cpp $(BUILD_OBJ_DIR)/Profile/.dir
718 @echo "Compiling $<"
719 $(VERB) $(CompileP) $< -o $@
721 $(BUILD_OBJ_DIR)/Profile/%.lo: $(SourceDir)%.c $(BUILD_OBJ_DIR)/Profile/.dir
722 @echo "Compiling $<"
723 $(VERB) $(CompileCP) $< -o $@
725 $(BUILD_OBJ_DIR)/Debug/%.lo: $(SourceDir)%.cpp $(BUILD_OBJ_DIR)/Debug/.dir
726 @echo "Compiling $<"
727 $(VERB) $(CompileG) $< -o $@
729 $(BUILD_OBJ_DIR)/Debug/%.lo: $(SourceDir)%.c $(BUILD_OBJ_DIR)/Debug/.dir
730 @echo "Compiling $<"
731 $(VERB) $(CompileCG) $< -o $@
733 $(BUILD_OBJ_DIR)/Bytecode/%.bc: $(SourceDir)%.cpp $(BUILD_OBJ_DIR)/Bytecode/.dir $(LCC1XX)
734 @echo "Compiling $< to bytecode"
735 $(VERB) $(LLVMGXX) $(CPPFLAGS) -c $< -o $@
737 $(BUILD_OBJ_DIR)/Bytecode/%.bc: $(SourceDir)%.c $(BUILD_OBJ_DIR)/Bytecode/.dir $(LCC1)
738 @echo "Compiling $< to bytecode"
739 $(VERB) $(LLVMGCC) $(CPPFLAGS) -c $< -o $@
741 $(BUILD_OBJ_DIR)/Bytecode/%.bc: $(SourceDir)%.ll $(BUILD_OBJ_DIR)/Bytecode/.dir $(LCC1)
742 @echo "Compiling $< to bytecode"
743 $(VERB) $(LLVMAS) $< -f -o $@
746 #
747 # Rules for building lex/yacc files
748 #
749 LEX_FILES = $(filter %.l, $(Source))
750 LEX_OUTPUT = $(LEX_FILES:%.l=%.cpp)
751 YACC_FILES = $(filter %.y, $(Source))
752 YACC_OUTPUT = $(addprefix $(YACC_FILES:%.y=%), .h .cpp .output)
753 .PRECIOUS: $(LEX_OUTPUT) $(YACC_OUTPUT)
755 # Create a .cpp source file from a flex input file... this uses sed to cut down
756 # on the warnings emited by GCC...
757 #
758 # The last line is a gross hack to work around flex aparently not being able to
759 # resize the buffer on a large token input. Currently, for uninitialized string
760 # buffers in LLVM we can generate very long tokens, so this is a hack around it.
761 # FIXME. (f.e. char Buffer[10000] )
762 #
763 %.cpp: %.l
764 @echo Flex\'ing $<...
765 $(VERB) $(FLEX) -t $< | \
766 $(SED) '/^find_rule/d' | \
767 $(SED) 's/void yyunput/inline void yyunput/' | \
768 $(SED) 's/void \*yy_flex_realloc/inline void *yy_flex_realloc/' | \
769 $(SED) 's/#define YY_BUF_SIZE 16384/#define YY_BUF_SIZE (16384*64)/' \
770 > $@.tmp
771 $(VERB) cmp -s $@ $@.tmp > /dev/null || ${MV} -f $@.tmp $@
772 @# remove the output of flex if it didn't get moved over...
773 @rm -f $@.tmp
775 # Rule for building the bison parsers...
776 %.c: %.y # Cancel built-in rules for yacc
777 %.h: %.y # Cancel built-in rules for yacc
778 %.cpp %.h : %.y
779 @echo Bison\'ing $<...
780 $(VERB) $(BISON) -v -d -p $(<:%Parser.y=%) $*.y
781 $(VERB) cmp -s $*.tab.c $*.cpp > /dev/null || ${MV} -f $*.tab.c $*.cpp
782 $(VERB) cmp -s $*.tab.h $*.h > /dev/null || ${MV} -f $*.tab.h $*.h
783 @# If the files were not updated, don't leave them lying around...
784 @rm -f $*.tab.c $*.tab.h
786 # To create the directories...
787 %/.dir:
788 $(VERB) ${MKDIR} $* > /dev/null
789 @$(DATE) > $@
791 # To create postscript files from dot files...
792 ifdef DOT
793 %.ps: %.dot
794 ${DOT} -Tps < $< > $@
795 else
796 %.ps: %.dot
797 ${ECHO} "Cannot build $@: The program dot is not installed"
798 endif
800 # 'make clean' nukes the tree
801 clean::
802 $(VERB) $(RM) -rf $(BUILD_OBJ_DIR)/Debug $(BUILD_OBJ_DIR)/Release
803 $(VERB) $(RM) -rf $(BUILD_OBJ_DIR)/Profile $(BUILD_OBJ_DIR)/Depend
804 $(VERB) $(RM) -rf $(BUILD_OBJ_DIR)/Bytecode
805 $(VERB) $(RM) -f core core.[0-9][0-9]* *.o *.d *.so *~ *.flc
806 $(VERB) $(RM) -f $(LEX_OUTPUT) $(YACC_OUTPUT)
808 ###########################################################################
809 # C/C++ Dependencies
810 # Define variables and rules that generate header file dependencies
811 # from C/C++ source files.
812 ###########################################################################
814 # If dependencies were generated for the file that included this file,
815 # include the dependancies now...
816 #
817 SourceBaseNames := $(basename $(notdir $(filter-out Debug/%, $(Source))))
818 SourceDepend := $(SourceBaseNames:%=$(BUILD_OBJ_DIR)/Depend/%.d)
820 # Create dependencies for the *.cpp files...
821 #$(SourceDepend): \x
822 $(BUILD_OBJ_DIR)/Depend/%.d: $(SourceDir)%.cpp $(BUILD_OBJ_DIR)/Depend/.dir
823 $(VERB) $(Depend) $< | $(SED) 's|\.o|\.lo|' | $(SED) 's|$*\.lo *|$(BUILD_OBJ_DIR)/Release/& $(BUILD_OBJ_DIR)/Profile/& $(BUILD_OBJ_DIR)/Debug/& $(BUILD_OBJ_DIR)/Depend/$(@F)|g' > $@
825 # Create dependencies for the *.c files...
826 #$(SourceDepend): \x
827 $(BUILD_OBJ_DIR)/Depend/%.d: $(SourceDir)%.c $(BUILD_OBJ_DIR)/Depend/.dir
828 $(VERB) $(DependC) -o $@ $< | $(SED) 's|\.o|\.lo|' | $(SED) 's|$*\.lo *|$(BUILD_OBJ_DIR)/Release/& $(BUILD_OBJ_DIR)/Profile/& $(BUILD_OBJ_DIR)/Debug/& $(BUILD_OBJ_DIR)/Depend/$(@F)|g' > $@
830 #
831 # Include dependencies generated from C/C++ source files, but not if we
832 # are cleaning (this example taken from the GNU Make Manual).
833 #
834 ifneq ($(MAKECMDGOALS),clean)
835 ifneq ($(MAKECMDGOALS),distclean)
836 ifneq ($(MAKECMDGOALS),cleandeps)
837 ifneq ($(SourceDepend),)
838 -include $(SourceDepend)
839 endif
840 endif
841 endif
842 endif
844 cleandeps::
845 $(VERB) rm -f $(SourceDepend)