1 #===-- Makefile.config - Local configuration for LLVM ------*- Makefile -*--===#
2 #
3 # The LLVM Compiler Infrastructure
4 #
5 # This file is distributed under the University of Illinois Open Source
6 # License. See LICENSE.TXT for details.
7 #
8 #===------------------------------------------------------------------------===#
9 #
10 # This file is included by Makefile.common. It defines paths and other
11 # values specific to a particular installation of LLVM.
12 #
13 #===------------------------------------------------------------------------===#
15 # Define LLVM specific info and directories based on the autoconf variables
16 LLVMPackageName := @PACKAGE_TARNAME@
17 LLVMVersion := @PACKAGE_VERSION@
18 LLVM_CONFIGTIME := @LLVM_CONFIGTIME@
20 ###########################################################################
21 # Directory Configuration
22 # This section of the Makefile determines what is where. To be
23 # specific, there are several locations that need to be defined:
24 #
25 # o LLVM_SRC_ROOT : The root directory of the LLVM source code.
26 # o LLVM_OBJ_ROOT : The root directory containing the built LLVM code.
27 #
28 # o PROJ_SRC_DIR : The directory containing the code to build.
29 # o PROJ_SRC_ROOT : The root directory of the code to build.
30 #
31 # o PROJ_OBJ_DIR : The directory in which compiled code will be placed.
32 # o PROJ_OBJ_ROOT : The root directory in which compiled code is placed.
33 #
34 ###########################################################################
36 PWD := @BINPWD@
37 # Set the project name to LLVM if its not defined
38 ifndef PROJECT_NAME
39 PROJECT_NAME := $(LLVMPackageName)
40 endif
42 # The macro below is expanded when 'realpath' is not built-in.
43 # Built-in 'realpath' is available on GNU Make 3.81.
44 realpath = $(shell cd $(1); $(PWD))
46 PROJ_OBJ_DIR := $(call realpath, .)
47 PROJ_OBJ_ROOT := $(call realpath, $(PROJ_OBJ_DIR)/$(LEVEL))
49 CLANG_SRC_ROOT := @CLANG_SRC_ROOT@
51 ifeq ($(PROJECT_NAME),$(LLVMPackageName))
52 LLVM_SRC_ROOT := $(call realpath, @abs_top_srcdir@)
53 LLVM_OBJ_ROOT := $(call realpath, @abs_top_builddir@)
54 PROJ_SRC_ROOT := $(LLVM_SRC_ROOT)
55 PROJ_SRC_DIR := $(LLVM_SRC_ROOT)$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR))
57 ifneq ($(CLANG_SRC_ROOT),)
58 CLANG_SRC_ROOT:= $(call realpath, $(CLANG_SRC_ROOT))
59 PROJ_SRC_DIR := $(patsubst $(LLVM_SRC_ROOT)/tools/clang%,$(CLANG_SRC_ROOT)%,$(PROJ_SRC_DIR))
60 endif
62 prefix := @prefix@
63 PROJ_prefix := $(prefix)
64 program_prefix := @program_prefix@
65 PROJ_VERSION := $(LLVMVersion)
66 else
67 ifndef PROJ_SRC_ROOT
68 $(error Projects must define PROJ_SRC_ROOT)
69 endif
70 ifndef PROJ_OBJ_ROOT
71 $(error Projects must define PROJ_OBJ_ROOT)
72 endif
73 ifndef PROJ_INSTALL_ROOT
74 $(error Projects must define PROJ_INSTALL_ROOT)
75 endif
76 ifndef LLVM_SRC_ROOT
77 $(error Projects must define LLVM_SRC_ROOT)
78 endif
79 ifndef LLVM_OBJ_ROOT
80 $(error Projects must define LLVM_OBJ_ROOT)
81 endif
82 PROJ_SRC_DIR := $(call realpath, $(PROJ_SRC_ROOT)/$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR)))
83 prefix := $(PROJ_INSTALL_ROOT)
84 PROJ_prefix := $(prefix)
85 ifndef PROJ_VERSION
86 PROJ_VERSION := 1.0
87 endif
88 endif
90 INTERNAL_PREFIX := @INTERNAL_PREFIX@
91 ifneq ($(INTERNAL_PREFIX),)
92 PROJ_internal_prefix := $(INTERNAL_PREFIX)
93 else
94 PROJ_internal_prefix := $(prefix)
95 endif
97 PROJ_bindir := $(PROJ_prefix)/bin
98 PROJ_libdir := $(PROJ_prefix)/lib
99 PROJ_datadir := $(PROJ_prefix)/share
100 PROJ_docsdir := $(PROJ_prefix)/docs/llvm
101 PROJ_etcdir := $(PROJ_prefix)/etc/llvm
102 PROJ_includedir := $(PROJ_prefix)/include
103 PROJ_infodir := $(PROJ_prefix)/info
104 PROJ_mandir := $(PROJ_prefix)/share/man
106 # Determine if we're on a unix type operating system
107 LLVM_ON_UNIX:=@LLVM_ON_UNIX@
108 LLVM_ON_WIN32:=@LLVM_ON_WIN32@
110 # Host operating system for which LLVM will be run.
111 OS=@OS@
112 HOST_OS=@HOST_OS@
113 # Target operating system for which LLVM will compile for.
114 TARGET_OS=@TARGET_OS@
116 # Host hardware architecture
117 HOST_ARCH=@HOST_ARCH@
118 # Target hardware architecture
119 ARCH=@ARCH@
120 TARGET_NATIVE_ARCH := $(ARCH)
122 # Indicates, whether we're cross-compiling LLVM or not
123 LLVM_CROSS_COMPILING=@LLVM_CROSS_COMPILING@
125 # Executable file extension for build platform (mainly for
126 # tablegen call if we're cross-compiling).
127 BUILD_EXEEXT=@BUILD_EXEEXT@
129 # Compilers for the build platflorm (mainly for tablegen
130 # call if we're cross-compiling).
131 BUILD_CC=@BUILD_CC@
132 BUILD_CXX=@BUILD_CXX@
134 # Triple for configuring build tools when cross-compiling
135 BUILD_TRIPLE=@build@
137 # Target triple (cpu-vendor-os) which LLVM is compiled for
138 HOST_TRIPLE=@host@
140 # Target triple (cpu-vendor-os) for which we should generate code
141 TARGET_TRIPLE=@target@
143 # Extra options to compile LLVM with
144 EXTRA_OPTIONS=@EXTRA_OPTIONS@
146 # Extra options to link LLVM with
147 EXTRA_LD_OPTIONS=@EXTRA_LD_OPTIONS@
149 # Endian-ness of the target
150 ENDIAN=@ENDIAN@
152 # Path to the C++ compiler to use. This is an optional setting, which defaults
153 # to whatever your gmake defaults to.
154 CXX = @CXX@
156 # Path to the CC binary, which use used by testcases for native builds.
157 CC := @CC@
159 # C/C++ preprocessor flags.
160 CPPFLAGS += @CPPFLAGS@
162 # C compiler flags.
163 CFLAGS += @CFLAGS@
165 # C++ compiler flags.
166 CXXFLAGS += @CXXFLAGS@
168 # Linker flags.
169 LDFLAGS += @LDFLAGS@
171 # Path to the library archiver program.
172 AR_PATH = @AR@
173 AR = @AR@
175 # Path to the nm program
176 NM_PATH = @NM@
178 # The pathnames of the programs we require to build
179 CMP := @CMP@
180 CP := @CP@
181 DATE := @DATE@
182 FIND := @FIND@
183 GREP := @GREP@
184 INSTALL := @INSTALL@
185 MKDIR := $(LLVM_SRC_ROOT)/autoconf/mkinstalldirs
186 MV := @MV@
187 RANLIB := @RANLIB@
188 RM := @RM@
189 SED := @SED@
190 TAR := @TAR@
191 PYTHON := @PYTHON@
193 # Paths to miscellaneous programs we hope are present but might not be
194 BZIP2 := @BZIP2@
195 CAT := @CAT@
196 DOT := @DOT@
197 DOXYGEN := @DOXYGEN@
198 GROFF := @GROFF@
199 GZIPBIN := @GZIPBIN@
200 OCAMLC := @OCAMLC@
201 OCAMLOPT := @OCAMLOPT@
202 OCAMLDEP := @OCAMLDEP@
203 OCAMLDOC := @OCAMLDOC@
204 GAS := @GAS@
205 POD2HTML := @POD2HTML@
206 POD2MAN := @POD2MAN@
207 PDFROFF := @PDFROFF@
208 ZIP := @ZIP@
210 HAVE_PTHREAD := @HAVE_PTHREAD@
212 LIBS := @LIBS@
214 # Targets that we should build
215 TARGETS_TO_BUILD=@TARGETS_TO_BUILD@
217 # Path to directory where object files should be stored during a build.
218 # Set OBJ_ROOT to "." if you do not want to use a separate place for
219 # object files.
220 OBJ_ROOT := .
222 # What to pass as rpath flag to g++
223 RPATH := @RPATH@
225 # What to pass as -rdynamic flag to g++
226 RDYNAMIC := @RDYNAMIC@
228 # These are options that can either be enabled here, or can be enabled on the
229 # make command line (ie, make ENABLE_PROFILING=1):
231 # When ENABLE_LIBCPP is enabled, LLVM uses libc++ by default to build.
232 #ENABLE_LIBCPP = 0
233 ENABLE_LIBCPP = @ENABLE_LIBCPP@
235 # When ENABLE_CXX11 is enabled, LLVM uses c++11 mode by default to build.
236 ENABLE_CXX11 = @ENABLE_CXX11@
238 # When ENABLE_CLANG_ARCMT is enabled, clang will have ARCMigrationTool.
239 ENABLE_CLANG_ARCMT = @ENABLE_CLANG_ARCMT@
241 # When ENABLE_CLANG_REWRITER is enabled, clang will have Rewriter.
242 ENABLE_CLANG_REWRITER = @ENABLE_CLANG_REWRITER@
244 # When ENABLE_CLANG_STATIC_ANALYZER is enabled, clang will have StaticAnalyzer.
245 ENABLE_CLANG_STATIC_ANALYZER = @ENABLE_CLANG_STATIC_ANALYZER@
247 # When ENABLE_WERROR is enabled, we'll pass -Werror on the command line
248 ENABLE_WERROR = @ENABLE_WERROR@
250 # When ENABLE_OPTIMIZED is enabled, LLVM code is optimized and output is put
251 # into the "Release" directories. Otherwise, LLVM code is not optimized and
252 # output is put in the "Debug" directories.
253 #ENABLE_OPTIMIZED = 1
254 @ENABLE_OPTIMIZED@
256 # When ENABLE_PROFILING is enabled, profile instrumentation is done
257 # and output is put into the "<Flavor>+Profile" directories, where
258 # <Flavor> is either Debug or Release depending on how other build
259 # flags are set. Otherwise, output is put in the <Flavor>
260 # directories.
261 #ENABLE_PROFILING = 1
262 @ENABLE_PROFILING@
264 # When DISABLE_ASSERTIONS is enabled, builds of all of the LLVM code will
265 # exclude assertion checks, otherwise they are included.
266 #DISABLE_ASSERTIONS = 1
267 @DISABLE_ASSERTIONS@
269 # When ENABLE_EXPENSIVE_CHECKS is enabled, builds of all of the LLVM
270 # code will include expensive checks, otherwise they are excluded.
271 #ENABLE_EXPENSIVE_CHECKS = 0
272 @ENABLE_EXPENSIVE_CHECKS@
274 # When DEBUG_RUNTIME is enabled, the runtime libraries will retain debug
275 # symbols.
276 #DEBUG_RUNTIME = 1
277 @DEBUG_RUNTIME@
279 # When DEBUG_SYMBOLS is enabled, the compiler libraries will retain debug
280 # symbols.
281 #DEBUG_SYMBOLS = 1
282 @DEBUG_SYMBOLS@
284 # When KEEP_SYMBOLS is enabled, installed executables will never have their
285 # symbols stripped.
286 #KEEP_SYMBOLS = 1
287 @KEEP_SYMBOLS@
289 # The compiler flags to use for optimized builds.
290 OPTIMIZE_OPTION := @OPTIMIZE_OPTION@
292 # When ENABLE_PROFILING is enabled, the llvm source base is built with profile
293 # information to allow gprof to be used to get execution frequencies.
294 #ENABLE_PROFILING = 1
296 # When ENABLE_DOCS is disabled, docs/ will not be built.
297 ENABLE_DOCS = @ENABLE_DOCS@
299 # When ENABLE_DOXYGEN is enabled, the doxygen documentation will be built
300 ENABLE_DOXYGEN = @ENABLE_DOXYGEN@
302 # Do we want to enable threads?
303 ENABLE_THREADS := @LLVM_ENABLE_THREADS@
305 # Do we want to build with position independent code?
306 ENABLE_PIC := @ENABLE_PIC@
308 # Do we want to build a shared library and link the tools with it?
309 ENABLE_SHARED := @ENABLE_SHARED@
311 # Do we want to link the stdc++ into a shared library? (Cygming)
312 ENABLE_EMBED_STDCXX := @ENABLE_EMBED_STDCXX@
314 # Use -fvisibility-inlines-hidden?
315 ENABLE_VISIBILITY_INLINES_HIDDEN := @ENABLE_VISIBILITY_INLINES_HIDDEN@
317 # Do we want to allow timestamping information into builds?
318 ENABLE_TIMESTAMPS := @ENABLE_TIMESTAMPS@
320 # This option tells the Makefiles to produce verbose output.
321 # It essentially prints the commands that make is executing
322 #VERBOSE = 1
324 # Enable JIT for this platform
325 TARGET_HAS_JIT = @TARGET_HAS_JIT@
327 # Environment variable to set to change the runtime shared library search path.
328 SHLIBPATH_VAR = @SHLIBPATH_VAR@
330 # Shared library extension for host platform.
331 SHLIBEXT = @SHLIBEXT@
333 # Executable file extension for host platform.
334 EXEEXT = @EXEEXT@
336 # Things we just assume are "there"
337 ECHO := echo
339 # Get the options for causing archives to link all their content instead of
340 # just missing symbols, and the inverse of that. This is used for certain LLVM
341 # tools that permit loadable modules. It ensures that the LLVM symbols will be
342 # available to those loadable modules.
343 LINKALL := @LINKALL@
344 NOLINKALL := @NOLINKALL@
346 # Get the value of HUGE_VAL_SANITY which will be either "yes" or "no" depending
347 # on the check.
348 HUGE_VAL_SANITY = @HUGE_VAL_SANITY@
350 # Bindings that we should build
351 BINDINGS_TO_BUILD := @BINDINGS_TO_BUILD@
352 ALL_BINDINGS := @ALL_BINDINGS@
353 OCAML_LIBDIR := @OCAML_LIBDIR@
355 # When compiling under Mingw/Cygwin, executables such as tblgen
356 # expect Windows paths, whereas the build system uses Unix paths.
357 # The function SYSPATH transforms Unix paths into Windows paths.
358 ifneq (,$(findstring -mno-cygwin, $(CXX)))
359 SYSPATH = $(shell echo $(1) | cygpath -m -f -)
360 else
361 SYSPATH = $(1)
362 endif
364 # Location of the plugin header file for gold.
365 BINUTILS_INCDIR := @BINUTILS_INCDIR@
367 # Optional flags supported by the compiler
368 # -Wno-missing-field-initializers
369 NO_MISSING_FIELD_INITIALIZERS = @NO_MISSING_FIELD_INITIALIZERS@
370 # -Wno-variadic-macros
371 NO_VARIADIC_MACROS = @NO_VARIADIC_MACROS@
372 # -Wcovered-switch-default
373 COVERED_SWITCH_DEFAULT = @COVERED_SWITCH_DEFAULT@
374 # -Wno-uninitialized
375 NO_UNINITIALIZED = @NO_UNINITIALIZED@
376 # -Wno-maybe-uninitialized
377 NO_MAYBE_UNINITIALIZED = @NO_MAYBE_UNINITIALIZED@
379 # Was polly found in tools/polly?
380 LLVM_HAS_POLLY = @LLVM_HAS_POLLY@
381 # Flags supported by the linker.
382 # bfd ld / gold --version-script=file
383 HAVE_LINK_VERSION_SCRIPT = @HAVE_LINK_VERSION_SCRIPT@
385 # Flags to control using libxml2
386 LIBXML2_LIBS := @LIBXML2_LIBS@
387 LIBXML2_INC := @LIBXML2_INC@
389 # Flags to control building support for Intel JIT Events API
390 USE_INTEL_JITEVENTS := @USE_INTEL_JITEVENTS@
391 INTEL_JITEVENTS_INCDIR := @INTEL_JITEVENTS_INCDIR@
392 INTEL_JITEVENTS_LIBDIR := @INTEL_JITEVENTS_LIBDIR@
394 # Flags to control building support for OProfile JIT API
395 USE_OPROFILE := @USE_OPROFILE@
397 ifeq ($(USE_INTEL_JITEVENTS), 1)
398 OPTIONAL_COMPONENTS += IntelJITEvents
399 endif
400 ifeq ($(USE_OPROFILE), 1)
401 OPTIONAL_COMPONENTS += OProfileJIT
402 endif