]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - Makefile.config.in
DIBuilder: Extract DIHeaderFieldIterator::getNumber(), NFC
[opencl/llvm.git] / Makefile.config.in
1 #===-- Makefile.config - Local configuration for LLVM ------*- Makefile -*--===#
2 #
3 #                     The LLVM Compiler Infrastructure
4 #
5 # This file is distributed under the University of Illinois Open Source
6 # License. See LICENSE.TXT for details.
7 #
8 #===------------------------------------------------------------------------===#
9 #
10 # This file is included by Makefile.common.  It defines paths and other
11 # values specific to a particular installation of LLVM.
12 #
13 #===------------------------------------------------------------------------===#
15 # Define LLVM specific info and directories based on the autoconf variables
16 LLVMPackageName   := @PACKAGE_TARNAME@
17 LLVMVersion       := @PACKAGE_VERSION@
18 LLVM_VERSION_MAJOR := @LLVM_VERSION_MAJOR@
19 LLVM_VERSION_MINOR := @LLVM_VERSION_MINOR@
20 LLVM_VERSION_PATCH := @LLVM_VERSION_PATCH@
21 LLVM_VERSION_SUFFIX := @LLVM_VERSION_SUFFIX@
22 LLVM_CONFIGTIME   := @LLVM_CONFIGTIME@
24 ###########################################################################
25 # Directory Configuration
26 #       This section of the Makefile determines what is where.  To be
27 #       specific, there are several locations that need to be defined:
28 #
29 #       o LLVM_SRC_ROOT  : The root directory of the LLVM source code.
30 #       o LLVM_OBJ_ROOT  : The root directory containing the built LLVM code.
31 #
32 #       o PROJ_SRC_DIR  : The directory containing the code to build.
33 #       o PROJ_SRC_ROOT : The root directory of the code to build.
34 #
35 #       o PROJ_OBJ_DIR  : The directory in which compiled code will be placed.
36 #       o PROJ_OBJ_ROOT : The root directory in which compiled code is placed.
37 #
38 ###########################################################################
40 PWD := @BINPWD@
41 # Set the project name to LLVM if its not defined
42 ifndef PROJECT_NAME
43 PROJECT_NAME := $(LLVMPackageName)
44 endif
46 # The macro below is expanded when 'realpath' is not built-in.
47 # Built-in 'realpath' is available on GNU Make 3.81.
48 realpath = $(shell cd $(1); $(PWD))
50 PROJ_OBJ_DIR  := $(call realpath, .)
51 PROJ_OBJ_ROOT := $(call realpath, $(PROJ_OBJ_DIR)/$(LEVEL))
53 CLANG_SRC_ROOT  := @CLANG_SRC_ROOT@
55 ifeq ($(PROJECT_NAME),$(LLVMPackageName))
56 LLVM_SRC_ROOT   := $(call realpath, @abs_top_srcdir@)
57 LLVM_OBJ_ROOT   := $(call realpath, @abs_top_builddir@)
58 PROJ_SRC_ROOT   := $(LLVM_SRC_ROOT)
59 PROJ_SRC_DIR    := $(LLVM_SRC_ROOT)$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR))
61 ifneq ($(CLANG_SRC_ROOT),)
62   CLANG_SRC_ROOT:= $(call realpath, $(CLANG_SRC_ROOT))
63   PROJ_SRC_DIR  := $(patsubst $(LLVM_SRC_ROOT)/tools/clang%,$(CLANG_SRC_ROOT)%,$(PROJ_SRC_DIR))
64 endif
66 prefix          := @prefix@
67 PROJ_prefix     := $(prefix)
68 program_prefix  := @program_prefix@
69 PROJ_VERSION    := $(LLVMVersion)
70 else
71 ifndef PROJ_SRC_ROOT
72 $(error Projects must define PROJ_SRC_ROOT)
73 endif
74 ifndef PROJ_OBJ_ROOT
75 $(error Projects must define PROJ_OBJ_ROOT)
76 endif
77 ifndef PROJ_INSTALL_ROOT
78 $(error Projects must define PROJ_INSTALL_ROOT)
79 endif
80 ifndef LLVM_SRC_ROOT
81 $(error Projects must define LLVM_SRC_ROOT)
82 endif
83 ifndef LLVM_OBJ_ROOT
84 $(error Projects must define LLVM_OBJ_ROOT)
85 endif
86 PROJ_SRC_DIR := $(call realpath, $(PROJ_SRC_ROOT)/$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR)))
87 prefix          := $(PROJ_INSTALL_ROOT)
88 PROJ_prefix     := $(prefix)
89 ifndef PROJ_VERSION
90 PROJ_VERSION := 1.0
91 endif
92 endif
94 INTERNAL_PREFIX := @INTERNAL_PREFIX@
95 ifneq ($(INTERNAL_PREFIX),)
96 PROJ_internal_prefix := $(INTERNAL_PREFIX)
97 else
98 PROJ_internal_prefix := $(prefix)
99 endif
101 PROJ_bindir     := $(PROJ_prefix)/bin
102 PROJ_libdir     := $(PROJ_prefix)/lib
103 PROJ_datadir    := $(PROJ_prefix)/share
104 PROJ_docsdir    := $(PROJ_prefix)/docs/llvm
105 PROJ_etcdir     := $(PROJ_prefix)/etc/llvm
106 PROJ_includedir := $(PROJ_prefix)/include
107 PROJ_infodir    := $(PROJ_prefix)/info
108 PROJ_mandir     := $(PROJ_prefix)/share/man
110 # Determine if we're on a unix type operating system
111 LLVM_ON_UNIX:=@LLVM_ON_UNIX@
112 LLVM_ON_WIN32:=@LLVM_ON_WIN32@
114 # Host operating system for which LLVM will be run.
115 OS=@OS@
116 HOST_OS=@HOST_OS@
117 # Target operating system for which LLVM will compile for.
118 TARGET_OS=@TARGET_OS@
120 # Host hardware architecture
121 HOST_ARCH=@HOST_ARCH@
122 # Target hardware architecture
123 ARCH=@ARCH@
124 TARGET_NATIVE_ARCH := $(ARCH)
125 LLVM_NATIVE_ARCH := @LLVM_NATIVE_ARCH@
127 # Indicates, whether we're cross-compiling LLVM or not
128 LLVM_CROSS_COMPILING=@LLVM_CROSS_COMPILING@
130 # Executable file extension for build platform (mainly for
131 # tablegen call if we're cross-compiling).
132 BUILD_EXEEXT=@BUILD_EXEEXT@
134 # Compilers for the build platflorm (mainly for tablegen
135 # call if we're cross-compiling).
136 BUILD_CC=@BUILD_CC@
137 BUILD_CXX=@BUILD_CXX@
139 # Triple for configuring build tools when cross-compiling
140 BUILD_TRIPLE=@build@
142 # Target triple (cpu-vendor-os) which LLVM is compiled for
143 HOST_TRIPLE=@host@
145 # Target triple (cpu-vendor-os) for which we should generate code
146 TARGET_TRIPLE=@target@
148 # Extra options to compile LLVM with
149 EXTRA_OPTIONS=@EXTRA_OPTIONS@
151 # Extra options to link LLVM with
152 EXTRA_LD_OPTIONS=@EXTRA_LD_OPTIONS@
154 # Endian-ness of the target
155 ENDIAN=@ENDIAN@
157 # Path to the C++ compiler to use.  This is an optional setting, which defaults
158 # to whatever your gmake defaults to.
159 CXX = @CXX@
161 # Path to the CC binary, which use used by testcases for native builds.
162 CC := @CC@
164 # C/C++ preprocessor flags.
165 CPPFLAGS += @CPPFLAGS@
167 # C compiler flags.
168 CFLAGS += @CFLAGS@
170 # C++ compiler flags.
171 CXXFLAGS += @CXXFLAGS@
173 # Linker flags.
174 LDFLAGS += @LDFLAGS@
176 # Path to the library archiver program.
177 AR_PATH = @AR@
178 AR = @AR@
180 # Path to the nm program
181 NM_PATH = @NM@
183 # The pathnames of the programs we require to build
184 CMP        := @CMP@
185 CP         := @CP@
186 DATE       := @DATE@
187 FIND       := @FIND@
188 GREP       := @GREP@
189 INSTALL    := @INSTALL@
190 MKDIR      := $(LLVM_SRC_ROOT)/autoconf/mkinstalldirs
191 MV         := @MV@
192 RANLIB     := @RANLIB@
193 RM         := @RM@
194 SED        := @SED@
195 TAR        := @TAR@
196 PYTHON     := @PYTHON@
198 # Paths to miscellaneous programs we hope are present but might not be
199 BZIP2      := @BZIP2@
200 CAT        := @CAT@
201 DOT        := @DOT@
202 DOXYGEN    := @DOXYGEN@
203 GROFF      := @GROFF@
204 GZIPBIN    := @GZIPBIN@
205 GO         := @GO@
206 OCAMLFIND  := @OCAMLFIND@
207 GAS        := @GAS@
208 POD2HTML   := @POD2HTML@
209 POD2MAN    := @POD2MAN@
210 PDFROFF    := @PDFROFF@
211 ZIP        := @ZIP@
213 HAVE_LIBZ  := @HAVE_LIBZ@
214 HAVE_DLOPEN := @HAVE_DLOPEN@
215 HAVE_PTHREAD := @HAVE_PTHREAD@
216 HAVE_TERMINFO := @HAVE_TERMINFO@
218 HAVE_OCAMLOPT := @HAVE_OCAMLOPT@
219 HAVE_OCAML_OUNIT := @HAVE_OCAML_OUNIT@
221 LIBS       := @LIBS@
223 # Targets that are possible to build
224 ALL_TARGETS := @ALL_TARGETS@
226 # Targets that we should build
227 TARGETS_TO_BUILD=@TARGETS_TO_BUILD@
229 # Targets supporting JIT
230 TARGETS_WITH_JIT := @TARGETS_WITH_JIT@
232 # Path to directory where object files should be stored during a build.
233 # Set OBJ_ROOT to "." if you do not want to use a separate place for
234 # object files.
235 OBJ_ROOT := .
237 # What to pass as rpath flag to g++
238 RPATH := @RPATH@
240 # What to pass as -rdynamic flag to g++
241 RDYNAMIC := @RDYNAMIC@
243 # These are options that can either be enabled here, or can be enabled on the
244 # make command line (ie, make ENABLE_PROFILING=1):
246 # When ENABLE_LIBCPP is enabled, LLVM uses libc++ by default to build.
247 #ENABLE_LIBCPP = 0
248 ENABLE_LIBCPP = @ENABLE_LIBCPP@
250 # When ENABLE_CXX1Y is enabled, LLVM uses c++1y mode by default to build.
251 # Otherwise it uses the baseline c++11.
252 ENABLE_CXX1Y = @ENABLE_CXX1Y@
254 # When ENABLE_SPLIT_DWARF is enabled, LLVM uses -gfission to build in debug mode.
255 ENABLE_SPLIT_DWARF = @ENABLE_SPLIT_DWARF@
257 # When enabled, clang will have plugin support.
258 CLANG_PLUGIN_SUPPORT = @CLANG_PLUGIN_SUPPORT@
260 # When ENABLE_CLANG_ARCMT is enabled, clang will have ARCMigrationTool.
261 ENABLE_CLANG_ARCMT = @ENABLE_CLANG_ARCMT@
263 # When ENABLE_CLANG_STATIC_ANALYZER is enabled, clang will have StaticAnalyzer.
264 ENABLE_CLANG_STATIC_ANALYZER = @ENABLE_CLANG_STATIC_ANALYZER@
266 # When ENABLE_WERROR is enabled, we'll pass -Werror on the command line
267 ENABLE_WERROR = @ENABLE_WERROR@
269 # When ENABLE_TERMINFO is enabled, we use terminfo.
270 ENABLE_TERMINFO = @ENABLE_TERMINFO@
272 # When ENABLE_OPTIMIZED is enabled, LLVM code is optimized and output is put
273 # into the "Release" directories. Otherwise, LLVM code is not optimized and
274 # output is put in the "Debug" directories.
275 #ENABLE_OPTIMIZED = 1
276 @ENABLE_OPTIMIZED@
278 # When ENABLE_PROFILING is enabled, profile instrumentation is done
279 # and output is put into the "<Flavor>+Profile" directories, where
280 # <Flavor> is either Debug or Release depending on how other build
281 # flags are set. Otherwise, output is put in the <Flavor>
282 # directories.
283 #ENABLE_PROFILING = 1
284 @ENABLE_PROFILING@
286 # When DISABLE_ASSERTIONS is enabled, builds of all of the LLVM code will
287 # exclude assertion checks, otherwise they are included.
288 #DISABLE_ASSERTIONS = 1
289 @DISABLE_ASSERTIONS@
291 # When ENABLE_EXPENSIVE_CHECKS is enabled, builds of all of the LLVM
292 # code will include expensive checks, otherwise they are excluded.
293 #ENABLE_EXPENSIVE_CHECKS = 0
294 @ENABLE_EXPENSIVE_CHECKS@
296 # When DEBUG_RUNTIME is enabled, the runtime libraries will retain debug
297 # symbols.
298 #DEBUG_RUNTIME = 1
299 @DEBUG_RUNTIME@
301 # When DEBUG_SYMBOLS is enabled, the compiler libraries will retain debug
302 # symbols.
303 #DEBUG_SYMBOLS = 1
304 @DEBUG_SYMBOLS@
306 # When KEEP_SYMBOLS is enabled, installed executables will never have their
307 # symbols stripped.
308 #KEEP_SYMBOLS = 1
309 @KEEP_SYMBOLS@
311 # The compiler flags to use for optimized builds.
312 OPTIMIZE_OPTION := @OPTIMIZE_OPTION@
314 # When ENABLE_PROFILING is enabled, the llvm source base is built with profile
315 # information to allow gprof to be used to get execution frequencies.
316 #ENABLE_PROFILING = 1
318 # When ENABLE_DOCS is disabled, docs/ will not be built.
319 ENABLE_DOCS = @ENABLE_DOCS@
321 # When ENABLE_DOXYGEN is enabled, the doxygen documentation will be built
322 ENABLE_DOXYGEN = @ENABLE_DOXYGEN@
324 # Do we want to enable threads?
325 ENABLE_THREADS := @LLVM_ENABLE_THREADS@
327 # Do we want to enable zlib?
328 ENABLE_ZLIB := @LLVM_ENABLE_ZLIB@
330 # Do we want to build with position independent code?
331 ENABLE_PIC := @ENABLE_PIC@
333 # Do we want to build a shared library and link the tools with it?
334 ENABLE_SHARED := @ENABLE_SHARED@
336 # Do we want to link the stdc++ into a shared library? (Cygming)
337 ENABLE_EMBED_STDCXX := @ENABLE_EMBED_STDCXX@
339 # Use -fvisibility-inlines-hidden?
340 ENABLE_VISIBILITY_INLINES_HIDDEN := @ENABLE_VISIBILITY_INLINES_HIDDEN@
342 # Do we want to allow timestamping information into builds?
343 ENABLE_TIMESTAMPS := @ENABLE_TIMESTAMPS@
345 # This option tells the Makefiles to produce verbose output.
346 # It essentially prints the commands that make is executing
347 #VERBOSE = 1
349 # Enable JIT for this platform
350 TARGET_HAS_JIT = @TARGET_HAS_JIT@
352 # Shared library extension for host platform.
353 SHLIBEXT = @SHLIBEXT@
355 # Executable file extension for host platform.
356 EXEEXT = @EXEEXT@
358 # Things we just assume are "there"
359 ECHO := echo
361 # Get the options for causing archives to link all their content instead of
362 # just missing symbols, and the inverse of that. This is used for certain LLVM
363 # tools that permit loadable modules. It ensures that the LLVM symbols will be
364 # available to those loadable modules.
365 LINKALL := @LINKALL@
366 NOLINKALL := @NOLINKALL@
368 # Get the value of HUGE_VAL_SANITY which will be either "yes" or "no" depending
369 # on the check.
370 HUGE_VAL_SANITY = @HUGE_VAL_SANITY@
372 # Bindings that we should build
373 BINDINGS_TO_BUILD := @BINDINGS_TO_BUILD@
374 OCAML_LIBDIR      := @OCAML_LIBDIR@
376 # When compiling under Mingw/Cygwin, executables such as tblgen
377 # expect Windows paths, whereas the build system uses Unix paths.
378 # The function SYSPATH transforms Unix paths into Windows paths.
379 ifneq (,$(findstring -mno-cygwin, $(CXX)))
380   SYSPATH = $(shell echo $(1) | cygpath -m -f -)
381 else
382   SYSPATH = $(1)
383 endif
385 # Location of the plugin header file for gold.
386 BINUTILS_INCDIR := @BINUTILS_INCDIR@
388 # Optional flags supported by the compiler
389 # -Wno-missing-field-initializers
390 NO_MISSING_FIELD_INITIALIZERS = @NO_MISSING_FIELD_INITIALIZERS@
391 # -Wno-variadic-macros
392 NO_VARIADIC_MACROS = @NO_VARIADIC_MACROS@
393 # -Wcovered-switch-default
394 COVERED_SWITCH_DEFAULT = @COVERED_SWITCH_DEFAULT@
395 # -Wno-uninitialized
396 NO_UNINITIALIZED = @NO_UNINITIALIZED@
397 # -Wno-maybe-uninitialized
398 NO_MAYBE_UNINITIALIZED = @NO_MAYBE_UNINITIALIZED@
399 # -Wno-comment
400 NO_COMMENT = @NO_COMMENT@
402 # Was polly found in tools/polly?
403 LLVM_HAS_POLLY = @LLVM_HAS_POLLY@
404 # Flags supported by the linker.
405 # bfd ld / gold --version-script=file
406 HAVE_LINK_VERSION_SCRIPT = @HAVE_LINK_VERSION_SCRIPT@
408 # Flags to control using libxml2
409 LIBXML2_LIBS := @LIBXML2_LIBS@
410 LIBXML2_INC  := @LIBXML2_INC@
412 # Flags to control building support for Intel JIT Events API
413 USE_INTEL_JITEVENTS := @USE_INTEL_JITEVENTS@
414 INTEL_JITEVENTS_INCDIR := @INTEL_JITEVENTS_INCDIR@
415 INTEL_JITEVENTS_LIBDIR := @INTEL_JITEVENTS_LIBDIR@
417 # Flags to control building support for OProfile JIT API
418 USE_OPROFILE := @USE_OPROFILE@
420 ifeq ($(USE_INTEL_JITEVENTS), 1)
421   OPTIONAL_COMPONENTS += IntelJITEvents
422 endif
423 ifeq ($(USE_OPROFILE), 1)
424   OPTIONAL_COMPONENTS += OProfileJIT
425 endif