1 #===-- Makefile.config - Local configuration for LLVM ------*- Makefile -*--===#
2 #
3 # The LLVM Compiler Infrastructure
4 #
5 # This file is distributed under the University of Illinois Open Source
6 # License. See LICENSE.TXT for details.
7 #
8 #===------------------------------------------------------------------------===#
9 #
10 # This file is included by Makefile.common. It defines paths and other
11 # values specific to a particular installation of LLVM.
12 #
13 #===------------------------------------------------------------------------===#
15 # Define LLVM specific info and directories based on the autoconf variables
16 LLVMPackageName := @PACKAGE_NAME@
17 LLVMVersion := @PACKAGE_VERSION@
18 LLVM_CONFIGTIME := @LLVM_CONFIGTIME@
20 ###########################################################################
21 # Directory Configuration
22 # This section of the Makefile determines what is where. To be
23 # specific, there are several locations that need to be defined:
24 #
25 # o LLVM_SRC_ROOT : The root directory of the LLVM source code.
26 # o LLVM_OBJ_ROOT : The root directory containing the built LLVM code.
27 #
28 # o PROJ_SRC_DIR : The directory containing the code to build.
29 # o PROJ_SRC_ROOT : The root directory of the code to build.
30 #
31 # o PROJ_OBJ_DIR : The directory in which compiled code will be placed.
32 # o PROJ_OBJ_ROOT : The root directory in which compiled code is placed.
33 #
34 ###########################################################################
36 PWD := @BINPWD@
37 # Set the project name to LLVM if its not defined
38 ifndef PROJECT_NAME
39 PROJECT_NAME := $(LLVMPackageName)
40 endif
42 # The macro below is expanded when 'realpath' is not built-in.
43 # Built-in 'realpath' is available on GNU Make 3.81.
44 realpath = $(shell cd $(1); $(PWD))
46 PROJ_OBJ_DIR := $(call realpath, .)
47 PROJ_OBJ_ROOT := $(call realpath, $(PROJ_OBJ_DIR)/$(LEVEL))
49 CLANG_SRC_ROOT := @CLANG_SRC_ROOT@
51 ifeq ($(PROJECT_NAME),llvm)
52 LLVM_SRC_ROOT := $(call realpath, @abs_top_srcdir@)
53 LLVM_OBJ_ROOT := $(call realpath, @abs_top_builddir@)
54 PROJ_SRC_ROOT := $(LLVM_SRC_ROOT)
55 PROJ_SRC_DIR := $(LLVM_SRC_ROOT)$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR))
57 ifneq ($(CLANG_SRC_ROOT),)
58 CLANG_SRC_ROOT:= $(call realpath, $(CLANG_SRC_ROOT))
59 PROJ_SRC_DIR := $(patsubst $(LLVM_SRC_ROOT)/tools/clang%,$(CLANG_SRC_ROOT)%,$(PROJ_SRC_DIR))
60 endif
62 prefix := @prefix@
63 PROJ_prefix := $(prefix)
64 PROJ_VERSION := $(LLVMVersion)
65 else
66 ifndef PROJ_SRC_ROOT
67 $(error Projects must define PROJ_SRC_ROOT)
68 endif
69 ifndef PROJ_OBJ_ROOT
70 $(error Projects must define PROJ_OBJ_ROOT)
71 endif
72 ifndef PROJ_INSTALL_ROOT
73 $(error Projects must define PROJ_INSTALL_ROOT)
74 endif
75 ifndef LLVM_SRC_ROOT
76 $(error Projects must define LLVM_SRC_ROOT)
77 endif
78 ifndef LLVM_OBJ_ROOT
79 $(error Projects must define LLVM_OBJ_ROOT)
80 endif
81 PROJ_SRC_DIR := $(call realpath, $(PROJ_SRC_ROOT)/$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR)))
82 prefix := $(PROJ_INSTALL_ROOT)
83 PROJ_prefix := $(prefix)
84 ifndef PROJ_VERSION
85 PROJ_VERSION := 1.0
86 endif
87 endif
89 PROJ_bindir := $(PROJ_prefix)/bin
90 PROJ_libdir := $(PROJ_prefix)/lib
91 PROJ_datadir := $(PROJ_prefix)/share
92 PROJ_docsdir := $(PROJ_prefix)/docs/llvm
93 PROJ_etcdir := $(PROJ_prefix)/etc/llvm
94 PROJ_includedir := $(PROJ_prefix)/include
95 PROJ_infodir := $(PROJ_prefix)/info
96 PROJ_mandir := $(PROJ_prefix)/share/man
98 # Determine if we're on a unix type operating system
99 LLVM_ON_UNIX:=@LLVM_ON_UNIX@
100 LLVM_ON_WIN32:=@LLVM_ON_WIN32@
102 # Host operating system for which LLVM will be run.
103 OS=@OS@
104 HOST_OS=@HOST_OS@
105 # Target operating system for which LLVM will compile for.
106 TARGET_OS=@TARGET_OS@
108 # Target hardware architecture
109 ARCH=@ARCH@
111 # Indicates, whether we're cross-compiling LLVM or not
112 LLVM_CROSS_COMPILING=@LLVM_CROSS_COMPILING@
114 # Executable file extension for build platform (mainly for
115 # tablegen call if we're cross-compiling).
116 BUILD_EXEEXT=@BUILD_EXEEXT@
118 # Compilers for the build platflorm (mainly for tablegen
119 # call if we're cross-compiling).
120 BUILD_CC=@BUILD_CC@
121 BUILD_CXX=@BUILD_CXX@
123 # Triple for configuring build tools when cross-compiling
124 BUILD_TRIPLE=@build@
126 # Target triple (cpu-vendor-os) for which we should generate code
127 TARGET_TRIPLE=@target@
129 # Extra options to compile LLVM with
130 EXTRA_OPTIONS=@EXTRA_OPTIONS@
132 # Extra options to link LLVM with
133 EXTRA_LD_OPTIONS=@EXTRA_LD_OPTIONS@
135 # Endian-ness of the target
136 ENDIAN=@ENDIAN@
138 # Path to the C++ compiler to use. This is an optional setting, which defaults
139 # to whatever your gmake defaults to.
140 CXX = @CXX@
142 # Path to the CC binary, which use used by testcases for native builds.
143 CC := @CC@
145 # Linker flags.
146 LDFLAGS+=@LDFLAGS@
148 # Path to the library archiver program.
149 AR_PATH = @AR@
150 AR = @AR@
152 # Path to the strip program,
153 STRIP = @STRIP@
155 # Path to the nm program
156 NM_PATH = @NM@
158 # The pathnames of the programs we require to build
159 CMP := @CMP@
160 CP := @CP@
161 DATE := @DATE@
162 FIND := @FIND@
163 GREP := @GREP@
164 INSTALL := @INSTALL@
165 MKDIR := $(LLVM_SRC_ROOT)/autoconf/mkinstalldirs
166 MV := @MV@
167 RANLIB := @RANLIB@
168 RM := @RM@
169 SED := @SED@
170 TAR := @TAR@
172 # Paths to miscellaneous programs we hope are present but might not be
173 PERL := @PERL@
174 BZIP2 := @BZIP2@
175 CAT := @CAT@
176 DOT := @DOT@
177 DOXYGEN := @DOXYGEN@
178 GROFF := @GROFF@
179 GZIPBIN := @GZIPBIN@
180 OCAMLC := @OCAMLC@
181 OCAMLOPT := @OCAMLOPT@
182 OCAMLDEP := @OCAMLDEP@
183 OCAMLDOC := @OCAMLDOC@
184 GAS := @GAS@
185 POD2HTML := @POD2HTML@
186 POD2MAN := @POD2MAN@
187 PDFROFF := @PDFROFF@
188 RUNTEST := @RUNTEST@
189 TCLSH := @TCLSH@
190 ZIP := @ZIP@
192 HAVE_PERL := @HAVE_PERL@
193 HAVE_PTHREAD := @HAVE_PTHREAD@
195 LIBS := @LIBS@
197 # Targets that we should build
198 TARGETS_TO_BUILD=@TARGETS_TO_BUILD@
200 # Path to directory where object files should be stored during a build.
201 # Set OBJ_ROOT to "." if you do not want to use a separate place for
202 # object files.
203 OBJ_ROOT := .
205 # What to pass as rpath flag to g++
206 RPATH := @RPATH@
208 # What to pass as -rdynamic flag to g++
209 RDYNAMIC := @RDYNAMIC@
211 # These are options that can either be enabled here, or can be enabled on the
212 # make command line (ie, make ENABLE_PROFILING=1):
214 # When ENABLE_OPTIMIZED is enabled, LLVM code is optimized and output is put
215 # into the "Release" directories. Otherwise, LLVM code is not optimized and
216 # output is put in the "Debug" directories.
217 #ENABLE_OPTIMIZED = 1
218 @ENABLE_OPTIMIZED@
220 # When ENABLE_PROFILING is enabled, profile instrumentation is done
221 # and output is put into the "<Flavor>+Profile" directories, where
222 # <Flavor> is either Debug or Release depending on how other build
223 # flags are set. Otherwise, output is put in the <Flavor>
224 # directories.
225 #ENABLE_PROFILING = 1
226 @ENABLE_PROFILING@
228 # When DISABLE_ASSERTIONS is enabled, builds of all of the LLVM code will
229 # exclude assertion checks, otherwise they are included.
230 #DISABLE_ASSERTIONS = 1
231 @DISABLE_ASSERTIONS@
233 # When ENABLE_EXPENSIVE_CHECKS is enabled, builds of all of the LLVM
234 # code will include expensive checks, otherwise they are excluded.
235 #ENABLE_EXPENSIVE_CHECKS = 0
236 @ENABLE_EXPENSIVE_CHECKS@
238 # When DEBUG_RUNTIME is enabled, the runtime libraries will retain debug
239 # symbols.
240 #DEBUG_RUNTIME = 1
241 @DEBUG_RUNTIME@
243 # When DEBUG_SYMBOLS is enabled, the compiler libraries will retain debug
244 # symbols.
245 #DEBUG_SYMBOLS = 1
246 @DEBUG_SYMBOLS@
248 # The compiler flags to use for optimized builds.
249 OPTIMIZE_OPTION := @OPTIMIZE_OPTION@
251 # When ENABLE_PROFILING is enabled, the llvm source base is built with profile
252 # information to allow gprof to be used to get execution frequencies.
253 #ENABLE_PROFILING = 1
255 # When ENABLE_DOCS is disabled, docs/ will not be built.
256 ENABLE_DOCS = @ENABLE_DOCS@
258 # When ENABLE_DOXYGEN is enabled, the doxygen documentation will be built
259 ENABLE_DOXYGEN = @ENABLE_DOXYGEN@
261 # Do we want to enable threads?
262 ENABLE_THREADS := @ENABLE_THREADS@
264 # Do we want to build with position independent code?
265 ENABLE_PIC := @ENABLE_PIC@
267 # Do we want to build a shared library and link the tools with it?
268 ENABLE_SHARED := @ENABLE_SHARED@
270 # Do we want to link the stdc++ into a shared library? (Cygming)
271 ENABLE_EMBED_STDCXX := @ENABLE_EMBED_STDCXX@
273 # Use -fvisibility-inlines-hidden?
274 ENABLE_VISIBILITY_INLINES_HIDDEN := @ENABLE_VISIBILITY_INLINES_HIDDEN@
276 # Do we want to allow timestamping information into builds?
277 ENABLE_TIMESTAMPS := @ENABLE_TIMESTAMPS@
279 # This option tells the Makefiles to produce verbose output.
280 # It essentially prints the commands that make is executing
281 #VERBOSE = 1
283 # Enable JIT for this platform
284 TARGET_HAS_JIT = @TARGET_HAS_JIT@
286 # Environment variable to set to change the runtime shared library search path.
287 SHLIBPATH_VAR = @SHLIBPATH_VAR@
289 # Shared library extension for host platform.
290 SHLIBEXT = @SHLIBEXT@
292 # Executable file extension for host platform.
293 EXEEXT = @EXEEXT@
295 # Things we just assume are "there"
296 ECHO := echo
298 # Get the options for causing archives to link all their content instead of
299 # just missing symbols, and the inverse of that. This is used for certain LLVM
300 # tools that permit loadable modules. It ensures that the LLVM symbols will be
301 # available to those loadable modules.
302 LINKALL := @LINKALL@
303 NOLINKALL := @NOLINKALL@
305 # Get the value of HUGE_VAL_SANITY which will be either "yes" or "no" depending
306 # on the check.
307 HUGE_VAL_SANITY = @HUGE_VAL_SANITY@
309 # Bindings that we should build
310 BINDINGS_TO_BUILD := @BINDINGS_TO_BUILD@
311 ALL_BINDINGS := @ALL_BINDINGS@
312 OCAML_LIBDIR := @OCAML_LIBDIR@
314 # When compiling under Mingw/Cygwin, executables such as tblgen
315 # expect Windows paths, whereas the build system uses Unix paths.
316 # The function SYSPATH transforms Unix paths into Windows paths.
317 ifneq (,$(findstring -mno-cygwin, $(CXX)))
318 SYSPATH = $(shell echo $(1) | cygpath -m -f -)
319 else
320 SYSPATH = $(1)
321 endif
323 # Location of the plugin header file for gold.
324 BINUTILS_INCDIR := @BINUTILS_INCDIR@
326 # Optional flags supported by the compiler
327 # -Wno-missing-field-initializers
328 NO_MISSING_FIELD_INITIALIZERS = @NO_MISSING_FIELD_INITIALIZERS@
329 # -Wno-variadic-macros
330 NO_VARIADIC_MACROS = @NO_VARIADIC_MACROS@
332 # Was polly found in tools/polly?
333 LLVM_HAS_POLLY = @LLVM_HAS_POLLY@
334 # Flags supported by the linker.
335 # bfd ld / gold --version-script=file
336 HAVE_LINK_VERSION_SCRIPT = @HAVE_LINK_VERSION_SCRIPT@