]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - Makefile
re-apply r80197, now that iterator.h is not mentioned any more
[opencl/llvm.git] / Makefile
1 #===- ./Makefile -------------------------------------------*- Makefile -*--===#
2 #
3 #                     The LLVM Compiler Infrastructure
4 #
5 # This file is distributed under the University of Illinois Open Source
6 # License. See LICENSE.TXT for details.
7 #
8 #===------------------------------------------------------------------------===#
10 LEVEL := .
12 # Top-Level LLVM Build Stages:
13 #   1. Build lib/System and lib/Support, which are used by utils (tblgen).
14 #   2. Build utils, which is used by VMCore.
15 #   3. Build VMCore, which builds the Intrinsics.inc file used by libs.
16 #   4. Build libs, which are needed by llvm-config.
17 #   5. Build llvm-config, which determines inter-lib dependencies for tools.
18 #   6. Build tools, runtime, docs.
19 #
20 # When cross-compiling, there are some things (tablegen) that need to
21 # be build for the build system first.
22 ifeq ($(BUILD_DIRS_ONLY),1)
23   DIRS := lib/System lib/Support utils
24   OPTIONAL_DIRS :=
25 else
26   DIRS := lib/System lib/Support utils lib/VMCore lib tools/llvm-config \
27           tools runtime docs
28   OPTIONAL_DIRS := examples projects bindings
29 endif
31 EXTRA_DIST := test unittests llvm.spec include win32 Xcode
33 include $(LEVEL)/Makefile.config
35 # llvm-gcc4 doesn't need runtime libs.  llvm-gcc4 is the only supported one.
36 # FIXME: Remove runtime entirely once we have an understanding of where
37 # libprofile etc should go.
38 #ifeq ($(LLVMGCC_MAJVERS),4)
39 #  DIRS := $(filter-out runtime, $(DIRS))
40 #endif
42 ifeq ($(MAKECMDGOALS),libs-only)
43   DIRS := $(filter-out tools runtime docs, $(DIRS))
44   OPTIONAL_DIRS :=
45 endif
47 ifeq ($(MAKECMDGOALS),install-libs)
48   DIRS := $(filter-out tools runtime docs, $(DIRS))
49   OPTIONAL_DIRS := $(filter bindings, $(OPTIONAL_DIRS))
50 endif
52 ifeq ($(MAKECMDGOALS),tools-only)
53   DIRS := $(filter-out runtime docs, $(DIRS))
54   OPTIONAL_DIRS :=
55 endif
57 ifeq ($(MAKECMDGOALS),install-clang)
58   DIRS := tools/clang/tools/driver tools/clang/tools/clang-cc \
59         tools/clang/lib/Headers tools/clang/docs
60   OPTIONAL_DIRS :=
61   NO_INSTALL = 1
62 endif
64 ifeq ($(MAKECMDGOALS),clang-only)
65   DIRS := $(filter-out tools runtime docs, $(DIRS)) tools/clang
66   OPTIONAL_DIRS :=
67 endif
69 ifeq ($(MAKECMDGOALS),unittests)
70   DIRS := $(filter-out tools runtime docs, $(DIRS)) utils unittests
71   OPTIONAL_DIRS :=
72 endif
74 # Use NO_INSTALL define of the Makefile of each directory for deciding
75 # if the directory is installed or not
76 ifeq ($(MAKECMDGOALS),install)
77   OPTIONAL_DIRS := $(filter bindings, $(OPTIONAL_DIRS))
78 endif
80 # If we're cross-compiling, build the build-hosted tools first
81 ifeq ($(LLVM_CROSS_COMPILING),1)
82 all:: cross-compile-build-tools
84 clean::
85         $(Verb) rm -rf BuildTools
87 cross-compile-build-tools:
88         $(Verb) if [ ! -f BuildTools/Makefile ]; then \
89           $(MKDIR) BuildTools; \
90           cd BuildTools ; \
91           $(PROJ_SRC_DIR)/configure ; \
92           cd .. ; \
93         fi; \
94         ($(MAKE) -C BuildTools BUILD_DIRS_ONLY=1 ) || exit 1;
95 endif
97 # Include the main makefile machinery.
98 include $(LLVM_SRC_ROOT)/Makefile.rules
100 # Specify options to pass to configure script when we're
101 # running the dist-check target
102 DIST_CHECK_CONFIG_OPTIONS = --with-llvmgccdir=$(LLVMGCCDIR)
104 .PHONY: debug-opt-prof
105 debug-opt-prof:
106         $(Echo) Building Debug Version
107         $(Verb) $(MAKE)
108         $(Echo)
109         $(Echo) Building Optimized Version
110         $(Echo)
111         $(Verb) $(MAKE) ENABLE_OPTIMIZED=1
112         $(Echo)
113         $(Echo) Building Profiling Version
114         $(Echo)
115         $(Verb) $(MAKE) ENABLE_PROFILING=1
117 dist-hook::
118         $(Echo) Eliminating files constructed by configure
119         $(Verb) $(RM) -f \
120           $(TopDistDir)/include/llvm/Config/config.h  \
121           $(TopDistDir)/include/llvm/Support/DataTypes.h  \
122           $(TopDistDir)/include/llvm/Support/ThreadSupport.h
124 clang-only: all
125 tools-only: all
126 libs-only: all
127 install-clang: install
128 install-libs: install
130 #------------------------------------------------------------------------
131 # Make sure the generated headers are up-to-date. This must be kept in
132 # sync with the AC_CONFIG_HEADER invocations in autoconf/configure.ac
133 #------------------------------------------------------------------------
134 FilesToConfig := \
135   include/llvm/Config/config.h \
136   include/llvm/Config/Targets.def \
137         include/llvm/Config/AsmPrinters.def \
138   include/llvm/Support/DataTypes.h
139 FilesToConfigPATH  := $(addprefix $(LLVM_OBJ_ROOT)/,$(FilesToConfig))
141 all-local:: $(FilesToConfigPATH)
142 $(FilesToConfigPATH) : $(LLVM_OBJ_ROOT)/% : $(LLVM_SRC_ROOT)/%.in
143         $(Echo) Regenerating $*
144         $(Verb) cd $(LLVM_OBJ_ROOT) && $(ConfigStatusScript) $*
145 .PRECIOUS: $(FilesToConfigPATH)
147 # NOTE: This needs to remain as the last target definition in this file so
148 # that it gets executed last.
149 ifneq ($(BUILD_DIRS_ONLY),1)
150 all::
151         $(Echo) '*****' Completed $(BuildMode)$(AssertMode) Build
152 ifeq ($(BuildMode),Debug)
153         $(Echo) '*****' Note: Debug build can be 10 times slower than an
154         $(Echo) '*****' optimized build. Use 'make ENABLE_OPTIMIZED=1' to
155         $(Echo) '*****' make an optimized build. Alternatively you can
156         $(Echo) '*****' configure with --enable-optimized.
157 endif
158 endif
160 check-llvm2cpp:
161         $(Verb)$(MAKE) check TESTSUITE=Feature RUNLLVM2CPP=1
163 check-one:
164         $(Verb)$(MAKE) -C test check-one TESTONE=$(TESTONE)
166 srpm: $(LLVM_OBJ_ROOT)/llvm.spec
167         rpmbuild -bs $(LLVM_OBJ_ROOT)/llvm.spec
169 rpm: $(LLVM_OBJ_ROOT)/llvm.spec
170         rpmbuild -bb --target $(TARGET_TRIPLE) $(LLVM_OBJ_ROOT)/llvm.spec
172 show-footprint:
173         $(Verb) du -sk $(LibDir)
174         $(Verb) du -sk $(ToolDir)
175         $(Verb) du -sk $(ExmplDir)
176         $(Verb) du -sk $(ObjDir)
178 build-for-llvm-top:
179         $(Verb) if test ! -f ./config.status ; then \
180           ./configure --prefix="$(LLVM_TOP)/install" \
181             --with-llvm-gcc="$(LLVM_TOP)/llvm-gcc" ; \
182         fi
183         $(Verb) $(MAKE) tools-only
185 SVN = svn
186 SVN-UPDATE-OPTIONS =
187 AWK = awk
188 SUB-SVN-DIRS = $(AWK) '/\?\ \ \ \ \ \ / {print $$2}'   \
189                 | LC_ALL=C xargs $(SVN) info 2>/dev/null \
190                 | $(AWK) '/Path:\ / {print $$2}'
192 update:
193         $(SVN) $(SVN-UPDATE-OPTIONS) update $(LLVM_SRC_ROOT)
194         @ $(SVN) status $(LLVM_SRC_ROOT) | $(SUB-SVN-DIRS) | xargs $(SVN) $(SVN-UPDATE-OPTIONS) update
196 happiness: update all check unittests
198 .PHONY: srpm rpm update happiness
200 # declare all targets at this level to be serial:
202 .NOTPARALLEL: