2ee0dd5b1b73414497ed20ca9d899eaf4660cb41
[opencl/llvm.git] / cmake / modules / HandleLLVMOptions.cmake
1 # This CMake module is responsible for interpreting the user defined LLVM_
2 # options and executing the appropriate CMake commands to realize the users'
3 # selections.
5 # This is commonly needed so make sure it's defined before we include anything
6 # else.
7 string(TOUPPER "${CMAKE_BUILD_TYPE}" uppercase_CMAKE_BUILD_TYPE)
9 include(HandleLLVMStdlib)
10 include(AddLLVMDefinitions)
11 include(CheckCCompilerFlag)
12 include(CheckCXXCompilerFlag)
14 if(NOT LLVM_FORCE_USE_OLD_TOOLCHAIN)
15   if(CMAKE_CXX_COMPILER_ID STREQUAL "GNU")
16     if(CMAKE_CXX_COMPILER_VERSION VERSION_LESS 4.7)
17       message(FATAL_ERROR "Host GCC version must be at least 4.7!")
18     endif()
19   elseif(CMAKE_CXX_COMPILER_ID STREQUAL "Clang")
20     if(CMAKE_CXX_COMPILER_VERSION VERSION_LESS 3.1)
21       message(FATAL_ERROR "Host Clang version must be at least 3.1!")
22     endif()
24     # Also test that we aren't using too old of a version of libstdc++ with the
25     # Clang compiler. This is tricky as there is no real way to check the
26     # version of libstdc++ directly. Instead we test for a known bug in
27     # libstdc++4.6 that is fixed in libstdc++4.7.
28     if(NOT LLVM_ENABLE_LIBCXX)
29       set(OLD_CMAKE_REQUIRED_FLAGS ${CMAKE_REQUIRED_FLAGS})
30       set(OLD_CMAKE_REQUIRED_LIBRARIES ${CMAKE_REQUIRED_LIBRARIES})
31       set(CMAKE_REQUIRED_FLAGS "-std=c++0x")
32       check_cxx_source_compiles("
33 #include <atomic>
34 std::atomic<float> x(0.0f);
35 int main() { return (float)x; }"
36         LLVM_NO_OLD_LIBSTDCXX)
37       if(NOT LLVM_NO_OLD_LIBSTDCXX)
38         message(FATAL_ERROR "Host Clang must be able to find libstdc++4.7 or newer!")
39       endif()
40       set(CMAKE_REQUIRED_FLAGS ${OLD_CMAKE_REQUIRED_FLAGS})
41       set(CMAKE_REQUIRED_LIBRARIES ${OLD_CMAKE_REQUIRED_LIBRARIES})
42     endif()
43   elseif(CMAKE_CXX_COMPILER_ID MATCHES "MSVC")
44     if(CMAKE_CXX_COMPILER_VERSION VERSION_LESS 17.0)
45       message(FATAL_ERROR "Host Visual Studio must be at least 2012 (MSVC 17.0)")
46     endif()
47   endif()
48 endif()
50 if( LLVM_ENABLE_ASSERTIONS )
51   # MSVC doesn't like _DEBUG on release builds. See PR 4379.
52   if( NOT MSVC )
53     add_definitions( -D_DEBUG )
54   endif()
55   # On non-Debug builds cmake automatically defines NDEBUG, so we
56   # explicitly undefine it:
57   if( NOT uppercase_CMAKE_BUILD_TYPE STREQUAL "DEBUG" )
58     add_definitions( -UNDEBUG )
59     # Also remove /D NDEBUG to avoid MSVC warnings about conflicting defines.
60     foreach (flags_var_to_scrub
61         CMAKE_CXX_FLAGS_RELEASE
62         CMAKE_CXX_FLAGS_RELWITHDEBINFO
63         CMAKE_CXX_FLAGS_MINSIZEREL
64         CMAKE_C_FLAGS_RELEASE
65         CMAKE_C_FLAGS_RELWITHDEBINFO
66         CMAKE_C_FLAGS_MINSIZEREL)
67       string (REGEX REPLACE "(^| )[/-]D *NDEBUG($| )" " "
68         "${flags_var_to_scrub}" "${${flags_var_to_scrub}}")
69     endforeach()
70   endif()
71 endif()
73 if(WIN32)
74   set(LLVM_HAVE_LINK_VERSION_SCRIPT 0)
75   if(CYGWIN)
76     set(LLVM_ON_WIN32 0)
77     set(LLVM_ON_UNIX 1)
78   else(CYGWIN)
79     set(LLVM_ON_WIN32 1)
80     set(LLVM_ON_UNIX 0)
81   endif(CYGWIN)
82 else(WIN32)
83   if(UNIX)
84     set(LLVM_ON_WIN32 0)
85     set(LLVM_ON_UNIX 1)
86     if(APPLE)
87       set(LLVM_HAVE_LINK_VERSION_SCRIPT 0)
88     else(APPLE)
89       set(LLVM_HAVE_LINK_VERSION_SCRIPT 1)
90     endif(APPLE)
91   else(UNIX)
92     MESSAGE(SEND_ERROR "Unable to determine platform")
93   endif(UNIX)
94 endif(WIN32)
96 set(EXEEXT ${CMAKE_EXECUTABLE_SUFFIX})
97 set(LTDL_SHLIB_EXT ${CMAKE_SHARED_LIBRARY_SUFFIX})
99 # We use *.dylib rather than *.so on darwin.
100 set(LLVM_PLUGIN_EXT ${CMAKE_SHARED_LIBRARY_SUFFIX})
102 if(APPLE)
103   # Darwin-specific linker flags for loadable modules.
104   set(CMAKE_MODULE_LINKER_FLAGS "${CMAKE_MODULE_LINKER_FLAGS} -Wl,-flat_namespace -Wl,-undefined -Wl,suppress")
105 endif()
107 function(append value)
108   foreach(variable ${ARGN})
109     set(${variable} "${${variable}} ${value}" PARENT_SCOPE)
110   endforeach(variable)
111 endfunction()
113 function(append_if condition value)
114   if (${condition})
115     foreach(variable ${ARGN})
116       set(${variable} "${${variable}} ${value}" PARENT_SCOPE)
117     endforeach(variable)
118   endif()
119 endfunction()
121 macro(add_flag_if_supported flag name)
122   check_c_compiler_flag("-Werror ${flag}" "C_SUPPORTS_${name}")
123   append_if("C_SUPPORTS_${name}" "${flag}" CMAKE_C_FLAGS)
124   check_cxx_compiler_flag("-Werror ${flag}" "CXX_SUPPORTS_${name}")
125   append_if("CXX_SUPPORTS_${name}" "${flag}" CMAKE_CXX_FLAGS)
126 endmacro()
128 function(add_flag_or_print_warning flag name)
129   check_c_compiler_flag("-Werror ${flag}" "C_SUPPORTS_${name}")
130   check_cxx_compiler_flag("-Werror ${flag}" "CXX_SUPPORTS_${name}")
131   if (C_SUPPORTS_${name} AND CXX_SUPPORTS_${name})
132     message(STATUS "Building with ${flag}")
133     set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} ${flag}" PARENT_SCOPE)
134     set(CMAKE_C_FLAGS "${CMAKE_C_FLAGS} ${flag}" PARENT_SCOPE)
135   else()
136     message(WARNING "${flag} is not supported.")
137   endif()
138 endfunction()
140 if( LLVM_ENABLE_PIC )
141   if( XCODE )
142     # Xcode has -mdynamic-no-pic on by default, which overrides -fPIC. I don't
143     # know how to disable this, so just force ENABLE_PIC off for now.
144     message(WARNING "-fPIC not supported with Xcode.")
145   elseif( WIN32 OR CYGWIN)
146     # On Windows all code is PIC. MinGW warns if -fPIC is used.
147   else()
148     add_flag_or_print_warning("-fPIC" FPIC)
150     if( WIN32 OR CYGWIN)
151       # MinGW warns if -fvisibility-inlines-hidden is used.
152     else()
153       check_cxx_compiler_flag("-fvisibility-inlines-hidden" SUPPORTS_FVISIBILITY_INLINES_HIDDEN_FLAG)
154       append_if(SUPPORTS_FVISIBILITY_INLINES_HIDDEN_FLAG "-fvisibility-inlines-hidden" CMAKE_CXX_FLAGS)
155     endif()
156   endif()
157 endif()
159 if( CMAKE_SIZEOF_VOID_P EQUAL 8 AND NOT WIN32 )
160   # TODO: support other platforms and toolchains.
161   if( LLVM_BUILD_32_BITS )
162     message(STATUS "Building 32 bits executables and libraries.")
163     add_llvm_definitions( -m32 )
164     set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -m32")
165     set(CMAKE_SHARED_LINKER_FLAGS "${CMAKE_SHARED_LINKER_FLAGS} -m32")
166     set(CMAKE_MODULE_LINKER_FLAGS "${CMAKE_MODULE_LINKER_FLAGS} -m32")
167   endif( LLVM_BUILD_32_BITS )
168 endif( CMAKE_SIZEOF_VOID_P EQUAL 8 AND NOT WIN32 )
170 if (LLVM_BUILD_STATIC)
171   set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -static")
172 endif()
174 if( XCODE )
175   # For Xcode enable several build settings that correspond to
176   # many warnings that are on by default in Clang but are
177   # not enabled for historical reasons.  For versions of Xcode
178   # that do not support these options they will simply
179   # be ignored.
180   set(CMAKE_XCODE_ATTRIBUTE_GCC_WARN_ABOUT_RETURN_TYPE "YES")
181   set(CMAKE_XCODE_ATTRIBUTE_GCC_WARN_ABOUT_MISSING_NEWLINE "YES")
182   set(CMAKE_XCODE_ATTRIBUTE_GCC_WARN_UNUSED_VALUE "YES")
183   set(CMAKE_XCODE_ATTRIBUTE_GCC_WARN_UNUSED_VARIABLE "YES")
184   set(CMAKE_XCODE_ATTRIBUTE_GCC_WARN_SIGN_COMPARE "YES")
185   set(CMAKE_XCODE_ATTRIBUTE_GCC_WARN_UNUSED_FUNCTION "YES")
186   set(CMAKE_XCODE_ATTRIBUTE_GCC_WARN_INITIALIZER_NOT_FULLY_BRACKETED "YES")
187   set(CMAKE_XCODE_ATTRIBUTE_GCC_WARN_HIDDEN_VIRTUAL_FUNCTIONS "YES")
188   set(CMAKE_XCODE_ATTRIBUTE_GCC_WARN_UNINITIALIZED_AUTOS "YES")
189   set(CMAKE_XCODE_ATTRIBUTE_CLANG_WARN_BOOL_CONVERSION "YES")
190   set(CMAKE_XCODE_ATTRIBUTE_CLANG_WARN_EMPTY_BODY "YES")
191   set(CMAKE_XCODE_ATTRIBUTE_CLANG_WARN_ENUM_CONVERSION "YES")
192   set(CMAKE_XCODE_ATTRIBUTE_CLANG_WARN_INT_CONVERSION "YES")
193   set(CMAKE_XCODE_ATTRIBUTE_CLANG_WARN_CONSTANT_CONVERSION "YES")
194   set(CMAKE_XCODE_ATTRIBUTE_GCC_WARN_NON_VIRTUAL_DESTRUCTOR "YES")
195 endif()
197 # On Win32 using MS tools, provide an option to set the number of parallel jobs
198 # to use.
199 if( MSVC_IDE )
200   set(LLVM_COMPILER_JOBS "0" CACHE STRING
201     "Number of parallel compiler jobs. 0 means use all processors. Default is 0.")
202   if( NOT LLVM_COMPILER_JOBS STREQUAL "1" )
203     if( LLVM_COMPILER_JOBS STREQUAL "0" )
204       add_llvm_definitions( /MP )
205     else()
206       message(STATUS "Number of parallel compiler jobs set to " ${LLVM_COMPILER_JOBS})
207       add_llvm_definitions( /MP${LLVM_COMPILER_JOBS} )
208     endif()
209   else()
210     message(STATUS "Parallel compilation disabled")
211   endif()
212 endif()
214 if( MSVC )
215   include(ChooseMSVCCRT)
217   if( NOT (${CMAKE_VERSION} VERSION_LESS 2.8.11) )
218     # set stack reserved size to ~10MB
219     # CMake previously automatically set this value for MSVC builds, but the
220     # behavior was changed in CMake 2.8.11 (Issue 12437) to use the MSVC default
221     # value (1 MB) which is not enough for us in tasks such as parsing recursive
222     # C++ templates in Clang.
223     set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} /STACK:10000000")
224   endif()
226   if( MSVC11 )
227     add_llvm_definitions(-D_VARIADIC_MAX=10)
228   endif()
229   
230   # Add definitions that make MSVC much less annoying.
231   add_llvm_definitions(
232     # For some reason MS wants to deprecate a bunch of standard functions...
233     -D_CRT_SECURE_NO_DEPRECATE
234     -D_CRT_SECURE_NO_WARNINGS
235     -D_CRT_NONSTDC_NO_DEPRECATE
236     -D_CRT_NONSTDC_NO_WARNINGS
237     -D_SCL_SECURE_NO_DEPRECATE
238     -D_SCL_SECURE_NO_WARNINGS
240     # Disabled warnings.
241     -wd4146 # Suppress 'unary minus operator applied to unsigned type, result still unsigned'
242     -wd4180 # Suppress 'qualifier applied to function type has no meaning; ignored'
243     -wd4244 # Suppress ''argument' : conversion from 'type1' to 'type2', possible loss of data'
244     -wd4258 # Suppress ''var' : definition from the for loop is ignored; the definition from the enclosing scope is used'
245     -wd4267 # Suppress ''var' : conversion from 'size_t' to 'type', possible loss of data'
246     -wd4291 # Suppress ''declaration' : no matching operator delete found; memory will not be freed if initialization throws an exception'
247     -wd4345 # Suppress 'behavior change: an object of POD type constructed with an initializer of the form () will be default-initialized'
248     -wd4351 # Suppress 'new behavior: elements of array 'array' will be default initialized'
249     -wd4355 # Suppress ''this' : used in base member initializer list'
250     -wd4456 # Suppress 'declaration of 'var' hides local variable'
251     -wd4457 # Suppress 'declaration of 'var' hides function parameter'
252     -wd4458 # Suppress 'declaration of 'var' hides class member'
253     -wd4459 # Suppress 'declaration of 'var' hides global declaration'
254     -wd4503 # Suppress ''identifier' : decorated name length exceeded, name was truncated'
255     -wd4624 # Suppress ''derived class' : destructor could not be generated because a base class destructor is inaccessible'
256     -wd4722 # Suppress 'function' : destructor never returns, potential memory leak
257     -wd4800 # Suppress ''type' : forcing value to bool 'true' or 'false' (performance warning)'
258     
259     # Promoted warnings.
260     -w14062 # Promote 'enumerator in switch of enum is not handled' to level 1 warning.
262     # Promoted warnings to errors.
263     -we4238 # Promote 'nonstandard extension used : class rvalue used as lvalue' to error.
264     )
266   # Enable warnings
267   if (LLVM_ENABLE_WARNINGS)
268     add_llvm_definitions( /W4 )
269     if (LLVM_ENABLE_PEDANTIC)
270       # No MSVC equivalent available
271     endif (LLVM_ENABLE_PEDANTIC)
272   endif (LLVM_ENABLE_WARNINGS)
273   if (LLVM_ENABLE_WERROR)
274     add_llvm_definitions( /WX )
275   endif (LLVM_ENABLE_WERROR)
276 elseif( LLVM_COMPILER_IS_GCC_COMPATIBLE )
277   if (LLVM_ENABLE_WARNINGS)
278     append("-Wall -W -Wno-unused-parameter -Wwrite-strings" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
279     append("-Wcast-qual" CMAKE_CXX_FLAGS)
281     # Turn off missing field initializer warnings for gcc to avoid noise from
282     # false positives with empty {}. Turn them on otherwise (they're off by
283     # default for clang).
284     check_cxx_compiler_flag("-Wmissing-field-initializers" CXX_SUPPORTS_MISSING_FIELD_INITIALIZERS_FLAG)
285     if (CXX_SUPPORTS_MISSING_FIELD_INITIALIZERS_FLAG)
286       if (CMAKE_COMPILER_IS_GNUCXX)
287         append("-Wno-missing-field-initializers" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
288       else()
289         append("-Wmissing-field-initializers" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
290       endif()
291     endif()
293     append_if(LLVM_ENABLE_PEDANTIC "-pedantic -Wno-long-long" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
294     add_flag_if_supported("-Wcovered-switch-default" COVERED_SWITCH_DEFAULT_FLAG)
295     append_if(USE_NO_UNINITIALIZED "-Wno-uninitialized" CMAKE_CXX_FLAGS)
296     append_if(USE_NO_MAYBE_UNINITIALIZED "-Wno-maybe-uninitialized" CMAKE_CXX_FLAGS)
298     # Check if -Wnon-virtual-dtor warns even though the class is marked final.
299     # If it does, don't add it. So it won't be added on clang 3.4 and older.
300     # This also catches cases when -Wnon-virtual-dtor isn't supported by
301     # the compiler at all.
302     set(OLD_CMAKE_REQUIRED_FLAGS ${CMAKE_REQUIRED_FLAGS})
303     set(CMAKE_REQUIRED_FLAGS "${CMAKE_REQUIRED_FLAGS} -std=c++11 -Werror=non-virtual-dtor")
304     CHECK_CXX_SOURCE_COMPILES("class base {public: virtual void anchor();protected: ~base();};
305                                class derived final : public base { public: ~derived();};
306                                int main() { return 0; }"
307                               CXX_WONT_WARN_ON_FINAL_NONVIRTUALDTOR)
308     set(CMAKE_REQUIRED_FLAGS ${OLD_CMAKE_REQUIRED_FLAGS})
309     append_if(CXX_WONT_WARN_ON_FINAL_NONVIRTUALDTOR
310               "-Wnon-virtual-dtor" CMAKE_CXX_FLAGS)
312     # Check if -Wcomment is OK with an // comment ending with '\' if the next
313     # line is also a // comment.
314     set(OLD_CMAKE_REQUIRED_FLAGS ${CMAKE_REQUIRED_FLAGS})
315     set(CMAKE_REQUIRED_FLAGS "${CMAKE_REQUIRED_FLAGS} -Werror -Wcomment")
316     CHECK_C_SOURCE_COMPILES("// \\\\\\n//\\nint main() {return 0;}"
317                             C_WCOMMENT_ALLOWS_LINE_WRAP)
318     set(CMAKE_REQUIRED_FLAGS ${OLD_CMAKE_REQUIRED_FLAGS})
319     if (NOT C_WCOMMENT_ALLOWS_LINE_WRAP)
320       append("-Wno-comment" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
321     endif()
322   endif (LLVM_ENABLE_WARNINGS)
323   append_if(LLVM_ENABLE_WERROR "-Werror" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
324   if (NOT LLVM_ENABLE_TIMESTAMPS)
325     add_flag_if_supported("-Werror=date-time" WERROR_DATE_TIME)
326   endif ()
327   if (LLVM_ENABLE_CXX1Y)
328     check_cxx_compiler_flag("-std=c++1y" CXX_SUPPORTS_CXX1Y)
329     append_if(CXX_SUPPORTS_CXX1Y "-std=c++1y" CMAKE_CXX_FLAGS)
330   else()
331     check_cxx_compiler_flag("-std=c++11" CXX_SUPPORTS_CXX11)
332     if (CXX_SUPPORTS_CXX11)
333       if (CYGWIN OR MINGW)
334         # MinGW and Cygwin are a bit stricter and lack things like
335         # 'strdup', 'stricmp', etc in c++11 mode.
336         append("-std=gnu++11" CMAKE_CXX_FLAGS)
337       else()
338         append("-std=c++11" CMAKE_CXX_FLAGS)
339       endif()
340     else()
341       message(FATAL_ERROR "LLVM requires C++11 support but the '-std=c++11' flag isn't supported.")
342     endif()
343   endif()
344   if (LLVM_ENABLE_MODULES)
345     set(OLD_CMAKE_REQUIRED_FLAGS ${CMAKE_REQUIRED_FLAGS})
346     set(CMAKE_REQUIRED_FLAGS "${CMAKE_REQUIRED_FLAGS} -fmodules -fcxx-modules")
347     # Check that we can build code with modules enabled, and that repeatedly
348     # including <cassert> still manages to respect NDEBUG properly.
349     CHECK_CXX_SOURCE_COMPILES("#undef NDEBUG
350                                #include <cassert>
351                                #define NDEBUG
352                                #include <cassert>
353                                int main() { assert(this code is not compiled); }"
354                                CXX_SUPPORTS_MODULES)
355     set(CMAKE_REQUIRED_FLAGS ${OLD_CMAKE_REQUIRED_FLAGS})
356     if (CXX_SUPPORTS_MODULES)
357       append_if(CXX_SUPPORTS_MODULES "-fmodules" CMAKE_C_FLAGS)
358       append_if(CXX_SUPPORTS_MODULES "-fmodules -fcxx-modules" CMAKE_CXX_FLAGS)
359     else()
360       message(FATAL_ERROR "LLVM_ENABLE_MODULES is not supported by this compiler")
361     endif()
362   endif(LLVM_ENABLE_MODULES)
363 endif( MSVC )
365 macro(append_common_sanitizer_flags)
366   # Append -fno-omit-frame-pointer and turn on debug info to get better
367   # stack traces.
368   add_flag_if_supported("-fno-omit-frame-pointer" FNO_OMIT_FRAME_POINTER)
369   if (NOT uppercase_CMAKE_BUILD_TYPE STREQUAL "DEBUG" AND
370       NOT uppercase_CMAKE_BUILD_TYPE STREQUAL "RELWITHDEBINFO")
371     add_flag_if_supported("-gline-tables-only" GLINE_TABLES_ONLY)
372   endif()
373   # Use -O1 even in debug mode, otherwise sanitizers slowdown is too large.
374   if (uppercase_CMAKE_BUILD_TYPE STREQUAL "DEBUG")
375     add_flag_if_supported("-O1" O1)
376   endif()
377 endmacro()
379 # Turn on sanitizers if necessary.
380 if(LLVM_USE_SANITIZER)
381   if (LLVM_ON_UNIX)
382     if (LLVM_USE_SANITIZER STREQUAL "Address")
383       append_common_sanitizer_flags()
384       append("-fsanitize=address" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
385     elseif (LLVM_USE_SANITIZER MATCHES "Memory(WithOrigins)?")
386       append_common_sanitizer_flags()
387       append("-fsanitize=memory" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
388       if(LLVM_USE_SANITIZER STREQUAL "MemoryWithOrigins")
389         append("-fsanitize-memory-track-origins" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
390       endif()
391     elseif (LLVM_USE_SANITIZER STREQUAL "Undefined")
392       append_common_sanitizer_flags()
393       append("-fsanitize=undefined -fno-sanitize=vptr,function -fno-sanitize-recover"
394               CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
395     elseif (LLVM_USE_SANITIZER STREQUAL "Thread")
396       append_common_sanitizer_flags()
397       append("-fsanitize=thread" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
398     else()
399       message(WARNING "Unsupported value of LLVM_USE_SANITIZER: ${LLVM_USE_SANITIZER}")
400     endif()
401   else()
402     message(WARNING "LLVM_USE_SANITIZER is not supported on this platform.")
403   endif()
404 endif()
406 # Turn on -gsplit-dwarf if requested
407 if(LLVM_USE_SPLIT_DWARF)
408   add_definitions("-gsplit-dwarf")
409 endif()
411 add_llvm_definitions( -D__STDC_CONSTANT_MACROS )
412 add_llvm_definitions( -D__STDC_FORMAT_MACROS )
413 add_llvm_definitions( -D__STDC_LIMIT_MACROS )
415 # clang doesn't print colored diagnostics when invoked from Ninja
416 if (UNIX AND
417     CMAKE_CXX_COMPILER_ID STREQUAL "Clang" AND
418     CMAKE_GENERATOR STREQUAL "Ninja")
419   append("-fcolor-diagnostics" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
420 endif()
422 # Add flags for add_dead_strip().
423 # FIXME: With MSVS, consider compiling with /Gy and linking with /OPT:REF?
424 # But MinSizeRel seems to add that automatically, so maybe disable these
425 # flags instead if LLVM_NO_DEAD_STRIP is set.
426 if(NOT CYGWIN AND NOT WIN32)
427   if(NOT ${CMAKE_SYSTEM_NAME} MATCHES "Darwin")
428     check_c_compiler_flag("-Werror -fno-function-sections" C_SUPPORTS_FNO_FUNCTION_SECTIONS)
429     if (C_SUPPORTS_FNO_FUNCTION_SECTIONS)
430       # Don't add -ffunction-section if it can be disabled with -fno-function-sections.
431       # Doing so will break sanitizers.
432       add_flag_if_supported("-ffunction-sections" FFUNCTION_SECTIONS)
433     endif()
434     add_flag_if_supported("-fdata-sections" FDATA_SECTIONS)
435   endif()
436 endif()
438 if(CYGWIN OR MINGW)
439   # Prune --out-implib from executables. It doesn't make sense even
440   # with --export-all-symbols.
441   string(REGEX REPLACE "-Wl,--out-implib,[^ ]+ " " "
442     CMAKE_C_LINK_EXECUTABLE "${CMAKE_C_LINK_EXECUTABLE}")
443   string(REGEX REPLACE "-Wl,--out-implib,[^ ]+ " " "
444     CMAKE_CXX_LINK_EXECUTABLE "${CMAKE_CXX_LINK_EXECUTABLE}")
445 endif()
447 if(MSVC)
448   # Remove flags here, for exceptions and RTTI.
449   # Each target property or source property should be responsible to control
450   # them.
451   # CL.EXE complains to override flags like "/GR /GR-".
452   string(REGEX REPLACE "(^| ) */EH[-cs]+ *( |$)" "\\1 \\2" CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS}")
453   string(REGEX REPLACE "(^| ) */GR-? *( |$)" "\\1 \\2" CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS}")
454 endif()
456 # Provide public options to globally control RTTI and EH
457 option(LLVM_ENABLE_EH "Enable Exception handling" OFF)
458 option(LLVM_ENABLE_RTTI "Enable run time type information" OFF)
459 if(LLVM_ENABLE_EH AND NOT LLVM_ENABLE_RTTI)
460   message(FATAL_ERROR "Exception handling requires RTTI. You must set LLVM_ENABLE_RTTI to ON")
461 endif()
463 # Plugin support
464 # FIXME: Make this configurable.
465 if(WIN32 OR CYGWIN)
466   if(BUILD_SHARED_LIBS)
467     set(LLVM_ENABLE_PLUGINS ON)
468   else()
469     set(LLVM_ENABLE_PLUGINS OFF)
470   endif()
471 else()
472   set(LLVM_ENABLE_PLUGINS ON)
473 endif()