1 # This CMake module is responsible for interpreting the user defined LLVM_
2 # options and executing the appropriate CMake commands to realize the users'
3 # selections.
5 include(AddLLVMDefinitions)
6 include(CheckCCompilerFlag)
7 include(CheckCXXCompilerFlag)
9 if( CMAKE_COMPILER_IS_GNUCXX )
10 set(LLVM_COMPILER_IS_GCC_COMPATIBLE ON)
11 elseif( "${CMAKE_CXX_COMPILER_ID}" MATCHES "Clang" )
12 set(LLVM_COMPILER_IS_GCC_COMPATIBLE ON)
13 endif()
15 if( LLVM_ENABLE_ASSERTIONS )
16 # MSVC doesn't like _DEBUG on release builds. See PR 4379.
17 if( NOT MSVC )
18 add_definitions( -D_DEBUG )
19 endif()
20 # On non-Debug builds cmake automatically defines NDEBUG, so we
21 # explicitly undefine it:
22 if( NOT uppercase_CMAKE_BUILD_TYPE STREQUAL "DEBUG" )
23 add_definitions( -UNDEBUG )
24 # Also remove /D NDEBUG to avoid MSVC warnings about conflicting defines.
25 string (REGEX REPLACE "(^| )[/-]D *NDEBUG($| )" " "
26 CMAKE_CXX_FLAGS_RELEASE "${CMAKE_CXX_FLAGS_RELEASE}")
27 endif()
28 else()
29 if( NOT uppercase_CMAKE_BUILD_TYPE STREQUAL "RELEASE" )
30 if( NOT MSVC_IDE AND NOT XCODE )
31 add_definitions( -DNDEBUG )
32 endif()
33 endif()
34 endif()
36 if(WIN32)
37 if(CYGWIN)
38 set(LLVM_ON_WIN32 0)
39 set(LLVM_ON_UNIX 1)
40 else(CYGWIN)
41 set(LLVM_ON_WIN32 1)
42 set(LLVM_ON_UNIX 0)
43 endif(CYGWIN)
44 set(LTDL_SHLIB_EXT ".dll")
45 set(EXEEXT ".exe")
46 # Maximum path length is 160 for non-unicode paths
47 set(MAXPATHLEN 160)
48 else(WIN32)
49 if(UNIX)
50 set(LLVM_ON_WIN32 0)
51 set(LLVM_ON_UNIX 1)
52 if(APPLE)
53 set(LTDL_SHLIB_EXT ".dylib")
54 else(APPLE)
55 set(LTDL_SHLIB_EXT ".so")
56 endif(APPLE)
57 set(EXEEXT "")
58 # FIXME: Maximum path length is currently set to 'safe' fixed value
59 set(MAXPATHLEN 2024)
60 else(UNIX)
61 MESSAGE(SEND_ERROR "Unable to determine platform")
62 endif(UNIX)
63 endif(WIN32)
65 function(add_flag_or_print_warning flag)
66 check_c_compiler_flag(${flag} C_SUPPORTS_FLAG)
67 check_cxx_compiler_flag(${flag} CXX_SUPPORTS_FLAG)
68 if (C_SUPPORTS_FLAG AND CXX_SUPPORTS_FLAG)
69 message(STATUS "Building with ${flag}")
70 set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} ${flag}" PARENT_SCOPE)
71 set(CMAKE_C_FLAGS "${CMAKE_C_FLAGS} ${flag}" PARENT_SCOPE)
72 else()
73 message(WARNING "${flag} is not supported.")
74 endif()
75 endfunction()
77 function(append value)
78 foreach(variable ${ARGN})
79 set(${variable} "${${variable}} ${value}" PARENT_SCOPE)
80 endforeach(variable)
81 endfunction()
83 function(append_if condition value)
84 if (${condition})
85 foreach(variable ${ARGN})
86 set(${variable} "${${variable}} ${value}" PARENT_SCOPE)
87 endforeach(variable)
88 endif()
89 endfunction()
91 macro(add_flag_if_supported flag)
92 check_c_compiler_flag(${flag} C_SUPPORTS_FLAG)
93 append_if(C_SUPPORTS_FLAG "${flag}" CMAKE_C_FLAGS)
94 check_cxx_compiler_flag(${flag} CXX_SUPPORTS_FLAG)
95 append_if(CXX_SUPPORTS_FLAG "${flag}" CMAKE_CXX_FLAGS)
96 endmacro()
98 if( LLVM_ENABLE_PIC )
99 if( XCODE )
100 # Xcode has -mdynamic-no-pic on by default, which overrides -fPIC. I don't
101 # know how to disable this, so just force ENABLE_PIC off for now.
102 message(WARNING "-fPIC not supported with Xcode.")
103 elseif( WIN32 OR CYGWIN)
104 # On Windows all code is PIC. MinGW warns if -fPIC is used.
105 else()
106 add_flag_or_print_warning("-fPIC")
108 if( WIN32 OR CYGWIN)
109 # MinGW warns if -fvisibility-inlines-hidden is used.
110 else()
111 check_cxx_compiler_flag("-fvisibility-inlines-hidden" SUPPORTS_FVISIBILITY_INLINES_HIDDEN_FLAG)
112 append_if(SUPPORTS_FVISIBILITY_INLINES_HIDDEN_FLAG "-fvisibility-inlines-hidden" CMAKE_CXX_FLAGS)
113 endif()
114 endif()
115 endif()
117 if( CMAKE_SIZEOF_VOID_P EQUAL 8 AND NOT WIN32 )
118 # TODO: support other platforms and toolchains.
119 if( LLVM_BUILD_32_BITS )
120 message(STATUS "Building 32 bits executables and libraries.")
121 add_llvm_definitions( -m32 )
122 set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -m32")
123 set(CMAKE_SHARED_LINKER_FLAGS "${CMAKE_SHARED_LINKER_FLAGS} -m32")
124 set(CMAKE_MODULE_LINKER_FLAGS "${CMAKE_MODULE_LINKER_FLAGS} -m32")
125 endif( LLVM_BUILD_32_BITS )
126 endif( CMAKE_SIZEOF_VOID_P EQUAL 8 AND NOT WIN32 )
128 # On Win32 using MS tools, provide an option to set the number of parallel jobs
129 # to use.
130 if( MSVC_IDE )
131 set(LLVM_COMPILER_JOBS "0" CACHE STRING
132 "Number of parallel compiler jobs. 0 means use all processors. Default is 0.")
133 if( NOT LLVM_COMPILER_JOBS STREQUAL "1" )
134 if( LLVM_COMPILER_JOBS STREQUAL "0" )
135 add_llvm_definitions( /MP )
136 else()
137 if (MSVC10)
138 message(FATAL_ERROR
139 "Due to a bug in CMake only 0 and 1 is supported for "
140 "LLVM_COMPILER_JOBS when generating for Visual Studio 2010")
141 else()
142 message(STATUS "Number of parallel compiler jobs set to " ${LLVM_COMPILER_JOBS})
143 add_llvm_definitions( /MP${LLVM_COMPILER_JOBS} )
144 endif()
145 endif()
146 else()
147 message(STATUS "Parallel compilation disabled")
148 endif()
149 endif()
151 if( MSVC )
152 include(ChooseMSVCCRT)
154 if( MSVC11 )
155 add_llvm_definitions(-D_VARIADIC_MAX=10)
156 endif()
158 # Add definitions that make MSVC much less annoying.
159 add_llvm_definitions(
160 # For some reason MS wants to deprecate a bunch of standard functions...
161 -D_CRT_SECURE_NO_DEPRECATE
162 -D_CRT_SECURE_NO_WARNINGS
163 -D_CRT_NONSTDC_NO_DEPRECATE
164 -D_CRT_NONSTDC_NO_WARNINGS
165 -D_SCL_SECURE_NO_DEPRECATE
166 -D_SCL_SECURE_NO_WARNINGS
168 # Disabled warnings.
169 -wd4146 # Suppress 'unary minus operator applied to unsigned type, result still unsigned'
170 -wd4180 # Suppress 'qualifier applied to function type has no meaning; ignored'
171 -wd4181 # Suppress 'qualifier applied to reference type; ignored'
172 -wd4244 # Suppress ''argument' : conversion from 'type1' to 'type2', possible loss of data'
173 -wd4267 # Suppress ''var' : conversion from 'size_t' to 'type', possible loss of data'
174 -wd4275 # Suppress 'An exported class was derived from a class that was not exported.'
175 -wd4345 # Suppress 'behavior change: an object of POD type constructed with an initializer of the form () will be default-initialized'
176 -wd4351 # Suppress 'new behavior: elements of array 'array' will be default initialized'
177 -wd4355 # Suppress ''this' : used in base member initializer list'
178 -wd4503 # Suppress ''identifier' : decorated name length exceeded, name was truncated'
179 -wd4551 # Suppress 'function call missing argument list'
180 -wd4624 # Suppress ''derived class' : destructor could not be generated because a base class destructor is inaccessible'
181 -wd4800 # Suppress ''type' : forcing value to bool 'true' or 'false' (performance warning)'
183 # Promoted warnings.
184 -w14062 # Promote 'enumerator in switch of enum is not handled' to level 1 warning.
186 # Promoted warnings to errors.
187 -we4238 # Promote 'nonstandard extension used : class rvalue used as lvalue' to error.
188 )
190 # Enable warnings
191 if (LLVM_ENABLE_WARNINGS)
192 add_llvm_definitions( /W4 )
193 if (LLVM_ENABLE_PEDANTIC)
194 # No MSVC equivalent available
195 endif (LLVM_ENABLE_PEDANTIC)
196 endif (LLVM_ENABLE_WARNINGS)
197 if (LLVM_ENABLE_WERROR)
198 add_llvm_definitions( /WX )
199 endif (LLVM_ENABLE_WERROR)
200 elseif( LLVM_COMPILER_IS_GCC_COMPATIBLE )
201 if (LLVM_ENABLE_WARNINGS)
202 append("-Wall -W -Wno-unused-parameter -Wwrite-strings" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
204 # Turn off missing field initializer warnings for gcc to avoid noise from
205 # false positives with empty {}. Turn them on otherwise (they're off by
206 # default for clang).
207 check_cxx_compiler_flag("-Wmissing-field-initializers" CXX_SUPPORTS_MISSING_FIELD_INITIALIZERS_FLAG)
208 if (CXX_SUPPORTS_MISSING_FIELD_INITIALIZERS_FLAG)
209 if (CMAKE_COMPILER_IS_GNUCXX)
210 append("-Wno-missing-field-initializers" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
211 else()
212 append("-Wmissing-field-initializers" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
213 endif()
214 endif()
216 append_if(LLVM_ENABLE_PEDANTIC "-pedantic -Wno-long-long" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
217 check_cxx_compiler_flag("-Werror -Wcovered-switch-default" CXX_SUPPORTS_COVERED_SWITCH_DEFAULT_FLAG)
218 append_if(CXX_SUPPORTS_COVERED_SWITCH_DEFAULT_FLAG "-Wcovered-switch-default" CMAKE_CXX_FLAGS)
219 check_c_compiler_flag("-Werror -Wcovered-switch-default" C_SUPPORTS_COVERED_SWITCH_DEFAULT_FLAG)
220 append_if(C_SUPPORTS_COVERED_SWITCH_DEFAULT_FLAG "-Wcovered-switch-default" CMAKE_C_FLAGS)
221 append_if(USE_NO_UNINITIALIZED "-Wno-uninitialized" CMAKE_CXX_FLAGS)
222 append_if(USE_NO_MAYBE_UNINITIALIZED "-Wno-maybe-uninitialized" CMAKE_CXX_FLAGS)
223 check_cxx_compiler_flag("-Werror -Wnon-virtual-dtor" CXX_SUPPORTS_NON_VIRTUAL_DTOR_FLAG)
224 append_if(CXX_SUPPORTS_NON_VIRTUAL_DTOR_FLAG "-Wnon-virtual-dtor" CMAKE_CXX_FLAGS)
225 endif (LLVM_ENABLE_WARNINGS)
226 if (LLVM_ENABLE_WERROR)
227 add_llvm_definitions( -Werror )
228 endif (LLVM_ENABLE_WERROR)
229 endif( MSVC )
231 macro(append_common_sanitizer_flags)
232 # Append -fno-omit-frame-pointer and turn on debug info to get better
233 # stack traces.
234 add_flag_if_supported("-fno-omit-frame-pointer")
235 if (NOT uppercase_CMAKE_BUILD_TYPE STREQUAL "DEBUG" AND
236 NOT uppercase_CMAKE_BUILD_TYPE STREQUAL "RELWITHDEBINFO")
237 add_flag_if_supported("-gline-tables-only")
238 endif()
239 endmacro()
241 # Turn on sanitizers if necessary.
242 if(LLVM_USE_SANITIZER)
243 if (LLVM_ON_UNIX)
244 if (LLVM_USE_SANITIZER STREQUAL "Address")
245 append_common_sanitizer_flags()
246 add_flag_or_print_warning("-fsanitize=address")
247 elseif (LLVM_USE_SANITIZER MATCHES "Memory(WithOrigins)?")
248 append_common_sanitizer_flags()
249 add_flag_or_print_warning("-fsanitize=memory")
250 if(LLVM_USE_SANITIZER STREQUAL "MemoryWithOrigins")
251 add_flag_or_print_warning("-fsanitize-memory-track-origins")
252 endif()
253 else()
254 message(WARNING "Unsupported value of LLVM_USE_SANITIZER: ${LLVM_USE_SANITIZER}")
255 endif()
256 else()
257 message(WARNING "LLVM_USE_SANITIZER is not supported on this platform.")
258 endif()
259 endif()
261 add_llvm_definitions( -D__STDC_CONSTANT_MACROS )
262 add_llvm_definitions( -D__STDC_FORMAT_MACROS )
263 add_llvm_definitions( -D__STDC_LIMIT_MACROS )
265 # clang doesn't print colored diagnostics when invoked from Ninja
266 if (UNIX AND
267 CMAKE_CXX_COMPILER_ID STREQUAL "Clang" AND
268 CMAKE_GENERATOR STREQUAL "Ninja")
269 append("-fcolor-diagnostics" CMAKE_C_FLAGS CMAKE_CXX_FLAGS)
270 endif()