1 //===--- StringMap.h - String Hash table map interface ----------*- C++ -*-===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file defines the StringMap class.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef LLVM_ADT_STRINGMAP_H
15 #define LLVM_ADT_STRINGMAP_H
17 #include "llvm/Support/Allocator.h"
18 #include <cstring>
19 #include <string>
21 namespace llvm {
22 template<typename ValueT>
23 class StringMapConstIterator;
24 template<typename ValueT>
25 class StringMapIterator;
26 template<typename ValueTy>
27 class StringMapEntry;
29 /// StringMapEntryInitializer - This datatype can be partially specialized for
30 /// various datatypes in a stringmap to allow them to be initialized when an
31 /// entry is default constructed for the map.
32 template<typename ValueTy>
33 class StringMapEntryInitializer {
34 public:
35 template <typename InitTy>
36 static void Initialize(StringMapEntry<ValueTy> &T, InitTy InitVal) {
37 }
38 };
41 /// StringMapEntryBase - Shared base class of StringMapEntry instances.
42 class StringMapEntryBase {
43 unsigned StrLen;
44 public:
45 explicit StringMapEntryBase(unsigned Len) : StrLen(Len) {}
47 unsigned getKeyLength() const { return StrLen; }
48 };
50 /// StringMapImpl - This is the base class of StringMap that is shared among
51 /// all of its instantiations.
52 class StringMapImpl {
53 public:
54 /// ItemBucket - The hash table consists of an array of these. If Item is
55 /// non-null, this is an extant entry, otherwise, it is a hole.
56 struct ItemBucket {
57 /// FullHashValue - This remembers the full hash value of the key for
58 /// easy scanning.
59 unsigned FullHashValue;
61 /// Item - This is a pointer to the actual item object.
62 StringMapEntryBase *Item;
63 };
65 protected:
66 ItemBucket *TheTable;
67 unsigned NumBuckets;
68 unsigned NumItems;
69 unsigned NumTombstones;
70 unsigned ItemSize;
71 protected:
72 explicit StringMapImpl(unsigned itemSize) : ItemSize(itemSize) {
73 // Initialize the map with zero buckets to allocation.
74 TheTable = 0;
75 NumBuckets = 0;
76 NumItems = 0;
77 NumTombstones = 0;
78 }
79 StringMapImpl(unsigned InitSize, unsigned ItemSize);
80 void RehashTable();
82 /// ShouldRehash - Return true if the table should be rehashed after a new
83 /// element was recently inserted.
84 bool ShouldRehash() const {
85 // If the hash table is now more than 3/4 full, or if fewer than 1/8 of
86 // the buckets are empty (meaning that many are filled with tombstones),
87 // grow the table.
88 return NumItems*4 > NumBuckets*3 ||
89 NumBuckets-(NumItems+NumTombstones) < NumBuckets/8;
90 }
92 /// LookupBucketFor - Look up the bucket that the specified string should end
93 /// up in. If it already exists as a key in the map, the Item pointer for the
94 /// specified bucket will be non-null. Otherwise, it will be null. In either
95 /// case, the FullHashValue field of the bucket will be set to the hash value
96 /// of the string.
97 unsigned LookupBucketFor(const char *KeyStart, const char *KeyEnd);
99 /// FindKey - Look up the bucket that contains the specified key. If it exists
100 /// in the map, return the bucket number of the key. Otherwise return -1.
101 /// This does not modify the map.
102 int FindKey(const char *KeyStart, const char *KeyEnd) const;
104 /// RemoveKey - Remove the specified StringMapEntry from the table, but do not
105 /// delete it. This aborts if the value isn't in the table.
106 void RemoveKey(StringMapEntryBase *V);
108 /// RemoveKey - Remove the StringMapEntry for the specified key from the
109 /// table, returning it. If the key is not in the table, this returns null.
110 StringMapEntryBase *RemoveKey(const char *KeyStart, const char *KeyEnd);
111 private:
112 void init(unsigned Size);
113 public:
114 static StringMapEntryBase *getTombstoneVal() {
115 return (StringMapEntryBase*)-1;
116 }
118 unsigned getNumBuckets() const { return NumBuckets; }
119 unsigned getNumItems() const { return NumItems; }
121 bool empty() const { return NumItems == 0; }
122 unsigned size() const { return NumItems; }
123 };
125 /// StringMapEntry - This is used to represent one value that is inserted into
126 /// a StringMap. It contains the Value itself and the key: the string length
127 /// and data.
128 template<typename ValueTy>
129 class StringMapEntry : public StringMapEntryBase {
130 public:
131 ValueTy second;
133 explicit StringMapEntry(unsigned StrLen)
134 : StringMapEntryBase(StrLen), second() {}
135 StringMapEntry(unsigned StrLen, const ValueTy &V)
136 : StringMapEntryBase(StrLen), second(V) {}
138 const ValueTy &getValue() const { return second; }
139 ValueTy &getValue() { return second; }
141 void setValue(const ValueTy &V) { second = V; }
143 /// getKeyData - Return the start of the string data that is the key for this
144 /// value. The string data is always stored immediately after the
145 /// StringMapEntry object.
146 const char *getKeyData() const {return reinterpret_cast<const char*>(this+1);}
148 const char *first() const { return getKeyData(); }
150 /// Create - Create a StringMapEntry for the specified key and default
151 /// construct the value.
152 template<typename AllocatorTy, typename InitType>
153 static StringMapEntry *Create(const char *KeyStart, const char *KeyEnd,
154 AllocatorTy &Allocator,
155 InitType InitVal) {
156 unsigned KeyLength = static_cast<unsigned>(KeyEnd-KeyStart);
158 // Okay, the item doesn't already exist, and 'Bucket' is the bucket to fill
159 // in. Allocate a new item with space for the string at the end and a null
160 // terminator.
162 unsigned AllocSize = static_cast<unsigned>(sizeof(StringMapEntry))+
163 KeyLength+1;
164 unsigned Alignment = alignof<StringMapEntry>();
166 StringMapEntry *NewItem =
167 static_cast<StringMapEntry*>(Allocator.Allocate(AllocSize,Alignment));
169 // Default construct the value.
170 new (NewItem) StringMapEntry(KeyLength);
172 // Copy the string information.
173 char *StrBuffer = const_cast<char*>(NewItem->getKeyData());
174 memcpy(StrBuffer, KeyStart, KeyLength);
175 StrBuffer[KeyLength] = 0; // Null terminate for convenience of clients.
177 // Initialize the value if the client wants to.
178 StringMapEntryInitializer<ValueTy>::Initialize(*NewItem, InitVal);
179 return NewItem;
180 }
182 template<typename AllocatorTy>
183 static StringMapEntry *Create(const char *KeyStart, const char *KeyEnd,
184 AllocatorTy &Allocator) {
185 return Create(KeyStart, KeyEnd, Allocator, (void*)0);
186 }
189 /// Create - Create a StringMapEntry with normal malloc/free.
190 template<typename InitType>
191 static StringMapEntry *Create(const char *KeyStart, const char *KeyEnd,
192 InitType InitVal) {
193 MallocAllocator A;
194 return Create(KeyStart, KeyEnd, A, InitVal);
195 }
197 static StringMapEntry *Create(const char *KeyStart, const char *KeyEnd) {
198 return Create(KeyStart, KeyEnd, (void*)0);
199 }
201 /// GetStringMapEntryFromValue - Given a value that is known to be embedded
202 /// into a StringMapEntry, return the StringMapEntry itself.
203 static StringMapEntry &GetStringMapEntryFromValue(ValueTy &V) {
204 StringMapEntry *EPtr = 0;
205 char *Ptr = reinterpret_cast<char*>(&V) -
206 (reinterpret_cast<char*>(&EPtr->second) -
207 reinterpret_cast<char*>(EPtr));
208 return *reinterpret_cast<StringMapEntry*>(Ptr);
209 }
210 static const StringMapEntry &GetStringMapEntryFromValue(const ValueTy &V) {
211 return GetStringMapEntryFromValue(const_cast<ValueTy&>(V));
212 }
214 /// Destroy - Destroy this StringMapEntry, releasing memory back to the
215 /// specified allocator.
216 template<typename AllocatorTy>
217 void Destroy(AllocatorTy &Allocator) {
218 // Free memory referenced by the item.
219 this->~StringMapEntry();
220 Allocator.Deallocate(this);
221 }
223 /// Destroy this object, releasing memory back to the malloc allocator.
224 void Destroy() {
225 MallocAllocator A;
226 Destroy(A);
227 }
228 };
231 /// StringMap - This is an unconventional map that is specialized for handling
232 /// keys that are "strings", which are basically ranges of bytes. This does some
233 /// funky memory allocation and hashing things to make it extremely efficient,
234 /// storing the string data *after* the value in the map.
235 template<typename ValueTy, typename AllocatorTy = MallocAllocator>
236 class StringMap : public StringMapImpl {
237 AllocatorTy Allocator;
238 typedef StringMapEntry<ValueTy> MapEntryTy;
239 public:
240 StringMap() : StringMapImpl(static_cast<unsigned>(sizeof(MapEntryTy))) {}
241 explicit StringMap(unsigned InitialSize)
242 : StringMapImpl(InitialSize, static_cast<unsigned>(sizeof(MapEntryTy))) {}
244 AllocatorTy &getAllocator() { return Allocator; }
245 const AllocatorTy &getAllocator() const { return Allocator; }
247 typedef const char* key_type;
248 typedef ValueTy mapped_type;
249 typedef StringMapEntry<ValueTy> value_type;
250 typedef size_t size_type;
252 typedef StringMapConstIterator<ValueTy> const_iterator;
253 typedef StringMapIterator<ValueTy> iterator;
255 iterator begin() {
256 return iterator(TheTable, NumBuckets == 0);
257 }
258 iterator end() {
259 return iterator(TheTable+NumBuckets, true);
260 }
261 const_iterator begin() const {
262 return const_iterator(TheTable, NumBuckets == 0);
263 }
264 const_iterator end() const {
265 return const_iterator(TheTable+NumBuckets, true);
266 }
268 iterator find(const char *KeyStart, const char *KeyEnd) {
269 int Bucket = FindKey(KeyStart, KeyEnd);
270 if (Bucket == -1) return end();
271 return iterator(TheTable+Bucket);
272 }
273 iterator find(const char *Key) {
274 return find(Key, Key + strlen(Key));
275 }
276 iterator find(const std::string &Key) {
277 const char* key_start = (Key.empty() ? NULL : &Key[0]);
278 return find(key_start, key_start + Key.size());
279 }
281 const_iterator find(const char *KeyStart, const char *KeyEnd) const {
282 int Bucket = FindKey(KeyStart, KeyEnd);
283 if (Bucket == -1) return end();
284 return const_iterator(TheTable+Bucket);
285 }
286 const_iterator find(const char *Key) const {
287 return find(Key, Key + strlen(Key));
288 }
289 const_iterator find(const std::string &Key) const {
290 const char* key_start = (Key.empty() ? NULL : &Key[0]);
291 return find(key_start, key_start + Key.size());
292 }
294 ValueTy& operator[](const char *Key) {
295 value_type& entry = GetOrCreateValue(Key, Key + strlen(Key));
296 return entry.getValue();
297 }
298 ValueTy& operator[](const std::string &Key) {
299 const char* key_start = (Key.empty() ? NULL : &Key[0]);
300 value_type& entry = GetOrCreateValue(key_start, key_start + Key.size());
301 return entry.getValue();
302 }
304 size_type count(const char *KeyStart, const char *KeyEnd) const {
305 return find(KeyStart, KeyEnd) == end() ? 0 : 1;
306 }
307 size_type count(const char *Key) const {
308 return count(Key, Key + strlen(Key));
309 }
310 size_type count(const std::string &Key) const {
311 const char* key_start = (Key.empty() ? NULL : &Key[0]);
312 return count(key_start, key_start + Key.size());
313 }
315 /// insert - Insert the specified key/value pair into the map. If the key
316 /// already exists in the map, return false and ignore the request, otherwise
317 /// insert it and return true.
318 bool insert(MapEntryTy *KeyValue) {
319 unsigned BucketNo =
320 LookupBucketFor(KeyValue->getKeyData(),
321 KeyValue->getKeyData()+KeyValue->getKeyLength());
322 ItemBucket &Bucket = TheTable[BucketNo];
323 if (Bucket.Item && Bucket.Item != getTombstoneVal())
324 return false; // Already exists in map.
326 if (Bucket.Item == getTombstoneVal())
327 --NumTombstones;
328 Bucket.Item = KeyValue;
329 ++NumItems;
331 if (ShouldRehash())
332 RehashTable();
333 return true;
334 }
336 /// GetOrCreateValue - Look up the specified key in the table. If a value
337 /// exists, return it. Otherwise, default construct a value, insert it, and
338 /// return.
339 template <typename InitTy>
340 StringMapEntry<ValueTy> &GetOrCreateValue(const char *KeyStart,
341 const char *KeyEnd,
342 InitTy Val) {
343 unsigned BucketNo = LookupBucketFor(KeyStart, KeyEnd);
344 ItemBucket &Bucket = TheTable[BucketNo];
345 if (Bucket.Item && Bucket.Item != getTombstoneVal())
346 return *static_cast<MapEntryTy*>(Bucket.Item);
348 MapEntryTy *NewItem = MapEntryTy::Create(KeyStart, KeyEnd, Allocator, Val);
350 if (Bucket.Item == getTombstoneVal())
351 --NumTombstones;
352 ++NumItems;
354 // Fill in the bucket for the hash table. The FullHashValue was already
355 // filled in by LookupBucketFor.
356 Bucket.Item = NewItem;
358 if (ShouldRehash())
359 RehashTable();
360 return *NewItem;
361 }
363 StringMapEntry<ValueTy> &GetOrCreateValue(const char *KeyStart,
364 const char *KeyEnd) {
365 return GetOrCreateValue(KeyStart, KeyEnd, (void*)0);
366 }
368 /// remove - Remove the specified key/value pair from the map, but do not
369 /// erase it. This aborts if the key is not in the map.
370 void remove(MapEntryTy *KeyValue) {
371 RemoveKey(KeyValue);
372 }
374 void erase(iterator I) {
375 MapEntryTy &V = *I;
376 remove(&V);
377 V.Destroy(Allocator);
378 }
380 bool erase(const char *Key) {
381 iterator I = find(Key);
382 if (I == end()) return false;
383 erase(I);
384 return true;
385 }
387 bool erase(std::string Key) {
388 iterator I = find(Key);
389 if (I == end()) return false;
390 erase(I);
391 return true;
392 }
394 ~StringMap() {
395 for (ItemBucket *I = TheTable, *E = TheTable+NumBuckets; I != E; ++I) {
396 if (I->Item && I->Item != getTombstoneVal())
397 static_cast<MapEntryTy*>(I->Item)->Destroy(Allocator);
398 }
399 free(TheTable);
400 }
401 private:
402 StringMap(const StringMap &); // FIXME: Implement.
403 void operator=(const StringMap &); // FIXME: Implement.
404 };
407 template<typename ValueTy>
408 class StringMapConstIterator {
409 protected:
410 StringMapImpl::ItemBucket *Ptr;
411 public:
412 explicit StringMapConstIterator(StringMapImpl::ItemBucket *Bucket,
413 bool NoAdvance = false)
414 : Ptr(Bucket) {
415 if (!NoAdvance) AdvancePastEmptyBuckets();
416 }
418 const StringMapEntry<ValueTy> &operator*() const {
419 return *static_cast<StringMapEntry<ValueTy>*>(Ptr->Item);
420 }
421 const StringMapEntry<ValueTy> *operator->() const {
422 return static_cast<StringMapEntry<ValueTy>*>(Ptr->Item);
423 }
425 bool operator==(const StringMapConstIterator &RHS) const {
426 return Ptr == RHS.Ptr;
427 }
428 bool operator!=(const StringMapConstIterator &RHS) const {
429 return Ptr != RHS.Ptr;
430 }
432 inline StringMapConstIterator& operator++() { // Preincrement
433 ++Ptr;
434 AdvancePastEmptyBuckets();
435 return *this;
436 }
437 StringMapConstIterator operator++(int) { // Postincrement
438 StringMapConstIterator tmp = *this; ++*this; return tmp;
439 }
441 private:
442 void AdvancePastEmptyBuckets() {
443 while (Ptr->Item == 0 || Ptr->Item == StringMapImpl::getTombstoneVal())
444 ++Ptr;
445 }
446 };
448 template<typename ValueTy>
449 class StringMapIterator : public StringMapConstIterator<ValueTy> {
450 public:
451 explicit StringMapIterator(StringMapImpl::ItemBucket *Bucket,
452 bool NoAdvance = false)
453 : StringMapConstIterator<ValueTy>(Bucket, NoAdvance) {
454 }
455 StringMapEntry<ValueTy> &operator*() const {
456 return *static_cast<StringMapEntry<ValueTy>*>(this->Ptr->Item);
457 }
458 StringMapEntry<ValueTy> *operator->() const {
459 return static_cast<StringMapEntry<ValueTy>*>(this->Ptr->Item);
460 }
461 };
463 }
465 #endif