1 //===--- StringMap.h - String Hash table map interface ----------*- C++ -*-===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file was developed by Chris Lattner and is distributed under
6 // the University of Illinois Open Source License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file defines the StringMap class.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef LLVM_ADT_STRINGMAP_H
15 #define LLVM_ADT_STRINGMAP_H
17 #include "llvm/Support/Allocator.h"
18 #include <cstring>
20 namespace llvm {
21 template<typename ValueT>
22 class StringMapConstIterator;
23 template<typename ValueT>
24 class StringMapIterator;
27 /// StringMapEntryBase - Shared base class of StringMapEntry instances.
28 class StringMapEntryBase {
29 unsigned StrLen;
30 public:
31 StringMapEntryBase(unsigned Len) : StrLen(Len) {}
33 unsigned getKeyLength() const { return StrLen; }
34 };
36 /// StringMapImpl - This is the base class of StringMap that is shared among
37 /// all of its instantiations.
38 class StringMapImpl {
39 public:
40 /// ItemBucket - The hash table consists of an array of these. If Item is
41 /// non-null, this is an extant entry, otherwise, it is a hole.
42 struct ItemBucket {
43 /// FullHashValue - This remembers the full hash value of the key for
44 /// easy scanning.
45 unsigned FullHashValue;
47 /// Item - This is a pointer to the actual item object.
48 StringMapEntryBase *Item;
49 };
51 protected:
52 ItemBucket *TheTable;
53 unsigned NumBuckets;
54 unsigned NumItems;
55 unsigned ItemSize;
56 protected:
57 StringMapImpl(unsigned InitSize, unsigned ItemSize);
58 void RehashTable();
60 /// LookupBucketFor - Look up the bucket that the specified string should end
61 /// up in. If it already exists as a key in the map, the Item pointer for the
62 /// specified bucket will be non-null. Otherwise, it will be null. In either
63 /// case, the FullHashValue field of the bucket will be set to the hash value
64 /// of the string.
65 unsigned LookupBucketFor(const char *KeyStart, const char *KeyEnd);
67 /// FindKey - Look up the bucket that contains the specified key. If it exists
68 /// in the map, return the bucket number of the key. Otherwise return -1.
69 /// This does not modify the map.
70 int FindKey(const char *KeyStart, const char *KeyEnd) const;
72 public:
73 static StringMapEntryBase *getTombstoneVal() {
74 return (StringMapEntryBase*)-1;
75 }
77 unsigned getNumBuckets() const { return NumBuckets; }
78 unsigned getNumItems() const { return NumItems; }
80 bool empty() const { return NumItems == 0; }
81 unsigned size() const { return NumItems; }
82 };
84 /// StringMapEntry - This is used to represent one value that is inserted into
85 /// a StringMap. It contains the Value itself and the key: the string length
86 /// and data.
87 template<typename ValueTy>
88 class StringMapEntry : public StringMapEntryBase {
89 ValueTy Val;
90 public:
91 StringMapEntry(unsigned StrLen)
92 : StringMapEntryBase(StrLen), Val() {}
93 StringMapEntry(unsigned StrLen, const ValueTy &V)
94 : StringMapEntryBase(StrLen), Val(V) {}
96 const ValueTy &getValue() const { return Val; }
97 ValueTy &getValue() { return Val; }
99 void setValue(const ValueTy &V) { Val = V; }
101 /// getKeyData - Return the start of the string data that is the key for this
102 /// value. The string data is always stored immediately after the
103 /// StringMapEntry object.
104 const char *getKeyData() const {return reinterpret_cast<const char*>(this+1);}
106 /// Create - Create a StringMapEntry for the specified key and default
107 /// construct the value.
108 template<typename AllocatorTy>
109 static StringMapEntry *Create(const char *KeyStart, const char *KeyEnd,
110 AllocatorTy &Allocator) {
111 unsigned KeyLength = KeyEnd-KeyStart;
113 // Okay, the item doesn't already exist, and 'Bucket' is the bucket to fill
114 // in. Allocate a new item with space for the string at the end and a null
115 // terminator.
116 unsigned AllocSize = sizeof(StringMapEntry)+KeyLength+1;
118 #ifdef __GNUC__
119 unsigned Alignment = __alignof__(StringMapEntry);
120 #else
121 // FIXME: ugly.
122 unsigned Alignment = 8;
123 #endif
124 StringMapEntry *NewItem =
125 static_cast<StringMapEntry*>(Allocator.Allocate(AllocSize, Alignment));
127 // Default construct the value.
128 new (NewItem) StringMapEntry(KeyLength);
130 // Copy the string information.
131 char *StrBuffer = const_cast<char*>(NewItem->getKeyData());
132 memcpy(StrBuffer, KeyStart, KeyLength);
133 StrBuffer[KeyLength] = 0; // Null terminate for convenience of clients.
134 return NewItem;
135 }
137 /// Create - Create a StringMapEntry with normal malloc/free.
138 static StringMapEntry *Create(const char *KeyStart, const char *KeyEnd) {
139 MallocAllocator A;
140 return Create(KeyStart, KeyEnd, A);
141 }
143 /// Destroy - Destroy this StringMapEntry, releasing memory back to the
144 /// specified allocator.
145 template<typename AllocatorTy>
146 void Destroy(AllocatorTy &Allocator) {
147 // Free memory referenced by the item.
148 this->~StringMapEntry();
149 Allocator.Deallocate(this);
150 }
152 /// Destroy this object, releasing memory back to the malloc allocator.
153 void Destroy() {
154 MallocAllocator A;
155 Destroy(A);
156 }
157 };
160 /// StringMap - This is an unconventional map that is specialized for handling
161 /// keys that are "strings", which are basically ranges of bytes. This does some
162 /// funky memory allocation and hashing things to make it extremely efficient,
163 /// storing the string data *after* the value in the map.
164 template<typename ValueTy, typename AllocatorTy = MallocAllocator>
165 class StringMap : public StringMapImpl {
166 AllocatorTy Allocator;
167 typedef StringMapEntry<ValueTy> MapEntryTy;
168 public:
169 StringMap(unsigned InitialSize = 0)
170 : StringMapImpl(InitialSize, sizeof(MapEntryTy)) {}
172 AllocatorTy &getAllocator() { return Allocator; }
173 const AllocatorTy &getAllocator() const { return Allocator; }
175 typedef StringMapConstIterator<ValueTy> const_iterator;
176 typedef StringMapIterator<ValueTy> iterator;
178 iterator begin() { return iterator(TheTable); }
179 iterator end() { return iterator(TheTable+NumBuckets); }
180 const_iterator begin() const { return const_iterator(TheTable); }
181 const_iterator end() const { return const_iterator(TheTable+NumBuckets); }
184 iterator find(const char *KeyStart, const char *KeyEnd) {
185 int Bucket = FindKey(KeyStart, KeyEnd);
186 if (Bucket == -1) return end();
187 return iterator(TheTable+Bucket);
188 }
190 const_iterator find(const char *KeyStart, const char *KeyEnd) const {
191 int Bucket = FindKey(KeyStart, KeyEnd);
192 if (Bucket == -1) return end();
193 return const_iterator(TheTable+Bucket);
194 }
196 /// GetOrCreateValue - Look up the specified key in the table. If a value
197 /// exists, return it. Otherwise, default construct a value, insert it, and
198 /// return.
199 StringMapEntry<ValueTy> &GetOrCreateValue(const char *KeyStart,
200 const char *KeyEnd) {
201 unsigned BucketNo = LookupBucketFor(KeyStart, KeyEnd);
202 ItemBucket &Bucket = TheTable[BucketNo];
203 if (Bucket.Item)
204 return *static_cast<MapEntryTy*>(Bucket.Item);
206 MapEntryTy *NewItem = MapEntryTy::Create(KeyStart, KeyEnd, Allocator);
207 ++NumItems;
209 // Fill in the bucket for the hash table. The FullHashValue was already
210 // filled in by LookupBucketFor.
211 Bucket.Item = NewItem;
213 // If the hash table is now more than 3/4 full, rehash into a larger table.
214 if (NumItems > NumBuckets*3/4)
215 RehashTable();
216 return *NewItem;
217 }
219 ~StringMap() {
220 for (ItemBucket *I = TheTable, *E = TheTable+NumBuckets; I != E; ++I) {
221 if (MapEntryTy *Id = static_cast<MapEntryTy*>(I->Item))
222 Id->Destroy(Allocator);
223 }
224 delete [] TheTable;
225 }
226 };
229 template<typename ValueTy>
230 class StringMapConstIterator {
231 StringMapImpl::ItemBucket *Ptr;
232 public:
233 StringMapConstIterator(StringMapImpl::ItemBucket *Bucket) : Ptr(Bucket) {
234 AdvancePastEmptyBuckets();
235 }
237 const StringMapEntry<ValueTy> &operator*() const {
238 return *static_cast<StringMapEntry<ValueTy>*>(Ptr->Item);
239 }
240 const StringMapEntry<ValueTy> *operator->() const {
241 return static_cast<StringMapEntry<ValueTy>*>(Ptr->Item);
242 }
244 bool operator==(const StringMapConstIterator &RHS) const {
245 return Ptr == RHS.Ptr;
246 }
247 bool operator!=(const StringMapConstIterator &RHS) const {
248 return Ptr != RHS.Ptr;
249 }
251 inline StringMapConstIterator& operator++() { // Preincrement
252 ++Ptr;
253 AdvancePastEmptyBuckets();
254 return *this;
255 }
256 StringMapConstIterator operator++(int) { // Postincrement
257 StringMapConstIterator tmp = *this; ++*this; return tmp;
258 }
260 private:
261 void AdvancePastEmptyBuckets() {
262 while (Ptr->Item == 0 || Ptr->Item == StringMapImpl::getTombstoneVal())
263 ++Ptr;
264 }
265 };
267 template<typename ValueTy>
268 class StringMapIterator : public StringMapConstIterator<ValueTy> {
269 public:
270 StringMapIterator(StringMapImpl::ItemBucket *Bucket)
271 : StringMapConstIterator<ValueTy>(Bucket) {
272 }
273 StringMapEntry<ValueTy> &operator*() const {
274 return *static_cast<StringMapEntry<ValueTy>*>(this->Ptr->Item);
275 }
276 StringMapEntry<ValueTy> *operator->() const {
277 return static_cast<StringMapEntry<ValueTy>*>(this->Ptr->Item);
278 }
279 };
281 }
283 #endif