1 //===-- LiveIntervalAnalysis.h - Live Interval Analysis ---------*- C++ -*-===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements the LiveInterval analysis pass. Given some numbering of
11 // each the machine instructions (in this implemention depth-first order) an
12 // interval [i, j) is said to be a live interval for register v if there is no
13 // instruction with number j' > j such that v is live at j' and there is no
14 // instruction with number i' < i such that v is live at i'. In this
15 // implementation intervals can have holes, i.e. an interval might look like
16 // [1,20), [50,65), [1000,1001).
17 //
18 //===----------------------------------------------------------------------===//
20 #ifndef LLVM_CODEGEN_LIVEINTERVAL_ANALYSIS_H
21 #define LLVM_CODEGEN_LIVEINTERVAL_ANALYSIS_H
23 #include "llvm/ADT/IndexedMap.h"
24 #include "llvm/ADT/SmallVector.h"
25 #include "llvm/CodeGen/LiveInterval.h"
26 #include "llvm/CodeGen/MachineBasicBlock.h"
27 #include "llvm/CodeGen/MachineFunctionPass.h"
28 #include "llvm/CodeGen/SlotIndexes.h"
29 #include "llvm/Support/Allocator.h"
30 #include "llvm/Target/TargetRegisterInfo.h"
31 #include <cmath>
32 #include <iterator>
34 namespace llvm {
36 class AliasAnalysis;
37 class BitVector;
38 class BlockFrequency;
39 class LiveRangeCalc;
40 class LiveVariables;
41 class MachineDominatorTree;
42 class MachineLoopInfo;
43 class TargetRegisterInfo;
44 class MachineRegisterInfo;
45 class TargetInstrInfo;
46 class TargetRegisterClass;
47 class VirtRegMap;
49 class LiveIntervals : public MachineFunctionPass {
50 MachineFunction* MF;
51 MachineRegisterInfo* MRI;
52 const TargetMachine* TM;
53 const TargetRegisterInfo* TRI;
54 const TargetInstrInfo* TII;
55 AliasAnalysis *AA;
56 SlotIndexes* Indexes;
57 MachineDominatorTree *DomTree;
58 LiveRangeCalc *LRCalc;
60 /// Special pool allocator for VNInfo's (LiveInterval val#).
61 ///
62 VNInfo::Allocator VNInfoAllocator;
64 /// Live interval pointers for all the virtual registers.
65 IndexedMap<LiveInterval*, VirtReg2IndexFunctor> VirtRegIntervals;
67 /// RegMaskSlots - Sorted list of instructions with register mask operands.
68 /// Always use the 'r' slot, RegMasks are normal clobbers, not early
69 /// clobbers.
70 SmallVector<SlotIndex, 8> RegMaskSlots;
72 /// RegMaskBits - This vector is parallel to RegMaskSlots, it holds a
73 /// pointer to the corresponding register mask. This pointer can be
74 /// recomputed as:
75 ///
76 /// MI = Indexes->getInstructionFromIndex(RegMaskSlot[N]);
77 /// unsigned OpNum = findRegMaskOperand(MI);
78 /// RegMaskBits[N] = MI->getOperand(OpNum).getRegMask();
79 ///
80 /// This is kept in a separate vector partly because some standard
81 /// libraries don't support lower_bound() with mixed objects, partly to
82 /// improve locality when searching in RegMaskSlots.
83 /// Also see the comment in LiveInterval::find().
84 SmallVector<const uint32_t*, 8> RegMaskBits;
86 /// For each basic block number, keep (begin, size) pairs indexing into the
87 /// RegMaskSlots and RegMaskBits arrays.
88 /// Note that basic block numbers may not be layout contiguous, that's why
89 /// we can't just keep track of the first register mask in each basic
90 /// block.
91 SmallVector<std::pair<unsigned, unsigned>, 8> RegMaskBlocks;
93 /// RegUnitIntervals - Keep a live interval for each register unit as a way
94 /// of tracking fixed physreg interference.
95 SmallVector<LiveInterval*, 0> RegUnitIntervals;
97 public:
98 static char ID; // Pass identification, replacement for typeid
99 LiveIntervals();
100 virtual ~LiveIntervals();
102 // Calculate the spill weight to assign to a single instruction.
103 static float getSpillWeight(bool isDef, bool isUse, BlockFrequency freq);
105 LiveInterval &getInterval(unsigned Reg) {
106 if (hasInterval(Reg))
107 return *VirtRegIntervals[Reg];
108 else
109 return createAndComputeVirtRegInterval(Reg);
110 }
112 const LiveInterval &getInterval(unsigned Reg) const {
113 return const_cast<LiveIntervals*>(this)->getInterval(Reg);
114 }
116 bool hasInterval(unsigned Reg) const {
117 return VirtRegIntervals.inBounds(Reg) && VirtRegIntervals[Reg];
118 }
120 // Interval creation.
121 LiveInterval &createEmptyInterval(unsigned Reg) {
122 assert(!hasInterval(Reg) && "Interval already exists!");
123 VirtRegIntervals.grow(Reg);
124 VirtRegIntervals[Reg] = createInterval(Reg);
125 return *VirtRegIntervals[Reg];
126 }
128 LiveInterval &createAndComputeVirtRegInterval(unsigned Reg) {
129 LiveInterval &LI = createEmptyInterval(Reg);
130 computeVirtRegInterval(&LI);
131 return LI;
132 }
134 // Interval removal.
135 void removeInterval(unsigned Reg) {
136 delete VirtRegIntervals[Reg];
137 VirtRegIntervals[Reg] = 0;
138 }
140 /// addLiveRangeToEndOfBlock - Given a register and an instruction,
141 /// adds a live range from that instruction to the end of its MBB.
142 LiveRange addLiveRangeToEndOfBlock(unsigned reg,
143 MachineInstr* startInst);
145 /// shrinkToUses - After removing some uses of a register, shrink its live
146 /// range to just the remaining uses. This method does not compute reaching
147 /// defs for new uses, and it doesn't remove dead defs.
148 /// Dead PHIDef values are marked as unused.
149 /// New dead machine instructions are added to the dead vector.
150 /// Return true if the interval may have been separated into multiple
151 /// connected components.
152 bool shrinkToUses(LiveInterval *li,
153 SmallVectorImpl<MachineInstr*> *dead = 0);
155 /// extendToIndices - Extend the live range of LI to reach all points in
156 /// Indices. The points in the Indices array must be jointly dominated by
157 /// existing defs in LI. PHI-defs are added as needed to maintain SSA form.
158 ///
159 /// If a SlotIndex in Indices is the end index of a basic block, LI will be
160 /// extended to be live out of the basic block.
161 ///
162 /// See also LiveRangeCalc::extend().
163 void extendToIndices(LiveInterval *LI, ArrayRef<SlotIndex> Indices);
165 /// pruneValue - If an LI value is live at Kill, prune its live range by
166 /// removing any liveness reachable from Kill. Add live range end points to
167 /// EndPoints such that extendToIndices(LI, EndPoints) will reconstruct the
168 /// value's live range.
169 ///
170 /// Calling pruneValue() and extendToIndices() can be used to reconstruct
171 /// SSA form after adding defs to a virtual register.
172 void pruneValue(LiveInterval *LI, SlotIndex Kill,
173 SmallVectorImpl<SlotIndex> *EndPoints);
175 SlotIndexes *getSlotIndexes() const {
176 return Indexes;
177 }
179 AliasAnalysis *getAliasAnalysis() const {
180 return AA;
181 }
183 /// isNotInMIMap - returns true if the specified machine instr has been
184 /// removed or was never entered in the map.
185 bool isNotInMIMap(const MachineInstr* Instr) const {
186 return !Indexes->hasIndex(Instr);
187 }
189 /// Returns the base index of the given instruction.
190 SlotIndex getInstructionIndex(const MachineInstr *instr) const {
191 return Indexes->getInstructionIndex(instr);
192 }
194 /// Returns the instruction associated with the given index.
195 MachineInstr* getInstructionFromIndex(SlotIndex index) const {
196 return Indexes->getInstructionFromIndex(index);
197 }
199 /// Return the first index in the given basic block.
200 SlotIndex getMBBStartIdx(const MachineBasicBlock *mbb) const {
201 return Indexes->getMBBStartIdx(mbb);
202 }
204 /// Return the last index in the given basic block.
205 SlotIndex getMBBEndIdx(const MachineBasicBlock *mbb) const {
206 return Indexes->getMBBEndIdx(mbb);
207 }
209 bool isLiveInToMBB(const LiveInterval &li,
210 const MachineBasicBlock *mbb) const {
211 return li.liveAt(getMBBStartIdx(mbb));
212 }
214 bool isLiveOutOfMBB(const LiveInterval &li,
215 const MachineBasicBlock *mbb) const {
216 return li.liveAt(getMBBEndIdx(mbb).getPrevSlot());
217 }
219 MachineBasicBlock* getMBBFromIndex(SlotIndex index) const {
220 return Indexes->getMBBFromIndex(index);
221 }
223 void insertMBBInMaps(MachineBasicBlock *MBB) {
224 Indexes->insertMBBInMaps(MBB);
225 assert(unsigned(MBB->getNumber()) == RegMaskBlocks.size() &&
226 "Blocks must be added in order.");
227 RegMaskBlocks.push_back(std::make_pair(RegMaskSlots.size(), 0));
228 }
230 SlotIndex InsertMachineInstrInMaps(MachineInstr *MI) {
231 return Indexes->insertMachineInstrInMaps(MI);
232 }
234 void InsertMachineInstrRangeInMaps(MachineBasicBlock::iterator B,
235 MachineBasicBlock::iterator E) {
236 for (MachineBasicBlock::iterator I = B; I != E; ++I)
237 Indexes->insertMachineInstrInMaps(I);
238 }
240 void RemoveMachineInstrFromMaps(MachineInstr *MI) {
241 Indexes->removeMachineInstrFromMaps(MI);
242 }
244 void ReplaceMachineInstrInMaps(MachineInstr *MI, MachineInstr *NewMI) {
245 Indexes->replaceMachineInstrInMaps(MI, NewMI);
246 }
248 bool findLiveInMBBs(SlotIndex Start, SlotIndex End,
249 SmallVectorImpl<MachineBasicBlock*> &MBBs) const {
250 return Indexes->findLiveInMBBs(Start, End, MBBs);
251 }
253 VNInfo::Allocator& getVNInfoAllocator() { return VNInfoAllocator; }
255 virtual void getAnalysisUsage(AnalysisUsage &AU) const;
256 virtual void releaseMemory();
258 /// runOnMachineFunction - pass entry point
259 virtual bool runOnMachineFunction(MachineFunction&);
261 /// print - Implement the dump method.
262 virtual void print(raw_ostream &O, const Module* = 0) const;
264 /// intervalIsInOneMBB - If LI is confined to a single basic block, return
265 /// a pointer to that block. If LI is live in to or out of any block,
266 /// return NULL.
267 MachineBasicBlock *intervalIsInOneMBB(const LiveInterval &LI) const;
269 /// Returns true if VNI is killed by any PHI-def values in LI.
270 /// This may conservatively return true to avoid expensive computations.
271 bool hasPHIKill(const LiveInterval &LI, const VNInfo *VNI) const;
273 /// addKillFlags - Add kill flags to any instruction that kills a virtual
274 /// register.
275 void addKillFlags(const VirtRegMap*);
277 /// handleMove - call this method to notify LiveIntervals that
278 /// instruction 'mi' has been moved within a basic block. This will update
279 /// the live intervals for all operands of mi. Moves between basic blocks
280 /// are not supported.
281 ///
282 /// \param UpdateFlags Update live intervals for nonallocatable physregs.
283 void handleMove(MachineInstr* MI, bool UpdateFlags = false);
285 /// moveIntoBundle - Update intervals for operands of MI so that they
286 /// begin/end on the SlotIndex for BundleStart.
287 ///
288 /// \param UpdateFlags Update live intervals for nonallocatable physregs.
289 ///
290 /// Requires MI and BundleStart to have SlotIndexes, and assumes
291 /// existing liveness is accurate. BundleStart should be the first
292 /// instruction in the Bundle.
293 void handleMoveIntoBundle(MachineInstr* MI, MachineInstr* BundleStart,
294 bool UpdateFlags = false);
296 /// repairIntervalsInRange - Update live intervals for instructions in a
297 /// range of iterators. It is intended for use after target hooks that may
298 /// insert or remove instructions, and is only efficient for a small number
299 /// of instructions.
300 ///
301 /// OrigRegs is a vector of registers that were originally used by the
302 /// instructions in the range between the two iterators.
303 ///
304 /// Currently, the only only changes that are supported are simple removal
305 /// and addition of uses.
306 void repairIntervalsInRange(MachineBasicBlock *MBB,
307 MachineBasicBlock::iterator Begin,
308 MachineBasicBlock::iterator End,
309 ArrayRef<unsigned> OrigRegs);
311 // Register mask functions.
312 //
313 // Machine instructions may use a register mask operand to indicate that a
314 // large number of registers are clobbered by the instruction. This is
315 // typically used for calls.
316 //
317 // For compile time performance reasons, these clobbers are not recorded in
318 // the live intervals for individual physical registers. Instead,
319 // LiveIntervalAnalysis maintains a sorted list of instructions with
320 // register mask operands.
322 /// getRegMaskSlots - Returns a sorted array of slot indices of all
323 /// instructions with register mask operands.
324 ArrayRef<SlotIndex> getRegMaskSlots() const { return RegMaskSlots; }
326 /// getRegMaskSlotsInBlock - Returns a sorted array of slot indices of all
327 /// instructions with register mask operands in the basic block numbered
328 /// MBBNum.
329 ArrayRef<SlotIndex> getRegMaskSlotsInBlock(unsigned MBBNum) const {
330 std::pair<unsigned, unsigned> P = RegMaskBlocks[MBBNum];
331 return getRegMaskSlots().slice(P.first, P.second);
332 }
334 /// getRegMaskBits() - Returns an array of register mask pointers
335 /// corresponding to getRegMaskSlots().
336 ArrayRef<const uint32_t*> getRegMaskBits() const { return RegMaskBits; }
338 /// getRegMaskBitsInBlock - Returns an array of mask pointers corresponding
339 /// to getRegMaskSlotsInBlock(MBBNum).
340 ArrayRef<const uint32_t*> getRegMaskBitsInBlock(unsigned MBBNum) const {
341 std::pair<unsigned, unsigned> P = RegMaskBlocks[MBBNum];
342 return getRegMaskBits().slice(P.first, P.second);
343 }
345 /// checkRegMaskInterference - Test if LI is live across any register mask
346 /// instructions, and compute a bit mask of physical registers that are not
347 /// clobbered by any of them.
348 ///
349 /// Returns false if LI doesn't cross any register mask instructions. In
350 /// that case, the bit vector is not filled in.
351 bool checkRegMaskInterference(LiveInterval &LI,
352 BitVector &UsableRegs);
354 // Register unit functions.
355 //
356 // Fixed interference occurs when MachineInstrs use physregs directly
357 // instead of virtual registers. This typically happens when passing
358 // arguments to a function call, or when instructions require operands in
359 // fixed registers.
360 //
361 // Each physreg has one or more register units, see MCRegisterInfo. We
362 // track liveness per register unit to handle aliasing registers more
363 // efficiently.
365 /// getRegUnit - Return the live range for Unit.
366 /// It will be computed if it doesn't exist.
367 LiveInterval &getRegUnit(unsigned Unit) {
368 LiveInterval *LI = RegUnitIntervals[Unit];
369 if (!LI) {
370 // Compute missing ranges on demand.
371 RegUnitIntervals[Unit] = LI = new LiveInterval(Unit, HUGE_VALF);
372 computeRegUnitInterval(LI);
373 }
374 return *LI;
375 }
377 /// getCachedRegUnit - Return the live range for Unit if it has already
378 /// been computed, or NULL if it hasn't been computed yet.
379 LiveInterval *getCachedRegUnit(unsigned Unit) {
380 return RegUnitIntervals[Unit];
381 }
383 const LiveInterval *getCachedRegUnit(unsigned Unit) const {
384 return RegUnitIntervals[Unit];
385 }
387 private:
388 /// Compute live intervals for all virtual registers.
389 void computeVirtRegs();
391 /// Compute RegMaskSlots and RegMaskBits.
392 void computeRegMasks();
394 static LiveInterval* createInterval(unsigned Reg);
396 void printInstrs(raw_ostream &O) const;
397 void dumpInstrs() const;
399 void computeLiveInRegUnits();
400 void computeRegUnitInterval(LiveInterval*);
401 void computeVirtRegInterval(LiveInterval*);
403 class HMEditor;
404 };
405 } // End llvm namespace
407 #endif