1 //===-- llvm/CodeGen/MachineInstr.h - MachineInstr class --------*- C++ -*-===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains the declaration of the MachineInstr class, which is the
11 // basic representation for all target dependent machine instructions used by
12 // the back end.
13 //
14 //===----------------------------------------------------------------------===//
16 #ifndef LLVM_CODEGEN_MACHINEINSTR_H
17 #define LLVM_CODEGEN_MACHINEINSTR_H
19 #include "llvm/CodeGen/MachineOperand.h"
20 #include "llvm/MC/MCInstrDesc.h"
21 #include "llvm/Target/TargetOpcodes.h"
22 #include "llvm/ADT/ArrayRef.h"
23 #include "llvm/ADT/ilist.h"
24 #include "llvm/ADT/ilist_node.h"
25 #include "llvm/ADT/STLExtras.h"
26 #include "llvm/ADT/StringRef.h"
27 #include "llvm/ADT/DenseMapInfo.h"
28 #include "llvm/Support/DebugLoc.h"
29 #include <vector>
31 namespace llvm {
33 template <typename T> class SmallVectorImpl;
34 class AliasAnalysis;
35 class TargetInstrInfo;
36 class TargetRegisterClass;
37 class TargetRegisterInfo;
38 class MachineFunction;
39 class MachineMemOperand;
41 //===----------------------------------------------------------------------===//
42 /// MachineInstr - Representation of each machine instruction.
43 ///
44 class MachineInstr : public ilist_node<MachineInstr> {
45 public:
46 typedef MachineMemOperand **mmo_iterator;
48 /// Flags to specify different kinds of comments to output in
49 /// assembly code. These flags carry semantic information not
50 /// otherwise easily derivable from the IR text.
51 ///
52 enum CommentFlag {
53 ReloadReuse = 0x1
54 };
56 enum MIFlag {
57 NoFlags = 0,
58 FrameSetup = 1 << 0, // Instruction is used as a part of
59 // function frame setup code.
60 InsideBundle = 1 << 1 // Instruction is inside a bundle (not
61 // the first MI in a bundle)
62 };
63 private:
64 const MCInstrDesc *MCID; // Instruction descriptor.
66 uint8_t Flags; // Various bits of additional
67 // information about machine
68 // instruction.
70 uint8_t AsmPrinterFlags; // Various bits of information used by
71 // the AsmPrinter to emit helpful
72 // comments. This is *not* semantic
73 // information. Do not use this for
74 // anything other than to convey comment
75 // information to AsmPrinter.
77 uint16_t NumMemRefs; // information on memory references
78 mmo_iterator MemRefs;
80 std::vector<MachineOperand> Operands; // the operands
81 MachineBasicBlock *Parent; // Pointer to the owning basic block.
82 DebugLoc debugLoc; // Source line information.
84 MachineInstr(const MachineInstr&); // DO NOT IMPLEMENT
85 void operator=(const MachineInstr&); // DO NOT IMPLEMENT
87 // Intrusive list support
88 friend struct ilist_traits<MachineInstr>;
89 friend struct ilist_traits<MachineBasicBlock>;
90 void setParent(MachineBasicBlock *P) { Parent = P; }
92 /// MachineInstr ctor - This constructor creates a copy of the given
93 /// MachineInstr in the given MachineFunction.
94 MachineInstr(MachineFunction &, const MachineInstr &);
96 /// MachineInstr ctor - This constructor creates a dummy MachineInstr with
97 /// MCID NULL and no operands.
98 MachineInstr();
100 // The next two constructors have DebugLoc and non-DebugLoc versions;
101 // over time, the non-DebugLoc versions should be phased out and eventually
102 // removed.
104 /// MachineInstr ctor - This constructor creates a MachineInstr and adds the
105 /// implicit operands. It reserves space for the number of operands specified
106 /// by the MCInstrDesc. The version with a DebugLoc should be preferred.
107 explicit MachineInstr(const MCInstrDesc &MCID, bool NoImp = false);
109 /// MachineInstr ctor - Work exactly the same as the ctor above, except that
110 /// the MachineInstr is created and added to the end of the specified basic
111 /// block. The version with a DebugLoc should be preferred.
112 MachineInstr(MachineBasicBlock *MBB, const MCInstrDesc &MCID);
114 /// MachineInstr ctor - This constructor create a MachineInstr and add the
115 /// implicit operands. It reserves space for number of operands specified by
116 /// MCInstrDesc. An explicit DebugLoc is supplied.
117 explicit MachineInstr(const MCInstrDesc &MCID, const DebugLoc dl,
118 bool NoImp = false);
120 /// MachineInstr ctor - Work exactly the same as the ctor above, except that
121 /// the MachineInstr is created and added to the end of the specified basic
122 /// block.
123 MachineInstr(MachineBasicBlock *MBB, const DebugLoc dl,
124 const MCInstrDesc &MCID);
126 ~MachineInstr();
128 // MachineInstrs are pool-allocated and owned by MachineFunction.
129 friend class MachineFunction;
131 public:
132 const MachineBasicBlock* getParent() const { return Parent; }
133 MachineBasicBlock* getParent() { return Parent; }
135 /// getAsmPrinterFlags - Return the asm printer flags bitvector.
136 ///
137 uint8_t getAsmPrinterFlags() const { return AsmPrinterFlags; }
139 /// clearAsmPrinterFlags - clear the AsmPrinter bitvector
140 ///
141 void clearAsmPrinterFlags() { AsmPrinterFlags = 0; }
143 /// getAsmPrinterFlag - Return whether an AsmPrinter flag is set.
144 ///
145 bool getAsmPrinterFlag(CommentFlag Flag) const {
146 return AsmPrinterFlags & Flag;
147 }
149 /// setAsmPrinterFlag - Set a flag for the AsmPrinter.
150 ///
151 void setAsmPrinterFlag(CommentFlag Flag) {
152 AsmPrinterFlags |= (uint8_t)Flag;
153 }
155 /// clearAsmPrinterFlag - clear specific AsmPrinter flags
156 ///
157 void clearAsmPrinterFlag(CommentFlag Flag) {
158 AsmPrinterFlags &= ~Flag;
159 }
161 /// getFlags - Return the MI flags bitvector.
162 uint8_t getFlags() const {
163 return Flags;
164 }
166 /// getFlag - Return whether an MI flag is set.
167 bool getFlag(MIFlag Flag) const {
168 return Flags & Flag;
169 }
171 /// setFlag - Set a MI flag.
172 void setFlag(MIFlag Flag) {
173 Flags |= (uint8_t)Flag;
174 }
176 void setFlags(unsigned flags) {
177 Flags = flags;
178 }
180 /// clearFlag - Clear a MI flag.
181 void clearFlag(MIFlag Flag) {
182 Flags &= ~((uint8_t)Flag);
183 }
185 /// isInsideBundle - Return true if MI is in a bundle (but not the first MI
186 /// in a bundle).
187 ///
188 /// A bundle looks like this before it's finalized:
189 /// ----------------
190 /// | MI |
191 /// ----------------
192 /// |
193 /// ----------------
194 /// | MI * |
195 /// ----------------
196 /// |
197 /// ----------------
198 /// | MI * |
199 /// ----------------
200 /// In this case, the first MI starts a bundle but is not inside a bundle, the
201 /// next 2 MIs are considered "inside" the bundle.
202 ///
203 /// After a bundle is finalized, it looks like this:
204 /// ----------------
205 /// | Bundle |
206 /// ----------------
207 /// |
208 /// ----------------
209 /// | MI * |
210 /// ----------------
211 /// |
212 /// ----------------
213 /// | MI * |
214 /// ----------------
215 /// |
216 /// ----------------
217 /// | MI * |
218 /// ----------------
219 /// The first instruction has the special opcode "BUNDLE". It's not "inside"
220 /// a bundle, but the next three MIs are.
221 bool isInsideBundle() const {
222 return getFlag(InsideBundle);
223 }
225 /// setIsInsideBundle - Set InsideBundle bit.
226 ///
227 void setIsInsideBundle(bool Val = true) {
228 if (Val)
229 setFlag(InsideBundle);
230 else
231 clearFlag(InsideBundle);
232 }
234 /// isBundled - Return true if this instruction part of a bundle. This is true
235 /// if either itself or its following instruction is marked "InsideBundle".
236 bool isBundled() const;
238 /// getDebugLoc - Returns the debug location id of this MachineInstr.
239 ///
240 DebugLoc getDebugLoc() const { return debugLoc; }
242 /// emitError - Emit an error referring to the source location of this
243 /// instruction. This should only be used for inline assembly that is somehow
244 /// impossible to compile. Other errors should have been handled much
245 /// earlier.
246 ///
247 /// If this method returns, the caller should try to recover from the error.
248 ///
249 void emitError(StringRef Msg) const;
251 /// getDesc - Returns the target instruction descriptor of this
252 /// MachineInstr.
253 const MCInstrDesc &getDesc() const { return *MCID; }
255 /// getOpcode - Returns the opcode of this MachineInstr.
256 ///
257 int getOpcode() const { return MCID->Opcode; }
259 /// Access to explicit operands of the instruction.
260 ///
261 unsigned getNumOperands() const { return (unsigned)Operands.size(); }
263 const MachineOperand& getOperand(unsigned i) const {
264 assert(i < getNumOperands() && "getOperand() out of range!");
265 return Operands[i];
266 }
267 MachineOperand& getOperand(unsigned i) {
268 assert(i < getNumOperands() && "getOperand() out of range!");
269 return Operands[i];
270 }
272 /// getNumExplicitOperands - Returns the number of non-implicit operands.
273 ///
274 unsigned getNumExplicitOperands() const;
276 /// iterator/begin/end - Iterate over all operands of a machine instruction.
277 typedef std::vector<MachineOperand>::iterator mop_iterator;
278 typedef std::vector<MachineOperand>::const_iterator const_mop_iterator;
280 mop_iterator operands_begin() { return Operands.begin(); }
281 mop_iterator operands_end() { return Operands.end(); }
283 const_mop_iterator operands_begin() const { return Operands.begin(); }
284 const_mop_iterator operands_end() const { return Operands.end(); }
286 /// Access to memory operands of the instruction
287 mmo_iterator memoperands_begin() const { return MemRefs; }
288 mmo_iterator memoperands_end() const { return MemRefs + NumMemRefs; }
289 bool memoperands_empty() const { return NumMemRefs == 0; }
291 /// hasOneMemOperand - Return true if this instruction has exactly one
292 /// MachineMemOperand.
293 bool hasOneMemOperand() const {
294 return NumMemRefs == 1;
295 }
297 /// API for querying MachineInstr properties. They are the same as MCInstrDesc
298 /// queries but they are bundle aware.
300 enum QueryType {
301 IgnoreBundle, // Ignore bundles
302 AnyInBundle, // Return true if any instruction in bundle has property
303 AllInBundle // Return true if all instructions in bundle have property
304 };
306 /// hasProperty - Return true if the instruction (or in the case of a bundle,
307 /// the instructions inside the bundle) has the specified property.
308 /// The first argument is the property being queried.
309 /// The second argument indicates whether the query should look inside
310 /// instruction bundles.
311 bool hasProperty(unsigned MCFlag, QueryType Type = AnyInBundle) const {
312 // Inline the fast path.
313 if (Type == IgnoreBundle || !isBundle())
314 return getDesc().getFlags() & (1 << MCFlag);
316 // If we have a bundle, take the slow path.
317 return hasPropertyInBundle(1 << MCFlag, Type);
318 }
320 /// isVariadic - Return true if this instruction can have a variable number of
321 /// operands. In this case, the variable operands will be after the normal
322 /// operands but before the implicit definitions and uses (if any are
323 /// present).
324 bool isVariadic(QueryType Type = IgnoreBundle) const {
325 return hasProperty(MCID::Variadic, Type);
326 }
328 /// hasOptionalDef - Set if this instruction has an optional definition, e.g.
329 /// ARM instructions which can set condition code if 's' bit is set.
330 bool hasOptionalDef(QueryType Type = IgnoreBundle) const {
331 return hasProperty(MCID::HasOptionalDef, Type);
332 }
334 /// isPseudo - Return true if this is a pseudo instruction that doesn't
335 /// correspond to a real machine instruction.
336 ///
337 bool isPseudo(QueryType Type = IgnoreBundle) const {
338 return hasProperty(MCID::Pseudo, Type);
339 }
341 bool isReturn(QueryType Type = AnyInBundle) const {
342 return hasProperty(MCID::Return, Type);
343 }
345 bool isCall(QueryType Type = AnyInBundle) const {
346 return hasProperty(MCID::Call, Type);
347 }
349 /// isBarrier - Returns true if the specified instruction stops control flow
350 /// from executing the instruction immediately following it. Examples include
351 /// unconditional branches and return instructions.
352 bool isBarrier(QueryType Type = AnyInBundle) const {
353 return hasProperty(MCID::Barrier, Type);
354 }
356 /// isTerminator - Returns true if this instruction part of the terminator for
357 /// a basic block. Typically this is things like return and branch
358 /// instructions.
359 ///
360 /// Various passes use this to insert code into the bottom of a basic block,
361 /// but before control flow occurs.
362 bool isTerminator(QueryType Type = AnyInBundle) const {
363 return hasProperty(MCID::Terminator, Type);
364 }
366 /// isBranch - Returns true if this is a conditional, unconditional, or
367 /// indirect branch. Predicates below can be used to discriminate between
368 /// these cases, and the TargetInstrInfo::AnalyzeBranch method can be used to
369 /// get more information.
370 bool isBranch(QueryType Type = AnyInBundle) const {
371 return hasProperty(MCID::Branch, Type);
372 }
374 /// isIndirectBranch - Return true if this is an indirect branch, such as a
375 /// branch through a register.
376 bool isIndirectBranch(QueryType Type = AnyInBundle) const {
377 return hasProperty(MCID::IndirectBranch, Type);
378 }
380 /// isConditionalBranch - Return true if this is a branch which may fall
381 /// through to the next instruction or may transfer control flow to some other
382 /// block. The TargetInstrInfo::AnalyzeBranch method can be used to get more
383 /// information about this branch.
384 bool isConditionalBranch(QueryType Type = AnyInBundle) const {
385 return isBranch(Type) & !isBarrier(Type) & !isIndirectBranch(Type);
386 }
388 /// isUnconditionalBranch - Return true if this is a branch which always
389 /// transfers control flow to some other block. The
390 /// TargetInstrInfo::AnalyzeBranch method can be used to get more information
391 /// about this branch.
392 bool isUnconditionalBranch(QueryType Type = AnyInBundle) const {
393 return isBranch(Type) & isBarrier(Type) & !isIndirectBranch(Type);
394 }
396 // isPredicable - Return true if this instruction has a predicate operand that
397 // controls execution. It may be set to 'always', or may be set to other
398 /// values. There are various methods in TargetInstrInfo that can be used to
399 /// control and modify the predicate in this instruction.
400 bool isPredicable(QueryType Type = AllInBundle) const {
401 // If it's a bundle than all bundled instructions must be predicable for this
402 // to return true.
403 return hasProperty(MCID::Predicable, Type);
404 }
406 /// isCompare - Return true if this instruction is a comparison.
407 bool isCompare(QueryType Type = IgnoreBundle) const {
408 return hasProperty(MCID::Compare, Type);
409 }
411 /// isMoveImmediate - Return true if this instruction is a move immediate
412 /// (including conditional moves) instruction.
413 bool isMoveImmediate(QueryType Type = IgnoreBundle) const {
414 return hasProperty(MCID::MoveImm, Type);
415 }
417 /// isBitcast - Return true if this instruction is a bitcast instruction.
418 ///
419 bool isBitcast(QueryType Type = IgnoreBundle) const {
420 return hasProperty(MCID::Bitcast, Type);
421 }
423 /// isSelect - Return true if this instruction is a select instruction.
424 ///
425 bool isSelect(QueryType Type = IgnoreBundle) const {
426 return hasProperty(MCID::Select, Type);
427 }
429 /// isNotDuplicable - Return true if this instruction cannot be safely
430 /// duplicated. For example, if the instruction has a unique labels attached
431 /// to it, duplicating it would cause multiple definition errors.
432 bool isNotDuplicable(QueryType Type = AnyInBundle) const {
433 return hasProperty(MCID::NotDuplicable, Type);
434 }
436 /// hasDelaySlot - Returns true if the specified instruction has a delay slot
437 /// which must be filled by the code generator.
438 bool hasDelaySlot(QueryType Type = AnyInBundle) const {
439 return hasProperty(MCID::DelaySlot, Type);
440 }
442 /// canFoldAsLoad - Return true for instructions that can be folded as
443 /// memory operands in other instructions. The most common use for this
444 /// is instructions that are simple loads from memory that don't modify
445 /// the loaded value in any way, but it can also be used for instructions
446 /// that can be expressed as constant-pool loads, such as V_SETALLONES
447 /// on x86, to allow them to be folded when it is beneficial.
448 /// This should only be set on instructions that return a value in their
449 /// only virtual register definition.
450 bool canFoldAsLoad(QueryType Type = IgnoreBundle) const {
451 return hasProperty(MCID::FoldableAsLoad, Type);
452 }
454 //===--------------------------------------------------------------------===//
455 // Side Effect Analysis
456 //===--------------------------------------------------------------------===//
458 /// mayLoad - Return true if this instruction could possibly read memory.
459 /// Instructions with this flag set are not necessarily simple load
460 /// instructions, they may load a value and modify it, for example.
461 bool mayLoad(QueryType Type = AnyInBundle) const {
462 return hasProperty(MCID::MayLoad, Type);
463 }
466 /// mayStore - Return true if this instruction could possibly modify memory.
467 /// Instructions with this flag set are not necessarily simple store
468 /// instructions, they may store a modified value based on their operands, or
469 /// may not actually modify anything, for example.
470 bool mayStore(QueryType Type = AnyInBundle) const {
471 return hasProperty(MCID::MayStore, Type);
472 }
474 //===--------------------------------------------------------------------===//
475 // Flags that indicate whether an instruction can be modified by a method.
476 //===--------------------------------------------------------------------===//
478 /// isCommutable - Return true if this may be a 2- or 3-address
479 /// instruction (of the form "X = op Y, Z, ..."), which produces the same
480 /// result if Y and Z are exchanged. If this flag is set, then the
481 /// TargetInstrInfo::commuteInstruction method may be used to hack on the
482 /// instruction.
483 ///
484 /// Note that this flag may be set on instructions that are only commutable
485 /// sometimes. In these cases, the call to commuteInstruction will fail.
486 /// Also note that some instructions require non-trivial modification to
487 /// commute them.
488 bool isCommutable(QueryType Type = IgnoreBundle) const {
489 return hasProperty(MCID::Commutable, Type);
490 }
492 /// isConvertibleTo3Addr - Return true if this is a 2-address instruction
493 /// which can be changed into a 3-address instruction if needed. Doing this
494 /// transformation can be profitable in the register allocator, because it
495 /// means that the instruction can use a 2-address form if possible, but
496 /// degrade into a less efficient form if the source and dest register cannot
497 /// be assigned to the same register. For example, this allows the x86
498 /// backend to turn a "shl reg, 3" instruction into an LEA instruction, which
499 /// is the same speed as the shift but has bigger code size.
500 ///
501 /// If this returns true, then the target must implement the
502 /// TargetInstrInfo::convertToThreeAddress method for this instruction, which
503 /// is allowed to fail if the transformation isn't valid for this specific
504 /// instruction (e.g. shl reg, 4 on x86).
505 ///
506 bool isConvertibleTo3Addr(QueryType Type = IgnoreBundle) const {
507 return hasProperty(MCID::ConvertibleTo3Addr, Type);
508 }
510 /// usesCustomInsertionHook - Return true if this instruction requires
511 /// custom insertion support when the DAG scheduler is inserting it into a
512 /// machine basic block. If this is true for the instruction, it basically
513 /// means that it is a pseudo instruction used at SelectionDAG time that is
514 /// expanded out into magic code by the target when MachineInstrs are formed.
515 ///
516 /// If this is true, the TargetLoweringInfo::InsertAtEndOfBasicBlock method
517 /// is used to insert this into the MachineBasicBlock.
518 bool usesCustomInsertionHook(QueryType Type = IgnoreBundle) const {
519 return hasProperty(MCID::UsesCustomInserter, Type);
520 }
522 /// hasPostISelHook - Return true if this instruction requires *adjustment*
523 /// after instruction selection by calling a target hook. For example, this
524 /// can be used to fill in ARM 's' optional operand depending on whether
525 /// the conditional flag register is used.
526 bool hasPostISelHook(QueryType Type = IgnoreBundle) const {
527 return hasProperty(MCID::HasPostISelHook, Type);
528 }
530 /// isRematerializable - Returns true if this instruction is a candidate for
531 /// remat. This flag is deprecated, please don't use it anymore. If this
532 /// flag is set, the isReallyTriviallyReMaterializable() method is called to
533 /// verify the instruction is really rematable.
534 bool isRematerializable(QueryType Type = AllInBundle) const {
535 // It's only possible to re-mat a bundle if all bundled instructions are
536 // re-materializable.
537 return hasProperty(MCID::Rematerializable, Type);
538 }
540 /// isAsCheapAsAMove - Returns true if this instruction has the same cost (or
541 /// less) than a move instruction. This is useful during certain types of
542 /// optimizations (e.g., remat during two-address conversion or machine licm)
543 /// where we would like to remat or hoist the instruction, but not if it costs
544 /// more than moving the instruction into the appropriate register. Note, we
545 /// are not marking copies from and to the same register class with this flag.
546 bool isAsCheapAsAMove(QueryType Type = AllInBundle) const {
547 // Only returns true for a bundle if all bundled instructions are cheap.
548 // FIXME: This probably requires a target hook.
549 return hasProperty(MCID::CheapAsAMove, Type);
550 }
552 /// hasExtraSrcRegAllocReq - Returns true if this instruction source operands
553 /// have special register allocation requirements that are not captured by the
554 /// operand register classes. e.g. ARM::STRD's two source registers must be an
555 /// even / odd pair, ARM::STM registers have to be in ascending order.
556 /// Post-register allocation passes should not attempt to change allocations
557 /// for sources of instructions with this flag.
558 bool hasExtraSrcRegAllocReq(QueryType Type = AnyInBundle) const {
559 return hasProperty(MCID::ExtraSrcRegAllocReq, Type);
560 }
562 /// hasExtraDefRegAllocReq - Returns true if this instruction def operands
563 /// have special register allocation requirements that are not captured by the
564 /// operand register classes. e.g. ARM::LDRD's two def registers must be an
565 /// even / odd pair, ARM::LDM registers have to be in ascending order.
566 /// Post-register allocation passes should not attempt to change allocations
567 /// for definitions of instructions with this flag.
568 bool hasExtraDefRegAllocReq(QueryType Type = AnyInBundle) const {
569 return hasProperty(MCID::ExtraDefRegAllocReq, Type);
570 }
573 enum MICheckType {
574 CheckDefs, // Check all operands for equality
575 CheckKillDead, // Check all operands including kill / dead markers
576 IgnoreDefs, // Ignore all definitions
577 IgnoreVRegDefs // Ignore virtual register definitions
578 };
580 /// isIdenticalTo - Return true if this instruction is identical to (same
581 /// opcode and same operands as) the specified instruction.
582 bool isIdenticalTo(const MachineInstr *Other,
583 MICheckType Check = CheckDefs) const;
585 /// removeFromParent - This method unlinks 'this' from the containing basic
586 /// block, and returns it, but does not delete it.
587 MachineInstr *removeFromParent();
589 /// eraseFromParent - This method unlinks 'this' from the containing basic
590 /// block and deletes it.
591 void eraseFromParent();
593 /// isLabel - Returns true if the MachineInstr represents a label.
594 ///
595 bool isLabel() const {
596 return getOpcode() == TargetOpcode::PROLOG_LABEL ||
597 getOpcode() == TargetOpcode::EH_LABEL ||
598 getOpcode() == TargetOpcode::GC_LABEL;
599 }
601 bool isPrologLabel() const {
602 return getOpcode() == TargetOpcode::PROLOG_LABEL;
603 }
604 bool isEHLabel() const { return getOpcode() == TargetOpcode::EH_LABEL; }
605 bool isGCLabel() const { return getOpcode() == TargetOpcode::GC_LABEL; }
606 bool isDebugValue() const { return getOpcode() == TargetOpcode::DBG_VALUE; }
608 bool isPHI() const { return getOpcode() == TargetOpcode::PHI; }
609 bool isKill() const { return getOpcode() == TargetOpcode::KILL; }
610 bool isImplicitDef() const { return getOpcode()==TargetOpcode::IMPLICIT_DEF; }
611 bool isInlineAsm() const { return getOpcode() == TargetOpcode::INLINEASM; }
612 bool isStackAligningInlineAsm() const;
613 bool isInsertSubreg() const {
614 return getOpcode() == TargetOpcode::INSERT_SUBREG;
615 }
616 bool isSubregToReg() const {
617 return getOpcode() == TargetOpcode::SUBREG_TO_REG;
618 }
619 bool isRegSequence() const {
620 return getOpcode() == TargetOpcode::REG_SEQUENCE;
621 }
622 bool isBundle() const {
623 return getOpcode() == TargetOpcode::BUNDLE;
624 }
625 bool isCopy() const {
626 return getOpcode() == TargetOpcode::COPY;
627 }
628 bool isFullCopy() const {
629 return isCopy() && !getOperand(0).getSubReg() && !getOperand(1).getSubReg();
630 }
632 /// isCopyLike - Return true if the instruction behaves like a copy.
633 /// This does not include native copy instructions.
634 bool isCopyLike() const {
635 return isCopy() || isSubregToReg();
636 }
638 /// isIdentityCopy - Return true is the instruction is an identity copy.
639 bool isIdentityCopy() const {
640 return isCopy() && getOperand(0).getReg() == getOperand(1).getReg() &&
641 getOperand(0).getSubReg() == getOperand(1).getSubReg();
642 }
644 /// isTransient - Return true if this is a transient instruction that is
645 /// either very likely to be eliminated during register allocation (such as
646 /// copy-like instructions), or if this instruction doesn't have an
647 /// execution-time cost.
648 bool isTransient() const {
649 switch(getOpcode()) {
650 default: return false;
651 // Copy-like instructions are usually eliminated during register allocation.
652 case TargetOpcode::PHI:
653 case TargetOpcode::COPY:
654 case TargetOpcode::INSERT_SUBREG:
655 case TargetOpcode::SUBREG_TO_REG:
656 case TargetOpcode::REG_SEQUENCE:
657 // Pseudo-instructions that don't produce any real output.
658 case TargetOpcode::IMPLICIT_DEF:
659 case TargetOpcode::KILL:
660 case TargetOpcode::PROLOG_LABEL:
661 case TargetOpcode::EH_LABEL:
662 case TargetOpcode::GC_LABEL:
663 case TargetOpcode::DBG_VALUE:
664 return true;
665 }
666 }
668 /// getBundleSize - Return the number of instructions inside the MI bundle.
669 unsigned getBundleSize() const;
671 /// readsRegister - Return true if the MachineInstr reads the specified
672 /// register. If TargetRegisterInfo is passed, then it also checks if there
673 /// is a read of a super-register.
674 /// This does not count partial redefines of virtual registers as reads:
675 /// %reg1024:6 = OP.
676 bool readsRegister(unsigned Reg, const TargetRegisterInfo *TRI = NULL) const {
677 return findRegisterUseOperandIdx(Reg, false, TRI) != -1;
678 }
680 /// readsVirtualRegister - Return true if the MachineInstr reads the specified
681 /// virtual register. Take into account that a partial define is a
682 /// read-modify-write operation.
683 bool readsVirtualRegister(unsigned Reg) const {
684 return readsWritesVirtualRegister(Reg).first;
685 }
687 /// readsWritesVirtualRegister - Return a pair of bools (reads, writes)
688 /// indicating if this instruction reads or writes Reg. This also considers
689 /// partial defines.
690 /// If Ops is not null, all operand indices for Reg are added.
691 std::pair<bool,bool> readsWritesVirtualRegister(unsigned Reg,
692 SmallVectorImpl<unsigned> *Ops = 0) const;
694 /// killsRegister - Return true if the MachineInstr kills the specified
695 /// register. If TargetRegisterInfo is passed, then it also checks if there is
696 /// a kill of a super-register.
697 bool killsRegister(unsigned Reg, const TargetRegisterInfo *TRI = NULL) const {
698 return findRegisterUseOperandIdx(Reg, true, TRI) != -1;
699 }
701 /// definesRegister - Return true if the MachineInstr fully defines the
702 /// specified register. If TargetRegisterInfo is passed, then it also checks
703 /// if there is a def of a super-register.
704 /// NOTE: It's ignoring subreg indices on virtual registers.
705 bool definesRegister(unsigned Reg, const TargetRegisterInfo *TRI=NULL) const {
706 return findRegisterDefOperandIdx(Reg, false, false, TRI) != -1;
707 }
709 /// modifiesRegister - Return true if the MachineInstr modifies (fully define
710 /// or partially define) the specified register.
711 /// NOTE: It's ignoring subreg indices on virtual registers.
712 bool modifiesRegister(unsigned Reg, const TargetRegisterInfo *TRI) const {
713 return findRegisterDefOperandIdx(Reg, false, true, TRI) != -1;
714 }
716 /// registerDefIsDead - Returns true if the register is dead in this machine
717 /// instruction. If TargetRegisterInfo is passed, then it also checks
718 /// if there is a dead def of a super-register.
719 bool registerDefIsDead(unsigned Reg,
720 const TargetRegisterInfo *TRI = NULL) const {
721 return findRegisterDefOperandIdx(Reg, true, false, TRI) != -1;
722 }
724 /// findRegisterUseOperandIdx() - Returns the operand index that is a use of
725 /// the specific register or -1 if it is not found. It further tightens
726 /// the search criteria to a use that kills the register if isKill is true.
727 int findRegisterUseOperandIdx(unsigned Reg, bool isKill = false,
728 const TargetRegisterInfo *TRI = NULL) const;
730 /// findRegisterUseOperand - Wrapper for findRegisterUseOperandIdx, it returns
731 /// a pointer to the MachineOperand rather than an index.
732 MachineOperand *findRegisterUseOperand(unsigned Reg, bool isKill = false,
733 const TargetRegisterInfo *TRI = NULL) {
734 int Idx = findRegisterUseOperandIdx(Reg, isKill, TRI);
735 return (Idx == -1) ? NULL : &getOperand(Idx);
736 }
738 /// findRegisterDefOperandIdx() - Returns the operand index that is a def of
739 /// the specified register or -1 if it is not found. If isDead is true, defs
740 /// that are not dead are skipped. If Overlap is true, then it also looks for
741 /// defs that merely overlap the specified register. If TargetRegisterInfo is
742 /// non-null, then it also checks if there is a def of a super-register.
743 /// This may also return a register mask operand when Overlap is true.
744 int findRegisterDefOperandIdx(unsigned Reg,
745 bool isDead = false, bool Overlap = false,
746 const TargetRegisterInfo *TRI = NULL) const;
748 /// findRegisterDefOperand - Wrapper for findRegisterDefOperandIdx, it returns
749 /// a pointer to the MachineOperand rather than an index.
750 MachineOperand *findRegisterDefOperand(unsigned Reg, bool isDead = false,
751 const TargetRegisterInfo *TRI = NULL) {
752 int Idx = findRegisterDefOperandIdx(Reg, isDead, false, TRI);
753 return (Idx == -1) ? NULL : &getOperand(Idx);
754 }
756 /// findFirstPredOperandIdx() - Find the index of the first operand in the
757 /// operand list that is used to represent the predicate. It returns -1 if
758 /// none is found.
759 int findFirstPredOperandIdx() const;
761 /// findInlineAsmFlagIdx() - Find the index of the flag word operand that
762 /// corresponds to operand OpIdx on an inline asm instruction. Returns -1 if
763 /// getOperand(OpIdx) does not belong to an inline asm operand group.
764 ///
765 /// If GroupNo is not NULL, it will receive the number of the operand group
766 /// containing OpIdx.
767 ///
768 /// The flag operand is an immediate that can be decoded with methods like
769 /// InlineAsm::hasRegClassConstraint().
770 ///
771 int findInlineAsmFlagIdx(unsigned OpIdx, unsigned *GroupNo = 0) const;
773 /// getRegClassConstraint - Compute the static register class constraint for
774 /// operand OpIdx. For normal instructions, this is derived from the
775 /// MCInstrDesc. For inline assembly it is derived from the flag words.
776 ///
777 /// Returns NULL if the static register classs constraint cannot be
778 /// determined.
779 ///
780 const TargetRegisterClass*
781 getRegClassConstraint(unsigned OpIdx,
782 const TargetInstrInfo *TII,
783 const TargetRegisterInfo *TRI) const;
785 /// tieOperands - Add a tie between the register operands at DefIdx and
786 /// UseIdx. The tie will cause the register allocator to ensure that the two
787 /// operands are assigned the same physical register.
788 ///
789 /// Tied operands are managed automatically for explicit operands in the
790 /// MCInstrDesc. This method is for exceptional cases like inline asm.
791 void tieOperands(unsigned DefIdx, unsigned UseIdx);
793 /// findTiedOperandIdx - Given the index of a tied register operand, find the
794 /// operand it is tied to. Defs are tied to uses and vice versa. Returns the
795 /// index of the tied operand which must exist.
796 unsigned findTiedOperandIdx(unsigned OpIdx) const;
798 /// isRegTiedToUseOperand - Given the index of a register def operand,
799 /// check if the register def is tied to a source operand, due to either
800 /// two-address elimination or inline assembly constraints. Returns the
801 /// first tied use operand index by reference if UseOpIdx is not null.
802 bool isRegTiedToUseOperand(unsigned DefOpIdx, unsigned *UseOpIdx = 0) const;
804 /// isRegTiedToDefOperand - Return true if the use operand of the specified
805 /// index is tied to an def operand. It also returns the def operand index by
806 /// reference if DefOpIdx is not null.
807 bool isRegTiedToDefOperand(unsigned UseOpIdx, unsigned *DefOpIdx = 0) const;
809 /// clearKillInfo - Clears kill flags on all operands.
810 ///
811 void clearKillInfo();
813 /// copyKillDeadInfo - Copies kill / dead operand properties from MI.
814 ///
815 void copyKillDeadInfo(const MachineInstr *MI);
817 /// copyPredicates - Copies predicate operand(s) from MI.
818 void copyPredicates(const MachineInstr *MI);
820 /// substituteRegister - Replace all occurrences of FromReg with ToReg:SubIdx,
821 /// properly composing subreg indices where necessary.
822 void substituteRegister(unsigned FromReg, unsigned ToReg, unsigned SubIdx,
823 const TargetRegisterInfo &RegInfo);
825 /// addRegisterKilled - We have determined MI kills a register. Look for the
826 /// operand that uses it and mark it as IsKill. If AddIfNotFound is true,
827 /// add a implicit operand if it's not found. Returns true if the operand
828 /// exists / is added.
829 bool addRegisterKilled(unsigned IncomingReg,
830 const TargetRegisterInfo *RegInfo,
831 bool AddIfNotFound = false);
833 /// clearRegisterKills - Clear all kill flags affecting Reg. If RegInfo is
834 /// provided, this includes super-register kills.
835 void clearRegisterKills(unsigned Reg, const TargetRegisterInfo *RegInfo);
837 /// addRegisterDead - We have determined MI defined a register without a use.
838 /// Look for the operand that defines it and mark it as IsDead. If
839 /// AddIfNotFound is true, add a implicit operand if it's not found. Returns
840 /// true if the operand exists / is added.
841 bool addRegisterDead(unsigned IncomingReg, const TargetRegisterInfo *RegInfo,
842 bool AddIfNotFound = false);
844 /// addRegisterDefined - We have determined MI defines a register. Make sure
845 /// there is an operand defining Reg.
846 void addRegisterDefined(unsigned IncomingReg,
847 const TargetRegisterInfo *RegInfo = 0);
849 /// setPhysRegsDeadExcept - Mark every physreg used by this instruction as
850 /// dead except those in the UsedRegs list.
851 ///
852 /// On instructions with register mask operands, also add implicit-def
853 /// operands for all registers in UsedRegs.
854 void setPhysRegsDeadExcept(ArrayRef<unsigned> UsedRegs,
855 const TargetRegisterInfo &TRI);
857 /// isSafeToMove - Return true if it is safe to move this instruction. If
858 /// SawStore is set to true, it means that there is a store (or call) between
859 /// the instruction's location and its intended destination.
860 bool isSafeToMove(const TargetInstrInfo *TII, AliasAnalysis *AA,
861 bool &SawStore) const;
863 /// isSafeToReMat - Return true if it's safe to rematerialize the specified
864 /// instruction which defined the specified register instead of copying it.
865 bool isSafeToReMat(const TargetInstrInfo *TII, AliasAnalysis *AA,
866 unsigned DstReg) const;
868 /// hasOrderedMemoryRef - Return true if this instruction may have an ordered
869 /// or volatile memory reference, or if the information describing the memory
870 /// reference is not available. Return false if it is known to have no
871 /// ordered or volatile memory references.
872 bool hasOrderedMemoryRef() const;
874 /// isInvariantLoad - Return true if this instruction is loading from a
875 /// location whose value is invariant across the function. For example,
876 /// loading a value from the constant pool or from the argument area of
877 /// a function if it does not change. This should only return true of *all*
878 /// loads the instruction does are invariant (if it does multiple loads).
879 bool isInvariantLoad(AliasAnalysis *AA) const;
881 /// isConstantValuePHI - If the specified instruction is a PHI that always
882 /// merges together the same virtual register, return the register, otherwise
883 /// return 0.
884 unsigned isConstantValuePHI() const;
886 /// hasUnmodeledSideEffects - Return true if this instruction has side
887 /// effects that are not modeled by mayLoad / mayStore, etc.
888 /// For all instructions, the property is encoded in MCInstrDesc::Flags
889 /// (see MCInstrDesc::hasUnmodeledSideEffects(). The only exception is
890 /// INLINEASM instruction, in which case the side effect property is encoded
891 /// in one of its operands (see InlineAsm::Extra_HasSideEffect).
892 ///
893 bool hasUnmodeledSideEffects() const;
895 /// allDefsAreDead - Return true if all the defs of this instruction are dead.
896 ///
897 bool allDefsAreDead() const;
899 /// copyImplicitOps - Copy implicit register operands from specified
900 /// instruction to this instruction.
901 void copyImplicitOps(const MachineInstr *MI);
903 //
904 // Debugging support
905 //
906 void print(raw_ostream &OS, const TargetMachine *TM = 0) const;
907 void dump() const;
909 //===--------------------------------------------------------------------===//
910 // Accessors used to build up machine instructions.
912 /// addOperand - Add the specified operand to the instruction. If it is an
913 /// implicit operand, it is added to the end of the operand list. If it is
914 /// an explicit operand it is added at the end of the explicit operand list
915 /// (before the first implicit operand).
916 void addOperand(const MachineOperand &Op);
918 /// setDesc - Replace the instruction descriptor (thus opcode) of
919 /// the current instruction with a new one.
920 ///
921 void setDesc(const MCInstrDesc &tid) { MCID = &tid; }
923 /// setDebugLoc - Replace current source information with new such.
924 /// Avoid using this, the constructor argument is preferable.
925 ///
926 void setDebugLoc(const DebugLoc dl) { debugLoc = dl; }
928 /// RemoveOperand - Erase an operand from an instruction, leaving it with one
929 /// fewer operand than it started with.
930 ///
931 void RemoveOperand(unsigned i);
933 /// addMemOperand - Add a MachineMemOperand to the machine instruction.
934 /// This function should be used only occasionally. The setMemRefs function
935 /// is the primary method for setting up a MachineInstr's MemRefs list.
936 void addMemOperand(MachineFunction &MF, MachineMemOperand *MO);
938 /// setMemRefs - Assign this MachineInstr's memory reference descriptor
939 /// list. This does not transfer ownership.
940 void setMemRefs(mmo_iterator NewMemRefs, mmo_iterator NewMemRefsEnd) {
941 MemRefs = NewMemRefs;
942 NumMemRefs = NewMemRefsEnd - NewMemRefs;
943 }
945 private:
946 /// getRegInfo - If this instruction is embedded into a MachineFunction,
947 /// return the MachineRegisterInfo object for the current function, otherwise
948 /// return null.
949 MachineRegisterInfo *getRegInfo();
951 /// untieRegOperand - Break any tie involving OpIdx.
952 void untieRegOperand(unsigned OpIdx) {
953 MachineOperand &MO = getOperand(OpIdx);
954 if (MO.isReg() && MO.isTied()) {
955 getOperand(findTiedOperandIdx(OpIdx)).TiedTo = false;
956 MO.TiedTo = false;
957 }
958 }
960 /// addImplicitDefUseOperands - Add all implicit def and use operands to
961 /// this instruction.
962 void addImplicitDefUseOperands();
964 /// RemoveRegOperandsFromUseLists - Unlink all of the register operands in
965 /// this instruction from their respective use lists. This requires that the
966 /// operands already be on their use lists.
967 void RemoveRegOperandsFromUseLists(MachineRegisterInfo&);
969 /// AddRegOperandsToUseLists - Add all of the register operands in
970 /// this instruction from their respective use lists. This requires that the
971 /// operands not be on their use lists yet.
972 void AddRegOperandsToUseLists(MachineRegisterInfo&);
974 /// hasPropertyInBundle - Slow path for hasProperty when we're dealing with a
975 /// bundle.
976 bool hasPropertyInBundle(unsigned Mask, QueryType Type) const;
977 };
979 /// MachineInstrExpressionTrait - Special DenseMapInfo traits to compare
980 /// MachineInstr* by *value* of the instruction rather than by pointer value.
981 /// The hashing and equality testing functions ignore definitions so this is
982 /// useful for CSE, etc.
983 struct MachineInstrExpressionTrait : DenseMapInfo<MachineInstr*> {
984 static inline MachineInstr *getEmptyKey() {
985 return 0;
986 }
988 static inline MachineInstr *getTombstoneKey() {
989 return reinterpret_cast<MachineInstr*>(-1);
990 }
992 static unsigned getHashValue(const MachineInstr* const &MI);
994 static bool isEqual(const MachineInstr* const &LHS,
995 const MachineInstr* const &RHS) {
996 if (RHS == getEmptyKey() || RHS == getTombstoneKey() ||
997 LHS == getEmptyKey() || LHS == getTombstoneKey())
998 return LHS == RHS;
999 return LHS->isIdenticalTo(RHS, MachineInstr::IgnoreVRegDefs);
1000 }
1001 };
1003 //===----------------------------------------------------------------------===//
1004 // Debugging Support
1006 inline raw_ostream& operator<<(raw_ostream &OS, const MachineInstr &MI) {
1007 MI.print(OS);
1008 return OS;
1009 }
1011 } // End llvm namespace
1013 #endif