]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - include/llvm/CodeGen/SelectionDAG.h
Roll out r125794 to help diagnose the llvm-gcc-i386-linux-selfhost failure.
[opencl/llvm.git] / include / llvm / CodeGen / SelectionDAG.h
1 //===-- llvm/CodeGen/SelectionDAG.h - InstSelection DAG ---------*- C++ -*-===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file declares the SelectionDAG class, and transitively defines the
11 // SDNode class and subclasses.
12 //
13 //===----------------------------------------------------------------------===//
15 #ifndef LLVM_CODEGEN_SELECTIONDAG_H
16 #define LLVM_CODEGEN_SELECTIONDAG_H
18 #include "llvm/ADT/ilist.h"
19 #include "llvm/ADT/DenseSet.h"
20 #include "llvm/ADT/StringMap.h"
21 #include "llvm/CodeGen/SelectionDAGNodes.h"
22 #include "llvm/Support/RecyclingAllocator.h"
23 #include "llvm/Target/TargetMachine.h"
24 #include <cassert>
25 #include <vector>
26 #include <map>
27 #include <string>
29 namespace llvm {
31 class AliasAnalysis;
32 class MachineConstantPoolValue;
33 class MachineFunction;
34 class MDNode;
35 class SDNodeOrdering;
36 class SDDbgValue;
37 class TargetLowering;
38 class TargetSelectionDAGInfo;
40 template<> struct ilist_traits<SDNode> : public ilist_default_traits<SDNode> {
41 private:
42   mutable ilist_half_node<SDNode> Sentinel;
43 public:
44   SDNode *createSentinel() const {
45     return static_cast<SDNode*>(&Sentinel);
46   }
47   static void destroySentinel(SDNode *) {}
49   SDNode *provideInitialHead() const { return createSentinel(); }
50   SDNode *ensureHead(SDNode*) const { return createSentinel(); }
51   static void noteHead(SDNode*, SDNode*) {}
53   static void deleteNode(SDNode *) {
54     assert(0 && "ilist_traits<SDNode> shouldn't see a deleteNode call!");
55   }
56 private:
57   static void createNode(const SDNode &);
58 };
60 /// SDDbgInfo - Keeps track of dbg_value information through SDISel.  We do
61 /// not build SDNodes for these so as not to perturb the generated code;
62 /// instead the info is kept off to the side in this structure. Each SDNode may
63 /// have one or more associated dbg_value entries. This information is kept in
64 /// DbgValMap.
65 /// Byval parameters are handled separately because they don't use alloca's,
66 /// which busts the normal mechanism.  There is good reason for handling all
67 /// parameters separately:  they may not have code generated for them, they
68 /// should always go at the beginning of the function regardless of other code
69 /// motion, and debug info for them is potentially useful even if the parameter
70 /// is unused.  Right now only byval parameters are handled separately.
71 class SDDbgInfo {
72   SmallVector<SDDbgValue*, 32> DbgValues;
73   SmallVector<SDDbgValue*, 32> ByvalParmDbgValues;
74   DenseMap<const SDNode*, SmallVector<SDDbgValue*, 2> > DbgValMap;
76   void operator=(const SDDbgInfo&);   // Do not implement.
77   SDDbgInfo(const SDDbgInfo&);   // Do not implement.
78 public:
79   SDDbgInfo() {}
81   void add(SDDbgValue *V, const SDNode *Node, bool isParameter) {
82     if (isParameter) {
83       ByvalParmDbgValues.push_back(V);
84     } else     DbgValues.push_back(V);
85     if (Node)
86       DbgValMap[Node].push_back(V);
87   }
89   void clear() {
90     DbgValMap.clear();
91     DbgValues.clear();
92     ByvalParmDbgValues.clear();
93   }
95   bool empty() const {
96     return DbgValues.empty() && ByvalParmDbgValues.empty();
97   }
99   SmallVector<SDDbgValue*,2> &getSDDbgValues(const SDNode *Node) {
100     return DbgValMap[Node];
101   }
103   void removeSDDbgValues(const SDNode *Node) {
104     DbgValMap.erase(Node);
105   }
107   typedef SmallVector<SDDbgValue*,32>::iterator DbgIterator;
108   DbgIterator DbgBegin() { return DbgValues.begin(); }
109   DbgIterator DbgEnd()   { return DbgValues.end(); }
110   DbgIterator ByvalParmDbgBegin() { return ByvalParmDbgValues.begin(); }
111   DbgIterator ByvalParmDbgEnd()   { return ByvalParmDbgValues.end(); }
112 };
114 enum CombineLevel {
115   Unrestricted,   // Combine may create illegal operations and illegal types.
116   NoIllegalTypes, // Combine may create illegal operations but no illegal types.
117   NoIllegalOperations // Combine may only create legal operations and types.
118 };
120 class SelectionDAG;
121 void checkForCycles(const SDNode *N);
122 void checkForCycles(const SelectionDAG *DAG);
124 /// SelectionDAG class - This is used to represent a portion of an LLVM function
125 /// in a low-level Data Dependence DAG representation suitable for instruction
126 /// selection.  This DAG is constructed as the first step of instruction
127 /// selection in order to allow implementation of machine specific optimizations
128 /// and code simplifications.
129 ///
130 /// The representation used by the SelectionDAG is a target-independent
131 /// representation, which has some similarities to the GCC RTL representation,
132 /// but is significantly more simple, powerful, and is a graph form instead of a
133 /// linear form.
134 ///
135 class SelectionDAG {
136   const TargetMachine &TM;
137   const TargetLowering &TLI;
138   const TargetSelectionDAGInfo &TSI;
139   MachineFunction *MF;
140   LLVMContext *Context;
142   /// EntryNode - The starting token.
143   SDNode EntryNode;
145   /// Root - The root of the entire DAG.
146   SDValue Root;
148   /// AllNodes - A linked list of nodes in the current DAG.
149   ilist<SDNode> AllNodes;
151   /// NodeAllocatorType - The AllocatorType for allocating SDNodes. We use
152   /// pool allocation with recycling.
153   typedef RecyclingAllocator<BumpPtrAllocator, SDNode, sizeof(LargestSDNode),
154                              AlignOf<MostAlignedSDNode>::Alignment>
155     NodeAllocatorType;
157   /// NodeAllocator - Pool allocation for nodes.
158   NodeAllocatorType NodeAllocator;
160   /// CSEMap - This structure is used to memoize nodes, automatically performing
161   /// CSE with existing nodes when a duplicate is requested.
162   FoldingSet<SDNode> CSEMap;
164   /// OperandAllocator - Pool allocation for machine-opcode SDNode operands.
165   BumpPtrAllocator OperandAllocator;
167   /// Allocator - Pool allocation for misc. objects that are created once per
168   /// SelectionDAG.
169   BumpPtrAllocator Allocator;
171   /// SDNodeOrdering - The ordering of the SDNodes. It roughly corresponds to
172   /// the ordering of the original LLVM instructions.
173   SDNodeOrdering *Ordering;
175   /// DbgInfo - Tracks dbg_value information through SDISel.
176   SDDbgInfo *DbgInfo;
178   /// setGraphColorHelper - Implementation of setSubgraphColor.
179   /// Return whether we had to truncate the search.
180   ///
181   bool setSubgraphColorHelper(SDNode *N, const char *Color,
182                               DenseSet<SDNode *> &visited,
183                               int level, bool &printed);
185   void operator=(const SelectionDAG&); // Do not implement.
186   SelectionDAG(const SelectionDAG&);   // Do not implement.
188 public:
189   explicit SelectionDAG(const TargetMachine &TM);
190   ~SelectionDAG();
192   /// init - Prepare this SelectionDAG to process code in the given
193   /// MachineFunction.
194   ///
195   void init(MachineFunction &mf);
197   /// clear - Clear state and free memory necessary to make this
198   /// SelectionDAG ready to process a new block.
199   ///
200   void clear();
202   MachineFunction &getMachineFunction() const { return *MF; }
203   const TargetMachine &getTarget() const { return TM; }
204   const TargetLowering &getTargetLoweringInfo() const { return TLI; }
205   const TargetSelectionDAGInfo &getSelectionDAGInfo() const { return TSI; }
206   LLVMContext *getContext() const {return Context; }
208   /// viewGraph - Pop up a GraphViz/gv window with the DAG rendered using 'dot'.
209   ///
210   void viewGraph(const std::string &Title);
211   void viewGraph();
213 #ifndef NDEBUG
214   std::map<const SDNode *, std::string> NodeGraphAttrs;
215 #endif
217   /// clearGraphAttrs - Clear all previously defined node graph attributes.
218   /// Intended to be used from a debugging tool (eg. gdb).
219   void clearGraphAttrs();
221   /// setGraphAttrs - Set graph attributes for a node. (eg. "color=red".)
222   ///
223   void setGraphAttrs(const SDNode *N, const char *Attrs);
225   /// getGraphAttrs - Get graph attributes for a node. (eg. "color=red".)
226   /// Used from getNodeAttributes.
227   const std::string getGraphAttrs(const SDNode *N) const;
229   /// setGraphColor - Convenience for setting node color attribute.
230   ///
231   void setGraphColor(const SDNode *N, const char *Color);
233   /// setGraphColor - Convenience for setting subgraph color attribute.
234   ///
235   void setSubgraphColor(SDNode *N, const char *Color);
237   typedef ilist<SDNode>::const_iterator allnodes_const_iterator;
238   allnodes_const_iterator allnodes_begin() const { return AllNodes.begin(); }
239   allnodes_const_iterator allnodes_end() const { return AllNodes.end(); }
240   typedef ilist<SDNode>::iterator allnodes_iterator;
241   allnodes_iterator allnodes_begin() { return AllNodes.begin(); }
242   allnodes_iterator allnodes_end() { return AllNodes.end(); }
243   ilist<SDNode>::size_type allnodes_size() const {
244     return AllNodes.size();
245   }
247   /// getRoot - Return the root tag of the SelectionDAG.
248   ///
249   const SDValue &getRoot() const { return Root; }
251   /// getEntryNode - Return the token chain corresponding to the entry of the
252   /// function.
253   SDValue getEntryNode() const {
254     return SDValue(const_cast<SDNode *>(&EntryNode), 0);
255   }
257   /// setRoot - Set the current root tag of the SelectionDAG.
258   ///
259   const SDValue &setRoot(SDValue N) {
260     assert((!N.getNode() || N.getValueType() == MVT::Other) &&
261            "DAG root value is not a chain!");
262     if (N.getNode())
263       checkForCycles(N.getNode());
264     Root = N;
265     if (N.getNode())
266       checkForCycles(this);
267     return Root;
268   }
270   /// Combine - This iterates over the nodes in the SelectionDAG, folding
271   /// certain types of nodes together, or eliminating superfluous nodes.  The
272   /// Level argument controls whether Combine is allowed to produce nodes and
273   /// types that are illegal on the target.
274   void Combine(CombineLevel Level, AliasAnalysis &AA,
275                CodeGenOpt::Level OptLevel);
277   /// LegalizeTypes - This transforms the SelectionDAG into a SelectionDAG that
278   /// only uses types natively supported by the target.  Returns "true" if it
279   /// made any changes.
280   ///
281   /// Note that this is an involved process that may invalidate pointers into
282   /// the graph.
283   bool LegalizeTypes();
285   /// Legalize - This transforms the SelectionDAG into a SelectionDAG that is
286   /// compatible with the target instruction selector, as indicated by the
287   /// TargetLowering object.
288   ///
289   /// Note that this is an involved process that may invalidate pointers into
290   /// the graph.
291   void Legalize(CodeGenOpt::Level OptLevel);
293   /// LegalizeVectors - This transforms the SelectionDAG into a SelectionDAG
294   /// that only uses vector math operations supported by the target.  This is
295   /// necessary as a separate step from Legalize because unrolling a vector
296   /// operation can introduce illegal types, which requires running
297   /// LegalizeTypes again.
298   ///
299   /// This returns true if it made any changes; in that case, LegalizeTypes
300   /// is called again before Legalize.
301   ///
302   /// Note that this is an involved process that may invalidate pointers into
303   /// the graph.
304   bool LegalizeVectors();
306   /// RemoveDeadNodes - This method deletes all unreachable nodes in the
307   /// SelectionDAG.
308   void RemoveDeadNodes();
310   /// DeleteNode - Remove the specified node from the system.  This node must
311   /// have no referrers.
312   void DeleteNode(SDNode *N);
314   /// getVTList - Return an SDVTList that represents the list of values
315   /// specified.
316   SDVTList getVTList(EVT VT);
317   SDVTList getVTList(EVT VT1, EVT VT2);
318   SDVTList getVTList(EVT VT1, EVT VT2, EVT VT3);
319   SDVTList getVTList(EVT VT1, EVT VT2, EVT VT3, EVT VT4);
320   SDVTList getVTList(const EVT *VTs, unsigned NumVTs);
322   //===--------------------------------------------------------------------===//
323   // Node creation methods.
324   //
325   SDValue getConstant(uint64_t Val, EVT VT, bool isTarget = false);
326   SDValue getConstant(const APInt &Val, EVT VT, bool isTarget = false);
327   SDValue getConstant(const ConstantInt &Val, EVT VT, bool isTarget = false);
328   SDValue getIntPtrConstant(uint64_t Val, bool isTarget = false);
329   SDValue getTargetConstant(uint64_t Val, EVT VT) {
330     return getConstant(Val, VT, true);
331   }
332   SDValue getTargetConstant(const APInt &Val, EVT VT) {
333     return getConstant(Val, VT, true);
334   }
335   SDValue getTargetConstant(const ConstantInt &Val, EVT VT) {
336     return getConstant(Val, VT, true);
337   }
338   // The forms below that take a double should only be used for simple
339   // constants that can be exactly represented in VT.  No checks are made.
340   SDValue getConstantFP(double Val, EVT VT, bool isTarget = false);
341   SDValue getConstantFP(const APFloat& Val, EVT VT, bool isTarget = false);
342   SDValue getConstantFP(const ConstantFP &CF, EVT VT, bool isTarget = false);
343   SDValue getTargetConstantFP(double Val, EVT VT) {
344     return getConstantFP(Val, VT, true);
345   }
346   SDValue getTargetConstantFP(const APFloat& Val, EVT VT) {
347     return getConstantFP(Val, VT, true);
348   }
349   SDValue getTargetConstantFP(const ConstantFP &Val, EVT VT) {
350     return getConstantFP(Val, VT, true);
351   }
352   SDValue getGlobalAddress(const GlobalValue *GV, DebugLoc DL, EVT VT,
353                            int64_t offset = 0, bool isTargetGA = false,
354                            unsigned char TargetFlags = 0);
355   SDValue getTargetGlobalAddress(const GlobalValue *GV, DebugLoc DL, EVT VT,
356                                  int64_t offset = 0,
357                                  unsigned char TargetFlags = 0) {
358     return getGlobalAddress(GV, DL, VT, offset, true, TargetFlags);
359   }
360   SDValue getFrameIndex(int FI, EVT VT, bool isTarget = false);
361   SDValue getTargetFrameIndex(int FI, EVT VT) {
362     return getFrameIndex(FI, VT, true);
363   }
364   SDValue getJumpTable(int JTI, EVT VT, bool isTarget = false,
365                        unsigned char TargetFlags = 0);
366   SDValue getTargetJumpTable(int JTI, EVT VT, unsigned char TargetFlags = 0) {
367     return getJumpTable(JTI, VT, true, TargetFlags);
368   }
369   SDValue getConstantPool(const Constant *C, EVT VT,
370                           unsigned Align = 0, int Offs = 0, bool isT=false,
371                           unsigned char TargetFlags = 0);
372   SDValue getTargetConstantPool(const Constant *C, EVT VT,
373                                 unsigned Align = 0, int Offset = 0,
374                                 unsigned char TargetFlags = 0) {
375     return getConstantPool(C, VT, Align, Offset, true, TargetFlags);
376   }
377   SDValue getConstantPool(MachineConstantPoolValue *C, EVT VT,
378                           unsigned Align = 0, int Offs = 0, bool isT=false,
379                           unsigned char TargetFlags = 0);
380   SDValue getTargetConstantPool(MachineConstantPoolValue *C,
381                                   EVT VT, unsigned Align = 0,
382                                   int Offset = 0, unsigned char TargetFlags=0) {
383     return getConstantPool(C, VT, Align, Offset, true, TargetFlags);
384   }
385   // When generating a branch to a BB, we don't in general know enough
386   // to provide debug info for the BB at that time, so keep this one around.
387   SDValue getBasicBlock(MachineBasicBlock *MBB);
388   SDValue getBasicBlock(MachineBasicBlock *MBB, DebugLoc dl);
389   SDValue getExternalSymbol(const char *Sym, EVT VT);
390   SDValue getExternalSymbol(const char *Sym, DebugLoc dl, EVT VT);
391   SDValue getTargetExternalSymbol(const char *Sym, EVT VT,
392                                   unsigned char TargetFlags = 0);
393   SDValue getValueType(EVT);
394   SDValue getRegister(unsigned Reg, EVT VT);
395   SDValue getEHLabel(DebugLoc dl, SDValue Root, MCSymbol *Label);
396   SDValue getBlockAddress(const BlockAddress *BA, EVT VT,
397                           bool isTarget = false, unsigned char TargetFlags = 0);
399   SDValue getCopyToReg(SDValue Chain, DebugLoc dl, unsigned Reg, SDValue N) {
400     return getNode(ISD::CopyToReg, dl, MVT::Other, Chain,
401                    getRegister(Reg, N.getValueType()), N);
402   }
404   // This version of the getCopyToReg method takes an extra operand, which
405   // indicates that there is potentially an incoming glue value (if Glue is not
406   // null) and that there should be a glue result.
407   SDValue getCopyToReg(SDValue Chain, DebugLoc dl, unsigned Reg, SDValue N,
408                        SDValue Glue) {
409     SDVTList VTs = getVTList(MVT::Other, MVT::Glue);
410     SDValue Ops[] = { Chain, getRegister(Reg, N.getValueType()), N, Glue };
411     return getNode(ISD::CopyToReg, dl, VTs, Ops, Glue.getNode() ? 4 : 3);
412   }
414   // Similar to last getCopyToReg() except parameter Reg is a SDValue
415   SDValue getCopyToReg(SDValue Chain, DebugLoc dl, SDValue Reg, SDValue N,
416                          SDValue Glue) {
417     SDVTList VTs = getVTList(MVT::Other, MVT::Glue);
418     SDValue Ops[] = { Chain, Reg, N, Glue };
419     return getNode(ISD::CopyToReg, dl, VTs, Ops, Glue.getNode() ? 4 : 3);
420   }
422   SDValue getCopyFromReg(SDValue Chain, DebugLoc dl, unsigned Reg, EVT VT) {
423     SDVTList VTs = getVTList(VT, MVT::Other);
424     SDValue Ops[] = { Chain, getRegister(Reg, VT) };
425     return getNode(ISD::CopyFromReg, dl, VTs, Ops, 2);
426   }
428   // This version of the getCopyFromReg method takes an extra operand, which
429   // indicates that there is potentially an incoming glue value (if Glue is not
430   // null) and that there should be a glue result.
431   SDValue getCopyFromReg(SDValue Chain, DebugLoc dl, unsigned Reg, EVT VT,
432                            SDValue Glue) {
433     SDVTList VTs = getVTList(VT, MVT::Other, MVT::Glue);
434     SDValue Ops[] = { Chain, getRegister(Reg, VT), Glue };
435     return getNode(ISD::CopyFromReg, dl, VTs, Ops, Glue.getNode() ? 3 : 2);
436   }
438   SDValue getCondCode(ISD::CondCode Cond);
440   /// Returns the ConvertRndSat Note: Avoid using this node because it may
441   /// disappear in the future and most targets don't support it.
442   SDValue getConvertRndSat(EVT VT, DebugLoc dl, SDValue Val, SDValue DTy,
443                            SDValue STy,
444                            SDValue Rnd, SDValue Sat, ISD::CvtCode Code);
445   
446   /// getVectorShuffle - Return an ISD::VECTOR_SHUFFLE node.  The number of
447   /// elements in VT, which must be a vector type, must match the number of
448   /// mask elements NumElts.  A integer mask element equal to -1 is treated as
449   /// undefined.
450   SDValue getVectorShuffle(EVT VT, DebugLoc dl, SDValue N1, SDValue N2, 
451                            const int *MaskElts);
453   /// getSExtOrTrunc - Convert Op, which must be of integer type, to the
454   /// integer type VT, by either sign-extending or truncating it.
455   SDValue getSExtOrTrunc(SDValue Op, DebugLoc DL, EVT VT);
457   /// getZExtOrTrunc - Convert Op, which must be of integer type, to the
458   /// integer type VT, by either zero-extending or truncating it.
459   SDValue getZExtOrTrunc(SDValue Op, DebugLoc DL, EVT VT);
461   /// getZeroExtendInReg - Return the expression required to zero extend the Op
462   /// value assuming it was the smaller SrcTy value.
463   SDValue getZeroExtendInReg(SDValue Op, DebugLoc DL, EVT SrcTy);
465   /// getNOT - Create a bitwise NOT operation as (XOR Val, -1).
466   SDValue getNOT(DebugLoc DL, SDValue Val, EVT VT);
468   /// getCALLSEQ_START - Return a new CALLSEQ_START node, which always must have
469   /// a glue result (to ensure it's not CSE'd).  CALLSEQ_START does not have a
470   /// useful DebugLoc.
471   SDValue getCALLSEQ_START(SDValue Chain, SDValue Op) {
472     SDVTList VTs = getVTList(MVT::Other, MVT::Glue);
473     SDValue Ops[] = { Chain,  Op };
474     return getNode(ISD::CALLSEQ_START, DebugLoc(), VTs, Ops, 2);
475   }
477   /// getCALLSEQ_END - Return a new CALLSEQ_END node, which always must have a
478   /// glue result (to ensure it's not CSE'd).  CALLSEQ_END does not have
479   /// a useful DebugLoc.
480   SDValue getCALLSEQ_END(SDValue Chain, SDValue Op1, SDValue Op2,
481                            SDValue InGlue) {
482     SDVTList NodeTys = getVTList(MVT::Other, MVT::Glue);
483     SmallVector<SDValue, 4> Ops;
484     Ops.push_back(Chain);
485     Ops.push_back(Op1);
486     Ops.push_back(Op2);
487     Ops.push_back(InGlue);
488     return getNode(ISD::CALLSEQ_END, DebugLoc(), NodeTys, &Ops[0],
489                    (unsigned)Ops.size() - (InGlue.getNode() == 0 ? 1 : 0));
490   }
492   /// getUNDEF - Return an UNDEF node.  UNDEF does not have a useful DebugLoc.
493   SDValue getUNDEF(EVT VT) {
494     return getNode(ISD::UNDEF, DebugLoc(), VT);
495   }
497   /// getGLOBAL_OFFSET_TABLE - Return a GLOBAL_OFFSET_TABLE node.  This does
498   /// not have a useful DebugLoc.
499   SDValue getGLOBAL_OFFSET_TABLE(EVT VT) {
500     return getNode(ISD::GLOBAL_OFFSET_TABLE, DebugLoc(), VT);
501   }
503   /// getNode - Gets or creates the specified node.
504   ///
505   SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT);
506   SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT, SDValue N);
507   SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT, SDValue N1, SDValue N2);
508   SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT,
509                   SDValue N1, SDValue N2, SDValue N3);
510   SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT,
511                   SDValue N1, SDValue N2, SDValue N3, SDValue N4);
512   SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT,
513                   SDValue N1, SDValue N2, SDValue N3, SDValue N4,
514                   SDValue N5);
515   SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT,
516                   const SDUse *Ops, unsigned NumOps);
517   SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT,
518                   const SDValue *Ops, unsigned NumOps);
519   SDValue getNode(unsigned Opcode, DebugLoc DL,
520                   const std::vector<EVT> &ResultTys,
521                   const SDValue *Ops, unsigned NumOps);
522   SDValue getNode(unsigned Opcode, DebugLoc DL, const EVT *VTs, unsigned NumVTs,
523                   const SDValue *Ops, unsigned NumOps);
524   SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs,
525                   const SDValue *Ops, unsigned NumOps);
526   SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs);
527   SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs, SDValue N);
528   SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs,
529                   SDValue N1, SDValue N2);
530   SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs,
531                   SDValue N1, SDValue N2, SDValue N3);
532   SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs,
533                   SDValue N1, SDValue N2, SDValue N3, SDValue N4);
534   SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs,
535                   SDValue N1, SDValue N2, SDValue N3, SDValue N4,
536                   SDValue N5);
538   /// getStackArgumentTokenFactor - Compute a TokenFactor to force all
539   /// the incoming stack arguments to be loaded from the stack. This is
540   /// used in tail call lowering to protect stack arguments from being
541   /// clobbered.
542   SDValue getStackArgumentTokenFactor(SDValue Chain);
544   SDValue getMemcpy(SDValue Chain, DebugLoc dl, SDValue Dst, SDValue Src,
545                     SDValue Size, unsigned Align, bool isVol, bool AlwaysInline,
546                     MachinePointerInfo DstPtrInfo,
547                     MachinePointerInfo SrcPtrInfo);
549   SDValue getMemmove(SDValue Chain, DebugLoc dl, SDValue Dst, SDValue Src,
550                      SDValue Size, unsigned Align, bool isVol,
551                      MachinePointerInfo DstPtrInfo,
552                      MachinePointerInfo SrcPtrInfo);
554   SDValue getMemset(SDValue Chain, DebugLoc dl, SDValue Dst, SDValue Src,
555                     SDValue Size, unsigned Align, bool isVol,
556                     MachinePointerInfo DstPtrInfo);
558   /// getSetCC - Helper function to make it easier to build SetCC's if you just
559   /// have an ISD::CondCode instead of an SDValue.
560   ///
561   SDValue getSetCC(DebugLoc DL, EVT VT, SDValue LHS, SDValue RHS,
562                    ISD::CondCode Cond) {
563     return getNode(ISD::SETCC, DL, VT, LHS, RHS, getCondCode(Cond));
564   }
566   /// getVSetCC - Helper function to make it easier to build VSetCC's nodes
567   /// if you just have an ISD::CondCode instead of an SDValue.
568   ///
569   SDValue getVSetCC(DebugLoc DL, EVT VT, SDValue LHS, SDValue RHS,
570                     ISD::CondCode Cond) {
571     return getNode(ISD::VSETCC, DL, VT, LHS, RHS, getCondCode(Cond));
572   }
574   /// getSelectCC - Helper function to make it easier to build SelectCC's if you
575   /// just have an ISD::CondCode instead of an SDValue.
576   ///
577   SDValue getSelectCC(DebugLoc DL, SDValue LHS, SDValue RHS,
578                       SDValue True, SDValue False, ISD::CondCode Cond) {
579     return getNode(ISD::SELECT_CC, DL, True.getValueType(),
580                    LHS, RHS, True, False, getCondCode(Cond));
581   }
583   /// getVAArg - VAArg produces a result and token chain, and takes a pointer
584   /// and a source value as input.
585   SDValue getVAArg(EVT VT, DebugLoc dl, SDValue Chain, SDValue Ptr,
586                    SDValue SV, unsigned Align);
588   /// getAtomic - Gets a node for an atomic op, produces result and chain and
589   /// takes 3 operands
590   SDValue getAtomic(unsigned Opcode, DebugLoc dl, EVT MemVT, SDValue Chain,
591                     SDValue Ptr, SDValue Cmp, SDValue Swp,
592                     MachinePointerInfo PtrInfo, unsigned Alignment=0);
593   SDValue getAtomic(unsigned Opcode, DebugLoc dl, EVT MemVT, SDValue Chain,
594                     SDValue Ptr, SDValue Cmp, SDValue Swp,
595                     MachineMemOperand *MMO);
597   /// getAtomic - Gets a node for an atomic op, produces result and chain and
598   /// takes 2 operands.
599   SDValue getAtomic(unsigned Opcode, DebugLoc dl, EVT MemVT, SDValue Chain,
600                     SDValue Ptr, SDValue Val, const Value* PtrVal,
601                     unsigned Alignment = 0);
602   SDValue getAtomic(unsigned Opcode, DebugLoc dl, EVT MemVT, SDValue Chain,
603                     SDValue Ptr, SDValue Val,
604                     MachineMemOperand *MMO);
606   /// getMemIntrinsicNode - Creates a MemIntrinsicNode that may produce a
607   /// result and takes a list of operands. Opcode may be INTRINSIC_VOID,
608   /// INTRINSIC_W_CHAIN, or a target-specific opcode with a value not
609   /// less than FIRST_TARGET_MEMORY_OPCODE.
610   SDValue getMemIntrinsicNode(unsigned Opcode, DebugLoc dl,
611                               const EVT *VTs, unsigned NumVTs,
612                               const SDValue *Ops, unsigned NumOps,
613                               EVT MemVT, MachinePointerInfo PtrInfo,
614                               unsigned Align = 0, bool Vol = false,
615                               bool ReadMem = true, bool WriteMem = true);
617   SDValue getMemIntrinsicNode(unsigned Opcode, DebugLoc dl, SDVTList VTList,
618                               const SDValue *Ops, unsigned NumOps,
619                               EVT MemVT, MachinePointerInfo PtrInfo,
620                               unsigned Align = 0, bool Vol = false,
621                               bool ReadMem = true, bool WriteMem = true);
623   SDValue getMemIntrinsicNode(unsigned Opcode, DebugLoc dl, SDVTList VTList,
624                               const SDValue *Ops, unsigned NumOps,
625                               EVT MemVT, MachineMemOperand *MMO);
627   /// getMergeValues - Create a MERGE_VALUES node from the given operands.
628   SDValue getMergeValues(const SDValue *Ops, unsigned NumOps, DebugLoc dl);
630   /// getLoad - Loads are not normal binary operators: their result type is not
631   /// determined by their operands, and they produce a value AND a token chain.
632   ///
633   SDValue getLoad(EVT VT, DebugLoc dl, SDValue Chain, SDValue Ptr,
634                   MachinePointerInfo PtrInfo, bool isVolatile,
635                   bool isNonTemporal, unsigned Alignment,
636                   const MDNode *TBAAInfo = 0);
637   SDValue getExtLoad(ISD::LoadExtType ExtType, DebugLoc dl, EVT VT,
638                      SDValue Chain, SDValue Ptr, MachinePointerInfo PtrInfo,
639                      EVT MemVT, bool isVolatile,
640                      bool isNonTemporal, unsigned Alignment,
641                      const MDNode *TBAAInfo = 0);
642   SDValue getIndexedLoad(SDValue OrigLoad, DebugLoc dl, SDValue Base,
643                          SDValue Offset, ISD::MemIndexedMode AM);
644   SDValue getLoad(ISD::MemIndexedMode AM, ISD::LoadExtType ExtType,
645                   EVT VT, DebugLoc dl,
646                   SDValue Chain, SDValue Ptr, SDValue Offset,
647                   MachinePointerInfo PtrInfo, EVT MemVT,
648                   bool isVolatile, bool isNonTemporal, unsigned Alignment,
649                   const MDNode *TBAAInfo = 0);
650   SDValue getLoad(ISD::MemIndexedMode AM, ISD::LoadExtType ExtType,
651                   EVT VT, DebugLoc dl,
652                   SDValue Chain, SDValue Ptr, SDValue Offset,
653                   EVT MemVT, MachineMemOperand *MMO);
655   /// getStore - Helper function to build ISD::STORE nodes.
656   ///
657   SDValue getStore(SDValue Chain, DebugLoc dl, SDValue Val, SDValue Ptr,
658                    MachinePointerInfo PtrInfo, bool isVolatile,
659                    bool isNonTemporal, unsigned Alignment,
660                    const MDNode *TBAAInfo = 0);
661   SDValue getStore(SDValue Chain, DebugLoc dl, SDValue Val, SDValue Ptr,
662                    MachineMemOperand *MMO);
663   SDValue getTruncStore(SDValue Chain, DebugLoc dl, SDValue Val, SDValue Ptr,
664                         MachinePointerInfo PtrInfo, EVT TVT,
665                         bool isNonTemporal, bool isVolatile,
666                         unsigned Alignment,
667                         const MDNode *TBAAInfo = 0);
668   SDValue getTruncStore(SDValue Chain, DebugLoc dl, SDValue Val, SDValue Ptr,
669                         EVT TVT, MachineMemOperand *MMO);
670   SDValue getIndexedStore(SDValue OrigStoe, DebugLoc dl, SDValue Base,
671                            SDValue Offset, ISD::MemIndexedMode AM);
673   /// getSrcValue - Construct a node to track a Value* through the backend.
674   SDValue getSrcValue(const Value *v);
676   /// getMDNode - Return an MDNodeSDNode which holds an MDNode.
677   SDValue getMDNode(const MDNode *MD);
678   
679   /// getShiftAmountOperand - Return the specified value casted to
680   /// the target's desired shift amount type.
681   SDValue getShiftAmountOperand(SDValue Op);
683   /// UpdateNodeOperands - *Mutate* the specified node in-place to have the
684   /// specified operands.  If the resultant node already exists in the DAG,
685   /// this does not modify the specified node, instead it returns the node that
686   /// already exists.  If the resultant node does not exist in the DAG, the
687   /// input node is returned.  As a degenerate case, if you specify the same
688   /// input operands as the node already has, the input node is returned.
689   SDNode *UpdateNodeOperands(SDNode *N, SDValue Op);
690   SDNode *UpdateNodeOperands(SDNode *N, SDValue Op1, SDValue Op2);
691   SDNode *UpdateNodeOperands(SDNode *N, SDValue Op1, SDValue Op2,
692                                SDValue Op3);
693   SDNode *UpdateNodeOperands(SDNode *N, SDValue Op1, SDValue Op2,
694                                SDValue Op3, SDValue Op4);
695   SDNode *UpdateNodeOperands(SDNode *N, SDValue Op1, SDValue Op2,
696                                SDValue Op3, SDValue Op4, SDValue Op5);
697   SDNode *UpdateNodeOperands(SDNode *N,
698                                const SDValue *Ops, unsigned NumOps);
700   /// SelectNodeTo - These are used for target selectors to *mutate* the
701   /// specified node to have the specified return type, Target opcode, and
702   /// operands.  Note that target opcodes are stored as
703   /// ~TargetOpcode in the node opcode field.  The resultant node is returned.
704   SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT);
705   SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT, SDValue Op1);
706   SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT,
707                        SDValue Op1, SDValue Op2);
708   SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT,
709                        SDValue Op1, SDValue Op2, SDValue Op3);
710   SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT,
711                        const SDValue *Ops, unsigned NumOps);
712   SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1, EVT VT2);
713   SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1,
714                        EVT VT2, const SDValue *Ops, unsigned NumOps);
715   SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1,
716                        EVT VT2, EVT VT3, const SDValue *Ops, unsigned NumOps);
717   SDNode *SelectNodeTo(SDNode *N, unsigned MachineOpc, EVT VT1,
718                        EVT VT2, EVT VT3, EVT VT4, const SDValue *Ops,
719                        unsigned NumOps);
720   SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1,
721                        EVT VT2, SDValue Op1);
722   SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1,
723                        EVT VT2, SDValue Op1, SDValue Op2);
724   SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1,
725                        EVT VT2, SDValue Op1, SDValue Op2, SDValue Op3);
726   SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1,
727                        EVT VT2, EVT VT3, SDValue Op1, SDValue Op2, SDValue Op3);
728   SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, SDVTList VTs,
729                        const SDValue *Ops, unsigned NumOps);
731   /// MorphNodeTo - This *mutates* the specified node to have the specified
732   /// return type, opcode, and operands.
733   SDNode *MorphNodeTo(SDNode *N, unsigned Opc, SDVTList VTs,
734                       const SDValue *Ops, unsigned NumOps);
736   /// getMachineNode - These are used for target selectors to create a new node
737   /// with specified return type(s), MachineInstr opcode, and operands.
738   ///
739   /// Note that getMachineNode returns the resultant node.  If there is already
740   /// a node of the specified opcode and operands, it returns that node instead
741   /// of the current one.
742   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT);
743   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT,
744                                 SDValue Op1);
745   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT,
746                                 SDValue Op1, SDValue Op2);
747   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT,
748                          SDValue Op1, SDValue Op2, SDValue Op3);
749   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT,
750                          const SDValue *Ops, unsigned NumOps);
751   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2);
752   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2,
753                          SDValue Op1);
754   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1,
755                          EVT VT2, SDValue Op1, SDValue Op2);
756   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1,
757                          EVT VT2, SDValue Op1, SDValue Op2, SDValue Op3);
758   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2,
759                          const SDValue *Ops, unsigned NumOps);
760   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2,
761                          EVT VT3, SDValue Op1, SDValue Op2);
762   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2,
763                          EVT VT3, SDValue Op1, SDValue Op2, SDValue Op3);
764   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2,
765                          EVT VT3, const SDValue *Ops, unsigned NumOps);
766   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2,
767                          EVT VT3, EVT VT4, const SDValue *Ops, unsigned NumOps);
768   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl,
769                          const std::vector<EVT> &ResultTys, const SDValue *Ops,
770                          unsigned NumOps);
771   MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, SDVTList VTs,
772                          const SDValue *Ops, unsigned NumOps);
774   /// getTargetExtractSubreg - A convenience function for creating
775   /// TargetInstrInfo::EXTRACT_SUBREG nodes.
776   SDValue getTargetExtractSubreg(int SRIdx, DebugLoc DL, EVT VT,
777                                  SDValue Operand);
779   /// getTargetInsertSubreg - A convenience function for creating
780   /// TargetInstrInfo::INSERT_SUBREG nodes.
781   SDValue getTargetInsertSubreg(int SRIdx, DebugLoc DL, EVT VT,
782                                 SDValue Operand, SDValue Subreg);
784   /// getNodeIfExists - Get the specified node if it's already available, or
785   /// else return NULL.
786   SDNode *getNodeIfExists(unsigned Opcode, SDVTList VTs,
787                           const SDValue *Ops, unsigned NumOps);
789   /// getDbgValue - Creates a SDDbgValue node.
790   ///
791   SDDbgValue *getDbgValue(MDNode *MDPtr, SDNode *N, unsigned R, uint64_t Off,
792                           DebugLoc DL, unsigned O);
793   SDDbgValue *getDbgValue(MDNode *MDPtr, const Value *C, uint64_t Off,
794                           DebugLoc DL, unsigned O);
795   SDDbgValue *getDbgValue(MDNode *MDPtr, unsigned FI, uint64_t Off,
796                           DebugLoc DL, unsigned O);
798   /// DAGUpdateListener - Clients of various APIs that cause global effects on
799   /// the DAG can optionally implement this interface.  This allows the clients
800   /// to handle the various sorts of updates that happen.
801   class DAGUpdateListener {
802   public:
803     virtual ~DAGUpdateListener();
805     /// NodeDeleted - The node N that was deleted and, if E is not null, an
806     /// equivalent node E that replaced it.
807     virtual void NodeDeleted(SDNode *N, SDNode *E) = 0;
809     /// NodeUpdated - The node N that was updated.
810     virtual void NodeUpdated(SDNode *N) = 0;
811   };
813   /// RemoveDeadNode - Remove the specified node from the system. If any of its
814   /// operands then becomes dead, remove them as well. Inform UpdateListener
815   /// for each node deleted.
816   void RemoveDeadNode(SDNode *N, DAGUpdateListener *UpdateListener = 0);
818   /// RemoveDeadNodes - This method deletes the unreachable nodes in the
819   /// given list, and any nodes that become unreachable as a result.
820   void RemoveDeadNodes(SmallVectorImpl<SDNode *> &DeadNodes,
821                        DAGUpdateListener *UpdateListener = 0);
823   /// ReplaceAllUsesWith - Modify anything using 'From' to use 'To' instead.
824   /// This can cause recursive merging of nodes in the DAG.  Use the first
825   /// version if 'From' is known to have a single result, use the second
826   /// if you have two nodes with identical results (or if 'To' has a superset
827   /// of the results of 'From'), use the third otherwise.
828   ///
829   /// These methods all take an optional UpdateListener, which (if not null) is
830   /// informed about nodes that are deleted and modified due to recursive
831   /// changes in the dag.
832   ///
833   /// These functions only replace all existing uses. It's possible that as
834   /// these replacements are being performed, CSE may cause the From node
835   /// to be given new uses. These new uses of From are left in place, and
836   /// not automatically transfered to To.
837   ///
838   void ReplaceAllUsesWith(SDValue From, SDValue Op,
839                           DAGUpdateListener *UpdateListener = 0);
840   void ReplaceAllUsesWith(SDNode *From, SDNode *To,
841                           DAGUpdateListener *UpdateListener = 0);
842   void ReplaceAllUsesWith(SDNode *From, const SDValue *To,
843                           DAGUpdateListener *UpdateListener = 0);
845   /// ReplaceAllUsesOfValueWith - Replace any uses of From with To, leaving
846   /// uses of other values produced by From.Val alone.
847   void ReplaceAllUsesOfValueWith(SDValue From, SDValue To,
848                                  DAGUpdateListener *UpdateListener = 0);
850   /// ReplaceAllUsesOfValuesWith - Like ReplaceAllUsesOfValueWith, but
851   /// for multiple values at once. This correctly handles the case where
852   /// there is an overlap between the From values and the To values.
853   void ReplaceAllUsesOfValuesWith(const SDValue *From, const SDValue *To,
854                                   unsigned Num,
855                                   DAGUpdateListener *UpdateListener = 0);
857   /// AssignTopologicalOrder - Topological-sort the AllNodes list and a
858   /// assign a unique node id for each node in the DAG based on their
859   /// topological order. Returns the number of nodes.
860   unsigned AssignTopologicalOrder();
862   /// RepositionNode - Move node N in the AllNodes list to be immediately
863   /// before the given iterator Position. This may be used to update the
864   /// topological ordering when the list of nodes is modified.
865   void RepositionNode(allnodes_iterator Position, SDNode *N) {
866     AllNodes.insert(Position, AllNodes.remove(N));
867   }
869   /// isCommutativeBinOp - Returns true if the opcode is a commutative binary
870   /// operation.
871   static bool isCommutativeBinOp(unsigned Opcode) {
872     // FIXME: This should get its info from the td file, so that we can include
873     // target info.
874     switch (Opcode) {
875     case ISD::ADD:
876     case ISD::MUL:
877     case ISD::MULHU:
878     case ISD::MULHS:
879     case ISD::SMUL_LOHI:
880     case ISD::UMUL_LOHI:
881     case ISD::FADD:
882     case ISD::FMUL:
883     case ISD::AND:
884     case ISD::OR:
885     case ISD::XOR:
886     case ISD::SADDO:
887     case ISD::UADDO:
888     case ISD::ADDC:
889     case ISD::ADDE: return true;
890     default: return false;
891     }
892   }
894   /// AssignOrdering - Assign an order to the SDNode.
895   void AssignOrdering(const SDNode *SD, unsigned Order);
897   /// GetOrdering - Get the order for the SDNode.
898   unsigned GetOrdering(const SDNode *SD) const;
900   /// AddDbgValue - Add a dbg_value SDNode. If SD is non-null that means the
901   /// value is produced by SD.
902   void AddDbgValue(SDDbgValue *DB, SDNode *SD, bool isParameter);
904   /// GetDbgValues - Get the debug values which reference the given SDNode.
905   SmallVector<SDDbgValue*,2> &GetDbgValues(const SDNode* SD) {
906     return DbgInfo->getSDDbgValues(SD);
907   }
908   
909   /// TransferDbgValues - Transfer SDDbgValues.
910   void TransferDbgValues(SDValue From, SDValue To);
912   /// hasDebugValues - Return true if there are any SDDbgValue nodes associated
913   /// with this SelectionDAG.
914   bool hasDebugValues() const { return !DbgInfo->empty(); }
916   SDDbgInfo::DbgIterator DbgBegin() { return DbgInfo->DbgBegin(); }
917   SDDbgInfo::DbgIterator DbgEnd()   { return DbgInfo->DbgEnd(); }
918   SDDbgInfo::DbgIterator ByvalParmDbgBegin() { 
919     return DbgInfo->ByvalParmDbgBegin(); 
920   }
921   SDDbgInfo::DbgIterator ByvalParmDbgEnd()   { 
922     return DbgInfo->ByvalParmDbgEnd(); 
923   }
925   void dump() const;
927   /// CreateStackTemporary - Create a stack temporary, suitable for holding the
928   /// specified value type.  If minAlign is specified, the slot size will have
929   /// at least that alignment.
930   SDValue CreateStackTemporary(EVT VT, unsigned minAlign = 1);
932   /// CreateStackTemporary - Create a stack temporary suitable for holding
933   /// either of the specified value types.
934   SDValue CreateStackTemporary(EVT VT1, EVT VT2);
936   /// FoldConstantArithmetic -
937   SDValue FoldConstantArithmetic(unsigned Opcode,
938                                  EVT VT,
939                                  ConstantSDNode *Cst1,
940                                  ConstantSDNode *Cst2);
942   /// FoldSetCC - Constant fold a setcc to true or false.
943   SDValue FoldSetCC(EVT VT, SDValue N1,
944                     SDValue N2, ISD::CondCode Cond, DebugLoc dl);
946   /// SignBitIsZero - Return true if the sign bit of Op is known to be zero.  We
947   /// use this predicate to simplify operations downstream.
948   bool SignBitIsZero(SDValue Op, unsigned Depth = 0) const;
950   /// MaskedValueIsZero - Return true if 'Op & Mask' is known to be zero.  We
951   /// use this predicate to simplify operations downstream.  Op and Mask are
952   /// known to be the same type.
953   bool MaskedValueIsZero(SDValue Op, const APInt &Mask, unsigned Depth = 0)
954     const;
956   /// ComputeMaskedBits - Determine which of the bits specified in Mask are
957   /// known to be either zero or one and return them in the KnownZero/KnownOne
958   /// bitsets.  This code only analyzes bits in Mask, in order to short-circuit
959   /// processing.  Targets can implement the computeMaskedBitsForTargetNode
960   /// method in the TargetLowering class to allow target nodes to be understood.
961   void ComputeMaskedBits(SDValue Op, const APInt &Mask, APInt &KnownZero,
962                          APInt &KnownOne, unsigned Depth = 0) const;
964   /// ComputeNumSignBits - Return the number of times the sign bit of the
965   /// register is replicated into the other bits.  We know that at least 1 bit
966   /// is always equal to the sign bit (itself), but other cases can give us
967   /// information.  For example, immediately after an "SRA X, 2", we know that
968   /// the top 3 bits are all equal to each other, so we return 3.  Targets can
969   /// implement the ComputeNumSignBitsForTarget method in the TargetLowering
970   /// class to allow target nodes to be understood.
971   unsigned ComputeNumSignBits(SDValue Op, unsigned Depth = 0) const;
973   /// isBaseWithConstantOffset - Return true if the specified operand is an
974   /// ISD::ADD with a ConstantSDNode on the right-hand side, or if it is an
975   /// ISD::OR with a ConstantSDNode that is guaranteed to have the same
976   /// semantics as an ADD.  This handles the equivalence:
977   ///     X|Cst == X+Cst iff X&Cst = 0.
978   bool isBaseWithConstantOffset(SDValue Op) const;
979   
980   /// isKnownNeverNan - Test whether the given SDValue is known to never be NaN.
981   bool isKnownNeverNaN(SDValue Op) const;
983   /// isKnownNeverZero - Test whether the given SDValue is known to never be
984   /// positive or negative Zero.
985   bool isKnownNeverZero(SDValue Op) const;
987   /// isEqualTo - Test whether two SDValues are known to compare equal. This
988   /// is true if they are the same value, or if one is negative zero and the
989   /// other positive zero.
990   bool isEqualTo(SDValue A, SDValue B) const;
992   /// isVerifiedDebugInfoDesc - Returns true if the specified SDValue has
993   /// been verified as a debug information descriptor.
994   bool isVerifiedDebugInfoDesc(SDValue Op) const;
996   /// UnrollVectorOp - Utility function used by legalize and lowering to
997   /// "unroll" a vector operation by splitting out the scalars and operating
998   /// on each element individually.  If the ResNE is 0, fully unroll the vector
999   /// op. If ResNE is less than the width of the vector op, unroll up to ResNE.
1000   /// If the  ResNE is greater than the width of the vector op, unroll the
1001   /// vector op and fill the end of the resulting vector with UNDEFS.
1002   SDValue UnrollVectorOp(SDNode *N, unsigned ResNE = 0);
1004   /// isConsecutiveLoad - Return true if LD is loading 'Bytes' bytes from a 
1005   /// location that is 'Dist' units away from the location that the 'Base' load 
1006   /// is loading from.
1007   bool isConsecutiveLoad(LoadSDNode *LD, LoadSDNode *Base,
1008                          unsigned Bytes, int Dist) const;
1010   /// InferPtrAlignment - Infer alignment of a load / store address. Return 0 if
1011   /// it cannot be inferred.
1012   unsigned InferPtrAlignment(SDValue Ptr) const;
1014 private:
1015   bool RemoveNodeFromCSEMaps(SDNode *N);
1016   void AddModifiedNodeToCSEMaps(SDNode *N, DAGUpdateListener *UpdateListener);
1017   SDNode *FindModifiedNodeSlot(SDNode *N, SDValue Op, void *&InsertPos);
1018   SDNode *FindModifiedNodeSlot(SDNode *N, SDValue Op1, SDValue Op2,
1019                                void *&InsertPos);
1020   SDNode *FindModifiedNodeSlot(SDNode *N, const SDValue *Ops, unsigned NumOps,
1021                                void *&InsertPos);
1023   void DeleteNodeNotInCSEMaps(SDNode *N);
1024   void DeallocateNode(SDNode *N);
1026   unsigned getEVTAlignment(EVT MemoryVT) const;
1028   void allnodes_clear();
1030   /// VTList - List of non-single value types.
1031   std::vector<SDVTList> VTList;
1033   /// CondCodeNodes - Maps to auto-CSE operations.
1034   std::vector<CondCodeSDNode*> CondCodeNodes;
1036   std::vector<SDNode*> ValueTypeNodes;
1037   std::map<EVT, SDNode*, EVT::compareRawBits> ExtendedValueTypeNodes;
1038   StringMap<SDNode*> ExternalSymbols;
1039   
1040   std::map<std::pair<std::string, unsigned char>,SDNode*> TargetExternalSymbols;
1041 };
1043 template <> struct GraphTraits<SelectionDAG*> : public GraphTraits<SDNode*> {
1044   typedef SelectionDAG::allnodes_iterator nodes_iterator;
1045   static nodes_iterator nodes_begin(SelectionDAG *G) {
1046     return G->allnodes_begin();
1047   }
1048   static nodes_iterator nodes_end(SelectionDAG *G) {
1049     return G->allnodes_end();
1050   }
1051 };
1053 }  // end namespace llvm
1055 #endif