1 //===-- llvm/CodeGen/SelectionDAG.h - InstSelection DAG ---------*- C++ -*-===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file declares the SelectionDAG class, and transitively defines the
11 // SDNode class and subclasses.
12 //
13 //===----------------------------------------------------------------------===//
15 #ifndef LLVM_CODEGEN_SELECTIONDAG_H
16 #define LLVM_CODEGEN_SELECTIONDAG_H
18 #include "llvm/ADT/ilist.h"
19 #include "llvm/ADT/DenseSet.h"
20 #include "llvm/ADT/StringMap.h"
21 #include "llvm/CodeGen/SelectionDAGNodes.h"
22 #include "llvm/Support/RecyclingAllocator.h"
23 #include "llvm/Target/TargetMachine.h"
24 #include <cassert>
25 #include <vector>
26 #include <map>
27 #include <string>
29 namespace llvm {
31 class AliasAnalysis;
32 class MachineConstantPoolValue;
33 class MachineFunction;
34 class MDNode;
35 class SDNodeOrdering;
36 class SDDbgValue;
37 class TargetLowering;
38 class TargetSelectionDAGInfo;
40 template<> struct ilist_traits<SDNode> : public ilist_default_traits<SDNode> {
41 private:
42 mutable ilist_half_node<SDNode> Sentinel;
43 public:
44 SDNode *createSentinel() const {
45 return static_cast<SDNode*>(&Sentinel);
46 }
47 static void destroySentinel(SDNode *) {}
49 SDNode *provideInitialHead() const { return createSentinel(); }
50 SDNode *ensureHead(SDNode*) const { return createSentinel(); }
51 static void noteHead(SDNode*, SDNode*) {}
53 static void deleteNode(SDNode *) {
54 assert(0 && "ilist_traits<SDNode> shouldn't see a deleteNode call!");
55 }
56 private:
57 static void createNode(const SDNode &);
58 };
60 /// SDDbgInfo - Keeps track of dbg_value information through SDISel. We do
61 /// not build SDNodes for these so as not to perturb the generated code;
62 /// instead the info is kept off to the side in this structure. Each SDNode may
63 /// have one or more associated dbg_value entries. This information is kept in
64 /// DbgValMap.
65 /// Byval parameters are handled separately because they don't use alloca's,
66 /// which busts the normal mechanism. There is good reason for handling all
67 /// parameters separately: they may not have code generated for them, they
68 /// should always go at the beginning of the function regardless of other code
69 /// motion, and debug info for them is potentially useful even if the parameter
70 /// is unused. Right now only byval parameters are handled separately.
71 class SDDbgInfo {
72 SmallVector<SDDbgValue*, 32> DbgValues;
73 SmallVector<SDDbgValue*, 32> ByvalParmDbgValues;
74 DenseMap<const SDNode*, SmallVector<SDDbgValue*, 2> > DbgValMap;
76 void operator=(const SDDbgInfo&); // Do not implement.
77 SDDbgInfo(const SDDbgInfo&); // Do not implement.
78 public:
79 SDDbgInfo() {}
81 void add(SDDbgValue *V, const SDNode *Node, bool isParameter) {
82 if (isParameter) {
83 ByvalParmDbgValues.push_back(V);
84 } else DbgValues.push_back(V);
85 if (Node)
86 DbgValMap[Node].push_back(V);
87 }
89 void clear() {
90 DbgValMap.clear();
91 DbgValues.clear();
92 ByvalParmDbgValues.clear();
93 }
95 bool empty() const {
96 return DbgValues.empty() && ByvalParmDbgValues.empty();
97 }
99 SmallVector<SDDbgValue*,2> &getSDDbgValues(const SDNode *Node) {
100 return DbgValMap[Node];
101 }
103 typedef SmallVector<SDDbgValue*,32>::iterator DbgIterator;
104 DbgIterator DbgBegin() { return DbgValues.begin(); }
105 DbgIterator DbgEnd() { return DbgValues.end(); }
106 DbgIterator ByvalParmDbgBegin() { return ByvalParmDbgValues.begin(); }
107 DbgIterator ByvalParmDbgEnd() { return ByvalParmDbgValues.end(); }
108 };
110 enum CombineLevel {
111 Unrestricted, // Combine may create illegal operations and illegal types.
112 NoIllegalTypes, // Combine may create illegal operations but no illegal types.
113 NoIllegalOperations // Combine may only create legal operations and types.
114 };
116 class SelectionDAG;
117 void checkForCycles(const SDNode *N);
118 void checkForCycles(const SelectionDAG *DAG);
120 /// SelectionDAG class - This is used to represent a portion of an LLVM function
121 /// in a low-level Data Dependence DAG representation suitable for instruction
122 /// selection. This DAG is constructed as the first step of instruction
123 /// selection in order to allow implementation of machine specific optimizations
124 /// and code simplifications.
125 ///
126 /// The representation used by the SelectionDAG is a target-independent
127 /// representation, which has some similarities to the GCC RTL representation,
128 /// but is significantly more simple, powerful, and is a graph form instead of a
129 /// linear form.
130 ///
131 class SelectionDAG {
132 const TargetMachine &TM;
133 const TargetLowering &TLI;
134 const TargetSelectionDAGInfo &TSI;
135 MachineFunction *MF;
136 LLVMContext *Context;
138 /// EntryNode - The starting token.
139 SDNode EntryNode;
141 /// Root - The root of the entire DAG.
142 SDValue Root;
144 /// AllNodes - A linked list of nodes in the current DAG.
145 ilist<SDNode> AllNodes;
147 /// NodeAllocatorType - The AllocatorType for allocating SDNodes. We use
148 /// pool allocation with recycling.
149 typedef RecyclingAllocator<BumpPtrAllocator, SDNode, sizeof(LargestSDNode),
150 AlignOf<MostAlignedSDNode>::Alignment>
151 NodeAllocatorType;
153 /// NodeAllocator - Pool allocation for nodes.
154 NodeAllocatorType NodeAllocator;
156 /// CSEMap - This structure is used to memoize nodes, automatically performing
157 /// CSE with existing nodes when a duplicate is requested.
158 FoldingSet<SDNode> CSEMap;
160 /// OperandAllocator - Pool allocation for machine-opcode SDNode operands.
161 BumpPtrAllocator OperandAllocator;
163 /// Allocator - Pool allocation for misc. objects that are created once per
164 /// SelectionDAG.
165 BumpPtrAllocator Allocator;
167 /// SDNodeOrdering - The ordering of the SDNodes. It roughly corresponds to
168 /// the ordering of the original LLVM instructions.
169 SDNodeOrdering *Ordering;
171 /// DbgInfo - Tracks dbg_value information through SDISel.
172 SDDbgInfo *DbgInfo;
174 /// VerifyNode - Sanity check the given node. Aborts if it is invalid.
175 void VerifyNode(SDNode *N);
177 /// setGraphColorHelper - Implementation of setSubgraphColor.
178 /// Return whether we had to truncate the search.
179 ///
180 bool setSubgraphColorHelper(SDNode *N, const char *Color,
181 DenseSet<SDNode *> &visited,
182 int level, bool &printed);
184 void operator=(const SelectionDAG&); // Do not implement.
185 SelectionDAG(const SelectionDAG&); // Do not implement.
187 public:
188 explicit SelectionDAG(const TargetMachine &TM);
189 ~SelectionDAG();
191 /// init - Prepare this SelectionDAG to process code in the given
192 /// MachineFunction.
193 ///
194 void init(MachineFunction &mf);
196 /// clear - Clear state and free memory necessary to make this
197 /// SelectionDAG ready to process a new block.
198 ///
199 void clear();
201 MachineFunction &getMachineFunction() const { return *MF; }
202 const TargetMachine &getTarget() const { return TM; }
203 const TargetLowering &getTargetLoweringInfo() const { return TLI; }
204 const TargetSelectionDAGInfo &getSelectionDAGInfo() const { return TSI; }
205 LLVMContext *getContext() const {return Context; }
207 /// viewGraph - Pop up a GraphViz/gv window with the DAG rendered using 'dot'.
208 ///
209 void viewGraph(const std::string &Title);
210 void viewGraph();
212 #ifndef NDEBUG
213 std::map<const SDNode *, std::string> NodeGraphAttrs;
214 #endif
216 /// clearGraphAttrs - Clear all previously defined node graph attributes.
217 /// Intended to be used from a debugging tool (eg. gdb).
218 void clearGraphAttrs();
220 /// setGraphAttrs - Set graph attributes for a node. (eg. "color=red".)
221 ///
222 void setGraphAttrs(const SDNode *N, const char *Attrs);
224 /// getGraphAttrs - Get graph attributes for a node. (eg. "color=red".)
225 /// Used from getNodeAttributes.
226 const std::string getGraphAttrs(const SDNode *N) const;
228 /// setGraphColor - Convenience for setting node color attribute.
229 ///
230 void setGraphColor(const SDNode *N, const char *Color);
232 /// setGraphColor - Convenience for setting subgraph color attribute.
233 ///
234 void setSubgraphColor(SDNode *N, const char *Color);
236 typedef ilist<SDNode>::const_iterator allnodes_const_iterator;
237 allnodes_const_iterator allnodes_begin() const { return AllNodes.begin(); }
238 allnodes_const_iterator allnodes_end() const { return AllNodes.end(); }
239 typedef ilist<SDNode>::iterator allnodes_iterator;
240 allnodes_iterator allnodes_begin() { return AllNodes.begin(); }
241 allnodes_iterator allnodes_end() { return AllNodes.end(); }
242 ilist<SDNode>::size_type allnodes_size() const {
243 return AllNodes.size();
244 }
246 /// getRoot - Return the root tag of the SelectionDAG.
247 ///
248 const SDValue &getRoot() const { return Root; }
250 /// getEntryNode - Return the token chain corresponding to the entry of the
251 /// function.
252 SDValue getEntryNode() const {
253 return SDValue(const_cast<SDNode *>(&EntryNode), 0);
254 }
256 /// setRoot - Set the current root tag of the SelectionDAG.
257 ///
258 const SDValue &setRoot(SDValue N) {
259 assert((!N.getNode() || N.getValueType() == MVT::Other) &&
260 "DAG root value is not a chain!");
261 if (N.getNode())
262 checkForCycles(N.getNode());
263 Root = N;
264 if (N.getNode())
265 checkForCycles(this);
266 return Root;
267 }
269 /// Combine - This iterates over the nodes in the SelectionDAG, folding
270 /// certain types of nodes together, or eliminating superfluous nodes. The
271 /// Level argument controls whether Combine is allowed to produce nodes and
272 /// types that are illegal on the target.
273 void Combine(CombineLevel Level, AliasAnalysis &AA,
274 CodeGenOpt::Level OptLevel);
276 /// LegalizeTypes - This transforms the SelectionDAG into a SelectionDAG that
277 /// only uses types natively supported by the target. Returns "true" if it
278 /// made any changes.
279 ///
280 /// Note that this is an involved process that may invalidate pointers into
281 /// the graph.
282 bool LegalizeTypes();
284 /// Legalize - This transforms the SelectionDAG into a SelectionDAG that is
285 /// compatible with the target instruction selector, as indicated by the
286 /// TargetLowering object.
287 ///
288 /// Note that this is an involved process that may invalidate pointers into
289 /// the graph.
290 void Legalize(CodeGenOpt::Level OptLevel);
292 /// LegalizeVectors - This transforms the SelectionDAG into a SelectionDAG
293 /// that only uses vector math operations supported by the target. This is
294 /// necessary as a separate step from Legalize because unrolling a vector
295 /// operation can introduce illegal types, which requires running
296 /// LegalizeTypes again.
297 ///
298 /// This returns true if it made any changes; in that case, LegalizeTypes
299 /// is called again before Legalize.
300 ///
301 /// Note that this is an involved process that may invalidate pointers into
302 /// the graph.
303 bool LegalizeVectors();
305 /// RemoveDeadNodes - This method deletes all unreachable nodes in the
306 /// SelectionDAG.
307 void RemoveDeadNodes();
309 /// DeleteNode - Remove the specified node from the system. This node must
310 /// have no referrers.
311 void DeleteNode(SDNode *N);
313 /// getVTList - Return an SDVTList that represents the list of values
314 /// specified.
315 SDVTList getVTList(EVT VT);
316 SDVTList getVTList(EVT VT1, EVT VT2);
317 SDVTList getVTList(EVT VT1, EVT VT2, EVT VT3);
318 SDVTList getVTList(EVT VT1, EVT VT2, EVT VT3, EVT VT4);
319 SDVTList getVTList(const EVT *VTs, unsigned NumVTs);
321 //===--------------------------------------------------------------------===//
322 // Node creation methods.
323 //
324 SDValue getConstant(uint64_t Val, EVT VT, bool isTarget = false);
325 SDValue getConstant(const APInt &Val, EVT VT, bool isTarget = false);
326 SDValue getConstant(const ConstantInt &Val, EVT VT, bool isTarget = false);
327 SDValue getIntPtrConstant(uint64_t Val, bool isTarget = false);
328 SDValue getTargetConstant(uint64_t Val, EVT VT) {
329 return getConstant(Val, VT, true);
330 }
331 SDValue getTargetConstant(const APInt &Val, EVT VT) {
332 return getConstant(Val, VT, true);
333 }
334 SDValue getTargetConstant(const ConstantInt &Val, EVT VT) {
335 return getConstant(Val, VT, true);
336 }
337 // The forms below that take a double should only be used for simple
338 // constants that can be exactly represented in VT. No checks are made.
339 SDValue getConstantFP(double Val, EVT VT, bool isTarget = false);
340 SDValue getConstantFP(const APFloat& Val, EVT VT, bool isTarget = false);
341 SDValue getConstantFP(const ConstantFP &CF, EVT VT, bool isTarget = false);
342 SDValue getTargetConstantFP(double Val, EVT VT) {
343 return getConstantFP(Val, VT, true);
344 }
345 SDValue getTargetConstantFP(const APFloat& Val, EVT VT) {
346 return getConstantFP(Val, VT, true);
347 }
348 SDValue getTargetConstantFP(const ConstantFP &Val, EVT VT) {
349 return getConstantFP(Val, VT, true);
350 }
351 SDValue getGlobalAddress(const GlobalValue *GV, DebugLoc DL, EVT VT,
352 int64_t offset = 0, bool isTargetGA = false,
353 unsigned char TargetFlags = 0);
354 SDValue getTargetGlobalAddress(const GlobalValue *GV, DebugLoc DL, EVT VT,
355 int64_t offset = 0,
356 unsigned char TargetFlags = 0) {
357 return getGlobalAddress(GV, DL, VT, offset, true, TargetFlags);
358 }
359 SDValue getFrameIndex(int FI, EVT VT, bool isTarget = false);
360 SDValue getTargetFrameIndex(int FI, EVT VT) {
361 return getFrameIndex(FI, VT, true);
362 }
363 SDValue getJumpTable(int JTI, EVT VT, bool isTarget = false,
364 unsigned char TargetFlags = 0);
365 SDValue getTargetJumpTable(int JTI, EVT VT, unsigned char TargetFlags = 0) {
366 return getJumpTable(JTI, VT, true, TargetFlags);
367 }
368 SDValue getConstantPool(const Constant *C, EVT VT,
369 unsigned Align = 0, int Offs = 0, bool isT=false,
370 unsigned char TargetFlags = 0);
371 SDValue getTargetConstantPool(const Constant *C, EVT VT,
372 unsigned Align = 0, int Offset = 0,
373 unsigned char TargetFlags = 0) {
374 return getConstantPool(C, VT, Align, Offset, true, TargetFlags);
375 }
376 SDValue getConstantPool(MachineConstantPoolValue *C, EVT VT,
377 unsigned Align = 0, int Offs = 0, bool isT=false,
378 unsigned char TargetFlags = 0);
379 SDValue getTargetConstantPool(MachineConstantPoolValue *C,
380 EVT VT, unsigned Align = 0,
381 int Offset = 0, unsigned char TargetFlags=0) {
382 return getConstantPool(C, VT, Align, Offset, true, TargetFlags);
383 }
384 // When generating a branch to a BB, we don't in general know enough
385 // to provide debug info for the BB at that time, so keep this one around.
386 SDValue getBasicBlock(MachineBasicBlock *MBB);
387 SDValue getBasicBlock(MachineBasicBlock *MBB, DebugLoc dl);
388 SDValue getExternalSymbol(const char *Sym, EVT VT);
389 SDValue getExternalSymbol(const char *Sym, DebugLoc dl, EVT VT);
390 SDValue getTargetExternalSymbol(const char *Sym, EVT VT,
391 unsigned char TargetFlags = 0);
392 SDValue getValueType(EVT);
393 SDValue getRegister(unsigned Reg, EVT VT);
394 SDValue getEHLabel(DebugLoc dl, SDValue Root, MCSymbol *Label);
395 SDValue getBlockAddress(const BlockAddress *BA, EVT VT,
396 bool isTarget = false, unsigned char TargetFlags = 0);
398 SDValue getCopyToReg(SDValue Chain, DebugLoc dl, unsigned Reg, SDValue N) {
399 return getNode(ISD::CopyToReg, dl, MVT::Other, Chain,
400 getRegister(Reg, N.getValueType()), N);
401 }
403 // This version of the getCopyToReg method takes an extra operand, which
404 // indicates that there is potentially an incoming flag value (if Flag is not
405 // null) and that there should be a flag result.
406 SDValue getCopyToReg(SDValue Chain, DebugLoc dl, unsigned Reg, SDValue N,
407 SDValue Flag) {
408 SDVTList VTs = getVTList(MVT::Other, MVT::Flag);
409 SDValue Ops[] = { Chain, getRegister(Reg, N.getValueType()), N, Flag };
410 return getNode(ISD::CopyToReg, dl, VTs, Ops, Flag.getNode() ? 4 : 3);
411 }
413 // Similar to last getCopyToReg() except parameter Reg is a SDValue
414 SDValue getCopyToReg(SDValue Chain, DebugLoc dl, SDValue Reg, SDValue N,
415 SDValue Flag) {
416 SDVTList VTs = getVTList(MVT::Other, MVT::Flag);
417 SDValue Ops[] = { Chain, Reg, N, Flag };
418 return getNode(ISD::CopyToReg, dl, VTs, Ops, Flag.getNode() ? 4 : 3);
419 }
421 SDValue getCopyFromReg(SDValue Chain, DebugLoc dl, unsigned Reg, EVT VT) {
422 SDVTList VTs = getVTList(VT, MVT::Other);
423 SDValue Ops[] = { Chain, getRegister(Reg, VT) };
424 return getNode(ISD::CopyFromReg, dl, VTs, Ops, 2);
425 }
427 // This version of the getCopyFromReg method takes an extra operand, which
428 // indicates that there is potentially an incoming flag value (if Flag is not
429 // null) and that there should be a flag result.
430 SDValue getCopyFromReg(SDValue Chain, DebugLoc dl, unsigned Reg, EVT VT,
431 SDValue Flag) {
432 SDVTList VTs = getVTList(VT, MVT::Other, MVT::Flag);
433 SDValue Ops[] = { Chain, getRegister(Reg, VT), Flag };
434 return getNode(ISD::CopyFromReg, dl, VTs, Ops, Flag.getNode() ? 3 : 2);
435 }
437 SDValue getCondCode(ISD::CondCode Cond);
439 /// Returns the ConvertRndSat Note: Avoid using this node because it may
440 /// disappear in the future and most targets don't support it.
441 SDValue getConvertRndSat(EVT VT, DebugLoc dl, SDValue Val, SDValue DTy,
442 SDValue STy,
443 SDValue Rnd, SDValue Sat, ISD::CvtCode Code);
445 /// getVectorShuffle - Return an ISD::VECTOR_SHUFFLE node. The number of
446 /// elements in VT, which must be a vector type, must match the number of
447 /// mask elements NumElts. A integer mask element equal to -1 is treated as
448 /// undefined.
449 SDValue getVectorShuffle(EVT VT, DebugLoc dl, SDValue N1, SDValue N2,
450 const int *MaskElts);
452 /// getSExtOrTrunc - Convert Op, which must be of integer type, to the
453 /// integer type VT, by either sign-extending or truncating it.
454 SDValue getSExtOrTrunc(SDValue Op, DebugLoc DL, EVT VT);
456 /// getZExtOrTrunc - Convert Op, which must be of integer type, to the
457 /// integer type VT, by either zero-extending or truncating it.
458 SDValue getZExtOrTrunc(SDValue Op, DebugLoc DL, EVT VT);
460 /// getZeroExtendInReg - Return the expression required to zero extend the Op
461 /// value assuming it was the smaller SrcTy value.
462 SDValue getZeroExtendInReg(SDValue Op, DebugLoc DL, EVT SrcTy);
464 /// getNOT - Create a bitwise NOT operation as (XOR Val, -1).
465 SDValue getNOT(DebugLoc DL, SDValue Val, EVT VT);
467 /// getCALLSEQ_START - Return a new CALLSEQ_START node, which always must have
468 /// a flag result (to ensure it's not CSE'd). CALLSEQ_START does not have a
469 /// useful DebugLoc.
470 SDValue getCALLSEQ_START(SDValue Chain, SDValue Op) {
471 SDVTList VTs = getVTList(MVT::Other, MVT::Flag);
472 SDValue Ops[] = { Chain, Op };
473 return getNode(ISD::CALLSEQ_START, DebugLoc(), VTs, Ops, 2);
474 }
476 /// getCALLSEQ_END - Return a new CALLSEQ_END node, which always must have a
477 /// flag result (to ensure it's not CSE'd). CALLSEQ_END does not have
478 /// a useful DebugLoc.
479 SDValue getCALLSEQ_END(SDValue Chain, SDValue Op1, SDValue Op2,
480 SDValue InFlag) {
481 SDVTList NodeTys = getVTList(MVT::Other, MVT::Flag);
482 SmallVector<SDValue, 4> Ops;
483 Ops.push_back(Chain);
484 Ops.push_back(Op1);
485 Ops.push_back(Op2);
486 Ops.push_back(InFlag);
487 return getNode(ISD::CALLSEQ_END, DebugLoc(), NodeTys, &Ops[0],
488 (unsigned)Ops.size() - (InFlag.getNode() == 0 ? 1 : 0));
489 }
491 /// getUNDEF - Return an UNDEF node. UNDEF does not have a useful DebugLoc.
492 SDValue getUNDEF(EVT VT) {
493 return getNode(ISD::UNDEF, DebugLoc(), VT);
494 }
496 /// getGLOBAL_OFFSET_TABLE - Return a GLOBAL_OFFSET_TABLE node. This does
497 /// not have a useful DebugLoc.
498 SDValue getGLOBAL_OFFSET_TABLE(EVT VT) {
499 return getNode(ISD::GLOBAL_OFFSET_TABLE, DebugLoc(), VT);
500 }
502 /// getNode - Gets or creates the specified node.
503 ///
504 SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT);
505 SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT, SDValue N);
506 SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT, SDValue N1, SDValue N2);
507 SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT,
508 SDValue N1, SDValue N2, SDValue N3);
509 SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT,
510 SDValue N1, SDValue N2, SDValue N3, SDValue N4);
511 SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT,
512 SDValue N1, SDValue N2, SDValue N3, SDValue N4,
513 SDValue N5);
514 SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT,
515 const SDUse *Ops, unsigned NumOps);
516 SDValue getNode(unsigned Opcode, DebugLoc DL, EVT VT,
517 const SDValue *Ops, unsigned NumOps);
518 SDValue getNode(unsigned Opcode, DebugLoc DL,
519 const std::vector<EVT> &ResultTys,
520 const SDValue *Ops, unsigned NumOps);
521 SDValue getNode(unsigned Opcode, DebugLoc DL, const EVT *VTs, unsigned NumVTs,
522 const SDValue *Ops, unsigned NumOps);
523 SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs,
524 const SDValue *Ops, unsigned NumOps);
525 SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs);
526 SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs, SDValue N);
527 SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs,
528 SDValue N1, SDValue N2);
529 SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs,
530 SDValue N1, SDValue N2, SDValue N3);
531 SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs,
532 SDValue N1, SDValue N2, SDValue N3, SDValue N4);
533 SDValue getNode(unsigned Opcode, DebugLoc DL, SDVTList VTs,
534 SDValue N1, SDValue N2, SDValue N3, SDValue N4,
535 SDValue N5);
537 /// getStackArgumentTokenFactor - Compute a TokenFactor to force all
538 /// the incoming stack arguments to be loaded from the stack. This is
539 /// used in tail call lowering to protect stack arguments from being
540 /// clobbered.
541 SDValue getStackArgumentTokenFactor(SDValue Chain);
543 SDValue getMemcpy(SDValue Chain, DebugLoc dl, SDValue Dst, SDValue Src,
544 SDValue Size, unsigned Align, bool isVol, bool AlwaysInline,
545 const Value *DstSV, uint64_t DstSVOff,
546 const Value *SrcSV, uint64_t SrcSVOff);
548 SDValue getMemmove(SDValue Chain, DebugLoc dl, SDValue Dst, SDValue Src,
549 SDValue Size, unsigned Align, bool isVol,
550 const Value *DstSV, uint64_t DstOSVff,
551 const Value *SrcSV, uint64_t SrcSVOff);
553 SDValue getMemset(SDValue Chain, DebugLoc dl, SDValue Dst, SDValue Src,
554 SDValue Size, unsigned Align, bool isVol,
555 const Value *DstSV, uint64_t DstSVOff);
557 /// getSetCC - Helper function to make it easier to build SetCC's if you just
558 /// have an ISD::CondCode instead of an SDValue.
559 ///
560 SDValue getSetCC(DebugLoc DL, EVT VT, SDValue LHS, SDValue RHS,
561 ISD::CondCode Cond) {
562 return getNode(ISD::SETCC, DL, VT, LHS, RHS, getCondCode(Cond));
563 }
565 /// getVSetCC - Helper function to make it easier to build VSetCC's nodes
566 /// if you just have an ISD::CondCode instead of an SDValue.
567 ///
568 SDValue getVSetCC(DebugLoc DL, EVT VT, SDValue LHS, SDValue RHS,
569 ISD::CondCode Cond) {
570 return getNode(ISD::VSETCC, DL, VT, LHS, RHS, getCondCode(Cond));
571 }
573 /// getSelectCC - Helper function to make it easier to build SelectCC's if you
574 /// just have an ISD::CondCode instead of an SDValue.
575 ///
576 SDValue getSelectCC(DebugLoc DL, SDValue LHS, SDValue RHS,
577 SDValue True, SDValue False, ISD::CondCode Cond) {
578 return getNode(ISD::SELECT_CC, DL, True.getValueType(),
579 LHS, RHS, True, False, getCondCode(Cond));
580 }
582 /// getVAArg - VAArg produces a result and token chain, and takes a pointer
583 /// and a source value as input.
584 SDValue getVAArg(EVT VT, DebugLoc dl, SDValue Chain, SDValue Ptr,
585 SDValue SV, unsigned Align);
587 /// getAtomic - Gets a node for an atomic op, produces result and chain and
588 /// takes 3 operands
589 SDValue getAtomic(unsigned Opcode, DebugLoc dl, EVT MemVT, SDValue Chain,
590 SDValue Ptr, SDValue Cmp, SDValue Swp, const Value* PtrVal,
591 unsigned Alignment=0);
592 SDValue getAtomic(unsigned Opcode, DebugLoc dl, EVT MemVT, SDValue Chain,
593 SDValue Ptr, SDValue Cmp, SDValue Swp,
594 MachineMemOperand *MMO);
596 /// getAtomic - Gets a node for an atomic op, produces result and chain and
597 /// takes 2 operands.
598 SDValue getAtomic(unsigned Opcode, DebugLoc dl, EVT MemVT, SDValue Chain,
599 SDValue Ptr, SDValue Val, const Value* PtrVal,
600 unsigned Alignment = 0);
601 SDValue getAtomic(unsigned Opcode, DebugLoc dl, EVT MemVT, SDValue Chain,
602 SDValue Ptr, SDValue Val,
603 MachineMemOperand *MMO);
605 /// getMemIntrinsicNode - Creates a MemIntrinsicNode that may produce a
606 /// result and takes a list of operands. Opcode may be INTRINSIC_VOID,
607 /// INTRINSIC_W_CHAIN, or a target-specific opcode with a value not
608 /// less than FIRST_TARGET_MEMORY_OPCODE.
609 SDValue getMemIntrinsicNode(unsigned Opcode, DebugLoc dl,
610 const EVT *VTs, unsigned NumVTs,
611 const SDValue *Ops, unsigned NumOps,
612 EVT MemVT, const Value *srcValue, int SVOff,
613 unsigned Align = 0, bool Vol = false,
614 bool ReadMem = true, bool WriteMem = true);
616 SDValue getMemIntrinsicNode(unsigned Opcode, DebugLoc dl, SDVTList VTList,
617 const SDValue *Ops, unsigned NumOps,
618 EVT MemVT, const Value *srcValue, int SVOff,
619 unsigned Align = 0, bool Vol = false,
620 bool ReadMem = true, bool WriteMem = true);
622 SDValue getMemIntrinsicNode(unsigned Opcode, DebugLoc dl, SDVTList VTList,
623 const SDValue *Ops, unsigned NumOps,
624 EVT MemVT, MachineMemOperand *MMO);
626 /// getMergeValues - Create a MERGE_VALUES node from the given operands.
627 SDValue getMergeValues(const SDValue *Ops, unsigned NumOps, DebugLoc dl);
629 /// getLoad - Loads are not normal binary operators: their result type is not
630 /// determined by their operands, and they produce a value AND a token chain.
631 ///
632 SDValue getLoad(EVT VT, DebugLoc dl, SDValue Chain, SDValue Ptr,
633 const Value *SV, int SVOffset, bool isVolatile,
634 bool isNonTemporal, unsigned Alignment);
635 SDValue getExtLoad(ISD::LoadExtType ExtType, EVT VT, DebugLoc dl,
636 SDValue Chain, SDValue Ptr, const Value *SV,
637 int SVOffset, EVT MemVT, bool isVolatile,
638 bool isNonTemporal, unsigned Alignment);
639 SDValue getIndexedLoad(SDValue OrigLoad, DebugLoc dl, SDValue Base,
640 SDValue Offset, ISD::MemIndexedMode AM);
641 SDValue getLoad(ISD::MemIndexedMode AM, ISD::LoadExtType ExtType,
642 EVT VT, DebugLoc dl,
643 SDValue Chain, SDValue Ptr, SDValue Offset,
644 const Value *SV, int SVOffset, EVT MemVT,
645 bool isVolatile, bool isNonTemporal, unsigned Alignment);
646 SDValue getLoad(ISD::MemIndexedMode AM, ISD::LoadExtType ExtType,
647 EVT VT, DebugLoc dl,
648 SDValue Chain, SDValue Ptr, SDValue Offset,
649 EVT MemVT, MachineMemOperand *MMO);
651 /// getStore - Helper function to build ISD::STORE nodes.
652 ///
653 SDValue getStore(SDValue Chain, DebugLoc dl, SDValue Val, SDValue Ptr,
654 const Value *SV, int SVOffset, bool isVolatile,
655 bool isNonTemporal, unsigned Alignment);
656 SDValue getStore(SDValue Chain, DebugLoc dl, SDValue Val, SDValue Ptr,
657 MachineMemOperand *MMO);
658 SDValue getTruncStore(SDValue Chain, DebugLoc dl, SDValue Val, SDValue Ptr,
659 const Value *SV, int SVOffset, EVT TVT,
660 bool isNonTemporal, bool isVolatile,
661 unsigned Alignment);
662 SDValue getTruncStore(SDValue Chain, DebugLoc dl, SDValue Val, SDValue Ptr,
663 EVT TVT, MachineMemOperand *MMO);
664 SDValue getIndexedStore(SDValue OrigStoe, DebugLoc dl, SDValue Base,
665 SDValue Offset, ISD::MemIndexedMode AM);
667 /// getSrcValue - Construct a node to track a Value* through the backend.
668 SDValue getSrcValue(const Value *v);
670 /// getMDNode - Return an MDNodeSDNode which holds an MDNode.
671 SDValue getMDNode(const MDNode *MD);
673 /// getShiftAmountOperand - Return the specified value casted to
674 /// the target's desired shift amount type.
675 SDValue getShiftAmountOperand(SDValue Op);
677 /// UpdateNodeOperands - *Mutate* the specified node in-place to have the
678 /// specified operands. If the resultant node already exists in the DAG,
679 /// this does not modify the specified node, instead it returns the node that
680 /// already exists. If the resultant node does not exist in the DAG, the
681 /// input node is returned. As a degenerate case, if you specify the same
682 /// input operands as the node already has, the input node is returned.
683 SDNode *UpdateNodeOperands(SDNode *N, SDValue Op);
684 SDNode *UpdateNodeOperands(SDNode *N, SDValue Op1, SDValue Op2);
685 SDNode *UpdateNodeOperands(SDNode *N, SDValue Op1, SDValue Op2,
686 SDValue Op3);
687 SDNode *UpdateNodeOperands(SDNode *N, SDValue Op1, SDValue Op2,
688 SDValue Op3, SDValue Op4);
689 SDNode *UpdateNodeOperands(SDNode *N, SDValue Op1, SDValue Op2,
690 SDValue Op3, SDValue Op4, SDValue Op5);
691 SDNode *UpdateNodeOperands(SDNode *N,
692 const SDValue *Ops, unsigned NumOps);
694 /// SelectNodeTo - These are used for target selectors to *mutate* the
695 /// specified node to have the specified return type, Target opcode, and
696 /// operands. Note that target opcodes are stored as
697 /// ~TargetOpcode in the node opcode field. The resultant node is returned.
698 SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT);
699 SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT, SDValue Op1);
700 SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT,
701 SDValue Op1, SDValue Op2);
702 SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT,
703 SDValue Op1, SDValue Op2, SDValue Op3);
704 SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT,
705 const SDValue *Ops, unsigned NumOps);
706 SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1, EVT VT2);
707 SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1,
708 EVT VT2, const SDValue *Ops, unsigned NumOps);
709 SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1,
710 EVT VT2, EVT VT3, const SDValue *Ops, unsigned NumOps);
711 SDNode *SelectNodeTo(SDNode *N, unsigned MachineOpc, EVT VT1,
712 EVT VT2, EVT VT3, EVT VT4, const SDValue *Ops,
713 unsigned NumOps);
714 SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1,
715 EVT VT2, SDValue Op1);
716 SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1,
717 EVT VT2, SDValue Op1, SDValue Op2);
718 SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1,
719 EVT VT2, SDValue Op1, SDValue Op2, SDValue Op3);
720 SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, EVT VT1,
721 EVT VT2, EVT VT3, SDValue Op1, SDValue Op2, SDValue Op3);
722 SDNode *SelectNodeTo(SDNode *N, unsigned TargetOpc, SDVTList VTs,
723 const SDValue *Ops, unsigned NumOps);
725 /// MorphNodeTo - This *mutates* the specified node to have the specified
726 /// return type, opcode, and operands.
727 SDNode *MorphNodeTo(SDNode *N, unsigned Opc, SDVTList VTs,
728 const SDValue *Ops, unsigned NumOps);
730 /// getMachineNode - These are used for target selectors to create a new node
731 /// with specified return type(s), MachineInstr opcode, and operands.
732 ///
733 /// Note that getMachineNode returns the resultant node. If there is already
734 /// a node of the specified opcode and operands, it returns that node instead
735 /// of the current one.
736 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT);
737 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT,
738 SDValue Op1);
739 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT,
740 SDValue Op1, SDValue Op2);
741 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT,
742 SDValue Op1, SDValue Op2, SDValue Op3);
743 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT,
744 const SDValue *Ops, unsigned NumOps);
745 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2);
746 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2,
747 SDValue Op1);
748 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1,
749 EVT VT2, SDValue Op1, SDValue Op2);
750 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1,
751 EVT VT2, SDValue Op1, SDValue Op2, SDValue Op3);
752 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2,
753 const SDValue *Ops, unsigned NumOps);
754 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2,
755 EVT VT3, SDValue Op1, SDValue Op2);
756 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2,
757 EVT VT3, SDValue Op1, SDValue Op2, SDValue Op3);
758 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2,
759 EVT VT3, const SDValue *Ops, unsigned NumOps);
760 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, EVT VT1, EVT VT2,
761 EVT VT3, EVT VT4, const SDValue *Ops, unsigned NumOps);
762 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl,
763 const std::vector<EVT> &ResultTys, const SDValue *Ops,
764 unsigned NumOps);
765 MachineSDNode *getMachineNode(unsigned Opcode, DebugLoc dl, SDVTList VTs,
766 const SDValue *Ops, unsigned NumOps);
768 /// getTargetExtractSubreg - A convenience function for creating
769 /// TargetInstrInfo::EXTRACT_SUBREG nodes.
770 SDValue getTargetExtractSubreg(int SRIdx, DebugLoc DL, EVT VT,
771 SDValue Operand);
773 /// getTargetInsertSubreg - A convenience function for creating
774 /// TargetInstrInfo::INSERT_SUBREG nodes.
775 SDValue getTargetInsertSubreg(int SRIdx, DebugLoc DL, EVT VT,
776 SDValue Operand, SDValue Subreg);
778 /// getNodeIfExists - Get the specified node if it's already available, or
779 /// else return NULL.
780 SDNode *getNodeIfExists(unsigned Opcode, SDVTList VTs,
781 const SDValue *Ops, unsigned NumOps);
783 /// getDbgValue - Creates a SDDbgValue node.
784 ///
785 SDDbgValue *getDbgValue(MDNode *MDPtr, SDNode *N, unsigned R, uint64_t Off,
786 DebugLoc DL, unsigned O);
787 SDDbgValue *getDbgValue(MDNode *MDPtr, const Value *C, uint64_t Off,
788 DebugLoc DL, unsigned O);
789 SDDbgValue *getDbgValue(MDNode *MDPtr, unsigned FI, uint64_t Off,
790 DebugLoc DL, unsigned O);
792 /// DAGUpdateListener - Clients of various APIs that cause global effects on
793 /// the DAG can optionally implement this interface. This allows the clients
794 /// to handle the various sorts of updates that happen.
795 class DAGUpdateListener {
796 public:
797 virtual ~DAGUpdateListener();
799 /// NodeDeleted - The node N that was deleted and, if E is not null, an
800 /// equivalent node E that replaced it.
801 virtual void NodeDeleted(SDNode *N, SDNode *E) = 0;
803 /// NodeUpdated - The node N that was updated.
804 virtual void NodeUpdated(SDNode *N) = 0;
805 };
807 /// RemoveDeadNode - Remove the specified node from the system. If any of its
808 /// operands then becomes dead, remove them as well. Inform UpdateListener
809 /// for each node deleted.
810 void RemoveDeadNode(SDNode *N, DAGUpdateListener *UpdateListener = 0);
812 /// RemoveDeadNodes - This method deletes the unreachable nodes in the
813 /// given list, and any nodes that become unreachable as a result.
814 void RemoveDeadNodes(SmallVectorImpl<SDNode *> &DeadNodes,
815 DAGUpdateListener *UpdateListener = 0);
817 /// ReplaceAllUsesWith - Modify anything using 'From' to use 'To' instead.
818 /// This can cause recursive merging of nodes in the DAG. Use the first
819 /// version if 'From' is known to have a single result, use the second
820 /// if you have two nodes with identical results (or if 'To' has a superset
821 /// of the results of 'From'), use the third otherwise.
822 ///
823 /// These methods all take an optional UpdateListener, which (if not null) is
824 /// informed about nodes that are deleted and modified due to recursive
825 /// changes in the dag.
826 ///
827 /// These functions only replace all existing uses. It's possible that as
828 /// these replacements are being performed, CSE may cause the From node
829 /// to be given new uses. These new uses of From are left in place, and
830 /// not automatically transfered to To.
831 ///
832 void ReplaceAllUsesWith(SDValue From, SDValue Op,
833 DAGUpdateListener *UpdateListener = 0);
834 void ReplaceAllUsesWith(SDNode *From, SDNode *To,
835 DAGUpdateListener *UpdateListener = 0);
836 void ReplaceAllUsesWith(SDNode *From, const SDValue *To,
837 DAGUpdateListener *UpdateListener = 0);
839 /// ReplaceAllUsesOfValueWith - Replace any uses of From with To, leaving
840 /// uses of other values produced by From.Val alone.
841 void ReplaceAllUsesOfValueWith(SDValue From, SDValue To,
842 DAGUpdateListener *UpdateListener = 0);
844 /// ReplaceAllUsesOfValuesWith - Like ReplaceAllUsesOfValueWith, but
845 /// for multiple values at once. This correctly handles the case where
846 /// there is an overlap between the From values and the To values.
847 void ReplaceAllUsesOfValuesWith(const SDValue *From, const SDValue *To,
848 unsigned Num,
849 DAGUpdateListener *UpdateListener = 0);
851 /// AssignTopologicalOrder - Topological-sort the AllNodes list and a
852 /// assign a unique node id for each node in the DAG based on their
853 /// topological order. Returns the number of nodes.
854 unsigned AssignTopologicalOrder();
856 /// RepositionNode - Move node N in the AllNodes list to be immediately
857 /// before the given iterator Position. This may be used to update the
858 /// topological ordering when the list of nodes is modified.
859 void RepositionNode(allnodes_iterator Position, SDNode *N) {
860 AllNodes.insert(Position, AllNodes.remove(N));
861 }
863 /// isCommutativeBinOp - Returns true if the opcode is a commutative binary
864 /// operation.
865 static bool isCommutativeBinOp(unsigned Opcode) {
866 // FIXME: This should get its info from the td file, so that we can include
867 // target info.
868 switch (Opcode) {
869 case ISD::ADD:
870 case ISD::MUL:
871 case ISD::MULHU:
872 case ISD::MULHS:
873 case ISD::SMUL_LOHI:
874 case ISD::UMUL_LOHI:
875 case ISD::FADD:
876 case ISD::FMUL:
877 case ISD::AND:
878 case ISD::OR:
879 case ISD::XOR:
880 case ISD::SADDO:
881 case ISD::UADDO:
882 case ISD::ADDC:
883 case ISD::ADDE: return true;
884 default: return false;
885 }
886 }
888 /// AssignOrdering - Assign an order to the SDNode.
889 void AssignOrdering(const SDNode *SD, unsigned Order);
891 /// GetOrdering - Get the order for the SDNode.
892 unsigned GetOrdering(const SDNode *SD) const;
894 /// AddDbgValue - Add a dbg_value SDNode. If SD is non-null that means the
895 /// value is produced by SD.
896 void AddDbgValue(SDDbgValue *DB, SDNode *SD, bool isParameter);
898 /// GetDbgValues - Get the debug values which reference the given SDNode.
899 SmallVector<SDDbgValue*,2> &GetDbgValues(const SDNode* SD) {
900 return DbgInfo->getSDDbgValues(SD);
901 }
903 /// hasDebugValues - Return true if there are any SDDbgValue nodes associated
904 /// with this SelectionDAG.
905 bool hasDebugValues() const { return !DbgInfo->empty(); }
907 SDDbgInfo::DbgIterator DbgBegin() { return DbgInfo->DbgBegin(); }
908 SDDbgInfo::DbgIterator DbgEnd() { return DbgInfo->DbgEnd(); }
909 SDDbgInfo::DbgIterator ByvalParmDbgBegin() {
910 return DbgInfo->ByvalParmDbgBegin();
911 }
912 SDDbgInfo::DbgIterator ByvalParmDbgEnd() {
913 return DbgInfo->ByvalParmDbgEnd();
914 }
916 void dump() const;
918 /// CreateStackTemporary - Create a stack temporary, suitable for holding the
919 /// specified value type. If minAlign is specified, the slot size will have
920 /// at least that alignment.
921 SDValue CreateStackTemporary(EVT VT, unsigned minAlign = 1);
923 /// CreateStackTemporary - Create a stack temporary suitable for holding
924 /// either of the specified value types.
925 SDValue CreateStackTemporary(EVT VT1, EVT VT2);
927 /// FoldConstantArithmetic -
928 SDValue FoldConstantArithmetic(unsigned Opcode,
929 EVT VT,
930 ConstantSDNode *Cst1,
931 ConstantSDNode *Cst2);
933 /// FoldSetCC - Constant fold a setcc to true or false.
934 SDValue FoldSetCC(EVT VT, SDValue N1,
935 SDValue N2, ISD::CondCode Cond, DebugLoc dl);
937 /// SignBitIsZero - Return true if the sign bit of Op is known to be zero. We
938 /// use this predicate to simplify operations downstream.
939 bool SignBitIsZero(SDValue Op, unsigned Depth = 0) const;
941 /// MaskedValueIsZero - Return true if 'Op & Mask' is known to be zero. We
942 /// use this predicate to simplify operations downstream. Op and Mask are
943 /// known to be the same type.
944 bool MaskedValueIsZero(SDValue Op, const APInt &Mask, unsigned Depth = 0)
945 const;
947 /// ComputeMaskedBits - Determine which of the bits specified in Mask are
948 /// known to be either zero or one and return them in the KnownZero/KnownOne
949 /// bitsets. This code only analyzes bits in Mask, in order to short-circuit
950 /// processing. Targets can implement the computeMaskedBitsForTargetNode
951 /// method in the TargetLowering class to allow target nodes to be understood.
952 void ComputeMaskedBits(SDValue Op, const APInt &Mask, APInt &KnownZero,
953 APInt &KnownOne, unsigned Depth = 0) const;
955 /// ComputeNumSignBits - Return the number of times the sign bit of the
956 /// register is replicated into the other bits. We know that at least 1 bit
957 /// is always equal to the sign bit (itself), but other cases can give us
958 /// information. For example, immediately after an "SRA X, 2", we know that
959 /// the top 3 bits are all equal to each other, so we return 3. Targets can
960 /// implement the ComputeNumSignBitsForTarget method in the TargetLowering
961 /// class to allow target nodes to be understood.
962 unsigned ComputeNumSignBits(SDValue Op, unsigned Depth = 0) const;
964 /// isKnownNeverNan - Test whether the given SDValue is known to never be NaN.
965 bool isKnownNeverNaN(SDValue Op) const;
967 /// isKnownNeverZero - Test whether the given SDValue is known to never be
968 /// positive or negative Zero.
969 bool isKnownNeverZero(SDValue Op) const;
971 /// isEqualTo - Test whether two SDValues are known to compare equal. This
972 /// is true if they are the same value, or if one is negative zero and the
973 /// other positive zero.
974 bool isEqualTo(SDValue A, SDValue B) const;
976 /// isVerifiedDebugInfoDesc - Returns true if the specified SDValue has
977 /// been verified as a debug information descriptor.
978 bool isVerifiedDebugInfoDesc(SDValue Op) const;
980 /// getShuffleScalarElt - Returns the scalar element that will make up the ith
981 /// element of the result of the vector shuffle.
982 SDValue getShuffleScalarElt(const ShuffleVectorSDNode *N, unsigned Idx);
984 /// UnrollVectorOp - Utility function used by legalize and lowering to
985 /// "unroll" a vector operation by splitting out the scalars and operating
986 /// on each element individually. If the ResNE is 0, fully unroll the vector
987 /// op. If ResNE is less than the width of the vector op, unroll up to ResNE.
988 /// If the ResNE is greater than the width of the vector op, unroll the
989 /// vector op and fill the end of the resulting vector with UNDEFS.
990 SDValue UnrollVectorOp(SDNode *N, unsigned ResNE = 0);
992 /// isConsecutiveLoad - Return true if LD is loading 'Bytes' bytes from a
993 /// location that is 'Dist' units away from the location that the 'Base' load
994 /// is loading from.
995 bool isConsecutiveLoad(LoadSDNode *LD, LoadSDNode *Base,
996 unsigned Bytes, int Dist) const;
998 /// InferPtrAlignment - Infer alignment of a load / store address. Return 0 if
999 /// it cannot be inferred.
1000 unsigned InferPtrAlignment(SDValue Ptr) const;
1002 private:
1003 bool RemoveNodeFromCSEMaps(SDNode *N);
1004 void AddModifiedNodeToCSEMaps(SDNode *N, DAGUpdateListener *UpdateListener);
1005 SDNode *FindModifiedNodeSlot(SDNode *N, SDValue Op, void *&InsertPos);
1006 SDNode *FindModifiedNodeSlot(SDNode *N, SDValue Op1, SDValue Op2,
1007 void *&InsertPos);
1008 SDNode *FindModifiedNodeSlot(SDNode *N, const SDValue *Ops, unsigned NumOps,
1009 void *&InsertPos);
1011 void DeleteNodeNotInCSEMaps(SDNode *N);
1012 void DeallocateNode(SDNode *N);
1014 unsigned getEVTAlignment(EVT MemoryVT) const;
1016 void allnodes_clear();
1018 /// VTList - List of non-single value types.
1019 std::vector<SDVTList> VTList;
1021 /// CondCodeNodes - Maps to auto-CSE operations.
1022 std::vector<CondCodeSDNode*> CondCodeNodes;
1024 std::vector<SDNode*> ValueTypeNodes;
1025 std::map<EVT, SDNode*, EVT::compareRawBits> ExtendedValueTypeNodes;
1026 StringMap<SDNode*> ExternalSymbols;
1028 std::map<std::pair<std::string, unsigned char>,SDNode*> TargetExternalSymbols;
1029 };
1031 template <> struct GraphTraits<SelectionDAG*> : public GraphTraits<SDNode*> {
1032 typedef SelectionDAG::allnodes_iterator nodes_iterator;
1033 static nodes_iterator nodes_begin(SelectionDAG *G) {
1034 return G->allnodes_begin();
1035 }
1036 static nodes_iterator nodes_end(SelectionDAG *G) {
1037 return G->allnodes_end();
1038 }
1039 };
1041 } // end namespace llvm
1043 #endif