1 //===- DIBuilder.h - Debug Information Builder ------------------*- C++ -*-===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file defines a DIBuilder that is useful for creating debugging
11 // information entries in LLVM IR form.
12 //
13 //===----------------------------------------------------------------------===//
15 #ifndef LLVM_IR_DIBUILDER_H
16 #define LLVM_IR_DIBUILDER_H
18 #include "llvm/ADT/ArrayRef.h"
19 #include "llvm/ADT/StringRef.h"
20 #include "llvm/IR/DebugInfo.h"
21 #include "llvm/IR/ValueHandle.h"
22 #include "llvm/Support/DataTypes.h"
24 namespace llvm {
25 class BasicBlock;
26 class Instruction;
27 class Function;
28 class Module;
29 class Value;
30 class LLVMContext;
31 class MDNode;
32 class StringRef;
33 class DIBasicType;
34 class DICompileUnit;
35 class DICompositeType;
36 class DIDerivedType;
37 class DIDescriptor;
38 class DIFile;
39 class DIEnumerator;
40 class DIType;
41 class DIArray;
42 class DIGlobalVariable;
43 class DIImportedEntity;
44 class DINameSpace;
45 class DIVariable;
46 class DISubrange;
47 class DILexicalBlockFile;
48 class DILexicalBlock;
49 class DIScope;
50 class DISubprogram;
51 class DITemplateTypeParameter;
52 class DITemplateValueParameter;
53 class DIObjCProperty;
55 class DIBuilder {
56 private:
57 Module &M;
58 LLVMContext &VMContext;
60 MDNode *TempEnumTypes;
61 MDNode *TempRetainTypes;
62 MDNode *TempSubprograms;
63 MDNode *TempGVs;
64 MDNode *TempImportedModules;
66 Function *DeclareFn; // llvm.dbg.declare
67 Function *ValueFn; // llvm.dbg.value
69 SmallVector<Value *, 4> AllEnumTypes;
70 /// Use TrackingVH to collect RetainTypes, since they can be updated
71 /// later on.
72 SmallVector<TrackingVH<MDNode>, 4> AllRetainTypes;
73 SmallVector<Value *, 4> AllSubprograms;
74 SmallVector<Value *, 4> AllGVs;
75 SmallVector<TrackingVH<MDNode>, 4> AllImportedModules;
77 // Private use for multiple types of template parameters.
78 DITemplateValueParameter
79 createTemplateValueParameter(unsigned Tag, DIDescriptor Scope,
80 StringRef Name, DIType Ty, Value *Val,
81 MDNode *File = nullptr, unsigned LineNo = 0,
82 unsigned ColumnNo = 0);
84 DIBuilder(const DIBuilder &) LLVM_DELETED_FUNCTION;
85 void operator=(const DIBuilder &) LLVM_DELETED_FUNCTION;
87 public:
88 explicit DIBuilder(Module &M);
89 enum ComplexAddrKind { OpPlus=1, OpDeref };
90 enum DebugEmissionKind { FullDebug=1, LineTablesOnly };
92 /// finalize - Construct any deferred debug info descriptors.
93 void finalize();
95 /// createCompileUnit - A CompileUnit provides an anchor for all debugging
96 /// information generated during this instance of compilation.
97 /// @param Lang Source programming language, eg. dwarf::DW_LANG_C99
98 /// @param File File name
99 /// @param Dir Directory
100 /// @param Producer Identify the producer of debugging information and code.
101 /// Usually this is a compiler version string.
102 /// @param isOptimized A boolean flag which indicates whether optimization
103 /// is ON or not.
104 /// @param Flags This string lists command line options. This string is
105 /// directly embedded in debug info output which may be used
106 /// by a tool analyzing generated debugging information.
107 /// @param RV This indicates runtime version for languages like
108 /// Objective-C.
109 /// @param SplitName The name of the file that we'll split debug info out
110 /// into.
111 /// @param Kind The kind of debug information to generate.
112 /// @param EmitDebugInfo A boolean flag which indicates whether debug
113 /// information should be written to the final
114 /// output or not. When this is false, debug
115 /// information annotations will be present in
116 /// the IL but they are not written to the final
117 /// assembly or object file. This supports tracking
118 /// source location information in the back end
119 /// without actually changing the output (e.g.,
120 /// when using optimization remarks).
121 DICompileUnit createCompileUnit(unsigned Lang, StringRef File,
122 StringRef Dir, StringRef Producer,
123 bool isOptimized, StringRef Flags,
124 unsigned RV,
125 StringRef SplitName = StringRef(),
126 DebugEmissionKind Kind = FullDebug,
127 bool EmitDebugInfo = true);
129 /// createFile - Create a file descriptor to hold debugging information
130 /// for a file.
131 DIFile createFile(StringRef Filename, StringRef Directory);
133 /// createEnumerator - Create a single enumerator value.
134 DIEnumerator createEnumerator(StringRef Name, int64_t Val);
136 /// \brief Create a DWARF unspecified type.
137 DIBasicType createUnspecifiedType(StringRef Name);
139 /// \brief Create C++11 nullptr type.
140 DIBasicType createNullPtrType();
142 /// createBasicType - Create debugging information entry for a basic
143 /// type.
144 /// @param Name Type name.
145 /// @param SizeInBits Size of the type.
146 /// @param AlignInBits Type alignment.
147 /// @param Encoding DWARF encoding code, e.g. dwarf::DW_ATE_float.
148 DIBasicType createBasicType(StringRef Name, uint64_t SizeInBits,
149 uint64_t AlignInBits, unsigned Encoding);
151 /// createQualifiedType - Create debugging information entry for a qualified
152 /// type, e.g. 'const int'.
153 /// @param Tag Tag identifing type, e.g. dwarf::TAG_volatile_type
154 /// @param FromTy Base Type.
155 DIDerivedType createQualifiedType(unsigned Tag, DIType FromTy);
157 /// createPointerType - Create debugging information entry for a pointer.
158 /// @param PointeeTy Type pointed by this pointer.
159 /// @param SizeInBits Size.
160 /// @param AlignInBits Alignment. (optional)
161 /// @param Name Pointer type name. (optional)
162 DIDerivedType
163 createPointerType(DIType PointeeTy, uint64_t SizeInBits,
164 uint64_t AlignInBits = 0, StringRef Name = StringRef());
166 /// \brief Create debugging information entry for a pointer to member.
167 /// @param PointeeTy Type pointed to by this pointer.
168 /// @param Class Type for which this pointer points to members of.
169 DIDerivedType createMemberPointerType(DIType PointeeTy, DIType Class);
171 /// createReferenceType - Create debugging information entry for a c++
172 /// style reference or rvalue reference type.
173 DIDerivedType createReferenceType(unsigned Tag, DIType RTy);
175 /// createTypedef - Create debugging information entry for a typedef.
176 /// @param Ty Original type.
177 /// @param Name Typedef name.
178 /// @param File File where this type is defined.
179 /// @param LineNo Line number.
180 /// @param Context The surrounding context for the typedef.
181 DIDerivedType createTypedef(DIType Ty, StringRef Name, DIFile File,
182 unsigned LineNo, DIDescriptor Context);
184 /// createFriend - Create debugging information entry for a 'friend'.
185 DIDerivedType createFriend(DIType Ty, DIType FriendTy);
187 /// createInheritance - Create debugging information entry to establish
188 /// inheritance relationship between two types.
189 /// @param Ty Original type.
190 /// @param BaseTy Base type. Ty is inherits from base.
191 /// @param BaseOffset Base offset.
192 /// @param Flags Flags to describe inheritance attribute,
193 /// e.g. private
194 DIDerivedType createInheritance(DIType Ty, DIType BaseTy,
195 uint64_t BaseOffset, unsigned Flags);
197 /// createMemberType - Create debugging information entry for a member.
198 /// @param Scope Member scope.
199 /// @param Name Member name.
200 /// @param File File where this member is defined.
201 /// @param LineNo Line number.
202 /// @param SizeInBits Member size.
203 /// @param AlignInBits Member alignment.
204 /// @param OffsetInBits Member offset.
205 /// @param Flags Flags to encode member attribute, e.g. private
206 /// @param Ty Parent type.
207 DIDerivedType
208 createMemberType(DIDescriptor Scope, StringRef Name, DIFile File,
209 unsigned LineNo, uint64_t SizeInBits, uint64_t AlignInBits,
210 uint64_t OffsetInBits, unsigned Flags, DIType Ty);
212 /// createStaticMemberType - Create debugging information entry for a
213 /// C++ static data member.
214 /// @param Scope Member scope.
215 /// @param Name Member name.
216 /// @param File File where this member is declared.
217 /// @param LineNo Line number.
218 /// @param Ty Type of the static member.
219 /// @param Flags Flags to encode member attribute, e.g. private.
220 /// @param Val Const initializer of the member.
221 DIDerivedType
222 createStaticMemberType(DIDescriptor Scope, StringRef Name,
223 DIFile File, unsigned LineNo, DIType Ty,
224 unsigned Flags, llvm::Value *Val);
226 /// createObjCIVar - Create debugging information entry for Objective-C
227 /// instance variable.
228 /// @param Name Member name.
229 /// @param File File where this member is defined.
230 /// @param LineNo Line number.
231 /// @param SizeInBits Member size.
232 /// @param AlignInBits Member alignment.
233 /// @param OffsetInBits Member offset.
234 /// @param Flags Flags to encode member attribute, e.g. private
235 /// @param Ty Parent type.
236 /// @param PropertyName Name of the Objective C property associated with
237 /// this ivar.
238 /// @param PropertyGetterName Name of the Objective C property getter
239 /// selector.
240 /// @param PropertySetterName Name of the Objective C property setter
241 /// selector.
242 /// @param PropertyAttributes Objective C property attributes.
243 DIDerivedType createObjCIVar(StringRef Name, DIFile File,
244 unsigned LineNo, uint64_t SizeInBits,
245 uint64_t AlignInBits, uint64_t OffsetInBits,
246 unsigned Flags, DIType Ty,
247 StringRef PropertyName = StringRef(),
248 StringRef PropertyGetterName = StringRef(),
249 StringRef PropertySetterName = StringRef(),
250 unsigned PropertyAttributes = 0);
252 /// createObjCIVar - Create debugging information entry for Objective-C
253 /// instance variable.
254 /// @param Name Member name.
255 /// @param File File where this member is defined.
256 /// @param LineNo Line number.
257 /// @param SizeInBits Member size.
258 /// @param AlignInBits Member alignment.
259 /// @param OffsetInBits Member offset.
260 /// @param Flags Flags to encode member attribute, e.g. private
261 /// @param Ty Parent type.
262 /// @param PropertyNode Property associated with this ivar.
263 DIDerivedType createObjCIVar(StringRef Name, DIFile File,
264 unsigned LineNo, uint64_t SizeInBits,
265 uint64_t AlignInBits, uint64_t OffsetInBits,
266 unsigned Flags, DIType Ty,
267 MDNode *PropertyNode);
269 /// createObjCProperty - Create debugging information entry for Objective-C
270 /// property.
271 /// @param Name Property name.
272 /// @param File File where this property is defined.
273 /// @param LineNumber Line number.
274 /// @param GetterName Name of the Objective C property getter selector.
275 /// @param SetterName Name of the Objective C property setter selector.
276 /// @param PropertyAttributes Objective C property attributes.
277 /// @param Ty Type.
278 DIObjCProperty createObjCProperty(StringRef Name,
279 DIFile File, unsigned LineNumber,
280 StringRef GetterName,
281 StringRef SetterName,
282 unsigned PropertyAttributes,
283 DIType Ty);
285 /// createClassType - Create debugging information entry for a class.
286 /// @param Scope Scope in which this class is defined.
287 /// @param Name class name.
288 /// @param File File where this member is defined.
289 /// @param LineNumber Line number.
290 /// @param SizeInBits Member size.
291 /// @param AlignInBits Member alignment.
292 /// @param OffsetInBits Member offset.
293 /// @param Flags Flags to encode member attribute, e.g. private
294 /// @param Elements class members.
295 /// @param VTableHolder Debug info of the base class that contains vtable
296 /// for this type. This is used in
297 /// DW_AT_containing_type. See DWARF documentation
298 /// for more info.
299 /// @param TemplateParms Template type parameters.
300 /// @param UniqueIdentifier A unique identifier for the class.
301 DICompositeType createClassType(DIDescriptor Scope, StringRef Name,
302 DIFile File, unsigned LineNumber,
303 uint64_t SizeInBits, uint64_t AlignInBits,
304 uint64_t OffsetInBits, unsigned Flags,
305 DIType DerivedFrom, DIArray Elements,
306 DIType VTableHolder = DIType(),
307 MDNode *TemplateParms = nullptr,
308 StringRef UniqueIdentifier = StringRef());
310 /// createStructType - Create debugging information entry for a struct.
311 /// @param Scope Scope in which this struct is defined.
312 /// @param Name Struct name.
313 /// @param File File where this member is defined.
314 /// @param LineNumber Line number.
315 /// @param SizeInBits Member size.
316 /// @param AlignInBits Member alignment.
317 /// @param Flags Flags to encode member attribute, e.g. private
318 /// @param Elements Struct elements.
319 /// @param RunTimeLang Optional parameter, Objective-C runtime version.
320 /// @param UniqueIdentifier A unique identifier for the struct.
321 DICompositeType createStructType(DIDescriptor Scope, StringRef Name,
322 DIFile File, unsigned LineNumber,
323 uint64_t SizeInBits, uint64_t AlignInBits,
324 unsigned Flags, DIType DerivedFrom,
325 DIArray Elements, unsigned RunTimeLang = 0,
326 DIType VTableHolder = DIType(),
327 StringRef UniqueIdentifier = StringRef());
329 /// createUnionType - Create debugging information entry for an union.
330 /// @param Scope Scope in which this union is defined.
331 /// @param Name Union name.
332 /// @param File File where this member is defined.
333 /// @param LineNumber Line number.
334 /// @param SizeInBits Member size.
335 /// @param AlignInBits Member alignment.
336 /// @param Flags Flags to encode member attribute, e.g. private
337 /// @param Elements Union elements.
338 /// @param RunTimeLang Optional parameter, Objective-C runtime version.
339 /// @param UniqueIdentifier A unique identifier for the union.
340 DICompositeType createUnionType(
341 DIDescriptor Scope, StringRef Name, DIFile File, unsigned LineNumber,
342 uint64_t SizeInBits, uint64_t AlignInBits, unsigned Flags,
343 DIArray Elements, unsigned RunTimeLang = 0,
344 StringRef UniqueIdentifier = StringRef());
346 /// createTemplateTypeParameter - Create debugging information for template
347 /// type parameter.
348 /// @param Scope Scope in which this type is defined.
349 /// @param Name Type parameter name.
350 /// @param Ty Parameter type.
351 /// @param File File where this type parameter is defined.
352 /// @param LineNo Line number.
353 /// @param ColumnNo Column Number.
354 DITemplateTypeParameter
355 createTemplateTypeParameter(DIDescriptor Scope, StringRef Name, DIType Ty,
356 MDNode *File = nullptr, unsigned LineNo = 0,
357 unsigned ColumnNo = 0);
359 /// createTemplateValueParameter - Create debugging information for template
360 /// value parameter.
361 /// @param Scope Scope in which this type is defined.
362 /// @param Name Value parameter name.
363 /// @param Ty Parameter type.
364 /// @param Val Constant parameter value.
365 /// @param File File where this type parameter is defined.
366 /// @param LineNo Line number.
367 /// @param ColumnNo Column Number.
368 DITemplateValueParameter
369 createTemplateValueParameter(DIDescriptor Scope, StringRef Name,
370 DIType Ty, Value *Val, MDNode *File = nullptr,
371 unsigned LineNo = 0, unsigned ColumnNo = 0);
373 /// \brief Create debugging information for a template template parameter.
374 /// @param Scope Scope in which this type is defined.
375 /// @param Name Value parameter name.
376 /// @param Ty Parameter type.
377 /// @param Val The fully qualified name of the template.
378 /// @param File File where this type parameter is defined.
379 /// @param LineNo Line number.
380 /// @param ColumnNo Column Number.
381 DITemplateValueParameter
382 createTemplateTemplateParameter(DIDescriptor Scope, StringRef Name,
383 DIType Ty, StringRef Val,
384 MDNode *File = nullptr, unsigned LineNo = 0,
385 unsigned ColumnNo = 0);
387 /// \brief Create debugging information for a template parameter pack.
388 /// @param Scope Scope in which this type is defined.
389 /// @param Name Value parameter name.
390 /// @param Ty Parameter type.
391 /// @param Val An array of types in the pack.
392 /// @param File File where this type parameter is defined.
393 /// @param LineNo Line number.
394 /// @param ColumnNo Column Number.
395 DITemplateValueParameter
396 createTemplateParameterPack(DIDescriptor Scope, StringRef Name,
397 DIType Ty, DIArray Val, MDNode *File = nullptr,
398 unsigned LineNo = 0, unsigned ColumnNo = 0);
400 /// createArrayType - Create debugging information entry for an array.
401 /// @param Size Array size.
402 /// @param AlignInBits Alignment.
403 /// @param Ty Element type.
404 /// @param Subscripts Subscripts.
405 DICompositeType createArrayType(uint64_t Size, uint64_t AlignInBits,
406 DIType Ty, DIArray Subscripts);
408 /// createVectorType - Create debugging information entry for a vector type.
409 /// @param Size Array size.
410 /// @param AlignInBits Alignment.
411 /// @param Ty Element type.
412 /// @param Subscripts Subscripts.
413 DICompositeType createVectorType(uint64_t Size, uint64_t AlignInBits,
414 DIType Ty, DIArray Subscripts);
416 /// createEnumerationType - Create debugging information entry for an
417 /// enumeration.
418 /// @param Scope Scope in which this enumeration is defined.
419 /// @param Name Union name.
420 /// @param File File where this member is defined.
421 /// @param LineNumber Line number.
422 /// @param SizeInBits Member size.
423 /// @param AlignInBits Member alignment.
424 /// @param Elements Enumeration elements.
425 /// @param UnderlyingType Underlying type of a C++11/ObjC fixed enum.
426 /// @param UniqueIdentifier A unique identifier for the enum.
427 DICompositeType createEnumerationType(DIDescriptor Scope, StringRef Name,
428 DIFile File, unsigned LineNumber, uint64_t SizeInBits,
429 uint64_t AlignInBits, DIArray Elements, DIType UnderlyingType,
430 StringRef UniqueIdentifier = StringRef());
432 /// createSubroutineType - Create subroutine type.
433 /// @param File File in which this subroutine is defined.
434 /// @param ParameterTypes An array of subroutine parameter types. This
435 /// includes return type at 0th index.
436 /// @param Flags E.g.: LValueReference.
437 /// These flags are used to emit dwarf attributes.
438 DICompositeType createSubroutineType(DIFile File, DIArray ParameterTypes,
439 unsigned Flags = 0);
441 /// createArtificialType - Create a new DIType with "artificial" flag set.
442 DIType createArtificialType(DIType Ty);
444 /// createObjectPointerType - Create a new DIType with the "object pointer"
445 /// flag set.
446 DIType createObjectPointerType(DIType Ty);
448 /// \brief Create a permanent forward-declared type.
449 DICompositeType createForwardDecl(unsigned Tag, StringRef Name,
450 DIDescriptor Scope, DIFile F,
451 unsigned Line, unsigned RuntimeLang = 0,
452 uint64_t SizeInBits = 0,
453 uint64_t AlignInBits = 0,
454 StringRef UniqueIdentifier = StringRef());
456 /// \brief Create a temporary forward-declared type.
457 DICompositeType createReplaceableForwardDecl(
458 unsigned Tag, StringRef Name, DIDescriptor Scope, DIFile F,
459 unsigned Line, unsigned RuntimeLang = 0, uint64_t SizeInBits = 0,
460 uint64_t AlignInBits = 0, StringRef UniqueIdentifier = StringRef());
462 /// retainType - Retain DIType in a module even if it is not referenced
463 /// through debug info anchors.
464 void retainType(DIType T);
466 /// createUnspecifiedParameter - Create unspecified parameter type
467 /// for a subroutine type.
468 DITrivialType createUnspecifiedParameter();
470 /// getOrCreateArray - Get a DIArray, create one if required.
471 DIArray getOrCreateArray(ArrayRef<Value *> Elements);
473 /// getOrCreateSubrange - Create a descriptor for a value range. This
474 /// implicitly uniques the values returned.
475 DISubrange getOrCreateSubrange(int64_t Lo, int64_t Count);
477 /// createGlobalVariable - Create a new descriptor for the specified global.
478 /// @param Name Name of the variable.
479 /// @param File File where this variable is defined.
480 /// @param LineNo Line number.
481 /// @param Ty Variable Type.
482 /// @param isLocalToUnit Boolean flag indicate whether this variable is
483 /// externally visible or not.
484 /// @param Val llvm::Value of the variable.
485 DIGlobalVariable
486 createGlobalVariable(StringRef Name, DIFile File, unsigned LineNo,
487 DITypeRef Ty, bool isLocalToUnit, llvm::Value *Val);
489 /// \brief Create a new descriptor for the specified global.
490 /// @param Name Name of the variable.
491 /// @param LinkageName Mangled variable name.
492 /// @param File File where this variable is defined.
493 /// @param LineNo Line number.
494 /// @param Ty Variable Type.
495 /// @param isLocalToUnit Boolean flag indicate whether this variable is
496 /// externally visible or not.
497 /// @param Val llvm::Value of the variable.
498 DIGlobalVariable
499 createGlobalVariable(StringRef Name, StringRef LinkageName, DIFile File,
500 unsigned LineNo, DITypeRef Ty, bool isLocalToUnit,
501 llvm::Value *Val);
503 /// createStaticVariable - Create a new descriptor for the specified
504 /// variable.
505 /// @param Context Variable scope.
506 /// @param Name Name of the variable.
507 /// @param LinkageName Mangled name of the variable.
508 /// @param File File where this variable is defined.
509 /// @param LineNo Line number.
510 /// @param Ty Variable Type.
511 /// @param isLocalToUnit Boolean flag indicate whether this variable is
512 /// externally visible or not.
513 /// @param Val llvm::Value of the variable.
514 /// @param Decl Reference to the corresponding declaration.
515 DIGlobalVariable
516 createStaticVariable(DIDescriptor Context, StringRef Name,
517 StringRef LinkageName, DIFile File, unsigned LineNo,
518 DITypeRef Ty, bool isLocalToUnit, llvm::Value *Val,
519 MDNode *Decl = nullptr);
522 /// createLocalVariable - Create a new descriptor for the specified
523 /// local variable.
524 /// @param Tag Dwarf TAG. Usually DW_TAG_auto_variable or
525 /// DW_TAG_arg_variable.
526 /// @param Scope Variable scope.
527 /// @param Name Variable name.
528 /// @param File File where this variable is defined.
529 /// @param LineNo Line number.
530 /// @param Ty Variable Type
531 /// @param AlwaysPreserve Boolean. Set to true if debug info for this
532 /// variable should be preserved in optimized build.
533 /// @param Flags Flags, e.g. artificial variable.
534 /// @param ArgNo If this variable is an argument then this argument's
535 /// number. 1 indicates 1st argument.
536 DIVariable createLocalVariable(unsigned Tag, DIDescriptor Scope,
537 StringRef Name,
538 DIFile File, unsigned LineNo,
539 DITypeRef Ty, bool AlwaysPreserve = false,
540 unsigned Flags = 0,
541 unsigned ArgNo = 0);
544 /// createComplexVariable - Create a new descriptor for the specified
545 /// variable which has a complex address expression for its address.
546 /// @param Tag Dwarf TAG. Usually DW_TAG_auto_variable or
547 /// DW_TAG_arg_variable.
548 /// @param Scope Variable scope.
549 /// @param Name Variable name.
550 /// @param F File where this variable is defined.
551 /// @param LineNo Line number.
552 /// @param Ty Variable Type
553 /// @param Addr An array of complex address operations.
554 /// @param ArgNo If this variable is an argument then this argument's
555 /// number. 1 indicates 1st argument.
556 DIVariable createComplexVariable(unsigned Tag, DIDescriptor Scope,
557 StringRef Name, DIFile F, unsigned LineNo,
558 DITypeRef Ty, ArrayRef<Value *> Addr,
559 unsigned ArgNo = 0);
561 /// createFunction - Create a new descriptor for the specified subprogram.
562 /// See comments in DISubprogram for descriptions of these fields.
563 /// @param Scope Function scope.
564 /// @param Name Function name.
565 /// @param LinkageName Mangled function name.
566 /// @param File File where this variable is defined.
567 /// @param LineNo Line number.
568 /// @param Ty Function type.
569 /// @param isLocalToUnit True if this function is not externally visible.
570 /// @param isDefinition True if this is a function definition.
571 /// @param ScopeLine Set to the beginning of the scope this starts
572 /// @param Flags e.g. is this function prototyped or not.
573 /// These flags are used to emit dwarf attributes.
574 /// @param isOptimized True if optimization is ON.
575 /// @param Fn llvm::Function pointer.
576 /// @param TParam Function template parameters.
577 DISubprogram createFunction(DIDescriptor Scope, StringRef Name,
578 StringRef LinkageName,
579 DIFile File, unsigned LineNo,
580 DICompositeType Ty, bool isLocalToUnit,
581 bool isDefinition,
582 unsigned ScopeLine,
583 unsigned Flags = 0,
584 bool isOptimized = false,
585 Function *Fn = nullptr,
586 MDNode *TParam = nullptr,
587 MDNode *Decl = nullptr);
589 /// FIXME: this is added for dragonegg. Once we update dragonegg
590 /// to call resolve function, this will be removed.
591 DISubprogram createFunction(DIScopeRef Scope, StringRef Name,
592 StringRef LinkageName,
593 DIFile File, unsigned LineNo,
594 DICompositeType Ty, bool isLocalToUnit,
595 bool isDefinition,
596 unsigned ScopeLine,
597 unsigned Flags = 0,
598 bool isOptimized = false,
599 Function *Fn = nullptr,
600 MDNode *TParam = nullptr,
601 MDNode *Decl = nullptr);
603 /// createMethod - Create a new descriptor for the specified C++ method.
604 /// See comments in DISubprogram for descriptions of these fields.
605 /// @param Scope Function scope.
606 /// @param Name Function name.
607 /// @param LinkageName Mangled function name.
608 /// @param File File where this variable is defined.
609 /// @param LineNo Line number.
610 /// @param Ty Function type.
611 /// @param isLocalToUnit True if this function is not externally visible..
612 /// @param isDefinition True if this is a function definition.
613 /// @param Virtuality Attributes describing virtualness. e.g. pure
614 /// virtual function.
615 /// @param VTableIndex Index no of this method in virtual table.
616 /// @param VTableHolder Type that holds vtable.
617 /// @param Flags e.g. is this function prototyped or not.
618 /// This flags are used to emit dwarf attributes.
619 /// @param isOptimized True if optimization is ON.
620 /// @param Fn llvm::Function pointer.
621 /// @param TParam Function template parameters.
622 DISubprogram createMethod(DIDescriptor Scope, StringRef Name,
623 StringRef LinkageName,
624 DIFile File, unsigned LineNo,
625 DICompositeType Ty, bool isLocalToUnit,
626 bool isDefinition,
627 unsigned Virtuality = 0, unsigned VTableIndex = 0,
628 DIType VTableHolder = DIType(),
629 unsigned Flags = 0,
630 bool isOptimized = false,
631 Function *Fn = nullptr,
632 MDNode *TParam = nullptr);
634 /// createNameSpace - This creates new descriptor for a namespace
635 /// with the specified parent scope.
636 /// @param Scope Namespace scope
637 /// @param Name Name of this namespace
638 /// @param File Source file
639 /// @param LineNo Line number
640 DINameSpace createNameSpace(DIDescriptor Scope, StringRef Name,
641 DIFile File, unsigned LineNo);
644 /// createLexicalBlockFile - This creates a descriptor for a lexical
645 /// block with a new file attached. This merely extends the existing
646 /// lexical block as it crosses a file.
647 /// @param Scope Lexical block.
648 /// @param File Source file.
649 DILexicalBlockFile createLexicalBlockFile(DIDescriptor Scope,
650 DIFile File);
652 /// createLexicalBlock - This creates a descriptor for a lexical block
653 /// with the specified parent context.
654 /// @param Scope Parent lexical scope.
655 /// @param File Source file.
656 /// @param Line Line number.
657 /// @param Col Column number.
658 /// @param Discriminator DWARF path discriminator value.
659 DILexicalBlock createLexicalBlock(DIDescriptor Scope, DIFile File,
660 unsigned Line, unsigned Col,
661 unsigned Discriminator);
663 /// \brief Create a descriptor for an imported module.
664 /// @param Context The scope this module is imported into
665 /// @param NS The namespace being imported here
666 /// @param Line Line number
667 DIImportedEntity createImportedModule(DIScope Context, DINameSpace NS,
668 unsigned Line);
670 /// \brief Create a descriptor for an imported module.
671 /// @param Context The scope this module is imported into
672 /// @param NS An aliased namespace
673 /// @param Line Line number
674 DIImportedEntity createImportedModule(DIScope Context, DIImportedEntity NS,
675 unsigned Line);
677 /// \brief Create a descriptor for an imported function.
678 /// @param Context The scope this module is imported into
679 /// @param Decl The declaration (or definition) of a function, type, or
680 /// variable
681 /// @param Line Line number
682 DIImportedEntity createImportedDeclaration(DIScope Context, DIScope Decl,
683 unsigned Line,
684 StringRef Name = StringRef());
685 DIImportedEntity createImportedDeclaration(DIScope Context,
686 DIImportedEntity NS,
687 unsigned Line,
688 StringRef Name = StringRef());
690 /// insertDeclare - Insert a new llvm.dbg.declare intrinsic call.
691 /// @param Storage llvm::Value of the variable
692 /// @param VarInfo Variable's debug info descriptor.
693 /// @param InsertAtEnd Location for the new intrinsic.
694 Instruction *insertDeclare(llvm::Value *Storage, DIVariable VarInfo,
695 BasicBlock *InsertAtEnd);
697 /// insertDeclare - Insert a new llvm.dbg.declare intrinsic call.
698 /// @param Storage llvm::Value of the variable
699 /// @param VarInfo Variable's debug info descriptor.
700 /// @param InsertBefore Location for the new intrinsic.
701 Instruction *insertDeclare(llvm::Value *Storage, DIVariable VarInfo,
702 Instruction *InsertBefore);
705 /// insertDbgValueIntrinsic - Insert a new llvm.dbg.value intrinsic call.
706 /// @param Val llvm::Value of the variable
707 /// @param Offset Offset
708 /// @param VarInfo Variable's debug info descriptor.
709 /// @param InsertAtEnd Location for the new intrinsic.
710 Instruction *insertDbgValueIntrinsic(llvm::Value *Val, uint64_t Offset,
711 DIVariable VarInfo,
712 BasicBlock *InsertAtEnd);
714 /// insertDbgValueIntrinsic - Insert a new llvm.dbg.value intrinsic call.
715 /// @param Val llvm::Value of the variable
716 /// @param Offset Offset
717 /// @param VarInfo Variable's debug info descriptor.
718 /// @param InsertBefore Location for the new intrinsic.
719 Instruction *insertDbgValueIntrinsic(llvm::Value *Val, uint64_t Offset,
720 DIVariable VarInfo,
721 Instruction *InsertBefore);
723 };
724 } // end namespace llvm
726 #endif