1 //===-- llvm/IR/Statepoint.h - gc.statepoint utilities ------ --*- C++ -*-===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains utility functions and a wrapper class analogous to
11 // CallSite for accessing the fields of gc.statepoint, gc.relocate, and
12 // gc.result intrinsics
13 //
14 //===----------------------------------------------------------------------===//
16 #ifndef __LLVM_IR_STATEPOINT_H
17 #define __LLVM_IR_STATEPOINT_H
19 #include "llvm/ADT/iterator_range.h"
20 #include "llvm/IR/CallSite.h"
21 #include "llvm/IR/Instructions.h"
22 #include "llvm/IR/Intrinsics.h"
23 #include "llvm/Support/Compiler.h"
25 namespace llvm {
27 bool isStatepoint(const ImmutableCallSite &CS);
28 bool isStatepoint(const Instruction *inst);
29 bool isStatepoint(const Instruction &inst);
31 bool isGCRelocate(const Instruction *inst);
32 bool isGCRelocate(const ImmutableCallSite &CS);
34 bool isGCResult(const Instruction *inst);
35 bool isGCResult(const ImmutableCallSite &CS);
37 /// Analogous to CallSiteBase, this provides most of the actual
38 /// functionality for Statepoint and ImmutableStatepoint. It is
39 /// templatized to allow easily specializing of const and non-const
40 /// concrete subtypes. This is structured analogous to CallSite
41 /// rather than the IntrinsicInst.h helpers since we want to support
42 /// invokable statepoints in the near future.
43 /// TODO: This does not currently allow the if(Statepoint S = ...)
44 /// idiom used with CallSites. Consider refactoring to support.
45 template <typename InstructionTy, typename ValueTy, typename CallSiteTy>
46 class StatepointBase {
47 CallSiteTy StatepointCS;
48 void *operator new(size_t, unsigned) LLVM_DELETED_FUNCTION;
49 void *operator new(size_t s) LLVM_DELETED_FUNCTION;
51 protected:
52 explicit StatepointBase(InstructionTy *I) : StatepointCS(I) {
53 assert(isStatepoint(I));
54 }
55 explicit StatepointBase(CallSiteTy CS) : StatepointCS(CS) {
56 assert(isStatepoint(CS));
57 }
59 public:
60 typedef typename CallSiteTy::arg_iterator arg_iterator;
62 /// Return the underlying CallSite.
63 CallSiteTy getCallSite() {
64 return StatepointCS;
65 }
67 /// Return the value actually being called or invoked.
68 ValueTy *actualCallee() {
69 return StatepointCS.getArgument(0);
70 }
71 /// Number of arguments to be passed to the actual callee.
72 int numCallArgs() {
73 return cast<ConstantInt>(StatepointCS.getArgument(1))->getZExtValue();
74 }
75 /// Number of additional arguments excluding those intended
76 /// for garbage collection.
77 int numTotalVMSArgs() {
78 return cast<ConstantInt>(StatepointCS.getArgument(3 + numCallArgs()))->getZExtValue();
79 }
81 typename CallSiteTy::arg_iterator call_args_begin() {
82 // 3 = callTarget, #callArgs, flag
83 int Offset = 3;
84 assert(Offset <= (int)StatepointCS.arg_size());
85 return StatepointCS.arg_begin() + Offset;
86 }
87 typename CallSiteTy::arg_iterator call_args_end() {
88 int Offset = 3 + numCallArgs();
89 assert(Offset <= (int)StatepointCS.arg_size());
90 return StatepointCS.arg_begin() + Offset;
91 }
93 /// range adapter for call arguments
94 iterator_range<arg_iterator> call_args() {
95 return iterator_range<arg_iterator>(call_args_begin(), call_args_end());
96 }
98 typename CallSiteTy::arg_iterator vm_state_begin() {
99 return call_args_end();
100 }
101 typename CallSiteTy::arg_iterator vm_state_end() {
102 int Offset = 3 + numCallArgs() + 1 + numTotalVMSArgs();
103 assert(Offset <= (int)StatepointCS.arg_size());
104 return StatepointCS.arg_begin() + Offset;
105 }
107 /// range adapter for vm state arguments
108 iterator_range<arg_iterator> vm_state_args() {
109 return iterator_range<arg_iterator>(vm_state_begin(), vm_state_end());
110 }
112 typename CallSiteTy::arg_iterator first_vm_state_stack_begin() {
113 // 6 = numTotalVMSArgs, 1st_objectID, 1st_bci,
114 // 1st_#stack, 1st_#local, 1st_#monitor
115 return vm_state_begin() + 6;
116 }
118 typename CallSiteTy::arg_iterator gc_args_begin() {
119 return vm_state_end();
120 }
121 typename CallSiteTy::arg_iterator gc_args_end() {
122 return StatepointCS.arg_end();
123 }
125 /// range adapter for gc arguments
126 iterator_range<arg_iterator> gc_args() {
127 return iterator_range<arg_iterator>(gc_args_begin(), gc_args_end());
128 }
131 #ifndef NDEBUG
132 /// Asserts if this statepoint is malformed. Common cases for failure
133 /// include incorrect length prefixes for variable length sections or
134 /// illegal values for parameters.
135 void verify() {
136 assert(numCallArgs() >= 0 &&
137 "number of arguments to actually callee can't be negative");
139 // The internal asserts in the iterator accessors do the rest.
140 (void)call_args_begin();
141 (void)call_args_end();
142 (void)vm_state_begin();
143 (void)vm_state_end();
144 (void)gc_args_begin();
145 (void)gc_args_end();
146 }
147 #endif
148 };
150 /// A specialization of it's base class for read only access
151 /// to a gc.statepoint.
152 class ImmutableStatepoint
153 : public StatepointBase<const Instruction, const Value,
154 ImmutableCallSite> {
155 typedef StatepointBase<const Instruction, const Value, ImmutableCallSite>
156 Base;
158 public:
159 explicit ImmutableStatepoint(const Instruction *I) : Base(I) {}
160 explicit ImmutableStatepoint(ImmutableCallSite CS) : Base(CS) {}
161 };
163 /// A specialization of it's base class for read-write access
164 /// to a gc.statepoint.
165 class Statepoint : public StatepointBase<Instruction, Value, CallSite> {
166 typedef StatepointBase<Instruction, Value, CallSite> Base;
168 public:
169 explicit Statepoint(Instruction *I) : Base(I) {}
170 explicit Statepoint(CallSite CS) : Base(CS) {}
171 };
173 /// Wraps a call to a gc.relocate and provides access to it's operands.
174 /// TODO: This should likely be refactored to resememble the wrappers in
175 /// InstrinsicInst.h.
176 class GCRelocateOperands {
177 ImmutableCallSite RelocateCS;
179 public:
180 GCRelocateOperands(const User* U) : RelocateCS(U) {
181 assert(isGCRelocate(U));
182 }
183 GCRelocateOperands(const Instruction *inst) : RelocateCS(inst) {
184 assert(isGCRelocate(inst));
185 }
186 GCRelocateOperands(CallSite CS) : RelocateCS(CS) {
187 assert(isGCRelocate(CS));
188 }
190 /// The statepoint with which this gc.relocate is associated.
191 const Instruction *statepoint() {
192 return cast<Instruction>(RelocateCS.getArgument(0));
193 }
194 /// The index into the associate statepoint's argument list
195 /// which contains the base pointer of the pointer whose
196 /// relocation this gc.relocate describes.
197 unsigned basePtrIndex() {
198 return cast<ConstantInt>(RelocateCS.getArgument(1))->getZExtValue();
199 }
200 /// The index into the associate statepoint's argument list which
201 /// contains the pointer whose relocation this gc.relocate describes.
202 unsigned derivedPtrIndex() {
203 return cast<ConstantInt>(RelocateCS.getArgument(2))->getZExtValue();
204 }
205 Value *basePtr() {
206 ImmutableCallSite CS(statepoint());
207 return *(CS.arg_begin() + basePtrIndex());
208 }
209 Value *derivedPtr() {
210 ImmutableCallSite CS(statepoint());
211 return *(CS.arg_begin() + derivedPtrIndex());
212 }
213 };
214 }
215 #endif