0f57f44340c23acd2d0a19cdf24160441f6ff37f
1 //===- llvm/Supporrt/YAMLTraits.h -------------------------------*- C++ -*-===//
2 //
3 // The LLVM Linker
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
10 #ifndef LLVM_SUPPORT_YAMLTRAITS_H
11 #define LLVM_SUPPORT_YAMLTRAITS_H
14 #include "llvm/ADT/DenseMap.h"
15 #include "llvm/ADT/DenseMapInfo.h"
16 #include "llvm/ADT/SmallVector.h"
17 #include "llvm/ADT/StringMap.h"
18 #include "llvm/ADT/StringRef.h"
19 #include "llvm/ADT/StringSwitch.h"
20 #include "llvm/ADT/Twine.h"
21 #include "llvm/Support/Compiler.h"
22 #include "llvm/Support/SourceMgr.h"
23 #include "llvm/Support/YAMLParser.h"
24 #include "llvm/Support/raw_ostream.h"
25 #include "llvm/Support/system_error.h"
26 #include "llvm/Support/type_traits.h"
29 namespace llvm {
30 namespace yaml {
33 /// This class should be specialized by any type that needs to be converted
34 /// to/from a YAML mapping. For example:
35 ///
36 /// struct ScalarBitSetTraits<MyStruct> {
37 /// static void mapping(IO &io, MyStruct &s) {
38 /// io.mapRequired("name", s.name);
39 /// io.mapRequired("size", s.size);
40 /// io.mapOptional("age", s.age);
41 /// }
42 /// };
43 template<class T>
44 struct MappingTraits {
45 // Must provide:
46 // static void mapping(IO &io, T &fields);
47 };
50 /// This class should be specialized by any integral type that converts
51 /// to/from a YAML scalar where there is a one-to-one mapping between
52 /// in-memory values and a string in YAML. For example:
53 ///
54 /// struct ScalarEnumerationTraits<Colors> {
55 /// static void enumeration(IO &io, Colors &value) {
56 /// io.enumCase(value, "red", cRed);
57 /// io.enumCase(value, "blue", cBlue);
58 /// io.enumCase(value, "green", cGreen);
59 /// }
60 /// };
61 template<typename T>
62 struct ScalarEnumerationTraits {
63 // Must provide:
64 // static void enumeration(IO &io, T &value);
65 };
68 /// This class should be specialized by any integer type that is a union
69 /// of bit values and the YAML representation is a flow sequence of
70 /// strings. For example:
71 ///
72 /// struct ScalarBitSetTraits<MyFlags> {
73 /// static void bitset(IO &io, MyFlags &value) {
74 /// io.bitSetCase(value, "big", flagBig);
75 /// io.bitSetCase(value, "flat", flagFlat);
76 /// io.bitSetCase(value, "round", flagRound);
77 /// }
78 /// };
79 template<typename T>
80 struct ScalarBitSetTraits {
81 // Must provide:
82 // static void bitset(IO &io, T &value);
83 };
86 /// This class should be specialized by type that requires custom conversion
87 /// to/from a yaml scalar. For example:
88 ///
89 /// template<>
90 /// struct ScalarTraits<MyType> {
91 /// static void output(const MyType &val, void*, llvm::raw_ostream &out) {
92 /// // stream out custom formatting
93 /// out << llvm::format("%x", val);
94 /// }
95 /// static StringRef input(StringRef scalar, void*, MyType &value) {
96 /// // parse scalar and set `value`
97 /// // return empty string on success, or error string
98 /// return StringRef();
99 /// }
100 /// };
101 template<typename T>
102 struct ScalarTraits {
103 // Must provide:
104 //
105 // Function to write the value as a string:
106 //static void output(const T &value, void *ctxt, llvm::raw_ostream &out);
107 //
108 // Function to convert a string to a value. Returns the empty
109 // StringRef on success or an error string if string is malformed:
110 //static StringRef input(StringRef scalar, void *ctxt, T &value);
111 };
114 /// This class should be specialized by any type that needs to be converted
115 /// to/from a YAML sequence. For example:
116 ///
117 /// template<>
118 /// struct SequenceTraits< std::vector<MyType> > {
119 /// static size_t size(IO &io, std::vector<MyType> &seq) {
120 /// return seq.size();
121 /// }
122 /// static MyType& element(IO &, std::vector<MyType> &seq, size_t index) {
123 /// if ( index >= seq.size() )
124 /// seq.resize(index+1);
125 /// return seq[index];
126 /// }
127 /// };
128 template<typename T>
129 struct SequenceTraits {
130 // Must provide:
131 // static size_t size(IO &io, T &seq);
132 // static T::value_type& element(IO &io, T &seq, size_t index);
133 //
134 // The following is option and will cause generated YAML to use
135 // a flow sequence (e.g. [a,b,c]).
136 // static const bool flow = true;
137 };
140 /// This class should be specialized by any type that needs to be converted
141 /// to/from a list of YAML documents.
142 template<typename T>
143 struct DocumentListTraits {
144 // Must provide:
145 // static size_t size(IO &io, T &seq);
146 // static T::value_type& element(IO &io, T &seq, size_t index);
147 };
150 // Only used by compiler if both template types are the same
151 template <typename T, T>
152 struct SameType;
154 // Only used for better diagnostics of missing traits
155 template <typename T>
156 struct MissingTrait;
160 // Test if ScalarEnumerationTraits<T> is defined on type T.
161 template <class T>
162 struct has_ScalarEnumerationTraits
163 {
164 typedef void (*Signature_enumeration)(class IO&, T&);
166 template <typename U>
167 static char test(SameType<Signature_enumeration, &U::enumeration>*);
169 template <typename U>
170 static double test(...);
172 public:
173 static bool const value = (sizeof(test<ScalarEnumerationTraits<T> >(0)) == 1);
174 };
177 // Test if ScalarBitSetTraits<T> is defined on type T.
178 template <class T>
179 struct has_ScalarBitSetTraits
180 {
181 typedef void (*Signature_bitset)(class IO&, T&);
183 template <typename U>
184 static char test(SameType<Signature_bitset, &U::bitset>*);
186 template <typename U>
187 static double test(...);
189 public:
190 static bool const value = (sizeof(test<ScalarBitSetTraits<T> >(0)) == 1);
191 };
194 // Test if ScalarTraits<T> is defined on type T.
195 template <class T>
196 struct has_ScalarTraits
197 {
198 typedef StringRef (*Signature_input)(StringRef, void*, T&);
199 typedef void (*Signature_output)(const T&, void*, llvm::raw_ostream&);
201 template <typename U>
202 static char test(SameType<Signature_input, &U::input>*,
203 SameType<Signature_output, &U::output>*);
205 template <typename U>
206 static double test(...);
208 public:
209 static bool const value = (sizeof(test<ScalarTraits<T> >(0,0)) == 1);
210 };
213 // Test if MappingTraits<T> is defined on type T.
214 template <class T>
215 struct has_MappingTraits
216 {
217 typedef void (*Signature_mapping)(class IO&, T&);
219 template <typename U>
220 static char test(SameType<Signature_mapping, &U::mapping>*);
222 template <typename U>
223 static double test(...);
225 public:
226 static bool const value = (sizeof(test<MappingTraits<T> >(0)) == 1);
227 };
230 // Test if SequenceTraits<T> is defined on type T.
231 template <class T>
232 struct has_SequenceMethodTraits
233 {
234 typedef size_t (*Signature_size)(class IO&, T&);
236 template <typename U>
237 static char test(SameType<Signature_size, &U::size>*);
239 template <typename U>
240 static double test(...);
242 public:
243 static bool const value = (sizeof(test<SequenceTraits<T> >(0)) == 1);
244 };
247 // has_FlowTraits<int> will cause an error with some compilers because
248 // it subclasses int. Using this wrapper only instantiates the
249 // real has_FlowTraits only if the template type is a class.
250 template <typename T, bool Enabled = llvm::is_class<T>::value>
251 class has_FlowTraits
252 {
253 public:
254 static const bool value = false;
255 };
257 // Some older gcc compilers don't support straight forward tests
258 // for members, so test for ambiguity cause by the base and derived
259 // classes both defining the member.
260 template <class T>
261 struct has_FlowTraits<T, true>
262 {
263 struct Fallback { bool flow; };
264 struct Derived : T, Fallback { };
266 template<typename C>
267 static char (&f(SameType<bool Fallback::*, &C::flow>*))[1];
269 template<typename C>
270 static char (&f(...))[2];
272 public:
273 static bool const value = sizeof(f<Derived>(0)) == 2;
274 };
278 // Test if SequenceTraits<T> is defined on type T
279 template<typename T>
280 struct has_SequenceTraits : public llvm::integral_constant<bool,
281 has_SequenceMethodTraits<T>::value > { };
284 // Test if DocumentListTraits<T> is defined on type T
285 template <class T>
286 struct has_DocumentListTraits
287 {
288 typedef size_t (*Signature_size)(class IO&, T&);
290 template <typename U>
291 static char test(SameType<Signature_size, &U::size>*);
293 template <typename U>
294 static double test(...);
296 public:
297 static bool const value = (sizeof(test<DocumentListTraits<T> >(0)) == 1);
298 };
303 template<typename T>
304 struct missingTraits : public llvm::integral_constant<bool,
305 !has_ScalarEnumerationTraits<T>::value
306 && !has_ScalarBitSetTraits<T>::value
307 && !has_ScalarTraits<T>::value
308 && !has_MappingTraits<T>::value
309 && !has_SequenceTraits<T>::value
310 && !has_DocumentListTraits<T>::value > {};
313 // Base class for Input and Output.
314 class IO {
315 public:
317 IO(void *Ctxt=NULL);
318 virtual ~IO();
320 virtual bool outputting() = 0;
322 virtual unsigned beginSequence() = 0;
323 virtual bool preflightElement(unsigned, void *&) = 0;
324 virtual void postflightElement(void*) = 0;
325 virtual void endSequence() = 0;
327 virtual unsigned beginFlowSequence() = 0;
328 virtual bool preflightFlowElement(unsigned, void *&) = 0;
329 virtual void postflightFlowElement(void*) = 0;
330 virtual void endFlowSequence() = 0;
332 virtual void beginMapping() = 0;
333 virtual void endMapping() = 0;
334 virtual bool preflightKey(const char*, bool, bool, bool &, void *&) = 0;
335 virtual void postflightKey(void*) = 0;
337 virtual void beginEnumScalar() = 0;
338 virtual bool matchEnumScalar(const char*, bool) = 0;
339 virtual void endEnumScalar() = 0;
341 virtual bool beginBitSetScalar(bool &) = 0;
342 virtual bool bitSetMatch(const char*, bool) = 0;
343 virtual void endBitSetScalar() = 0;
345 virtual void scalarString(StringRef &) = 0;
347 virtual void setError(const Twine &) = 0;
349 template <typename T>
350 void enumCase(T &Val, const char* Str, const T ConstVal) {
351 if ( matchEnumScalar(Str, outputting() && Val == ConstVal) ) {
352 Val = ConstVal;
353 }
354 }
356 // allow anonymous enum values to be used with LLVM_YAML_STRONG_TYPEDEF
357 template <typename T>
358 void enumCase(T &Val, const char* Str, const uint32_t ConstVal) {
359 if ( matchEnumScalar(Str, outputting() && Val == static_cast<T>(ConstVal)) ) {
360 Val = ConstVal;
361 }
362 }
364 template <typename T>
365 void bitSetCase(T &Val, const char* Str, const T ConstVal) {
366 if ( bitSetMatch(Str, outputting() && (Val & ConstVal) == ConstVal) ) {
367 Val = Val | ConstVal;
368 }
369 }
371 // allow anonymous enum values to be used with LLVM_YAML_STRONG_TYPEDEF
372 template <typename T>
373 void bitSetCase(T &Val, const char* Str, const uint32_t ConstVal) {
374 if ( bitSetMatch(Str, outputting() && (Val & ConstVal) == ConstVal) ) {
375 Val = Val | ConstVal;
376 }
377 }
379 void *getContext();
380 void setContext(void *);
382 template <typename T>
383 void mapRequired(const char* Key, T& Val) {
384 this->processKey(Key, Val, true);
385 }
387 template <typename T>
388 typename llvm::enable_if_c<has_SequenceTraits<T>::value,void>::type
389 mapOptional(const char* Key, T& Val) {
390 // omit key/value instead of outputting empty sequence
391 if ( this->outputting() && !(Val.begin() != Val.end()) )
392 return;
393 this->processKey(Key, Val, false);
394 }
396 template <typename T>
397 typename llvm::enable_if_c<!has_SequenceTraits<T>::value,void>::type
398 mapOptional(const char* Key, T& Val) {
399 this->processKey(Key, Val, false);
400 }
402 template <typename T>
403 void mapOptional(const char* Key, T& Val, const T& Default) {
404 this->processKeyWithDefault(Key, Val, Default, false);
405 }
408 private:
409 template <typename T>
410 void processKeyWithDefault(const char *Key, T &Val, const T& DefaultValue,
411 bool Required) {
412 void *SaveInfo;
413 bool UseDefault;
414 const bool sameAsDefault = outputting() && Val == DefaultValue;
415 if ( this->preflightKey(Key, Required, sameAsDefault, UseDefault,
416 SaveInfo) ) {
417 yamlize(*this, Val, Required);
418 this->postflightKey(SaveInfo);
419 }
420 else {
421 if ( UseDefault )
422 Val = DefaultValue;
423 }
424 }
426 template <typename T>
427 void processKey(const char *Key, T &Val, bool Required) {
428 void *SaveInfo;
429 bool UseDefault;
430 if ( this->preflightKey(Key, Required, false, UseDefault, SaveInfo) ) {
431 yamlize(*this, Val, Required);
432 this->postflightKey(SaveInfo);
433 }
434 }
436 private:
437 void *Ctxt;
438 };
442 template<typename T>
443 typename llvm::enable_if_c<has_ScalarEnumerationTraits<T>::value,void>::type
444 yamlize(IO &io, T &Val, bool) {
445 io.beginEnumScalar();
446 ScalarEnumerationTraits<T>::enumeration(io, Val);
447 io.endEnumScalar();
448 }
450 template<typename T>
451 typename llvm::enable_if_c<has_ScalarBitSetTraits<T>::value,void>::type
452 yamlize(IO &io, T &Val, bool) {
453 bool DoClear;
454 if ( io.beginBitSetScalar(DoClear) ) {
455 if ( DoClear )
456 Val = static_cast<T>(0);
457 ScalarBitSetTraits<T>::bitset(io, Val);
458 io.endBitSetScalar();
459 }
460 }
463 template<typename T>
464 typename llvm::enable_if_c<has_ScalarTraits<T>::value,void>::type
465 yamlize(IO &io, T &Val, bool) {
466 if ( io.outputting() ) {
467 std::string Storage;
468 llvm::raw_string_ostream Buffer(Storage);
469 ScalarTraits<T>::output(Val, io.getContext(), Buffer);
470 StringRef Str = Buffer.str();
471 io.scalarString(Str);
472 }
473 else {
474 StringRef Str;
475 io.scalarString(Str);
476 StringRef Result = ScalarTraits<T>::input(Str, io.getContext(), Val);
477 if ( !Result.empty() ) {
478 io.setError(llvm::Twine(Result));
479 }
480 }
481 }
484 template<typename T>
485 typename llvm::enable_if_c<has_MappingTraits<T>::value, void>::type
486 yamlize(IO &io, T &Val, bool) {
487 io.beginMapping();
488 MappingTraits<T>::mapping(io, Val);
489 io.endMapping();
490 }
492 template<typename T>
493 typename llvm::enable_if_c<missingTraits<T>::value, void>::type
494 yamlize(IO &io, T &Val, bool) {
495 char missing_yaml_trait_for_type[sizeof(MissingTrait<T>)];
496 }
498 template<typename T>
499 typename llvm::enable_if_c<has_SequenceTraits<T>::value,void>::type
500 yamlize(IO &io, T &Seq, bool) {
501 if ( has_FlowTraits< SequenceTraits<T> >::value ) {
502 unsigned incnt = io.beginFlowSequence();
503 unsigned count = io.outputting() ? SequenceTraits<T>::size(io, Seq) : incnt;
504 for(unsigned i=0; i < count; ++i) {
505 void *SaveInfo;
506 if ( io.preflightFlowElement(i, SaveInfo) ) {
507 yamlize(io, SequenceTraits<T>::element(io, Seq, i), true);
508 io.postflightFlowElement(SaveInfo);
509 }
510 }
511 io.endFlowSequence();
512 }
513 else {
514 unsigned incnt = io.beginSequence();
515 unsigned count = io.outputting() ? SequenceTraits<T>::size(io, Seq) : incnt;
516 for(unsigned i=0; i < count; ++i) {
517 void *SaveInfo;
518 if ( io.preflightElement(i, SaveInfo) ) {
519 yamlize(io, SequenceTraits<T>::element(io, Seq, i), true);
520 io.postflightElement(SaveInfo);
521 }
522 }
523 io.endSequence();
524 }
525 }
528 template<>
529 struct ScalarTraits<bool> {
530 static void output(const bool &, void*, llvm::raw_ostream &);
531 static StringRef input(StringRef, void*, bool &);
532 };
534 template<>
535 struct ScalarTraits<StringRef> {
536 static void output(const StringRef &, void*, llvm::raw_ostream &);
537 static StringRef input(StringRef, void*, StringRef &);
538 };
540 template<>
541 struct ScalarTraits<uint8_t> {
542 static void output(const uint8_t &, void*, llvm::raw_ostream &);
543 static StringRef input(StringRef, void*, uint8_t &);
544 };
546 template<>
547 struct ScalarTraits<uint16_t> {
548 static void output(const uint16_t &, void*, llvm::raw_ostream &);
549 static StringRef input(StringRef, void*, uint16_t &);
550 };
552 template<>
553 struct ScalarTraits<uint32_t> {
554 static void output(const uint32_t &, void*, llvm::raw_ostream &);
555 static StringRef input(StringRef, void*, uint32_t &);
556 };
558 template<>
559 struct ScalarTraits<uint64_t> {
560 static void output(const uint64_t &, void*, llvm::raw_ostream &);
561 static StringRef input(StringRef, void*, uint64_t &);
562 };
564 template<>
565 struct ScalarTraits<int8_t> {
566 static void output(const int8_t &, void*, llvm::raw_ostream &);
567 static StringRef input(StringRef, void*, int8_t &);
568 };
570 template<>
571 struct ScalarTraits<int16_t> {
572 static void output(const int16_t &, void*, llvm::raw_ostream &);
573 static StringRef input(StringRef, void*, int16_t &);
574 };
576 template<>
577 struct ScalarTraits<int32_t> {
578 static void output(const int32_t &, void*, llvm::raw_ostream &);
579 static StringRef input(StringRef, void*, int32_t &);
580 };
582 template<>
583 struct ScalarTraits<int64_t> {
584 static void output(const int64_t &, void*, llvm::raw_ostream &);
585 static StringRef input(StringRef, void*, int64_t &);
586 };
588 template<>
589 struct ScalarTraits<float> {
590 static void output(const float &, void*, llvm::raw_ostream &);
591 static StringRef input(StringRef, void*, float &);
592 };
594 template<>
595 struct ScalarTraits<double> {
596 static void output(const double &, void*, llvm::raw_ostream &);
597 static StringRef input(StringRef, void*, double &);
598 };
602 // Utility for use within MappingTraits<>::mapping() method
603 // to [de]normalize an object for use with YAML conversion.
604 template <typename TNorm, typename TFinal>
605 struct MappingNormalization {
606 MappingNormalization(IO &i_o, TFinal &Obj)
607 : io(i_o), BufPtr(NULL), Result(Obj) {
608 if ( io.outputting() ) {
609 BufPtr = new (&Buffer) TNorm(io, Obj);
610 }
611 else {
612 BufPtr = new (&Buffer) TNorm(io);
613 }
614 }
616 ~MappingNormalization() {
617 if ( ! io.outputting() ) {
618 Result = BufPtr->denormalize(io);
619 }
620 BufPtr->~TNorm();
621 }
623 TNorm* operator->() { return BufPtr; }
625 private:
626 typedef llvm::AlignedCharArrayUnion<TNorm> Storage;
628 Storage Buffer;
629 IO &io;
630 TNorm *BufPtr;
631 TFinal &Result;
632 };
636 // Utility for use within MappingTraits<>::mapping() method
637 // to [de]normalize an object for use with YAML conversion.
638 template <typename TNorm, typename TFinal>
639 struct MappingNormalizationHeap {
640 MappingNormalizationHeap(IO &i_o, TFinal &Obj)
641 : io(i_o), BufPtr(NULL), Result(Obj) {
642 if ( io.outputting() ) {
643 BufPtr = new (&Buffer) TNorm(io, Obj);
644 }
645 else {
646 BufPtr = new TNorm(io);
647 }
648 }
650 ~MappingNormalizationHeap() {
651 if ( io.outputting() ) {
652 BufPtr->~TNorm();
653 }
654 else {
655 Result = BufPtr->denormalize(io);
656 }
657 }
659 TNorm* operator->() { return BufPtr; }
661 private:
662 typedef llvm::AlignedCharArrayUnion<TNorm> Storage;
664 Storage Buffer;
665 IO &io;
666 TNorm *BufPtr;
667 TFinal &Result;
668 };
672 ///
673 /// The Input class is used to parse a yaml document into in-memory structs
674 /// and vectors.
675 ///
676 /// It works by using YAMLParser to do a syntax parse of the entire yaml
677 /// document, then the Input class builds a graph of HNodes which wraps
678 /// each yaml Node. The extra layer is buffering. The low level yaml
679 /// parser only lets you look at each node once. The buffering layer lets
680 /// you search and interate multiple times. This is necessary because
681 /// the mapRequired() method calls may not be in the same order
682 /// as the keys in the document.
683 ///
684 class Input : public IO {
685 public:
686 // Construct a yaml Input object from a StringRef and optional user-data.
687 Input(StringRef InputContent, void *Ctxt=NULL);
688 ~Input();
690 // Check if there was an syntax or semantic error during parsing.
691 llvm::error_code error();
693 // To set alternate error reporting.
694 void setDiagHandler(llvm::SourceMgr::DiagHandlerTy Handler, void *Ctxt = 0);
696 private:
697 virtual bool outputting();
698 virtual void beginMapping();
699 virtual void endMapping();
700 virtual bool preflightKey(const char *, bool, bool, bool &, void *&);
701 virtual void postflightKey(void *);
702 virtual unsigned beginSequence();
703 virtual void endSequence();
704 virtual bool preflightElement(unsigned index, void *&);
705 virtual void postflightElement(void *);
706 virtual unsigned beginFlowSequence();
707 virtual bool preflightFlowElement(unsigned , void *&);
708 virtual void postflightFlowElement(void *);
709 virtual void endFlowSequence();
710 virtual void beginEnumScalar();
711 virtual bool matchEnumScalar(const char*, bool);
712 virtual void endEnumScalar();
713 virtual bool beginBitSetScalar(bool &);
714 virtual bool bitSetMatch(const char *, bool );
715 virtual void endBitSetScalar();
716 virtual void scalarString(StringRef &);
717 virtual void setError(const Twine &message);
719 class HNode {
720 public:
721 HNode(Node *n) : _node(n) { }
722 virtual ~HNode() { }
723 static inline bool classof(const HNode *) { return true; }
725 Node *_node;
726 };
728 class EmptyHNode : public HNode {
729 public:
730 EmptyHNode(Node *n) : HNode(n) { }
731 virtual ~EmptyHNode() {}
732 static inline bool classof(const HNode *n) {
733 return NullNode::classof(n->_node);
734 }
735 static inline bool classof(const EmptyHNode *) { return true; }
736 };
738 class ScalarHNode : public HNode {
739 public:
740 ScalarHNode(Node *n, StringRef s) : HNode(n), _value(s) { }
741 virtual ~ScalarHNode() { }
743 StringRef value() const { return _value; }
745 static inline bool classof(const HNode *n) {
746 return ScalarNode::classof(n->_node);
747 }
748 static inline bool classof(const ScalarHNode *) { return true; }
749 protected:
750 StringRef _value;
751 };
753 class MapHNode : public HNode {
754 public:
755 MapHNode(Node *n) : HNode(n) { }
756 virtual ~MapHNode();
758 static inline bool classof(const HNode *n) {
759 return MappingNode::classof(n->_node);
760 }
761 static inline bool classof(const MapHNode *) { return true; }
763 typedef llvm::StringMap<HNode*> NameToNode;
765 bool isValidKey(StringRef key);
767 NameToNode Mapping;
768 llvm::SmallVector<const char*, 6> ValidKeys;
769 };
771 class SequenceHNode : public HNode {
772 public:
773 SequenceHNode(Node *n) : HNode(n) { }
774 virtual ~SequenceHNode();
776 static inline bool classof(const HNode *n) {
777 return SequenceNode::classof(n->_node);
778 }
779 static inline bool classof(const SequenceHNode *) { return true; }
781 std::vector<HNode*> Entries;
782 };
784 Input::HNode *createHNodes(Node *node);
785 void setError(HNode *hnode, const Twine &message);
786 void setError(Node *node, const Twine &message);
789 public:
790 // These are only used by operator>>. They could be private
791 // if those templated things could be made friends.
792 bool setCurrentDocument();
793 void nextDocument();
795 private:
796 llvm::SourceMgr SrcMgr; // must be before Strm
797 OwningPtr<llvm::yaml::Stream> Strm;
798 OwningPtr<HNode> TopNode;
799 llvm::error_code EC;
800 llvm::BumpPtrAllocator StringAllocator;
801 llvm::yaml::document_iterator DocIterator;
802 std::vector<bool> BitValuesUsed;
803 HNode *CurrentNode;
804 bool ScalarMatchFound;
805 };
810 ///
811 /// The Output class is used to generate a yaml document from in-memory structs
812 /// and vectors.
813 ///
814 class Output : public IO {
815 public:
816 Output(llvm::raw_ostream &, void *Ctxt=NULL);
817 virtual ~Output();
819 virtual bool outputting();
820 virtual void beginMapping();
821 virtual void endMapping();
822 virtual bool preflightKey(const char *key, bool, bool, bool &, void *&);
823 virtual void postflightKey(void *);
824 virtual unsigned beginSequence();
825 virtual void endSequence();
826 virtual bool preflightElement(unsigned, void *&);
827 virtual void postflightElement(void *);
828 virtual unsigned beginFlowSequence();
829 virtual bool preflightFlowElement(unsigned, void *&);
830 virtual void postflightFlowElement(void *);
831 virtual void endFlowSequence();
832 virtual void beginEnumScalar();
833 virtual bool matchEnumScalar(const char*, bool);
834 virtual void endEnumScalar();
835 virtual bool beginBitSetScalar(bool &);
836 virtual bool bitSetMatch(const char *, bool );
837 virtual void endBitSetScalar();
838 virtual void scalarString(StringRef &);
839 virtual void setError(const Twine &message);
841 public:
842 // These are only used by operator<<. They could be private
843 // if that templated operator could be made a friend.
844 void beginDocuments();
845 bool preflightDocument(unsigned);
846 void postflightDocument();
847 void endDocuments();
849 private:
850 void output(StringRef s);
851 void outputUpToEndOfLine(StringRef s);
852 void newLineCheck();
853 void outputNewLine();
854 void paddedKey(StringRef key);
856 enum InState { inSeq, inFlowSeq, inMapFirstKey, inMapOtherKey };
858 llvm::raw_ostream &Out;
859 SmallVector<InState, 8> StateStack;
860 int Column;
861 int ColumnAtFlowStart;
862 bool NeedBitValueComma;
863 bool NeedFlowSequenceComma;
864 bool EnumerationMatchFound;
865 bool NeedsNewLine;
866 };
871 /// YAML I/O does conversion based on types. But often native data types
872 /// are just a typedef of built in intergral types (e.g. int). But the C++
873 /// type matching system sees through the typedef and all the typedefed types
874 /// look like a built in type. This will cause the generic YAML I/O conversion
875 /// to be used. To provide better control over the YAML conversion, you can
876 /// use this macro instead of typedef. It will create a class with one field
877 /// and automatic conversion operators to and from the base type.
878 /// Based on BOOST_STRONG_TYPEDEF
879 #define LLVM_YAML_STRONG_TYPEDEF(_base, _type) \
880 struct _type { \
881 _type() { } \
882 _type(const _base v) : value(v) { } \
883 _type(const _type &v) : value(v.value) {} \
884 _type &operator=(const _type &rhs) { value = rhs.value; return *this; }\
885 _type &operator=(const _base &rhs) { value = rhs; return *this; } \
886 operator const _base & () const { return value; } \
887 bool operator==(const _type &rhs) const { return value == rhs.value; } \
888 bool operator==(const _base &rhs) const { return value == rhs; } \
889 bool operator<(const _type &rhs) const { return value < rhs.value; } \
890 _base value; \
891 };
895 ///
896 /// Use these types instead of uintXX_t in any mapping to have
897 /// its yaml output formatted as hexadecimal.
898 ///
899 LLVM_YAML_STRONG_TYPEDEF(uint8_t, Hex8)
900 LLVM_YAML_STRONG_TYPEDEF(uint16_t, Hex16)
901 LLVM_YAML_STRONG_TYPEDEF(uint32_t, Hex32)
902 LLVM_YAML_STRONG_TYPEDEF(uint64_t, Hex64)
905 template<>
906 struct ScalarTraits<Hex8> {
907 static void output(const Hex8 &, void*, llvm::raw_ostream &);
908 static StringRef input(StringRef, void*, Hex8 &);
909 };
911 template<>
912 struct ScalarTraits<Hex16> {
913 static void output(const Hex16 &, void*, llvm::raw_ostream &);
914 static StringRef input(StringRef, void*, Hex16 &);
915 };
917 template<>
918 struct ScalarTraits<Hex32> {
919 static void output(const Hex32 &, void*, llvm::raw_ostream &);
920 static StringRef input(StringRef, void*, Hex32 &);
921 };
923 template<>
924 struct ScalarTraits<Hex64> {
925 static void output(const Hex64 &, void*, llvm::raw_ostream &);
926 static StringRef input(StringRef, void*, Hex64 &);
927 };
930 // Define non-member operator>> so that Input can stream in a document list.
931 template <typename T>
932 inline
933 typename llvm::enable_if_c<has_DocumentListTraits<T>::value,Input &>::type
934 operator>>(Input &yin, T &docList) {
935 int i = 0;
936 while ( yin.setCurrentDocument() ) {
937 yamlize(yin, DocumentListTraits<T>::element(yin, docList, i), true);
938 if ( yin.error() )
939 return yin;
940 yin.nextDocument();
941 ++i;
942 }
943 return yin;
944 }
946 // Define non-member operator>> so that Input can stream in a map as a document.
947 template <typename T>
948 inline
949 typename llvm::enable_if_c<has_MappingTraits<T>::value,Input &>::type
950 operator>>(Input &yin, T &docMap) {
951 yin.setCurrentDocument();
952 yamlize(yin, docMap, true);
953 return yin;
954 }
956 // Define non-member operator>> so that Input can stream in a sequence as
957 // a document.
958 template <typename T>
959 inline
960 typename llvm::enable_if_c<has_SequenceTraits<T>::value,Input &>::type
961 operator>>(Input &yin, T &docSeq) {
962 yin.setCurrentDocument();
963 yamlize(yin, docSeq, true);
964 return yin;
965 }
967 // Provide better error message about types missing a trait specialization
968 template <typename T>
969 inline
970 typename llvm::enable_if_c<missingTraits<T>::value,Input &>::type
971 operator>>(Input &yin, T &docSeq) {
972 char missing_yaml_trait_for_type[sizeof(MissingTrait<T>)];
973 return yin;
974 }
977 // Define non-member operator<< so that Output can stream out document list.
978 template <typename T>
979 inline
980 typename llvm::enable_if_c<has_DocumentListTraits<T>::value,Output &>::type
981 operator<<(Output &yout, T &docList) {
982 yout.beginDocuments();
983 const size_t count = DocumentListTraits<T>::size(yout, docList);
984 for(size_t i=0; i < count; ++i) {
985 if ( yout.preflightDocument(i) ) {
986 yamlize(yout, DocumentListTraits<T>::element(yout, docList, i), true);
987 yout.postflightDocument();
988 }
989 }
990 yout.endDocuments();
991 return yout;
992 }
994 // Define non-member operator<< so that Output can stream out a map.
995 template <typename T>
996 inline
997 typename llvm::enable_if_c<has_MappingTraits<T>::value,Output &>::type
998 operator<<(Output &yout, T &map) {
999 yout.beginDocuments();
1000 if ( yout.preflightDocument(0) ) {
1001 yamlize(yout, map, true);
1002 yout.postflightDocument();
1003 }
1004 yout.endDocuments();
1005 return yout;
1006 }
1008 // Define non-member operator<< so that Output can stream out a sequence.
1009 template <typename T>
1010 inline
1011 typename llvm::enable_if_c<has_SequenceTraits<T>::value,Output &>::type
1012 operator<<(Output &yout, T &seq) {
1013 yout.beginDocuments();
1014 if ( yout.preflightDocument(0) ) {
1015 yamlize(yout, seq, true);
1016 yout.postflightDocument();
1017 }
1018 yout.endDocuments();
1019 return yout;
1020 }
1022 // Provide better error message about types missing a trait specialization
1023 template <typename T>
1024 inline
1025 typename llvm::enable_if_c<missingTraits<T>::value,Output &>::type
1026 operator<<(Output &yout, T &seq) {
1027 char missing_yaml_trait_for_type[sizeof(MissingTrait<T>)];
1028 return yout;
1029 }
1032 } // namespace yaml
1033 } // namespace llvm
1036 /// Utility for declaring that a std::vector of a particular type
1037 /// should be considered a YAML sequence.
1038 #define LLVM_YAML_IS_SEQUENCE_VECTOR(_type) \
1039 namespace llvm { \
1040 namespace yaml { \
1041 template<> \
1042 struct SequenceTraits< std::vector<_type> > { \
1043 static size_t size(IO &io, std::vector<_type> &seq) { \
1044 return seq.size(); \
1045 } \
1046 static _type& element(IO &io, std::vector<_type> &seq, size_t index) {\
1047 if ( index >= seq.size() ) \
1048 seq.resize(index+1); \
1049 return seq[index]; \
1050 } \
1051 }; \
1052 } \
1053 }
1055 /// Utility for declaring that a std::vector of a particular type
1056 /// should be considered a YAML flow sequence.
1057 #define LLVM_YAML_IS_FLOW_SEQUENCE_VECTOR(_type) \
1058 namespace llvm { \
1059 namespace yaml { \
1060 template<> \
1061 struct SequenceTraits< std::vector<_type> > { \
1062 static size_t size(IO &io, std::vector<_type> &seq) { \
1063 return seq.size(); \
1064 } \
1065 static _type& element(IO &io, std::vector<_type> &seq, size_t index) {\
1066 if ( index >= seq.size() ) \
1067 seq.resize(index+1); \
1068 return seq[index]; \
1069 } \
1070 static const bool flow = true; \
1071 }; \
1072 } \
1073 }
1075 /// Utility for declaring that a std::vector of a particular type
1076 /// should be considered a YAML document list.
1077 #define LLVM_YAML_IS_DOCUMENT_LIST_VECTOR(_type) \
1078 namespace llvm { \
1079 namespace yaml { \
1080 template<> \
1081 struct DocumentListTraits< std::vector<_type> > { \
1082 static size_t size(IO &io, std::vector<_type> &seq) { \
1083 return seq.size(); \
1084 } \
1085 static _type& element(IO &io, std::vector<_type> &seq, size_t index) {\
1086 if ( index >= seq.size() ) \
1087 seq.resize(index+1); \
1088 return seq[index]; \
1089 } \
1090 }; \
1091 } \
1092 }
1096 #endif // LLVM_SUPPORT_YAMLTRAITS_H