88bb84a8002085ace288288cd34941e964358d91
[opencl/llvm.git] / lib / Analysis / CFLAliasAnalysis.cpp
1 //===- CFLAliasAnalysis.cpp - CFL-Based Alias Analysis Implementation ------==//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements a CFL-based context-insensitive alias analysis
11 // algorithm. It does not depend on types. The algorithm is a mixture of the one
12 // described in "Demand-driven alias analysis for C" by Xin Zheng and Radu
13 // Rugina, and "Fast algorithms for Dyck-CFL-reachability with applications to
14 // Alias Analysis" by Zhang Q, Lyu M R, Yuan H, and Su Z. -- to summarize the
15 // papers, we build a graph of the uses of a variable, where each node is a
16 // memory location, and each edge is an action that happened on that memory
17 // location.  The "actions" can be one of Dereference, Reference, Assign, or
18 // Assign.
19 //
20 // Two variables are considered as aliasing iff you can reach one value's node
21 // from the other value's node and the language formed by concatenating all of
22 // the edge labels (actions) conforms to a context-free grammar.
23 //
24 // Because this algorithm requires a graph search on each query, we execute the
25 // algorithm outlined in "Fast algorithms..." (mentioned above)
26 // in order to transform the graph into sets of variables that may alias in
27 // ~nlogn time (n = number of variables.), which makes queries take constant
28 // time.
29 //===----------------------------------------------------------------------===//
31 #include "StratifiedSets.h"
32 #include "llvm/ADT/BitVector.h"
33 #include "llvm/ADT/DenseMap.h"
34 #include "llvm/ADT/None.h"
35 #include "llvm/ADT/Optional.h"
36 #include "llvm/Analysis/AliasAnalysis.h"
37 #include "llvm/Analysis/Passes.h"
38 #include "llvm/IR/Constants.h"
39 #include "llvm/IR/Function.h"
40 #include "llvm/IR/InstVisitor.h"
41 #include "llvm/IR/Instructions.h"
42 #include "llvm/IR/ValueHandle.h"
43 #include "llvm/Pass.h"
44 #include "llvm/Support/Allocator.h"
45 #include "llvm/Support/Compiler.h"
46 #include "llvm/Support/ErrorHandling.h"
47 #include <algorithm>
48 #include <cassert>
49 #include <forward_list>
50 #include <tuple>
52 using namespace llvm;
54 // Try to go from a Value* to a Function*. Never returns nullptr.
55 static Optional<Function *> parentFunctionOfValue(Value *);
57 // Returns possible functions called by the Inst* into the given
58 // SmallVectorImpl. Returns true if targets found, false otherwise.
59 // This is templated because InvokeInst/CallInst give us the same
60 // set of functions that we care about, and I don't like repeating
61 // myself.
62 template <typename Inst>
63 static bool getPossibleTargets(Inst *, SmallVectorImpl<Function *> &);
65 // Some instructions need to have their users tracked. Instructions like
66 // `add` require you to get the users of the Instruction* itself, other
67 // instructions like `store` require you to get the users of the first
68 // operand. This function gets the "proper" value to track for each
69 // type of instruction we support.
70 static Optional<Value *> getTargetValue(Instruction *);
72 // There are certain instructions (i.e. FenceInst, etc.) that we ignore.
73 // This notes that we should ignore those.
74 static bool hasUsefulEdges(Instruction *);
76 const StratifiedIndex StratifiedLink::SetSentinel =
77   std::numeric_limits<StratifiedIndex>::max();
79 namespace {
80 // StratifiedInfo Attribute things.
81 typedef unsigned StratifiedAttr;
82 LLVM_CONSTEXPR unsigned MaxStratifiedAttrIndex = NumStratifiedAttrs;
83 LLVM_CONSTEXPR unsigned AttrAllIndex = 0;
84 LLVM_CONSTEXPR unsigned AttrGlobalIndex = 1;
85 LLVM_CONSTEXPR unsigned AttrFirstArgIndex = 2;
86 LLVM_CONSTEXPR unsigned AttrLastArgIndex = MaxStratifiedAttrIndex;
87 LLVM_CONSTEXPR unsigned AttrMaxNumArgs = AttrLastArgIndex - AttrFirstArgIndex;
89 LLVM_CONSTEXPR StratifiedAttr AttrNone = 0;
90 LLVM_CONSTEXPR StratifiedAttr AttrAll = ~AttrNone;
92 // \brief StratifiedSets call for knowledge of "direction", so this is how we
93 // represent that locally.
94 enum class Level { Same, Above, Below };
96 // \brief Edges can be one of four "weights" -- each weight must have an inverse
97 // weight (Assign has Assign; Reference has Dereference).
98 enum class EdgeType {
99   // The weight assigned when assigning from or to a value. For example, in:
100   // %b = getelementptr %a, 0
101   // ...The relationships are %b assign %a, and %a assign %b. This used to be
102   // two edges, but having a distinction bought us nothing.
103   Assign,
105   // The edge used when we have an edge going from some handle to a Value.
106   // Examples of this include:
107   // %b = load %a              (%b Dereference %a)
108   // %b = extractelement %a, 0 (%a Dereference %b)
109   Dereference,
111   // The edge used when our edge goes from a value to a handle that may have
112   // contained it at some point. Examples:
113   // %b = load %a              (%a Reference %b)
114   // %b = extractelement %a, 0 (%b Reference %a)
115   Reference
116 };
118 // \brief Encodes the notion of a "use"
119 struct Edge {
120   // \brief Which value the edge is coming from
121   Value *From;
123   // \brief Which value the edge is pointing to
124   Value *To;
126   // \brief Edge weight
127   EdgeType Weight;
129   // \brief Whether we aliased any external values along the way that may be
130   // invisible to the analysis (i.e. landingpad for exceptions, calls for
131   // interprocedural analysis, etc.)
132   StratifiedAttrs AdditionalAttrs;
134   Edge(Value *From, Value *To, EdgeType W, StratifiedAttrs A)
135       : From(From), To(To), Weight(W), AdditionalAttrs(A) {}
136 };
138 // \brief Information we have about a function and would like to keep around
139 struct FunctionInfo {
140   StratifiedSets<Value *> Sets;
141   // Lots of functions have < 4 returns. Adjust as necessary.
142   SmallVector<Value *, 4> ReturnedValues;
144   FunctionInfo(StratifiedSets<Value *> &&S,
145                SmallVector<Value *, 4> &&RV)
146     : Sets(std::move(S)), ReturnedValues(std::move(RV)) {}
147 };
149 struct CFLAliasAnalysis;
151 struct FunctionHandle : public CallbackVH {
152   FunctionHandle(Function *Fn, CFLAliasAnalysis *CFLAA)
153       : CallbackVH(Fn), CFLAA(CFLAA) {
154     assert(Fn != nullptr);
155     assert(CFLAA != nullptr);
156   }
158   virtual ~FunctionHandle() {}
160   void deleted() override { removeSelfFromCache(); }
161   void allUsesReplacedWith(Value *) override { removeSelfFromCache(); }
163 private:
164   CFLAliasAnalysis *CFLAA;
166   void removeSelfFromCache();
167 };
169 struct CFLAliasAnalysis : public ImmutablePass, public AliasAnalysis {
170 private:
171   /// \brief Cached mapping of Functions to their StratifiedSets.
172   /// If a function's sets are currently being built, it is marked
173   /// in the cache as an Optional without a value. This way, if we
174   /// have any kind of recursion, it is discernable from a function
175   /// that simply has empty sets.
176   DenseMap<Function *, Optional<FunctionInfo>> Cache;
177   std::forward_list<FunctionHandle> Handles;
179 public:
180   static char ID;
182   CFLAliasAnalysis() : ImmutablePass(ID) {
183     initializeCFLAliasAnalysisPass(*PassRegistry::getPassRegistry());
184   }
186   virtual ~CFLAliasAnalysis() {}
188   void getAnalysisUsage(AnalysisUsage &AU) const override {
189     AliasAnalysis::getAnalysisUsage(AU);
190   }
192   void *getAdjustedAnalysisPointer(const void *ID) override {
193     if (ID == &AliasAnalysis::ID)
194       return (AliasAnalysis *)this;
195     return this;
196   }
198   /// \brief Inserts the given Function into the cache.
199   void scan(Function *Fn);
201   void evict(Function *Fn) { Cache.erase(Fn); }
203   /// \brief Ensures that the given function is available in the cache.
204   /// Returns the appropriate entry from the cache.
205   const Optional<FunctionInfo> &ensureCached(Function *Fn) {
206     auto Iter = Cache.find(Fn);
207     if (Iter == Cache.end()) {
208       scan(Fn);
209       Iter = Cache.find(Fn);
210       assert(Iter != Cache.end());
211       assert(Iter->second.hasValue());
212     }
213     return Iter->second;
214   }
216   AliasResult query(const Location &LocA, const Location &LocB);
218   AliasResult alias(const Location &LocA, const Location &LocB) override {
219     if (LocA.Ptr == LocB.Ptr) {
220       if (LocA.Size == LocB.Size) {
221         return MustAlias;
222       } else {
223         return PartialAlias;
224       }
225     }
227     // Comparisons between global variables and other constants should be
228     // handled by BasicAA.
229     if (isa<Constant>(LocA.Ptr) && isa<Constant>(LocB.Ptr)) {
230       return MayAlias;
231     }
233     return query(LocA, LocB);
234   }
236   void initializePass() override { InitializeAliasAnalysis(this); }
237 };
239 void FunctionHandle::removeSelfFromCache() {
240   assert(CFLAA != nullptr);
241   auto *Val = getValPtr();
242   CFLAA->evict(cast<Function>(Val));
243   setValPtr(nullptr);
246 // \brief Gets the edges our graph should have, based on an Instruction*
247 class GetEdgesVisitor : public InstVisitor<GetEdgesVisitor, void> {
248   CFLAliasAnalysis &AA;
249   SmallVectorImpl<Edge> &Output;
251 public:
252   GetEdgesVisitor(CFLAliasAnalysis &AA, SmallVectorImpl<Edge> &Output)
253       : AA(AA), Output(Output) {}
255   void visitInstruction(Instruction &) {
256     llvm_unreachable("Unsupported instruction encountered");
257   }
259   void visitCastInst(CastInst &Inst) {
260     Output.push_back(Edge(&Inst, Inst.getOperand(0), EdgeType::Assign,
261                           AttrNone));
262   }
264   void visitBinaryOperator(BinaryOperator &Inst) {
265     auto *Op1 = Inst.getOperand(0);
266     auto *Op2 = Inst.getOperand(1);
267     Output.push_back(Edge(&Inst, Op1, EdgeType::Assign, AttrNone));
268     Output.push_back(Edge(&Inst, Op2, EdgeType::Assign, AttrNone));
269   }
271   void visitAtomicCmpXchgInst(AtomicCmpXchgInst &Inst) {
272     auto *Ptr = Inst.getPointerOperand();
273     auto *Val = Inst.getNewValOperand();
274     Output.push_back(Edge(Ptr, Val, EdgeType::Dereference, AttrNone));
275   }
277   void visitAtomicRMWInst(AtomicRMWInst &Inst) {
278     auto *Ptr = Inst.getPointerOperand();
279     auto *Val = Inst.getValOperand();
280     Output.push_back(Edge(Ptr, Val, EdgeType::Dereference, AttrNone));
281   }
283   void visitPHINode(PHINode &Inst) {
284     for (unsigned I = 0, E = Inst.getNumIncomingValues(); I != E; ++I) {
285       Value *Val = Inst.getIncomingValue(I);
286       Output.push_back(Edge(&Inst, Val, EdgeType::Assign, AttrNone));
287     }
288   }
290   void visitGetElementPtrInst(GetElementPtrInst &Inst) {
291     auto *Op = Inst.getPointerOperand();
292     Output.push_back(Edge(&Inst, Op, EdgeType::Assign, AttrNone));
293     for (auto I = Inst.idx_begin(), E = Inst.idx_end(); I != E; ++I)
294       Output.push_back(Edge(&Inst, *I, EdgeType::Assign, AttrNone));
295   }
297   void visitSelectInst(SelectInst &Inst) {
298     auto *Condition = Inst.getCondition();
299     Output.push_back(Edge(&Inst, Condition, EdgeType::Assign, AttrNone));
300     auto *TrueVal = Inst.getTrueValue();
301     Output.push_back(Edge(&Inst, TrueVal, EdgeType::Assign, AttrNone));
302     auto *FalseVal = Inst.getFalseValue();
303     Output.push_back(Edge(&Inst, FalseVal, EdgeType::Assign, AttrNone));
304   }
306   void visitAllocaInst(AllocaInst &) {}
308   void visitLoadInst(LoadInst &Inst) {
309     auto *Ptr = Inst.getPointerOperand();
310     auto *Val = &Inst;
311     Output.push_back(Edge(Val, Ptr, EdgeType::Reference, AttrNone));
312   }
314   void visitStoreInst(StoreInst &Inst) {
315     auto *Ptr = Inst.getPointerOperand();
316     auto *Val = Inst.getValueOperand();
317     Output.push_back(Edge(Ptr, Val, EdgeType::Dereference, AttrNone));
318   }
320   void visitVAArgInst(VAArgInst &Inst) {
321     // We can't fully model va_arg here. For *Ptr = Inst.getOperand(0), it does
322     // two things:
323     //  1. Loads a value from *((T*)*Ptr).
324     //  2. Increments (stores to) *Ptr by some target-specific amount.
325     // For now, we'll handle this like a landingpad instruction (by placing the
326     // result in its own group, and having that group alias externals).
327     auto *Val = &Inst;
328     Output.push_back(Edge(Val, Val, EdgeType::Assign, AttrAll));
329   }
331   static bool isFunctionExternal(Function *Fn) {
332     return Fn->isDeclaration() || !Fn->hasLocalLinkage();
333   }
335   // Gets whether the sets at Index1 above, below, or equal to the sets at
336   // Index2. Returns None if they are not in the same set chain.
337   static Optional<Level> getIndexRelation(const StratifiedSets<Value *> &Sets,
338                                           StratifiedIndex Index1,
339                                           StratifiedIndex Index2) {
340     if (Index1 == Index2)
341       return Level::Same;
343     const auto *Current = &Sets.getLink(Index1);
344     while (Current->hasBelow()) {
345       if (Current->Below == Index2)
346         return Level::Below;
347       Current = &Sets.getLink(Current->Below);
348     }
350     Current = &Sets.getLink(Index1);
351     while (Current->hasAbove()) {
352       if (Current->Above == Index2)
353         return Level::Above;
354       Current = &Sets.getLink(Current->Above);
355     }
357     return NoneType();
358   }
360   bool
361   tryInterproceduralAnalysis(const SmallVectorImpl<Function *> &Fns,
362                              Value *FuncValue,
363                              const iterator_range<User::op_iterator> &Args) {
364     const unsigned ExpectedMaxArgs = 8;
365     const unsigned MaxSupportedArgs = 50;
366     assert(Fns.size() > 0);
368     // I put this here to give us an upper bound on time taken by IPA. Is it
369     // really (realistically) needed? Keep in mind that we do have an n^2 algo.
370     if (std::distance(Args.begin(), Args.end()) > (int) MaxSupportedArgs)
371       return false;
373     // Exit early if we'll fail anyway
374     for (auto *Fn : Fns) {
375       if (isFunctionExternal(Fn) || Fn->isVarArg())
376         return false;
377       auto &MaybeInfo = AA.ensureCached(Fn);
378       if (!MaybeInfo.hasValue())
379         return false;
380     }
382     SmallVector<Value *, ExpectedMaxArgs> Arguments(Args.begin(), Args.end());
383     SmallVector<StratifiedInfo, ExpectedMaxArgs> Parameters;
384     for (auto *Fn : Fns) {
385       auto &Info = *AA.ensureCached(Fn);
386       auto &Sets = Info.Sets;
387       auto &RetVals = Info.ReturnedValues;
389       Parameters.clear();
390       for (auto &Param : Fn->args()) {
391         auto MaybeInfo = Sets.find(&Param);
392         // Did a new parameter somehow get added to the function/slip by?
393         if (!MaybeInfo.hasValue())
394           return false;
395         Parameters.push_back(*MaybeInfo);
396       }
398       // Adding an edge from argument -> return value for each parameter that
399       // may alias the return value
400       for (unsigned I = 0, E = Parameters.size(); I != E; ++I) {
401         auto &ParamInfo = Parameters[I];
402         auto &ArgVal = Arguments[I];
403         bool AddEdge = false;
404         StratifiedAttrs Externals;
405         for (unsigned X = 0, XE = RetVals.size(); X != XE; ++X) {
406           auto MaybeInfo = Sets.find(RetVals[X]);
407           if (!MaybeInfo.hasValue())
408             return false;
410           auto &RetInfo = *MaybeInfo;
411           auto RetAttrs = Sets.getLink(RetInfo.Index).Attrs;
412           auto ParamAttrs = Sets.getLink(ParamInfo.Index).Attrs;
413           auto MaybeRelation =
414               getIndexRelation(Sets, ParamInfo.Index, RetInfo.Index);
415           if (MaybeRelation.hasValue()) {
416             AddEdge = true;
417             Externals |= RetAttrs | ParamAttrs;
418           }
419         }
420         if (AddEdge)
421           Output.push_back(Edge(FuncValue, ArgVal, EdgeType::Assign,
422                             StratifiedAttrs().flip()));
423       }
425       if (Parameters.size() != Arguments.size())
426         return false;
428       // Adding edges between arguments for arguments that may end up aliasing
429       // each other. This is necessary for functions such as
430       // void foo(int** a, int** b) { *a = *b; }
431       // (Technically, the proper sets for this would be those below
432       // Arguments[I] and Arguments[X], but our algorithm will produce
433       // extremely similar, and equally correct, results either way)
434       for (unsigned I = 0, E = Arguments.size(); I != E; ++I) {
435         auto &MainVal = Arguments[I];
436         auto &MainInfo = Parameters[I];
437         auto &MainAttrs = Sets.getLink(MainInfo.Index).Attrs;
438         for (unsigned X = I + 1; X != E; ++X) {
439           auto &SubInfo = Parameters[X];
440           auto &SubVal = Arguments[X];
441           auto &SubAttrs = Sets.getLink(SubInfo.Index).Attrs;
442           auto MaybeRelation =
443               getIndexRelation(Sets, MainInfo.Index, SubInfo.Index);
445           if (!MaybeRelation.hasValue())
446             continue;
448           auto NewAttrs = SubAttrs | MainAttrs;
449           Output.push_back(Edge(MainVal, SubVal, EdgeType::Assign, NewAttrs));
450         }
451       }
452     }
453     return true;
454   }
456   template <typename InstT> void visitCallLikeInst(InstT &Inst) {
457     SmallVector<Function *, 4> Targets;
458     if (getPossibleTargets(&Inst, Targets)) {
459       if (tryInterproceduralAnalysis(Targets, &Inst, Inst.arg_operands()))
460         return;
461       // Cleanup from interprocedural analysis
462       Output.clear();
463     }
465     for (Value *V : Inst.arg_operands())
466       Output.push_back(Edge(&Inst, V, EdgeType::Assign, AttrAll));
467   }
469   void visitCallInst(CallInst &Inst) { visitCallLikeInst(Inst); }
471   void visitInvokeInst(InvokeInst &Inst) { visitCallLikeInst(Inst); }
473   // Because vectors/aggregates are immutable and unaddressable,
474   // there's nothing we can do to coax a value out of them, other
475   // than calling Extract{Element,Value}. We can effectively treat
476   // them as pointers to arbitrary memory locations we can store in
477   // and load from.
478   void visitExtractElementInst(ExtractElementInst &Inst) {
479     auto *Ptr = Inst.getVectorOperand();
480     auto *Val = &Inst;
481     Output.push_back(Edge(Val, Ptr, EdgeType::Reference, AttrNone));
482   }
484   void visitInsertElementInst(InsertElementInst &Inst) {
485     auto *Vec = Inst.getOperand(0);
486     auto *Val = Inst.getOperand(1);
487     Output.push_back(Edge(&Inst, Vec, EdgeType::Assign, AttrNone));
488     Output.push_back(Edge(&Inst, Val, EdgeType::Dereference, AttrNone));
489   }
491   void visitLandingPadInst(LandingPadInst &Inst) {
492     // Exceptions come from "nowhere", from our analysis' perspective.
493     // So we place the instruction its own group, noting that said group may
494     // alias externals
495     Output.push_back(Edge(&Inst, &Inst, EdgeType::Assign, AttrAll));
496   }
498   void visitInsertValueInst(InsertValueInst &Inst) {
499     auto *Agg = Inst.getOperand(0);
500     auto *Val = Inst.getOperand(1);
501     Output.push_back(Edge(&Inst, Agg, EdgeType::Assign, AttrNone));
502     Output.push_back(Edge(&Inst, Val, EdgeType::Dereference, AttrNone));
503   }
505   void visitExtractValueInst(ExtractValueInst &Inst) {
506     auto *Ptr = Inst.getAggregateOperand();
507     Output.push_back(Edge(&Inst, Ptr, EdgeType::Reference, AttrNone));
508   }
510   void visitShuffleVectorInst(ShuffleVectorInst &Inst) {
511     auto *From1 = Inst.getOperand(0);
512     auto *From2 = Inst.getOperand(1);
513     Output.push_back(Edge(&Inst, From1, EdgeType::Assign, AttrNone));
514     Output.push_back(Edge(&Inst, From2, EdgeType::Assign, AttrNone));
515   }
516 };
518 // For a given instruction, we need to know which Value* to get the
519 // users of in order to build our graph. In some cases (i.e. add),
520 // we simply need the Instruction*. In other cases (i.e. store),
521 // finding the users of the Instruction* is useless; we need to find
522 // the users of the first operand. This handles determining which
523 // value to follow for us.
524 //
525 // Note: we *need* to keep this in sync with GetEdgesVisitor. Add
526 // something to GetEdgesVisitor, add it here -- remove something from
527 // GetEdgesVisitor, remove it here.
528 class GetTargetValueVisitor
529     : public InstVisitor<GetTargetValueVisitor, Value *> {
530 public:
531   Value *visitInstruction(Instruction &Inst) { return &Inst; }
533   Value *visitStoreInst(StoreInst &Inst) { return Inst.getPointerOperand(); }
535   Value *visitAtomicCmpXchgInst(AtomicCmpXchgInst &Inst) {
536     return Inst.getPointerOperand();
537   }
539   Value *visitAtomicRMWInst(AtomicRMWInst &Inst) {
540     return Inst.getPointerOperand();
541   }
543   Value *visitInsertElementInst(InsertElementInst &Inst) {
544     return Inst.getOperand(0);
545   }
547   Value *visitInsertValueInst(InsertValueInst &Inst) {
548     return Inst.getAggregateOperand();
549   }
550 };
552 // Set building requires a weighted bidirectional graph.
553 template <typename EdgeTypeT> class WeightedBidirectionalGraph {
554 public:
555   typedef std::size_t Node;
557 private:
558   const static Node StartNode = Node(0);
560   struct Edge {
561     EdgeTypeT Weight;
562     Node Other;
564     Edge(const EdgeTypeT &W, const Node &N)
565       : Weight(W), Other(N) {}
567     bool operator==(const Edge &E) const {
568       return Weight == E.Weight && Other == E.Other;
569     }
571     bool operator!=(const Edge &E) const { return !operator==(E); }
572   };
574   struct NodeImpl {
575     std::vector<Edge> Edges;
576   };
578   std::vector<NodeImpl> NodeImpls;
580   bool inbounds(Node NodeIndex) const { return NodeIndex < NodeImpls.size(); }
582   const NodeImpl &getNode(Node N) const { return NodeImpls[N]; }
583   NodeImpl &getNode(Node N) { return NodeImpls[N]; }
585 public:
586   // ----- Various Edge iterators for the graph ----- //
588   // \brief Iterator for edges. Because this graph is bidirected, we don't
589   // allow modificaiton of the edges using this iterator. Additionally, the
590   // iterator becomes invalid if you add edges to or from the node you're
591   // getting the edges of.
592   struct EdgeIterator : public std::iterator<std::forward_iterator_tag,
593                                              std::tuple<EdgeTypeT, Node *>> {
594     EdgeIterator(const typename std::vector<Edge>::const_iterator &Iter)
595         : Current(Iter) {}
597     EdgeIterator(NodeImpl &Impl) : Current(Impl.begin()) {}
599     EdgeIterator &operator++() {
600       ++Current;
601       return *this;
602     }
604     EdgeIterator operator++(int) {
605       EdgeIterator Copy(Current);
606       operator++();
607       return Copy;
608     }
610     std::tuple<EdgeTypeT, Node> &operator*() {
611       Store = std::make_tuple(Current->Weight, Current->Other);
612       return Store;
613     }
615     bool operator==(const EdgeIterator &Other) const {
616       return Current == Other.Current;
617     }
619     bool operator!=(const EdgeIterator &Other) const {
620       return !operator==(Other);
621     }
623   private:
624     typename std::vector<Edge>::const_iterator Current;
625     std::tuple<EdgeTypeT, Node> Store;
626   };
628   // Wrapper for EdgeIterator with begin()/end() calls.
629   struct EdgeIterable {
630     EdgeIterable(const std::vector<Edge> &Edges)
631         : BeginIter(Edges.begin()), EndIter(Edges.end()) {}
633     EdgeIterator begin() { return EdgeIterator(BeginIter); }
635     EdgeIterator end() { return EdgeIterator(EndIter); }
637   private:
638     typename std::vector<Edge>::const_iterator BeginIter;
639     typename std::vector<Edge>::const_iterator EndIter;
640   };
642   // ----- Actual graph-related things ----- //
644   WeightedBidirectionalGraph() {}
646   WeightedBidirectionalGraph(WeightedBidirectionalGraph<EdgeTypeT> &&Other)
647       : NodeImpls(std::move(Other.NodeImpls)) {}
649   WeightedBidirectionalGraph<EdgeTypeT> &
650   operator=(WeightedBidirectionalGraph<EdgeTypeT> &&Other) {
651     NodeImpls = std::move(Other.NodeImpls);
652     return *this;
653   }
655   Node addNode() {
656     auto Index = NodeImpls.size();
657     auto NewNode = Node(Index);
658     NodeImpls.push_back(NodeImpl());
659     return NewNode;
660   }
662   void addEdge(Node From, Node To, const EdgeTypeT &Weight,
663                const EdgeTypeT &ReverseWeight) {
664     assert(inbounds(From));
665     assert(inbounds(To));
666     auto &FromNode = getNode(From);
667     auto &ToNode = getNode(To);
668     FromNode.Edges.push_back(Edge(Weight, To));
669     ToNode.Edges.push_back(Edge(ReverseWeight, From));
670   }
672   EdgeIterable edgesFor(const Node &N) const {
673     const auto &Node = getNode(N);
674     return EdgeIterable(Node.Edges);
675   }
677   bool empty() const { return NodeImpls.empty(); }
678   std::size_t size() const { return NodeImpls.size(); }
680   // \brief Gets an arbitrary node in the graph as a starting point for
681   // traversal.
682   Node getEntryNode() {
683     assert(inbounds(StartNode));
684     return StartNode;
685   }
686 };
688 typedef WeightedBidirectionalGraph<std::pair<EdgeType, StratifiedAttrs>> GraphT;
689 typedef DenseMap<Value *, GraphT::Node> NodeMapT;
692 // -- Setting up/registering CFLAA pass -- //
693 char CFLAliasAnalysis::ID = 0;
695 INITIALIZE_AG_PASS(CFLAliasAnalysis, AliasAnalysis, "cfl-aa",
696                    "CFL-Based AA implementation", false, true, false)
698 ImmutablePass *llvm::createCFLAliasAnalysisPass() {
699   return new CFLAliasAnalysis();
702 //===----------------------------------------------------------------------===//
703 // Function declarations that require types defined in the namespace above
704 //===----------------------------------------------------------------------===//
706 // Given an argument number, returns the appropriate Attr index to set.
707 static StratifiedAttr argNumberToAttrIndex(StratifiedAttr);
709 // Given a Value, potentially return which AttrIndex it maps to.
710 static Optional<StratifiedAttr> valueToAttrIndex(Value *Val);
712 // Gets the inverse of a given EdgeType.
713 static EdgeType flipWeight(EdgeType);
715 // Gets edges of the given Instruction*, writing them to the SmallVector*.
716 static void argsToEdges(CFLAliasAnalysis &, Instruction *,
717                         SmallVectorImpl<Edge> &);
719 // Gets the "Level" that one should travel in StratifiedSets
720 // given an EdgeType.
721 static Level directionOfEdgeType(EdgeType);
723 // Builds the graph needed for constructing the StratifiedSets for the
724 // given function
725 static void buildGraphFrom(CFLAliasAnalysis &, Function *,
726                            SmallVectorImpl<Value *> &, NodeMapT &, GraphT &);
728 // Builds the graph + StratifiedSets for a function.
729 static FunctionInfo buildSetsFrom(CFLAliasAnalysis &, Function *);
731 static Optional<Function *> parentFunctionOfValue(Value *Val) {
732   if (auto *Inst = dyn_cast<Instruction>(Val)) {
733     auto *Bb = Inst->getParent();
734     return Bb->getParent();
735   }
737   if (auto *Arg = dyn_cast<Argument>(Val))
738     return Arg->getParent();
739   return NoneType();
742 template <typename Inst>
743 static bool getPossibleTargets(Inst *Call,
744                                SmallVectorImpl<Function *> &Output) {
745   if (auto *Fn = Call->getCalledFunction()) {
746     Output.push_back(Fn);
747     return true;
748   }
750   // TODO: If the call is indirect, we might be able to enumerate all potential
751   // targets of the call and return them, rather than just failing.
752   return false;
755 static Optional<Value *> getTargetValue(Instruction *Inst) {
756   GetTargetValueVisitor V;
757   return V.visit(Inst);
760 static bool hasUsefulEdges(Instruction *Inst) {
761   bool IsNonInvokeTerminator =
762       isa<TerminatorInst>(Inst) && !isa<InvokeInst>(Inst);
763   return !isa<CmpInst>(Inst) && !isa<FenceInst>(Inst) && !IsNonInvokeTerminator;
766 static Optional<StratifiedAttr> valueToAttrIndex(Value *Val) {
767   if (isa<GlobalValue>(Val))
768     return AttrGlobalIndex;
770   if (auto *Arg = dyn_cast<Argument>(Val))
771     if (!Arg->hasNoAliasAttr())
772       return argNumberToAttrIndex(Arg->getArgNo());
773   return NoneType();
776 static StratifiedAttr argNumberToAttrIndex(unsigned ArgNum) {
777   if (ArgNum > AttrMaxNumArgs)
778     return AttrAllIndex;
779   return ArgNum + AttrFirstArgIndex;
782 static EdgeType flipWeight(EdgeType Initial) {
783   switch (Initial) {
784   case EdgeType::Assign:
785     return EdgeType::Assign;
786   case EdgeType::Dereference:
787     return EdgeType::Reference;
788   case EdgeType::Reference:
789     return EdgeType::Dereference;
790   }
791   llvm_unreachable("Incomplete coverage of EdgeType enum");
794 static void argsToEdges(CFLAliasAnalysis &Analysis, Instruction *Inst,
795                         SmallVectorImpl<Edge> &Output) {
796   GetEdgesVisitor v(Analysis, Output);
797   v.visit(Inst);
800 static Level directionOfEdgeType(EdgeType Weight) {
801   switch (Weight) {
802   case EdgeType::Reference:
803     return Level::Above;
804   case EdgeType::Dereference:
805     return Level::Below;
806   case EdgeType::Assign:
807     return Level::Same;
808   }
809   llvm_unreachable("Incomplete switch coverage");
812 // Aside: We may remove graph construction entirely, because it doesn't really
813 // buy us much that we don't already have. I'd like to add interprocedural
814 // analysis prior to this however, in case that somehow requires the graph
815 // produced by this for efficient execution
816 static void buildGraphFrom(CFLAliasAnalysis &Analysis, Function *Fn,
817                            SmallVectorImpl<Value *> &ReturnedValues,
818                            NodeMapT &Map, GraphT &Graph) {
819   const auto findOrInsertNode = [&Map, &Graph](Value *Val) {
820     auto Pair = Map.insert(std::make_pair(Val, GraphT::Node()));
821     auto &Iter = Pair.first;
822     if (Pair.second) {
823       auto NewNode = Graph.addNode();
824       Iter->second = NewNode;
825     }
826     return Iter->second;
827   };
829   SmallVector<Edge, 8> Edges;
830   for (auto &Bb : Fn->getBasicBlockList()) {
831     for (auto &Inst : Bb.getInstList()) {
832       // We don't want the edges of most "return" instructions, but we *do* want
833       // to know what can be returned.
834       if (auto *Ret = dyn_cast<ReturnInst>(&Inst))
835         ReturnedValues.push_back(Ret);
837       if (!hasUsefulEdges(&Inst))
838         continue;
840       Edges.clear();
841       argsToEdges(Analysis, &Inst, Edges);
843       // In the case of an unused alloca (or similar), edges may be empty. Note
844       // that it exists so we can potentially answer NoAlias.
845       if (Edges.empty()) {
846         auto MaybeVal = getTargetValue(&Inst);
847         assert(MaybeVal.hasValue());
848         auto *Target = *MaybeVal;
849         findOrInsertNode(Target);
850         continue;
851       }
853       for (const Edge &E : Edges) {
854         auto To = findOrInsertNode(E.To);
855         auto From = findOrInsertNode(E.From);
856         auto FlippedWeight = flipWeight(E.Weight);
857         auto Attrs = E.AdditionalAttrs;
858         Graph.addEdge(From, To, std::make_pair(E.Weight, Attrs),
859                                 std::make_pair(FlippedWeight, Attrs));
860       }
861     }
862   }
865 static FunctionInfo buildSetsFrom(CFLAliasAnalysis &Analysis, Function *Fn) {
866   NodeMapT Map;
867   GraphT Graph;
868   SmallVector<Value *, 4> ReturnedValues;
870   buildGraphFrom(Analysis, Fn, ReturnedValues, Map, Graph);
872   DenseMap<GraphT::Node, Value *> NodeValueMap;
873   NodeValueMap.resize(Map.size());
874   for (const auto &Pair : Map)
875     NodeValueMap.insert(std::make_pair(Pair.second, Pair.first));
877   const auto findValueOrDie = [&NodeValueMap](GraphT::Node Node) {
878     auto ValIter = NodeValueMap.find(Node);
879     assert(ValIter != NodeValueMap.end());
880     return ValIter->second;
881   };
883   StratifiedSetsBuilder<Value *> Builder;
885   SmallVector<GraphT::Node, 16> Worklist;
886   for (auto &Pair : Map) {
887     Worklist.clear();
889     auto *Value = Pair.first;
890     Builder.add(Value);
891     auto InitialNode = Pair.second;
892     Worklist.push_back(InitialNode);
893     while (!Worklist.empty()) {
894       auto Node = Worklist.pop_back_val();
895       auto *CurValue = findValueOrDie(Node);
896       if (isa<Constant>(CurValue) && !isa<GlobalValue>(CurValue))
897         continue;
899       for (const auto &EdgeTuple : Graph.edgesFor(Node)) {
900         auto Weight = std::get<0>(EdgeTuple);
901         auto Label = Weight.first;
902         auto &OtherNode = std::get<1>(EdgeTuple);
903         auto *OtherValue = findValueOrDie(OtherNode);
905         if (isa<Constant>(OtherValue) && !isa<GlobalValue>(OtherValue))
906           continue;
908         bool Added;
909         switch (directionOfEdgeType(Label)) {
910         case Level::Above:
911           Added = Builder.addAbove(CurValue, OtherValue);
912           break;
913         case Level::Below:
914           Added = Builder.addBelow(CurValue, OtherValue);
915           break;
916         case Level::Same:
917           Added = Builder.addWith(CurValue, OtherValue);
918           break;
919         }
921         if (Added) {
922           auto Aliasing = Weight.second;
923           if (auto MaybeCurIndex = valueToAttrIndex(CurValue))
924             Aliasing.set(*MaybeCurIndex);
925           if (auto MaybeOtherIndex = valueToAttrIndex(OtherValue))
926             Aliasing.set(*MaybeOtherIndex);
927           Builder.noteAttributes(CurValue, Aliasing);
928           Builder.noteAttributes(OtherValue, Aliasing);
929           Worklist.push_back(OtherNode);
930         }
931       }
932     }
933   }
935   // There are times when we end up with parameters not in our graph (i.e. if
936   // it's only used as the condition of a branch). Other bits of code depend on
937   // things that were present during construction being present in the graph.
938   // So, we add all present arguments here.
939   for (auto &Arg : Fn->args()) {
940     Builder.add(&Arg);
941   }
943   return FunctionInfo(Builder.build(), std::move(ReturnedValues));
946 void CFLAliasAnalysis::scan(Function *Fn) {
947   auto InsertPair = Cache.insert(std::make_pair(Fn, Optional<FunctionInfo>()));
948   (void)InsertPair;
949   assert(InsertPair.second &&
950          "Trying to scan a function that has already been cached");
952   FunctionInfo Info(buildSetsFrom(*this, Fn));
953   Cache[Fn] = std::move(Info);
954   Handles.push_front(FunctionHandle(Fn, this));
957 AliasAnalysis::AliasResult
958 CFLAliasAnalysis::query(const AliasAnalysis::Location &LocA,
959                         const AliasAnalysis::Location &LocB) {
960   auto *ValA = const_cast<Value *>(LocA.Ptr);
961   auto *ValB = const_cast<Value *>(LocB.Ptr);
963   Function *Fn = nullptr;
964   auto MaybeFnA = parentFunctionOfValue(ValA);
965   auto MaybeFnB = parentFunctionOfValue(ValB);
966   if (!MaybeFnA.hasValue() && !MaybeFnB.hasValue()) {
967     llvm_unreachable("Don't know how to extract the parent function "
968                      "from values A or B");
969   }
971   if (MaybeFnA.hasValue()) {
972     Fn = *MaybeFnA;
973     assert((!MaybeFnB.hasValue() || *MaybeFnB == *MaybeFnA) &&
974            "Interprocedural queries not supported");
975   } else {
976     Fn = *MaybeFnB;
977   }
979   assert(Fn != nullptr);
980   auto &MaybeInfo = ensureCached(Fn);
981   assert(MaybeInfo.hasValue());
983   auto &Sets = MaybeInfo->Sets;
984   auto MaybeA = Sets.find(ValA);
985   if (!MaybeA.hasValue())
986     return AliasAnalysis::MayAlias;
988   auto MaybeB = Sets.find(ValB);
989   if (!MaybeB.hasValue())
990     return AliasAnalysis::MayAlias;
992   auto SetA = *MaybeA;
993   auto SetB = *MaybeB;
995   if (SetA.Index == SetB.Index)
996     return AliasAnalysis::PartialAlias;
998   auto AttrsA = Sets.getLink(SetA.Index).Attrs;
999   auto AttrsB = Sets.getLink(SetB.Index).Attrs;
1000   // Stratified set attributes are used as markets to signify whether a member
1001   // of a StratifiedSet (or a member of a set above the current set) has 
1002   // interacted with either arguments or globals. "Interacted with" meaning
1003   // its value may be different depending on the value of an argument or 
1004   // global. The thought behind this is that, because arguments and globals
1005   // may alias each other, if AttrsA and AttrsB have touched args/globals,
1006   // we must conservatively say that they alias. However, if at least one of 
1007   // the sets has no values that could legally be altered by changing the value 
1008   // of an argument or global, then we don't have to be as conservative.
1009   if (AttrsA.any() && AttrsB.any())
1010     return AliasAnalysis::MayAlias;
1012   return AliasAnalysis::NoAlias;