]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/CodeGen/AllocationOrder.h
Don't pre-populate the set of keys in the map with variable locations history.
[opencl/llvm.git] / lib / CodeGen / AllocationOrder.h
1 //===-- llvm/CodeGen/AllocationOrder.h - Allocation Order -*- C++ -*-------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements an allocation order for virtual registers.
11 //
12 // The preferred allocation order for a virtual register depends on allocation
13 // hints and target hooks. The AllocationOrder class encapsulates all of that.
14 //
15 //===----------------------------------------------------------------------===//
17 #ifndef LLVM_CODEGEN_ALLOCATIONORDER_H
18 #define LLVM_CODEGEN_ALLOCATIONORDER_H
20 #include "llvm/ADT/ArrayRef.h"
21 #include "llvm/MC/MCRegisterInfo.h"
23 namespace llvm {
25 class RegisterClassInfo;
26 class VirtRegMap;
28 class AllocationOrder {
29   SmallVector<MCPhysReg, 16> Hints;
30   ArrayRef<MCPhysReg> Order;
31   int Pos;
33 public:
34   /// Create a new AllocationOrder for VirtReg.
35   /// @param VirtReg      Virtual register to allocate for.
36   /// @param VRM          Virtual register map for function.
37   /// @param RegClassInfo Information about reserved and allocatable registers.
38   AllocationOrder(unsigned VirtReg,
39                   const VirtRegMap &VRM,
40                   const RegisterClassInfo &RegClassInfo);
42   /// Get the allocation order without reordered hints.
43   ArrayRef<MCPhysReg> getOrder() const { return Order; }
45   /// Return the next physical register in the allocation order, or 0.
46   /// It is safe to call next() again after it returned 0, it will keep
47   /// returning 0 until rewind() is called.
48   unsigned next(unsigned Limit = 0) {
49     if (Pos < 0)
50       return Hints.end()[Pos++];
51     if (!Limit)
52       Limit = Order.size();
53     while (Pos < int(Limit)) {
54       unsigned Reg = Order[Pos++];
55       if (!isHint(Reg))
56         return Reg;
57     }
58     return 0;
59   }
61   /// As next(), but allow duplicates to be returned, and stop before the
62   /// Limit'th register in the RegisterClassInfo allocation order.
63   ///
64   /// This can produce more than Limit registers if there are hints.
65   unsigned nextWithDups(unsigned Limit) {
66     if (Pos < 0)
67       return Hints.end()[Pos++];
68     if (Pos < int(Limit))
69       return Order[Pos++];
70     return 0;
71   }
73   /// Start over from the beginning.
74   void rewind() { Pos = -int(Hints.size()); }
76   /// Return true if the last register returned from next() was a preferred register.
77   bool isHint() const { return Pos <= 0; }
79   /// Return true if PhysReg is a preferred register.
80   bool isHint(unsigned PhysReg) const {
81     return std::find(Hints.begin(), Hints.end(), PhysReg) != Hints.end();
82   }
83 };
85 } // end namespace llvm
87 #endif