1 //===-- llvm/CodeGen/AllocationOrder.h - Allocation Order -*- C++ -*-------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements an allocation order for virtual registers.
11 //
12 // The preferred allocation order for a virtual register depends on allocation
13 // hints and target hooks. The AllocationOrder class encapsulates all of that.
14 //
15 //===----------------------------------------------------------------------===//
17 #ifndef LLVM_CODEGEN_ALLOCATIONORDER_H
18 #define LLVM_CODEGEN_ALLOCATIONORDER_H
20 #include "llvm/ADT/ArrayRef.h"
21 #include "llvm/MC/MCRegisterInfo.h"
23 namespace llvm {
25 class RegisterClassInfo;
26 class VirtRegMap;
28 class AllocationOrder {
29 SmallVector<MCPhysReg, 16> Hints;
30 ArrayRef<MCPhysReg> Order;
31 int Pos;
33 public:
34 /// Create a new AllocationOrder for VirtReg.
35 /// @param VirtReg Virtual register to allocate for.
36 /// @param VRM Virtual register map for function.
37 /// @param RegClassInfo Information about reserved and allocatable registers.
38 AllocationOrder(unsigned VirtReg,
39 const VirtRegMap &VRM,
40 const RegisterClassInfo &RegClassInfo);
42 /// Get the allocation order without reordered hints.
43 ArrayRef<MCPhysReg> getOrder() const { return Order; }
45 /// Return the next physical register in the allocation order, or 0.
46 /// It is safe to call next() again after it returned 0, it will keep
47 /// returning 0 until rewind() is called.
48 unsigned next(unsigned Limit = 0) {
49 if (Pos < 0)
50 return Hints.end()[Pos++];
51 if (!Limit)
52 Limit = Order.size();
53 while (Pos < int(Limit)) {
54 unsigned Reg = Order[Pos++];
55 if (!isHint(Reg))
56 return Reg;
57 }
58 return 0;
59 }
61 /// As next(), but allow duplicates to be returned, and stop before the
62 /// Limit'th register in the RegisterClassInfo allocation order.
63 ///
64 /// This can produce more than Limit registers if there are hints.
65 unsigned nextWithDups(unsigned Limit) {
66 if (Pos < 0)
67 return Hints.end()[Pos++];
68 if (Pos < int(Limit))
69 return Order[Pos++];
70 return 0;
71 }
73 /// Start over from the beginning.
74 void rewind() { Pos = -int(Hints.size()); }
76 /// Return true if the last register returned from next() was a preferred register.
77 bool isHint() const { return Pos <= 0; }
79 /// Return true if PhysReg is a preferred register.
80 bool isHint(unsigned PhysReg) const {
81 return std::find(Hints.begin(), Hints.end(), PhysReg) != Hints.end();
82 }
83 };
85 } // end namespace llvm
87 #endif