]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/CodeGen/Analysis.cpp
Debug info: Implement (rvalue) reference qualifiers for C++11 non-static
[opencl/llvm.git] / lib / CodeGen / Analysis.cpp
1 //===-- Analysis.cpp - CodeGen LLVM IR Analysis Utilities -----------------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file defines several CodeGen-specific LLVM IR analysis utilties.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "llvm/CodeGen/Analysis.h"
15 #include "llvm/Analysis/ValueTracking.h"
16 #include "llvm/CodeGen/MachineFunction.h"
17 #include "llvm/IR/DataLayout.h"
18 #include "llvm/IR/DerivedTypes.h"
19 #include "llvm/IR/Function.h"
20 #include "llvm/IR/Instructions.h"
21 #include "llvm/IR/IntrinsicInst.h"
22 #include "llvm/IR/LLVMContext.h"
23 #include "llvm/IR/Module.h"
24 #include "llvm/Support/ErrorHandling.h"
25 #include "llvm/Support/MathExtras.h"
26 #include "llvm/Target/TargetLowering.h"
27 using namespace llvm;
29 /// ComputeLinearIndex - Given an LLVM IR aggregate type and a sequence
30 /// of insertvalue or extractvalue indices that identify a member, return
31 /// the linearized index of the start of the member.
32 ///
33 unsigned llvm::ComputeLinearIndex(Type *Ty,
34                                   const unsigned *Indices,
35                                   const unsigned *IndicesEnd,
36                                   unsigned CurIndex) {
37   // Base case: We're done.
38   if (Indices && Indices == IndicesEnd)
39     return CurIndex;
41   // Given a struct type, recursively traverse the elements.
42   if (StructType *STy = dyn_cast<StructType>(Ty)) {
43     for (StructType::element_iterator EB = STy->element_begin(),
44                                       EI = EB,
45                                       EE = STy->element_end();
46         EI != EE; ++EI) {
47       if (Indices && *Indices == unsigned(EI - EB))
48         return ComputeLinearIndex(*EI, Indices+1, IndicesEnd, CurIndex);
49       CurIndex = ComputeLinearIndex(*EI, 0, 0, CurIndex);
50     }
51     return CurIndex;
52   }
53   // Given an array type, recursively traverse the elements.
54   else if (ArrayType *ATy = dyn_cast<ArrayType>(Ty)) {
55     Type *EltTy = ATy->getElementType();
56     for (unsigned i = 0, e = ATy->getNumElements(); i != e; ++i) {
57       if (Indices && *Indices == i)
58         return ComputeLinearIndex(EltTy, Indices+1, IndicesEnd, CurIndex);
59       CurIndex = ComputeLinearIndex(EltTy, 0, 0, CurIndex);
60     }
61     return CurIndex;
62   }
63   // We haven't found the type we're looking for, so keep searching.
64   return CurIndex + 1;
65 }
67 /// ComputeValueVTs - Given an LLVM IR type, compute a sequence of
68 /// EVTs that represent all the individual underlying
69 /// non-aggregate types that comprise it.
70 ///
71 /// If Offsets is non-null, it points to a vector to be filled in
72 /// with the in-memory offsets of each of the individual values.
73 ///
74 void llvm::ComputeValueVTs(const TargetLowering &TLI, Type *Ty,
75                            SmallVectorImpl<EVT> &ValueVTs,
76                            SmallVectorImpl<uint64_t> *Offsets,
77                            uint64_t StartingOffset) {
78   // Given a struct type, recursively traverse the elements.
79   if (StructType *STy = dyn_cast<StructType>(Ty)) {
80     const StructLayout *SL = TLI.getDataLayout()->getStructLayout(STy);
81     for (StructType::element_iterator EB = STy->element_begin(),
82                                       EI = EB,
83                                       EE = STy->element_end();
84          EI != EE; ++EI)
85       ComputeValueVTs(TLI, *EI, ValueVTs, Offsets,
86                       StartingOffset + SL->getElementOffset(EI - EB));
87     return;
88   }
89   // Given an array type, recursively traverse the elements.
90   if (ArrayType *ATy = dyn_cast<ArrayType>(Ty)) {
91     Type *EltTy = ATy->getElementType();
92     uint64_t EltSize = TLI.getDataLayout()->getTypeAllocSize(EltTy);
93     for (unsigned i = 0, e = ATy->getNumElements(); i != e; ++i)
94       ComputeValueVTs(TLI, EltTy, ValueVTs, Offsets,
95                       StartingOffset + i * EltSize);
96     return;
97   }
98   // Interpret void as zero return values.
99   if (Ty->isVoidTy())
100     return;
101   // Base case: we can get an EVT for this LLVM IR type.
102   ValueVTs.push_back(TLI.getValueType(Ty));
103   if (Offsets)
104     Offsets->push_back(StartingOffset);
107 /// ExtractTypeInfo - Returns the type info, possibly bitcast, encoded in V.
108 GlobalVariable *llvm::ExtractTypeInfo(Value *V) {
109   V = V->stripPointerCasts();
110   GlobalVariable *GV = dyn_cast<GlobalVariable>(V);
112   if (GV && GV->getName() == "llvm.eh.catch.all.value") {
113     assert(GV->hasInitializer() &&
114            "The EH catch-all value must have an initializer");
115     Value *Init = GV->getInitializer();
116     GV = dyn_cast<GlobalVariable>(Init);
117     if (!GV) V = cast<ConstantPointerNull>(Init);
118   }
120   assert((GV || isa<ConstantPointerNull>(V)) &&
121          "TypeInfo must be a global variable or NULL");
122   return GV;
125 /// hasInlineAsmMemConstraint - Return true if the inline asm instruction being
126 /// processed uses a memory 'm' constraint.
127 bool
128 llvm::hasInlineAsmMemConstraint(InlineAsm::ConstraintInfoVector &CInfos,
129                                 const TargetLowering &TLI) {
130   for (unsigned i = 0, e = CInfos.size(); i != e; ++i) {
131     InlineAsm::ConstraintInfo &CI = CInfos[i];
132     for (unsigned j = 0, ee = CI.Codes.size(); j != ee; ++j) {
133       TargetLowering::ConstraintType CType = TLI.getConstraintType(CI.Codes[j]);
134       if (CType == TargetLowering::C_Memory)
135         return true;
136     }
138     // Indirect operand accesses access memory.
139     if (CI.isIndirect)
140       return true;
141   }
143   return false;
146 /// getFCmpCondCode - Return the ISD condition code corresponding to
147 /// the given LLVM IR floating-point condition code.  This includes
148 /// consideration of global floating-point math flags.
149 ///
150 ISD::CondCode llvm::getFCmpCondCode(FCmpInst::Predicate Pred) {
151   switch (Pred) {
152   case FCmpInst::FCMP_FALSE: return ISD::SETFALSE;
153   case FCmpInst::FCMP_OEQ:   return ISD::SETOEQ;
154   case FCmpInst::FCMP_OGT:   return ISD::SETOGT;
155   case FCmpInst::FCMP_OGE:   return ISD::SETOGE;
156   case FCmpInst::FCMP_OLT:   return ISD::SETOLT;
157   case FCmpInst::FCMP_OLE:   return ISD::SETOLE;
158   case FCmpInst::FCMP_ONE:   return ISD::SETONE;
159   case FCmpInst::FCMP_ORD:   return ISD::SETO;
160   case FCmpInst::FCMP_UNO:   return ISD::SETUO;
161   case FCmpInst::FCMP_UEQ:   return ISD::SETUEQ;
162   case FCmpInst::FCMP_UGT:   return ISD::SETUGT;
163   case FCmpInst::FCMP_UGE:   return ISD::SETUGE;
164   case FCmpInst::FCMP_ULT:   return ISD::SETULT;
165   case FCmpInst::FCMP_ULE:   return ISD::SETULE;
166   case FCmpInst::FCMP_UNE:   return ISD::SETUNE;
167   case FCmpInst::FCMP_TRUE:  return ISD::SETTRUE;
168   default: llvm_unreachable("Invalid FCmp predicate opcode!");
169   }
172 ISD::CondCode llvm::getFCmpCodeWithoutNaN(ISD::CondCode CC) {
173   switch (CC) {
174     case ISD::SETOEQ: case ISD::SETUEQ: return ISD::SETEQ;
175     case ISD::SETONE: case ISD::SETUNE: return ISD::SETNE;
176     case ISD::SETOLT: case ISD::SETULT: return ISD::SETLT;
177     case ISD::SETOLE: case ISD::SETULE: return ISD::SETLE;
178     case ISD::SETOGT: case ISD::SETUGT: return ISD::SETGT;
179     case ISD::SETOGE: case ISD::SETUGE: return ISD::SETGE;
180     default: return CC;
181   }
184 /// getICmpCondCode - Return the ISD condition code corresponding to
185 /// the given LLVM IR integer condition code.
186 ///
187 ISD::CondCode llvm::getICmpCondCode(ICmpInst::Predicate Pred) {
188   switch (Pred) {
189   case ICmpInst::ICMP_EQ:  return ISD::SETEQ;
190   case ICmpInst::ICMP_NE:  return ISD::SETNE;
191   case ICmpInst::ICMP_SLE: return ISD::SETLE;
192   case ICmpInst::ICMP_ULE: return ISD::SETULE;
193   case ICmpInst::ICMP_SGE: return ISD::SETGE;
194   case ICmpInst::ICMP_UGE: return ISD::SETUGE;
195   case ICmpInst::ICMP_SLT: return ISD::SETLT;
196   case ICmpInst::ICMP_ULT: return ISD::SETULT;
197   case ICmpInst::ICMP_SGT: return ISD::SETGT;
198   case ICmpInst::ICMP_UGT: return ISD::SETUGT;
199   default:
200     llvm_unreachable("Invalid ICmp predicate opcode!");
201   }
204 static bool isNoopBitcast(Type *T1, Type *T2,
205                           const TargetLoweringBase& TLI) {
206   return T1 == T2 || (T1->isPointerTy() && T2->isPointerTy()) ||
207          (isa<VectorType>(T1) && isa<VectorType>(T2) &&
208           TLI.isTypeLegal(EVT::getEVT(T1)) && TLI.isTypeLegal(EVT::getEVT(T2)));
211 /// Look through operations that will be free to find the earliest source of
212 /// this value.
213 ///
214 /// @param ValLoc If V has aggegate type, we will be interested in a particular
215 /// scalar component. This records its address; the reverse of this list gives a
216 /// sequence of indices appropriate for an extractvalue to locate the important
217 /// value. This value is updated during the function and on exit will indicate
218 /// similar information for the Value returned.
219 ///
220 /// @param DataBits If this function looks through truncate instructions, this
221 /// will record the smallest size attained.
222 static const Value *getNoopInput(const Value *V,
223                                  SmallVectorImpl<unsigned> &ValLoc,
224                                  unsigned &DataBits,
225                                  const TargetLoweringBase &TLI) {
226   while (true) {
227     // Try to look through V1; if V1 is not an instruction, it can't be looked
228     // through.
229     const Instruction *I = dyn_cast<Instruction>(V);
230     if (!I || I->getNumOperands() == 0) return V;
231     const Value *NoopInput = 0;
233     Value *Op = I->getOperand(0);
234     if (isa<BitCastInst>(I)) {
235       // Look through truly no-op bitcasts.
236       if (isNoopBitcast(Op->getType(), I->getType(), TLI))
237         NoopInput = Op;
238     } else if (isa<GetElementPtrInst>(I)) {
239       // Look through getelementptr
240       if (cast<GetElementPtrInst>(I)->hasAllZeroIndices())
241         NoopInput = Op;
242     } else if (isa<IntToPtrInst>(I)) {
243       // Look through inttoptr.
244       // Make sure this isn't a truncating or extending cast.  We could
245       // support this eventually, but don't bother for now.
246       if (!isa<VectorType>(I->getType()) &&
247           TLI.getPointerTy().getSizeInBits() ==
248           cast<IntegerType>(Op->getType())->getBitWidth())
249         NoopInput = Op;
250     } else if (isa<PtrToIntInst>(I)) {
251       // Look through ptrtoint.
252       // Make sure this isn't a truncating or extending cast.  We could
253       // support this eventually, but don't bother for now.
254       if (!isa<VectorType>(I->getType()) &&
255           TLI.getPointerTy().getSizeInBits() ==
256           cast<IntegerType>(I->getType())->getBitWidth())
257         NoopInput = Op;
258     } else if (isa<TruncInst>(I) &&
259                TLI.allowTruncateForTailCall(Op->getType(), I->getType())) {
260       DataBits = std::min(DataBits, I->getType()->getPrimitiveSizeInBits());
261       NoopInput = Op;
262     } else if (isa<CallInst>(I)) {
263       // Look through call (skipping callee)
264       for (User::const_op_iterator i = I->op_begin(), e = I->op_end() - 1;
265            i != e; ++i) {
266         unsigned attrInd = i - I->op_begin() + 1;
267         if (cast<CallInst>(I)->paramHasAttr(attrInd, Attribute::Returned) &&
268             isNoopBitcast((*i)->getType(), I->getType(), TLI)) {
269           NoopInput = *i;
270           break;
271         }
272       }
273     } else if (isa<InvokeInst>(I)) {
274       // Look through invoke (skipping BB, BB, Callee)
275       for (User::const_op_iterator i = I->op_begin(), e = I->op_end() - 3;
276            i != e; ++i) {
277         unsigned attrInd = i - I->op_begin() + 1;
278         if (cast<InvokeInst>(I)->paramHasAttr(attrInd, Attribute::Returned) &&
279             isNoopBitcast((*i)->getType(), I->getType(), TLI)) {
280           NoopInput = *i;
281           break;
282         }
283       }
284     } else if (const InsertValueInst *IVI = dyn_cast<InsertValueInst>(V)) {
285       // Value may come from either the aggregate or the scalar
286       ArrayRef<unsigned> InsertLoc = IVI->getIndices();
287       if (std::equal(InsertLoc.rbegin(), InsertLoc.rend(),
288                      ValLoc.rbegin())) {
289         // The type being inserted is a nested sub-type of the aggregate; we
290         // have to remove those initial indices to get the location we're
291         // interested in for the operand.
292         ValLoc.resize(ValLoc.size() - InsertLoc.size());
293         NoopInput = IVI->getInsertedValueOperand();
294       } else {
295         // The struct we're inserting into has the value we're interested in, no
296         // change of address.
297         NoopInput = Op;
298       }
299     } else if (const ExtractValueInst *EVI = dyn_cast<ExtractValueInst>(V)) {
300       // The part we're interested in will inevitably be some sub-section of the
301       // previous aggregate. Combine the two paths to obtain the true address of
302       // our element.
303       ArrayRef<unsigned> ExtractLoc = EVI->getIndices();
304       std::copy(ExtractLoc.rbegin(), ExtractLoc.rend(),
305                 std::back_inserter(ValLoc));
306       NoopInput = Op;
307     }
308     // Terminate if we couldn't find anything to look through.
309     if (!NoopInput)
310       return V;
312     V = NoopInput;
313   }
316 /// Return true if this scalar return value only has bits discarded on its path
317 /// from the "tail call" to the "ret". This includes the obvious noop
318 /// instructions handled by getNoopInput above as well as free truncations (or
319 /// extensions prior to the call).
320 static bool slotOnlyDiscardsData(const Value *RetVal, const Value *CallVal,
321                                  SmallVectorImpl<unsigned> &RetIndices,
322                                  SmallVectorImpl<unsigned> &CallIndices,
323                                  bool AllowDifferingSizes,
324                                  const TargetLoweringBase &TLI) {
326   // Trace the sub-value needed by the return value as far back up the graph as
327   // possible, in the hope that it will intersect with the value produced by the
328   // call. In the simple case with no "returned" attribute, the hope is actually
329   // that we end up back at the tail call instruction itself.
330   unsigned BitsRequired = UINT_MAX;
331   RetVal = getNoopInput(RetVal, RetIndices, BitsRequired, TLI);
333   // If this slot in the value returned is undef, it doesn't matter what the
334   // call puts there, it'll be fine.
335   if (isa<UndefValue>(RetVal))
336     return true;
338   // Now do a similar search up through the graph to find where the value
339   // actually returned by the "tail call" comes from. In the simple case without
340   // a "returned" attribute, the search will be blocked immediately and the loop
341   // a Noop.
342   unsigned BitsProvided = UINT_MAX;
343   CallVal = getNoopInput(CallVal, CallIndices, BitsProvided, TLI);
345   // There's no hope if we can't actually trace them to (the same part of!) the
346   // same value.
347   if (CallVal != RetVal || CallIndices != RetIndices)
348     return false;
350   // However, intervening truncates may have made the call non-tail. Make sure
351   // all the bits that are needed by the "ret" have been provided by the "tail
352   // call". FIXME: with sufficiently cunning bit-tracking, we could look through
353   // extensions too.
354   if (BitsProvided < BitsRequired ||
355       (!AllowDifferingSizes && BitsProvided != BitsRequired))
356     return false;
358   return true;
361 /// For an aggregate type, determine whether a given index is within bounds or
362 /// not.
363 static bool indexReallyValid(CompositeType *T, unsigned Idx) {
364   if (ArrayType *AT = dyn_cast<ArrayType>(T))
365     return Idx < AT->getNumElements();
367   return Idx < cast<StructType>(T)->getNumElements();
370 /// Move the given iterators to the next leaf type in depth first traversal.
371 ///
372 /// Performs a depth-first traversal of the type as specified by its arguments,
373 /// stopping at the next leaf node (which may be a legitimate scalar type or an
374 /// empty struct or array).
375 ///
376 /// @param SubTypes List of the partial components making up the type from
377 /// outermost to innermost non-empty aggregate. The element currently
378 /// represented is SubTypes.back()->getTypeAtIndex(Path.back() - 1).
379 ///
380 /// @param Path Set of extractvalue indices leading from the outermost type
381 /// (SubTypes[0]) to the leaf node currently represented.
382 ///
383 /// @returns true if a new type was found, false otherwise. Calling this
384 /// function again on a finished iterator will repeatedly return
385 /// false. SubTypes.back()->getTypeAtIndex(Path.back()) is either an empty
386 /// aggregate or a non-aggregate
387 static bool advanceToNextLeafType(SmallVectorImpl<CompositeType *> &SubTypes,
388                                   SmallVectorImpl<unsigned> &Path) {
389   // First march back up the tree until we can successfully increment one of the
390   // coordinates in Path.
391   while (!Path.empty() && !indexReallyValid(SubTypes.back(), Path.back() + 1)) {
392     Path.pop_back();
393     SubTypes.pop_back();
394   }
396   // If we reached the top, then the iterator is done.
397   if (Path.empty())
398     return false;
400   // We know there's *some* valid leaf now, so march back down the tree picking
401   // out the left-most element at each node.
402   ++Path.back();
403   Type *DeeperType = SubTypes.back()->getTypeAtIndex(Path.back());
404   while (DeeperType->isAggregateType()) {
405     CompositeType *CT = cast<CompositeType>(DeeperType);
406     if (!indexReallyValid(CT, 0))
407       return true;
409     SubTypes.push_back(CT);
410     Path.push_back(0);
412     DeeperType = CT->getTypeAtIndex(0U);
413   }
415   return true;
418 /// Find the first non-empty, scalar-like type in Next and setup the iterator
419 /// components.
420 ///
421 /// Assuming Next is an aggregate of some kind, this function will traverse the
422 /// tree from left to right (i.e. depth-first) looking for the first
423 /// non-aggregate type which will play a role in function return.
424 ///
425 /// For example, if Next was {[0 x i64], {{}, i32, {}}, i32} then we would setup
426 /// Path as [1, 1] and SubTypes as [Next, {{}, i32, {}}] to represent the first
427 /// i32 in that type.
428 static bool firstRealType(Type *Next,
429                           SmallVectorImpl<CompositeType *> &SubTypes,
430                           SmallVectorImpl<unsigned> &Path) {
431   // First initialise the iterator components to the first "leaf" node
432   // (i.e. node with no valid sub-type at any index, so {} does count as a leaf
433   // despite nominally being an aggregate).
434   while (Next->isAggregateType() &&
435          indexReallyValid(cast<CompositeType>(Next), 0)) {
436     SubTypes.push_back(cast<CompositeType>(Next));
437     Path.push_back(0);
438     Next = cast<CompositeType>(Next)->getTypeAtIndex(0U);
439   }
441   // If there's no Path now, Next was originally scalar already (or empty
442   // leaf). We're done.
443   if (Path.empty())
444     return true;
446   // Otherwise, use normal iteration to keep looking through the tree until we
447   // find a non-aggregate type.
448   while (SubTypes.back()->getTypeAtIndex(Path.back())->isAggregateType()) {
449     if (!advanceToNextLeafType(SubTypes, Path))
450       return false;
451   }
453   return true;
456 /// Set the iterator data-structures to the next non-empty, non-aggregate
457 /// subtype.
458 static bool nextRealType(SmallVectorImpl<CompositeType *> &SubTypes,
459                          SmallVectorImpl<unsigned> &Path) {
460   do {
461     if (!advanceToNextLeafType(SubTypes, Path))
462       return false;
464     assert(!Path.empty() && "found a leaf but didn't set the path?");
465   } while (SubTypes.back()->getTypeAtIndex(Path.back())->isAggregateType());
467   return true;
471 /// Test if the given instruction is in a position to be optimized
472 /// with a tail-call. This roughly means that it's in a block with
473 /// a return and there's nothing that needs to be scheduled
474 /// between it and the return.
475 ///
476 /// This function only tests target-independent requirements.
477 bool llvm::isInTailCallPosition(ImmutableCallSite CS,
478                                 const TargetLowering &TLI) {
479   const Instruction *I = CS.getInstruction();
480   const BasicBlock *ExitBB = I->getParent();
481   const TerminatorInst *Term = ExitBB->getTerminator();
482   const ReturnInst *Ret = dyn_cast<ReturnInst>(Term);
484   // The block must end in a return statement or unreachable.
485   //
486   // FIXME: Decline tailcall if it's not guaranteed and if the block ends in
487   // an unreachable, for now. The way tailcall optimization is currently
488   // implemented means it will add an epilogue followed by a jump. That is
489   // not profitable. Also, if the callee is a special function (e.g.
490   // longjmp on x86), it can end up causing miscompilation that has not
491   // been fully understood.
492   if (!Ret &&
493       (!TLI.getTargetMachine().Options.GuaranteedTailCallOpt ||
494        !isa<UnreachableInst>(Term)))
495     return false;
497   // If I will have a chain, make sure no other instruction that will have a
498   // chain interposes between I and the return.
499   if (I->mayHaveSideEffects() || I->mayReadFromMemory() ||
500       !isSafeToSpeculativelyExecute(I))
501     for (BasicBlock::const_iterator BBI = prior(prior(ExitBB->end())); ;
502          --BBI) {
503       if (&*BBI == I)
504         break;
505       // Debug info intrinsics do not get in the way of tail call optimization.
506       if (isa<DbgInfoIntrinsic>(BBI))
507         continue;
508       if (BBI->mayHaveSideEffects() || BBI->mayReadFromMemory() ||
509           !isSafeToSpeculativelyExecute(BBI))
510         return false;
511     }
513   return returnTypeIsEligibleForTailCall(ExitBB->getParent(), I, Ret, TLI);
516 bool llvm::returnTypeIsEligibleForTailCall(const Function *F,
517                                            const Instruction *I,
518                                            const ReturnInst *Ret,
519                                            const TargetLoweringBase &TLI) {
520   // If the block ends with a void return or unreachable, it doesn't matter
521   // what the call's return type is.
522   if (!Ret || Ret->getNumOperands() == 0) return true;
524   // If the return value is undef, it doesn't matter what the call's
525   // return type is.
526   if (isa<UndefValue>(Ret->getOperand(0))) return true;
528   // Make sure the attributes attached to each return are compatible.
529   AttrBuilder CallerAttrs(F->getAttributes(),
530                           AttributeSet::ReturnIndex);
531   AttrBuilder CalleeAttrs(cast<CallInst>(I)->getAttributes(),
532                           AttributeSet::ReturnIndex);
534   // Noalias is completely benign as far as calling convention goes, it
535   // shouldn't affect whether the call is a tail call.
536   CallerAttrs = CallerAttrs.removeAttribute(Attribute::NoAlias);
537   CalleeAttrs = CalleeAttrs.removeAttribute(Attribute::NoAlias);
539   bool AllowDifferingSizes = true;
540   if (CallerAttrs.contains(Attribute::ZExt)) {
541     if (!CalleeAttrs.contains(Attribute::ZExt))
542       return false;
544     AllowDifferingSizes = false;
545     CallerAttrs.removeAttribute(Attribute::ZExt);
546     CalleeAttrs.removeAttribute(Attribute::ZExt);
547   } else if (CallerAttrs.contains(Attribute::SExt)) {
548     if (!CalleeAttrs.contains(Attribute::SExt))
549       return false;
551     AllowDifferingSizes = false;
552     CallerAttrs.removeAttribute(Attribute::SExt);
553     CalleeAttrs.removeAttribute(Attribute::SExt);
554   }
556   // If they're still different, there's some facet we don't understand
557   // (currently only "inreg", but in future who knows). It may be OK but the
558   // only safe option is to reject the tail call.
559   if (CallerAttrs != CalleeAttrs)
560     return false;
562   const Value *RetVal = Ret->getOperand(0), *CallVal = I;
563   SmallVector<unsigned, 4> RetPath, CallPath;
564   SmallVector<CompositeType *, 4> RetSubTypes, CallSubTypes;
566   bool RetEmpty = !firstRealType(RetVal->getType(), RetSubTypes, RetPath);
567   bool CallEmpty = !firstRealType(CallVal->getType(), CallSubTypes, CallPath);
569   // Nothing's actually returned, it doesn't matter what the callee put there
570   // it's a valid tail call.
571   if (RetEmpty)
572     return true;
574   // Iterate pairwise through each of the value types making up the tail call
575   // and the corresponding return. For each one we want to know whether it's
576   // essentially going directly from the tail call to the ret, via operations
577   // that end up not generating any code.
578   //
579   // We allow a certain amount of covariance here. For example it's permitted
580   // for the tail call to define more bits than the ret actually cares about
581   // (e.g. via a truncate).
582   do {
583     if (CallEmpty) {
584       // We've exhausted the values produced by the tail call instruction, the
585       // rest are essentially undef. The type doesn't really matter, but we need
586       // *something*.
587       Type *SlotType = RetSubTypes.back()->getTypeAtIndex(RetPath.back());
588       CallVal = UndefValue::get(SlotType);
589     }
591     // The manipulations performed when we're looking through an insertvalue or
592     // an extractvalue would happen at the front of the RetPath list, so since
593     // we have to copy it anyway it's more efficient to create a reversed copy.
594     using std::copy;
595     SmallVector<unsigned, 4> TmpRetPath, TmpCallPath;
596     copy(RetPath.rbegin(), RetPath.rend(), std::back_inserter(TmpRetPath));
597     copy(CallPath.rbegin(), CallPath.rend(), std::back_inserter(TmpCallPath));
599     // Finally, we can check whether the value produced by the tail call at this
600     // index is compatible with the value we return.
601     if (!slotOnlyDiscardsData(RetVal, CallVal, TmpRetPath, TmpCallPath,
602                               AllowDifferingSizes, TLI))
603       return false;
605     CallEmpty  = !nextRealType(CallSubTypes, CallPath);
606   } while(nextRealType(RetSubTypes, RetPath));
608   return true;