Make DwarfExpression store the AsmPrinter instead of the TargetMachine.
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / AsmPrinterDwarf.cpp
1 //===-- AsmPrinterDwarf.cpp - AsmPrinter Dwarf Support --------------------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements the Dwarf emissions parts of AsmPrinter.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "ByteStreamer.h"
15 #include "DwarfExpression.h"
16 #include "llvm/CodeGen/AsmPrinter.h"
17 #include "llvm/ADT/Twine.h"
18 #include "llvm/IR/DataLayout.h"
19 #include "llvm/MC/MCAsmInfo.h"
20 #include "llvm/MC/MCSection.h"
21 #include "llvm/MC/MCStreamer.h"
22 #include "llvm/MC/MCSymbol.h"
23 #include "llvm/MC/MachineLocation.h"
24 #include "llvm/Support/Dwarf.h"
25 #include "llvm/Support/ErrorHandling.h"
26 #include "llvm/Target/TargetFrameLowering.h"
27 #include "llvm/Target/TargetLoweringObjectFile.h"
28 #include "llvm/Target/TargetMachine.h"
29 #include "llvm/Target/TargetRegisterInfo.h"
30 #include "llvm/Target/TargetSubtargetInfo.h"
31 using namespace llvm;
33 #define DEBUG_TYPE "asm-printer"
35 /// DwarfExpression implementation for .debug_loc entries.
36 class DebugLocDwarfExpression : public DwarfExpression {
37   ByteStreamer &BS;
39 public:
40   DebugLocDwarfExpression(const AsmPrinter &AP, ByteStreamer &BS)
41       : DwarfExpression(AP), BS(BS) {}
43   void EmitOp(uint8_t Op, const char *Comment) override;
44   void EmitSigned(int Value) override;
45   void EmitUnsigned(unsigned Value) override;
46   unsigned getFrameRegister() override { llvm_unreachable("not available"); };
47 };
49 void DebugLocDwarfExpression::EmitOp(uint8_t Op, const char *Comment) {
50   BS.EmitInt8(
51       Op, Comment ? Twine(Comment) + " " + dwarf::OperationEncodingString(Op)
52                   : dwarf::OperationEncodingString(Op));
53 }
54 void DebugLocDwarfExpression::EmitSigned(int Value) {
55   BS.EmitSLEB128(Value, Twine(Value));
56 }
57 void DebugLocDwarfExpression::EmitUnsigned(unsigned Value) {
58   BS.EmitULEB128(Value, Twine(Value));
59 }
61 //===----------------------------------------------------------------------===//
62 // Dwarf Emission Helper Routines
63 //===----------------------------------------------------------------------===//
65 /// EmitSLEB128 - emit the specified signed leb128 value.
66 void AsmPrinter::EmitSLEB128(int64_t Value, const char *Desc) const {
67   if (isVerbose() && Desc)
68     OutStreamer.AddComment(Desc);
70   OutStreamer.EmitSLEB128IntValue(Value);
71 }
73 /// EmitULEB128 - emit the specified signed leb128 value.
74 void AsmPrinter::EmitULEB128(uint64_t Value, const char *Desc,
75                              unsigned PadTo) const {
76   if (isVerbose() && Desc)
77     OutStreamer.AddComment(Desc);
79   OutStreamer.EmitULEB128IntValue(Value, PadTo);
80 }
82 /// EmitCFAByte - Emit a .byte 42 directive for a DW_CFA_xxx value.
83 void AsmPrinter::EmitCFAByte(unsigned Val) const {
84   if (isVerbose()) {
85     if (Val >= dwarf::DW_CFA_offset && Val < dwarf::DW_CFA_offset + 64)
86       OutStreamer.AddComment("DW_CFA_offset + Reg (" +
87                              Twine(Val - dwarf::DW_CFA_offset) + ")");
88     else
89       OutStreamer.AddComment(dwarf::CallFrameString(Val));
90   }
91   OutStreamer.EmitIntValue(Val, 1);
92 }
94 static const char *DecodeDWARFEncoding(unsigned Encoding) {
95   switch (Encoding) {
96   case dwarf::DW_EH_PE_absptr:
97     return "absptr";
98   case dwarf::DW_EH_PE_omit:
99     return "omit";
100   case dwarf::DW_EH_PE_pcrel:
101     return "pcrel";
102   case dwarf::DW_EH_PE_udata4:
103     return "udata4";
104   case dwarf::DW_EH_PE_udata8:
105     return "udata8";
106   case dwarf::DW_EH_PE_sdata4:
107     return "sdata4";
108   case dwarf::DW_EH_PE_sdata8:
109     return "sdata8";
110   case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata4:
111     return "pcrel udata4";
112   case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata4:
113     return "pcrel sdata4";
114   case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata8:
115     return "pcrel udata8";
116   case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata8:
117     return "pcrel sdata8";
118   case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata4
119       :
120     return "indirect pcrel udata4";
121   case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata4
122       :
123     return "indirect pcrel sdata4";
124   case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata8
125       :
126     return "indirect pcrel udata8";
127   case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata8
128       :
129     return "indirect pcrel sdata8";
130   }
132   return "<unknown encoding>";
135 /// EmitEncodingByte - Emit a .byte 42 directive that corresponds to an
136 /// encoding.  If verbose assembly output is enabled, we output comments
137 /// describing the encoding.  Desc is an optional string saying what the
138 /// encoding is specifying (e.g. "LSDA").
139 void AsmPrinter::EmitEncodingByte(unsigned Val, const char *Desc) const {
140   if (isVerbose()) {
141     if (Desc)
142       OutStreamer.AddComment(Twine(Desc) + " Encoding = " +
143                              Twine(DecodeDWARFEncoding(Val)));
144     else
145       OutStreamer.AddComment(Twine("Encoding = ") + DecodeDWARFEncoding(Val));
146   }
148   OutStreamer.EmitIntValue(Val, 1);
151 /// GetSizeOfEncodedValue - Return the size of the encoding in bytes.
152 unsigned AsmPrinter::GetSizeOfEncodedValue(unsigned Encoding) const {
153   if (Encoding == dwarf::DW_EH_PE_omit)
154     return 0;
156   switch (Encoding & 0x07) {
157   default:
158     llvm_unreachable("Invalid encoded value.");
159   case dwarf::DW_EH_PE_absptr:
160     return TM.getSubtargetImpl()->getDataLayout()->getPointerSize();
161   case dwarf::DW_EH_PE_udata2:
162     return 2;
163   case dwarf::DW_EH_PE_udata4:
164     return 4;
165   case dwarf::DW_EH_PE_udata8:
166     return 8;
167   }
170 void AsmPrinter::EmitTTypeReference(const GlobalValue *GV,
171                                     unsigned Encoding) const {
172   if (GV) {
173     const TargetLoweringObjectFile &TLOF = getObjFileLowering();
175     const MCExpr *Exp =
176         TLOF.getTTypeGlobalReference(GV, Encoding, *Mang, TM, MMI, OutStreamer);
177     OutStreamer.EmitValue(Exp, GetSizeOfEncodedValue(Encoding));
178   } else
179     OutStreamer.EmitIntValue(0, GetSizeOfEncodedValue(Encoding));
182 /// EmitSectionOffset - Emit the 4-byte offset of Label from the start of its
183 /// section.  This can be done with a special directive if the target supports
184 /// it (e.g. cygwin) or by emitting it as an offset from a label at the start
185 /// of the section.
186 ///
187 /// SectionLabel is a temporary label emitted at the start of the section that
188 /// Label lives in.
189 void AsmPrinter::EmitSectionOffset(const MCSymbol *Label,
190                                    const MCSymbol *SectionLabel) const {
191   // On COFF targets, we have to emit the special .secrel32 directive.
192   if (MAI->needsDwarfSectionOffsetDirective()) {
193     OutStreamer.EmitCOFFSecRel32(Label);
194     return;
195   }
197   // Get the section that we're referring to, based on SectionLabel.
198   const MCSection &Section = SectionLabel->getSection();
200   // If Label has already been emitted, verify that it is in the same section as
201   // section label for sanity.
202   assert((!Label->isInSection() || &Label->getSection() == &Section) &&
203          "Section offset using wrong section base for label");
205   // If the section in question will end up with an address of 0 anyway, we can
206   // just emit an absolute reference to save a relocation.
207   if (Section.isBaseAddressKnownZero()) {
208     OutStreamer.EmitSymbolValue(Label, 4);
209     return;
210   }
212   // Otherwise, emit it as a label difference from the start of the section.
213   EmitLabelDifference(Label, SectionLabel, 4);
216 // Some targets do not provide a DWARF register number for every
217 // register.  This function attempts to emit a DWARF register by
218 // emitting a piece of a super-register or by piecing together
219 // multiple subregisters that alias the register.
220 void AsmPrinter::EmitDwarfRegOpPiece(ByteStreamer &Streamer,
221                                      const MachineLocation &MLoc,
222                                      unsigned PieceSizeInBits,
223                                      unsigned PieceOffsetInBits) const {
224   assert(MLoc.isReg() && "MLoc must be a register");
225   DebugLocDwarfExpression Expr(*this, Streamer);
226   Expr.AddMachineRegPiece(MLoc.getReg(), PieceSizeInBits, PieceOffsetInBits);
229 void AsmPrinter::EmitDwarfOpPiece(ByteStreamer &Streamer,
230                                   unsigned PieceSizeInBits,
231                                   unsigned PieceOffsetInBits) const {
232   DebugLocDwarfExpression Expr(*this, Streamer);
233   Expr.AddOpPiece(PieceSizeInBits, PieceOffsetInBits);
236 /// EmitDwarfRegOp - Emit dwarf register operation.
237 void AsmPrinter::EmitDwarfRegOp(ByteStreamer &Streamer,
238                                 const MachineLocation &MLoc,
239                                 bool Indirect) const {
240   DebugLocDwarfExpression Expr(*this, Streamer);
241   const TargetRegisterInfo *TRI = TM.getSubtargetImpl()->getRegisterInfo();
242   int Reg = TRI->getDwarfRegNum(MLoc.getReg(), false);
243   if (Reg < 0) {
244     // We assume that pointers are always in an addressable register.
245     if (Indirect || MLoc.isIndirect())
246       // FIXME: We have no reasonable way of handling errors in here. The
247       // caller might be in the middle of a dwarf expression. We should
248       // probably assert that Reg >= 0 once debug info generation is more
249       // mature.
250       return Expr.EmitOp(dwarf::DW_OP_nop,
251                          "nop (could not find a dwarf register number)");
253     // Attempt to find a valid super- or sub-register.
254     return Expr.AddMachineRegPiece(MLoc.getReg());
255   }
257   if (MLoc.isIndirect())
258     Expr.AddRegIndirect(Reg, MLoc.getOffset(), Indirect);
259   else if (Indirect)
260     Expr.AddRegIndirect(Reg, 0, false);
261   else
262     Expr.AddReg(Reg);
265 //===----------------------------------------------------------------------===//
266 // Dwarf Lowering Routines
267 //===----------------------------------------------------------------------===//
269 void AsmPrinter::emitCFIInstruction(const MCCFIInstruction &Inst) const {
270   switch (Inst.getOperation()) {
271   default:
272     llvm_unreachable("Unexpected instruction");
273   case MCCFIInstruction::OpDefCfaOffset:
274     OutStreamer.EmitCFIDefCfaOffset(Inst.getOffset());
275     break;
276   case MCCFIInstruction::OpDefCfa:
277     OutStreamer.EmitCFIDefCfa(Inst.getRegister(), Inst.getOffset());
278     break;
279   case MCCFIInstruction::OpDefCfaRegister:
280     OutStreamer.EmitCFIDefCfaRegister(Inst.getRegister());
281     break;
282   case MCCFIInstruction::OpOffset:
283     OutStreamer.EmitCFIOffset(Inst.getRegister(), Inst.getOffset());
284     break;
285   case MCCFIInstruction::OpRegister:
286     OutStreamer.EmitCFIRegister(Inst.getRegister(), Inst.getRegister2());
287     break;
288   case MCCFIInstruction::OpWindowSave:
289     OutStreamer.EmitCFIWindowSave();
290     break;
291   case MCCFIInstruction::OpSameValue:
292     OutStreamer.EmitCFISameValue(Inst.getRegister());
293     break;
294   }