1 //===-- AsmPrinterDwarf.cpp - AsmPrinter Dwarf Support --------------------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements the Dwarf emissions parts of AsmPrinter.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "ByteStreamer.h"
15 #include "DwarfExpression.h"
16 #include "llvm/CodeGen/AsmPrinter.h"
17 #include "llvm/ADT/Twine.h"
18 #include "llvm/IR/DataLayout.h"
19 #include "llvm/MC/MCAsmInfo.h"
20 #include "llvm/MC/MCSection.h"
21 #include "llvm/MC/MCStreamer.h"
22 #include "llvm/MC/MCSymbol.h"
23 #include "llvm/MC/MachineLocation.h"
24 #include "llvm/Support/Dwarf.h"
25 #include "llvm/Support/ErrorHandling.h"
26 #include "llvm/Target/TargetFrameLowering.h"
27 #include "llvm/Target/TargetLoweringObjectFile.h"
28 #include "llvm/Target/TargetMachine.h"
29 #include "llvm/Target/TargetRegisterInfo.h"
30 #include "llvm/Target/TargetSubtargetInfo.h"
31 using namespace llvm;
33 #define DEBUG_TYPE "asm-printer"
35 void DebugLocDwarfExpression::EmitOp(uint8_t Op, const char *Comment) {
36 BS.EmitInt8(
37 Op, Comment ? Twine(Comment) + " " + dwarf::OperationEncodingString(Op)
38 : dwarf::OperationEncodingString(Op));
39 }
41 void DebugLocDwarfExpression::EmitSigned(int Value) {
42 BS.EmitSLEB128(Value, Twine(Value));
43 }
45 void DebugLocDwarfExpression::EmitUnsigned(unsigned Value) {
46 BS.EmitULEB128(Value, Twine(Value));
47 }
49 bool DebugLocDwarfExpression::isFrameRegister(unsigned MachineReg) {
50 // This information is not available while emitting .debug_loc entries.
51 return false;
52 }
54 //===----------------------------------------------------------------------===//
55 // Dwarf Emission Helper Routines
56 //===----------------------------------------------------------------------===//
58 /// EmitSLEB128 - emit the specified signed leb128 value.
59 void AsmPrinter::EmitSLEB128(int64_t Value, const char *Desc) const {
60 if (isVerbose() && Desc)
61 OutStreamer.AddComment(Desc);
63 OutStreamer.EmitSLEB128IntValue(Value);
64 }
66 /// EmitULEB128 - emit the specified signed leb128 value.
67 void AsmPrinter::EmitULEB128(uint64_t Value, const char *Desc,
68 unsigned PadTo) const {
69 if (isVerbose() && Desc)
70 OutStreamer.AddComment(Desc);
72 OutStreamer.EmitULEB128IntValue(Value, PadTo);
73 }
75 /// EmitCFAByte - Emit a .byte 42 directive for a DW_CFA_xxx value.
76 void AsmPrinter::EmitCFAByte(unsigned Val) const {
77 if (isVerbose()) {
78 if (Val >= dwarf::DW_CFA_offset && Val < dwarf::DW_CFA_offset + 64)
79 OutStreamer.AddComment("DW_CFA_offset + Reg (" +
80 Twine(Val - dwarf::DW_CFA_offset) + ")");
81 else
82 OutStreamer.AddComment(dwarf::CallFrameString(Val));
83 }
84 OutStreamer.EmitIntValue(Val, 1);
85 }
87 static const char *DecodeDWARFEncoding(unsigned Encoding) {
88 switch (Encoding) {
89 case dwarf::DW_EH_PE_absptr:
90 return "absptr";
91 case dwarf::DW_EH_PE_omit:
92 return "omit";
93 case dwarf::DW_EH_PE_pcrel:
94 return "pcrel";
95 case dwarf::DW_EH_PE_udata4:
96 return "udata4";
97 case dwarf::DW_EH_PE_udata8:
98 return "udata8";
99 case dwarf::DW_EH_PE_sdata4:
100 return "sdata4";
101 case dwarf::DW_EH_PE_sdata8:
102 return "sdata8";
103 case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata4:
104 return "pcrel udata4";
105 case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata4:
106 return "pcrel sdata4";
107 case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata8:
108 return "pcrel udata8";
109 case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata8:
110 return "pcrel sdata8";
111 case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata4
112 :
113 return "indirect pcrel udata4";
114 case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata4
115 :
116 return "indirect pcrel sdata4";
117 case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata8
118 :
119 return "indirect pcrel udata8";
120 case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata8
121 :
122 return "indirect pcrel sdata8";
123 }
125 return "<unknown encoding>";
126 }
128 /// EmitEncodingByte - Emit a .byte 42 directive that corresponds to an
129 /// encoding. If verbose assembly output is enabled, we output comments
130 /// describing the encoding. Desc is an optional string saying what the
131 /// encoding is specifying (e.g. "LSDA").
132 void AsmPrinter::EmitEncodingByte(unsigned Val, const char *Desc) const {
133 if (isVerbose()) {
134 if (Desc)
135 OutStreamer.AddComment(Twine(Desc) + " Encoding = " +
136 Twine(DecodeDWARFEncoding(Val)));
137 else
138 OutStreamer.AddComment(Twine("Encoding = ") + DecodeDWARFEncoding(Val));
139 }
141 OutStreamer.EmitIntValue(Val, 1);
142 }
144 /// GetSizeOfEncodedValue - Return the size of the encoding in bytes.
145 unsigned AsmPrinter::GetSizeOfEncodedValue(unsigned Encoding) const {
146 if (Encoding == dwarf::DW_EH_PE_omit)
147 return 0;
149 switch (Encoding & 0x07) {
150 default:
151 llvm_unreachable("Invalid encoded value.");
152 case dwarf::DW_EH_PE_absptr:
153 return TM.getSubtargetImpl()->getDataLayout()->getPointerSize();
154 case dwarf::DW_EH_PE_udata2:
155 return 2;
156 case dwarf::DW_EH_PE_udata4:
157 return 4;
158 case dwarf::DW_EH_PE_udata8:
159 return 8;
160 }
161 }
163 void AsmPrinter::EmitTTypeReference(const GlobalValue *GV,
164 unsigned Encoding) const {
165 if (GV) {
166 const TargetLoweringObjectFile &TLOF = getObjFileLowering();
168 const MCExpr *Exp =
169 TLOF.getTTypeGlobalReference(GV, Encoding, *Mang, TM, MMI, OutStreamer);
170 OutStreamer.EmitValue(Exp, GetSizeOfEncodedValue(Encoding));
171 } else
172 OutStreamer.EmitIntValue(0, GetSizeOfEncodedValue(Encoding));
173 }
175 /// EmitSectionOffset - Emit the 4-byte offset of Label from the start of its
176 /// section. This can be done with a special directive if the target supports
177 /// it (e.g. cygwin) or by emitting it as an offset from a label at the start
178 /// of the section.
179 ///
180 /// SectionLabel is a temporary label emitted at the start of the section that
181 /// Label lives in.
182 void AsmPrinter::EmitSectionOffset(const MCSymbol *Label,
183 const MCSymbol *SectionLabel) const {
184 // On COFF targets, we have to emit the special .secrel32 directive.
185 if (MAI->needsDwarfSectionOffsetDirective()) {
186 OutStreamer.EmitCOFFSecRel32(Label);
187 return;
188 }
190 // Get the section that we're referring to, based on SectionLabel.
191 const MCSection &Section = SectionLabel->getSection();
193 // If Label has already been emitted, verify that it is in the same section as
194 // section label for sanity.
195 assert((!Label->isInSection() || &Label->getSection() == &Section) &&
196 "Section offset using wrong section base for label");
198 // If the section in question will end up with an address of 0 anyway, we can
199 // just emit an absolute reference to save a relocation.
200 if (Section.isBaseAddressKnownZero()) {
201 OutStreamer.EmitSymbolValue(Label, 4);
202 return;
203 }
205 // Otherwise, emit it as a label difference from the start of the section.
206 EmitLabelDifference(Label, SectionLabel, 4);
207 }
209 // Some targets do not provide a DWARF register number for every
210 // register. This function attempts to emit a DWARF register by
211 // emitting a piece of a super-register or by piecing together
212 // multiple subregisters that alias the register.
213 void AsmPrinter::EmitDwarfRegOpPiece(ByteStreamer &Streamer,
214 const MachineLocation &MLoc,
215 unsigned PieceSizeInBits,
216 unsigned PieceOffsetInBits) const {
217 assert(MLoc.isReg() && "MLoc must be a register");
218 DebugLocDwarfExpression Expr(*this, Streamer);
219 Expr.AddMachineRegPiece(MLoc.getReg(), PieceSizeInBits, PieceOffsetInBits);
220 }
222 void AsmPrinter::EmitDwarfOpPiece(ByteStreamer &Streamer,
223 unsigned PieceSizeInBits,
224 unsigned PieceOffsetInBits) const {
225 DebugLocDwarfExpression Expr(*this, Streamer);
226 Expr.AddOpPiece(PieceSizeInBits, PieceOffsetInBits);
227 }
229 /// EmitDwarfRegOp - Emit dwarf register operation.
230 void AsmPrinter::EmitDwarfRegOp(ByteStreamer &Streamer,
231 const MachineLocation &MLoc,
232 bool Indirect) const {
233 DebugLocDwarfExpression Expr(*this, Streamer);
234 const TargetRegisterInfo *TRI = TM.getSubtargetImpl()->getRegisterInfo();
235 int Reg = TRI->getDwarfRegNum(MLoc.getReg(), false);
236 if (Reg < 0) {
237 // We assume that pointers are always in an addressable register.
238 if (Indirect || MLoc.isIndirect())
239 // FIXME: We have no reasonable way of handling errors in here. The
240 // caller might be in the middle of a dwarf expression. We should
241 // probably assert that Reg >= 0 once debug info generation is more
242 // mature.
243 return Expr.EmitOp(dwarf::DW_OP_nop,
244 "nop (could not find a dwarf register number)");
246 // Attempt to find a valid super- or sub-register.
247 if (!Expr.AddMachineRegPiece(MLoc.getReg()))
248 Expr.EmitOp(dwarf::DW_OP_nop,
249 "nop (could not find a dwarf register number)");
250 return;
251 }
253 if (MLoc.isIndirect())
254 Expr.AddRegIndirect(Reg, MLoc.getOffset(), Indirect);
255 else if (Indirect)
256 Expr.AddRegIndirect(Reg, 0, false);
257 else
258 Expr.AddReg(Reg);
259 }
261 //===----------------------------------------------------------------------===//
262 // Dwarf Lowering Routines
263 //===----------------------------------------------------------------------===//
265 void AsmPrinter::emitCFIInstruction(const MCCFIInstruction &Inst) const {
266 switch (Inst.getOperation()) {
267 default:
268 llvm_unreachable("Unexpected instruction");
269 case MCCFIInstruction::OpDefCfaOffset:
270 OutStreamer.EmitCFIDefCfaOffset(Inst.getOffset());
271 break;
272 case MCCFIInstruction::OpDefCfa:
273 OutStreamer.EmitCFIDefCfa(Inst.getRegister(), Inst.getOffset());
274 break;
275 case MCCFIInstruction::OpDefCfaRegister:
276 OutStreamer.EmitCFIDefCfaRegister(Inst.getRegister());
277 break;
278 case MCCFIInstruction::OpOffset:
279 OutStreamer.EmitCFIOffset(Inst.getRegister(), Inst.getOffset());
280 break;
281 case MCCFIInstruction::OpRegister:
282 OutStreamer.EmitCFIRegister(Inst.getRegister(), Inst.getRegister2());
283 break;
284 case MCCFIInstruction::OpWindowSave:
285 OutStreamer.EmitCFIWindowSave();
286 break;
287 case MCCFIInstruction::OpSameValue:
288 OutStreamer.EmitCFISameValue(Inst.getRegister());
289 break;
290 }
291 }