1 //===-- llvm/CodeGen/DIEHash.cpp - Dwarf Hashing Framework ----------------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for DWARF4 hashing of DIEs.
11 //
12 //===----------------------------------------------------------------------===//
14 #define DEBUG_TYPE "dwarfdebug"
16 #include "DIEHash.h"
18 #include "DIE.h"
19 #include "llvm/ADT/ArrayRef.h"
20 #include "llvm/ADT/StringRef.h"
21 #include "llvm/Support/Debug.h"
22 #include "llvm/Support/Dwarf.h"
23 #include "llvm/Support/Endian.h"
24 #include "llvm/Support/MD5.h"
25 #include "llvm/Support/raw_ostream.h"
27 using namespace llvm;
29 /// \brief Grabs the string in whichever attribute is passed in and returns
30 /// a reference to it.
31 static StringRef getDIEStringAttr(const DIE &Die, uint16_t Attr) {
32 const SmallVectorImpl<DIEValue *> &Values = Die.getValues();
33 const DIEAbbrev &Abbrevs = Die.getAbbrev();
35 // Iterate through all the attributes until we find the one we're
36 // looking for, if we can't find it return an empty string.
37 for (size_t i = 0; i < Values.size(); ++i) {
38 if (Abbrevs.getData()[i].getAttribute() == Attr) {
39 DIEValue *V = Values[i];
40 assert(isa<DIEString>(V) && "String requested. Not a string.");
41 DIEString *S = cast<DIEString>(V);
42 return S->getString();
43 }
44 }
45 return StringRef("");
46 }
48 /// \brief Adds the string in \p Str to the hash. This also hashes
49 /// a trailing NULL with the string.
50 void DIEHash::addString(StringRef Str) {
51 DEBUG(dbgs() << "Adding string " << Str << " to hash.\n");
52 Hash.update(Str);
53 Hash.update(makeArrayRef((uint8_t)'\0'));
54 }
56 // FIXME: The LEB128 routines are copied and only slightly modified out of
57 // LEB128.h.
59 /// \brief Adds the unsigned in \p Value to the hash encoded as a ULEB128.
60 void DIEHash::addULEB128(uint64_t Value) {
61 DEBUG(dbgs() << "Adding ULEB128 " << Value << " to hash.\n");
62 do {
63 uint8_t Byte = Value & 0x7f;
64 Value >>= 7;
65 if (Value != 0)
66 Byte |= 0x80; // Mark this byte to show that more bytes will follow.
67 Hash.update(Byte);
68 } while (Value != 0);
69 }
71 void DIEHash::addSLEB128(int64_t Value) {
72 DEBUG(dbgs() << "Adding ULEB128 " << Value << " to hash.\n");
73 bool More;
74 do {
75 uint8_t Byte = Value & 0x7f;
76 Value >>= 7;
77 More = !((((Value == 0 ) && ((Byte & 0x40) == 0)) ||
78 ((Value == -1) && ((Byte & 0x40) != 0))));
79 if (More)
80 Byte |= 0x80; // Mark this byte to show that more bytes will follow.
81 Hash.update(Byte);
82 } while (More);
83 }
85 /// \brief Including \p Parent adds the context of Parent to the hash..
86 void DIEHash::addParentContext(const DIE &Parent) {
88 DEBUG(dbgs() << "Adding parent context to hash...\n");
90 // [7.27.2] For each surrounding type or namespace beginning with the
91 // outermost such construct...
92 SmallVector<const DIE *, 1> Parents;
93 const DIE *Cur = &Parent;
94 while (Cur->getParent()) {
95 Parents.push_back(Cur);
96 Cur = Cur->getParent();
97 }
98 assert(Cur->getTag() == dwarf::DW_TAG_compile_unit ||
99 Cur->getTag() == dwarf::DW_TAG_type_unit);
101 // Reverse iterate over our list to go from the outermost construct to the
102 // innermost.
103 for (SmallVectorImpl<const DIE *>::reverse_iterator I = Parents.rbegin(),
104 E = Parents.rend();
105 I != E; ++I) {
106 const DIE &Die = **I;
108 // ... Append the letter "C" to the sequence...
109 addULEB128('C');
111 // ... Followed by the DWARF tag of the construct...
112 addULEB128(Die.getTag());
114 // ... Then the name, taken from the DW_AT_name attribute.
115 StringRef Name = getDIEStringAttr(Die, dwarf::DW_AT_name);
116 DEBUG(dbgs() << "... adding context: " << Name << "\n");
117 if (!Name.empty())
118 addString(Name);
119 }
120 }
122 // Collect all of the attributes for a particular DIE in single structure.
123 void DIEHash::collectAttributes(const DIE &Die, DIEAttrs &Attrs) {
124 const SmallVectorImpl<DIEValue *> &Values = Die.getValues();
125 const DIEAbbrev &Abbrevs = Die.getAbbrev();
127 #define COLLECT_ATTR(NAME) \
128 case dwarf::NAME: \
129 Attrs.NAME.Val = Values[i]; \
130 Attrs.NAME.Desc = &Abbrevs.getData()[i]; \
131 break
133 for (size_t i = 0, e = Values.size(); i != e; ++i) {
134 DEBUG(dbgs() << "Attribute: "
135 << dwarf::AttributeString(Abbrevs.getData()[i].getAttribute())
136 << " added.\n");
137 switch (Abbrevs.getData()[i].getAttribute()) {
138 COLLECT_ATTR(DW_AT_name);
139 COLLECT_ATTR(DW_AT_accessibility);
140 COLLECT_ATTR(DW_AT_address_class);
141 COLLECT_ATTR(DW_AT_allocated);
142 COLLECT_ATTR(DW_AT_artificial);
143 COLLECT_ATTR(DW_AT_associated);
144 COLLECT_ATTR(DW_AT_binary_scale);
145 COLLECT_ATTR(DW_AT_bit_offset);
146 COLLECT_ATTR(DW_AT_bit_size);
147 COLLECT_ATTR(DW_AT_bit_stride);
148 COLLECT_ATTR(DW_AT_byte_size);
149 COLLECT_ATTR(DW_AT_byte_stride);
150 COLLECT_ATTR(DW_AT_const_expr);
151 COLLECT_ATTR(DW_AT_const_value);
152 COLLECT_ATTR(DW_AT_containing_type);
153 COLLECT_ATTR(DW_AT_count);
154 COLLECT_ATTR(DW_AT_data_bit_offset);
155 COLLECT_ATTR(DW_AT_data_location);
156 COLLECT_ATTR(DW_AT_data_member_location);
157 COLLECT_ATTR(DW_AT_decimal_scale);
158 COLLECT_ATTR(DW_AT_decimal_sign);
159 COLLECT_ATTR(DW_AT_default_value);
160 COLLECT_ATTR(DW_AT_digit_count);
161 COLLECT_ATTR(DW_AT_discr);
162 COLLECT_ATTR(DW_AT_discr_list);
163 COLLECT_ATTR(DW_AT_discr_value);
164 COLLECT_ATTR(DW_AT_encoding);
165 COLLECT_ATTR(DW_AT_enum_class);
166 COLLECT_ATTR(DW_AT_endianity);
167 COLLECT_ATTR(DW_AT_explicit);
168 COLLECT_ATTR(DW_AT_is_optional);
169 COLLECT_ATTR(DW_AT_location);
170 COLLECT_ATTR(DW_AT_lower_bound);
171 COLLECT_ATTR(DW_AT_mutable);
172 COLLECT_ATTR(DW_AT_ordering);
173 COLLECT_ATTR(DW_AT_picture_string);
174 COLLECT_ATTR(DW_AT_prototyped);
175 COLLECT_ATTR(DW_AT_small);
176 COLLECT_ATTR(DW_AT_segment);
177 COLLECT_ATTR(DW_AT_string_length);
178 COLLECT_ATTR(DW_AT_threads_scaled);
179 COLLECT_ATTR(DW_AT_upper_bound);
180 COLLECT_ATTR(DW_AT_use_location);
181 COLLECT_ATTR(DW_AT_use_UTF8);
182 COLLECT_ATTR(DW_AT_variable_parameter);
183 COLLECT_ATTR(DW_AT_virtuality);
184 COLLECT_ATTR(DW_AT_visibility);
185 COLLECT_ATTR(DW_AT_vtable_elem_location);
186 COLLECT_ATTR(DW_AT_type);
187 default:
188 break;
189 }
190 }
191 }
193 void DIEHash::hashShallowTypeReference(dwarf::Attribute Attribute,
194 const DIE &Entry, StringRef Name) {
195 // append the letter 'N'
196 addULEB128('N');
198 // the DWARF attribute code (DW_AT_type or DW_AT_friend),
199 addULEB128(Attribute);
201 // the context of the tag,
202 if (const DIE *Parent = Entry.getParent())
203 addParentContext(*Parent);
205 // the letter 'E',
206 addULEB128('E');
208 // and the name of the type.
209 addString(Name);
211 // Currently DW_TAG_friends are not used by Clang, but if they do become so,
212 // here's the relevant spec text to implement:
213 //
214 // For DW_TAG_friend, if the referenced entry is the DW_TAG_subprogram,
215 // the context is omitted and the name to be used is the ABI-specific name
216 // of the subprogram (e.g., the mangled linker name).
217 }
219 void DIEHash::hashRepeatedTypeReference(dwarf::Attribute Attribute,
220 unsigned DieNumber) {
221 // a) If T is in the list of [previously hashed types], use the letter
222 // 'R' as the marker
223 addULEB128('R');
225 addULEB128(Attribute);
227 // and use the unsigned LEB128 encoding of [the index of T in the
228 // list] as the attribute value;
229 addULEB128(DieNumber);
230 }
232 void DIEHash::hashDIEEntry(dwarf::Attribute Attribute, dwarf::Tag Tag,
233 const DIE &Entry) {
234 assert(Tag != dwarf::DW_TAG_friend && "No current LLVM clients emit friend "
235 "tags. Add support here when there's "
236 "a use case");
237 // Step 5
238 // If the tag in Step 3 is one of [the below tags]
239 if ((Tag == dwarf::DW_TAG_pointer_type ||
240 Tag == dwarf::DW_TAG_reference_type ||
241 Tag == dwarf::DW_TAG_rvalue_reference_type ||
242 Tag == dwarf::DW_TAG_ptr_to_member_type) &&
243 // and the referenced type (via the [below attributes])
244 // FIXME: This seems overly restrictive, and causes hash mismatches
245 // there's a decl/def difference in the containing type of a
246 // ptr_to_member_type, but it's what DWARF says, for some reason.
247 Attribute == dwarf::DW_AT_type) {
248 // ... has a DW_AT_name attribute,
249 StringRef Name = getDIEStringAttr(Entry, dwarf::DW_AT_name);
250 if (!Name.empty()) {
251 hashShallowTypeReference(Attribute, Entry, Name);
252 return;
253 }
254 }
256 unsigned &DieNumber = Numbering[&Entry];
257 if (DieNumber) {
258 hashRepeatedTypeReference(Attribute, DieNumber);
259 return;
260 }
262 // otherwise, b) use the letter 'T' as a the marker, ...
263 addULEB128('T');
265 addULEB128(Attribute);
267 // ... process the type T recursively by performing Steps 2 through 7, and
268 // use the result as the attribute value.
269 DieNumber = Numbering.size();
270 computeHash(Entry);
271 }
273 // Hash an individual attribute \param Attr based on the type of attribute and
274 // the form.
275 void DIEHash::hashAttribute(AttrEntry Attr, dwarf::Tag Tag) {
276 const DIEValue *Value = Attr.Val;
277 const DIEAbbrevData *Desc = Attr.Desc;
278 dwarf::Attribute Attribute = Desc->getAttribute();
280 // 7.27 Step 3
281 // ... An attribute that refers to another type entry T is processed as
282 // follows:
283 if (const DIEEntry *EntryAttr = dyn_cast<DIEEntry>(Value)) {
284 hashDIEEntry(Attribute, Tag, *EntryAttr->getEntry());
285 return;
286 }
288 // Other attribute values use the letter 'A' as the marker, ...
289 addULEB128('A');
291 addULEB128(Attribute);
293 // ... and the value consists of the form code (encoded as an unsigned LEB128
294 // value) followed by the encoding of the value according to the form code. To
295 // ensure reproducibility of the signature, the set of forms used in the
296 // signature computation is limited to the following: DW_FORM_sdata,
297 // DW_FORM_flag, DW_FORM_string, and DW_FORM_block.
298 switch (Desc->getForm()) {
299 case dwarf::DW_FORM_string:
300 llvm_unreachable(
301 "Add support for DW_FORM_string if we ever start emitting them again");
302 case dwarf::DW_FORM_GNU_str_index:
303 case dwarf::DW_FORM_strp:
304 addULEB128(dwarf::DW_FORM_string);
305 addString(cast<DIEString>(Value)->getString());
306 break;
307 case dwarf::DW_FORM_data1:
308 case dwarf::DW_FORM_data2:
309 case dwarf::DW_FORM_data4:
310 case dwarf::DW_FORM_data8:
311 case dwarf::DW_FORM_udata:
312 addULEB128(dwarf::DW_FORM_sdata);
313 addSLEB128((int64_t)cast<DIEInteger>(Value)->getValue());
314 break;
315 default:
316 llvm_unreachable("Add support for additional forms");
317 }
318 }
320 // Go through the attributes from \param Attrs in the order specified in 7.27.4
321 // and hash them.
322 void DIEHash::hashAttributes(const DIEAttrs &Attrs, dwarf::Tag Tag) {
323 #define ADD_ATTR(ATTR) \
324 { \
325 if (ATTR.Val != 0) \
326 hashAttribute(ATTR, Tag); \
327 }
329 ADD_ATTR(Attrs.DW_AT_name);
330 ADD_ATTR(Attrs.DW_AT_accessibility);
331 ADD_ATTR(Attrs.DW_AT_address_class);
332 ADD_ATTR(Attrs.DW_AT_allocated);
333 ADD_ATTR(Attrs.DW_AT_artificial);
334 ADD_ATTR(Attrs.DW_AT_associated);
335 ADD_ATTR(Attrs.DW_AT_binary_scale);
336 ADD_ATTR(Attrs.DW_AT_bit_offset);
337 ADD_ATTR(Attrs.DW_AT_bit_size);
338 ADD_ATTR(Attrs.DW_AT_bit_stride);
339 ADD_ATTR(Attrs.DW_AT_byte_size);
340 ADD_ATTR(Attrs.DW_AT_byte_stride);
341 ADD_ATTR(Attrs.DW_AT_const_expr);
342 ADD_ATTR(Attrs.DW_AT_const_value);
343 ADD_ATTR(Attrs.DW_AT_containing_type);
344 ADD_ATTR(Attrs.DW_AT_count);
345 ADD_ATTR(Attrs.DW_AT_data_bit_offset);
346 ADD_ATTR(Attrs.DW_AT_data_location);
347 ADD_ATTR(Attrs.DW_AT_data_member_location);
348 ADD_ATTR(Attrs.DW_AT_decimal_scale);
349 ADD_ATTR(Attrs.DW_AT_decimal_sign);
350 ADD_ATTR(Attrs.DW_AT_default_value);
351 ADD_ATTR(Attrs.DW_AT_digit_count);
352 ADD_ATTR(Attrs.DW_AT_discr);
353 ADD_ATTR(Attrs.DW_AT_discr_list);
354 ADD_ATTR(Attrs.DW_AT_discr_value);
355 ADD_ATTR(Attrs.DW_AT_encoding);
356 ADD_ATTR(Attrs.DW_AT_enum_class);
357 ADD_ATTR(Attrs.DW_AT_endianity);
358 ADD_ATTR(Attrs.DW_AT_explicit);
359 ADD_ATTR(Attrs.DW_AT_is_optional);
360 ADD_ATTR(Attrs.DW_AT_location);
361 ADD_ATTR(Attrs.DW_AT_lower_bound);
362 ADD_ATTR(Attrs.DW_AT_mutable);
363 ADD_ATTR(Attrs.DW_AT_ordering);
364 ADD_ATTR(Attrs.DW_AT_picture_string);
365 ADD_ATTR(Attrs.DW_AT_prototyped);
366 ADD_ATTR(Attrs.DW_AT_small);
367 ADD_ATTR(Attrs.DW_AT_segment);
368 ADD_ATTR(Attrs.DW_AT_string_length);
369 ADD_ATTR(Attrs.DW_AT_threads_scaled);
370 ADD_ATTR(Attrs.DW_AT_upper_bound);
371 ADD_ATTR(Attrs.DW_AT_use_location);
372 ADD_ATTR(Attrs.DW_AT_use_UTF8);
373 ADD_ATTR(Attrs.DW_AT_variable_parameter);
374 ADD_ATTR(Attrs.DW_AT_virtuality);
375 ADD_ATTR(Attrs.DW_AT_visibility);
376 ADD_ATTR(Attrs.DW_AT_vtable_elem_location);
377 ADD_ATTR(Attrs.DW_AT_type);
379 // FIXME: Add the extended attributes.
380 }
382 // Add all of the attributes for \param Die to the hash.
383 void DIEHash::addAttributes(const DIE &Die) {
384 DIEAttrs Attrs = {};
385 collectAttributes(Die, Attrs);
386 hashAttributes(Attrs, Die.getTag());
387 }
389 void DIEHash::hashNestedType(const DIE &Die, StringRef Name) {
390 // 7.27 Step 7
391 // ... append the letter 'S',
392 addULEB128('S');
394 // the tag of C,
395 addULEB128(Die.getTag());
397 // and the name.
398 addString(Name);
399 }
401 // Compute the hash of a DIE. This is based on the type signature computation
402 // given in section 7.27 of the DWARF4 standard. It is the md5 hash of a
403 // flattened description of the DIE.
404 void DIEHash::computeHash(const DIE &Die) {
405 // Append the letter 'D', followed by the DWARF tag of the DIE.
406 addULEB128('D');
407 addULEB128(Die.getTag());
409 // Add each of the attributes of the DIE.
410 addAttributes(Die);
412 // Then hash each of the children of the DIE.
413 for (std::vector<DIE *>::const_iterator I = Die.getChildren().begin(),
414 E = Die.getChildren().end();
415 I != E; ++I) {
416 // 7.27 Step 7
417 // If C is a nested type entry or a member function entry, ...
418 if (isType((*I)->getTag()) || (*I)->getTag() == dwarf::DW_TAG_subprogram) {
419 StringRef Name = getDIEStringAttr(**I, dwarf::DW_AT_name);
420 // ... and has a DW_AT_name attribute
421 if (!Name.empty()) {
422 hashNestedType(**I, Name);
423 continue;
424 }
425 }
426 computeHash(**I);
427 }
429 // Following the last (or if there are no children), append a zero byte.
430 Hash.update(makeArrayRef((uint8_t)'\0'));
431 }
433 /// This is based on the type signature computation given in section 7.27 of the
434 /// DWARF4 standard. It is the md5 hash of a flattened description of the DIE
435 /// with the exception that we are hashing only the context and the name of the
436 /// type.
437 uint64_t DIEHash::computeDIEODRSignature(const DIE &Die) {
439 // Add the contexts to the hash. We won't be computing the ODR hash for
440 // function local types so it's safe to use the generic context hashing
441 // algorithm here.
442 // FIXME: If we figure out how to account for linkage in some way we could
443 // actually do this with a slight modification to the parent hash algorithm.
444 if (const DIE *Parent = Die.getParent())
445 addParentContext(*Parent);
447 // Add the current DIE information.
449 // Add the DWARF tag of the DIE.
450 addULEB128(Die.getTag());
452 // Add the name of the type to the hash.
453 addString(getDIEStringAttr(Die, dwarf::DW_AT_name));
455 // Now get the result.
456 MD5::MD5Result Result;
457 Hash.final(Result);
459 // ... take the least significant 8 bytes and return those. Our MD5
460 // implementation always returns its results in little endian, swap bytes
461 // appropriately.
462 return *reinterpret_cast<support::ulittle64_t *>(Result + 8);
463 }
465 /// This is based on the type signature computation given in section 7.27 of the
466 /// DWARF4 standard. It is an md5 hash of the flattened description of the DIE
467 /// with the inclusion of the full CU and all top level CU entities.
468 // TODO: Initialize the type chain at 0 instead of 1 for CU signatures.
469 uint64_t DIEHash::computeCUSignature(const DIE &Die) {
470 Numbering.clear();
471 Numbering[&Die] = 1;
473 // Hash the DIE.
474 computeHash(Die);
476 // Now return the result.
477 MD5::MD5Result Result;
478 Hash.final(Result);
480 // ... take the least significant 8 bytes and return those. Our MD5
481 // implementation always returns its results in little endian, swap bytes
482 // appropriately.
483 return *reinterpret_cast<support::ulittle64_t *>(Result + 8);
484 }
486 /// This is based on the type signature computation given in section 7.27 of the
487 /// DWARF4 standard. It is an md5 hash of the flattened description of the DIE
488 /// with the inclusion of additional forms not specifically called out in the
489 /// standard.
490 uint64_t DIEHash::computeTypeSignature(const DIE &Die) {
491 Numbering.clear();
492 Numbering[&Die] = 1;
494 if (const DIE *Parent = Die.getParent())
495 addParentContext(*Parent);
497 // Hash the DIE.
498 computeHash(Die);
500 // Now return the result.
501 MD5::MD5Result Result;
502 Hash.final(Result);
504 // ... take the least significant 8 bytes and return those. Our MD5
505 // implementation always returns its results in little endian, swap bytes
506 // appropriately.
507 return *reinterpret_cast<support::ulittle64_t *>(Result + 8);
508 }