Debug info: Infrastructure to support debug locations for fragmented
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DbgValueHistoryCalculator.cpp
1 //===-- llvm/CodeGen/AsmPrinter/DbgValueHistoryCalculator.cpp -------------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
10 #include "DbgValueHistoryCalculator.h"
11 #include "llvm/ADT/SmallVector.h"
12 #include "llvm/CodeGen/MachineBasicBlock.h"
13 #include "llvm/CodeGen/MachineFunction.h"
14 #include "llvm/IR/DebugInfo.h"
15 #include "llvm/Support/Debug.h"
16 #include "llvm/Target/TargetRegisterInfo.h"
17 #include <algorithm>
18 #include <map>
19 #include <set>
21 #define DEBUG_TYPE "dwarfdebug"
23 namespace llvm {
25 // \brief If @MI is a DBG_VALUE with debug value described by a
26 // defined register, returns the number of this register.
27 // In the other case, returns 0.
28 static unsigned isDescribedByReg(const MachineInstr &MI) {
29   assert(MI.isDebugValue());
30   assert(MI.getNumOperands() == 3);
31   // If location of variable is described using a register (directly or
32   // indirecltly), this register is always a first operand.
33   return MI.getOperand(0).isReg() ? MI.getOperand(0).getReg() : 0;
34 }
36 void DbgValueHistoryMap::startInstrRange(const MDNode *Var,
37                                          const MachineInstr &MI) {
38   // Instruction range should start with a DBG_VALUE instruction for the
39   // variable.
40   assert(MI.isDebugValue() && getEntireVariable(MI.getDebugVariable()) == Var);
41   auto &Ranges = VarInstrRanges[Var];
42   if (!Ranges.empty() && Ranges.back().second == nullptr &&
43       Ranges.back().first->isIdenticalTo(&MI)) {
44     DEBUG(dbgs() << "Coalescing identical DBG_VALUE entries:\n"
45                  << "\t" << Ranges.back().first << "\t" << MI << "\n");
46     return;
47   }
48   Ranges.push_back(std::make_pair(&MI, nullptr));
49 }
51 void DbgValueHistoryMap::endInstrRange(const MDNode *Var,
52                                        const MachineInstr &MI) {
53   auto &Ranges = VarInstrRanges[Var];
54   // Verify that the current instruction range is not yet closed.
55   assert(!Ranges.empty() && Ranges.back().second == nullptr);
56   // For now, instruction ranges are not allowed to cross basic block
57   // boundaries.
58   assert(Ranges.back().first->getParent() == MI.getParent());
59   Ranges.back().second = &MI;
60 }
62 unsigned DbgValueHistoryMap::getRegisterForVar(const MDNode *Var) const {
63   const auto &I = VarInstrRanges.find(Var);
64   if (I == VarInstrRanges.end())
65     return 0;
66   const auto &Ranges = I->second;
67   if (Ranges.empty() || Ranges.back().second != nullptr)
68     return 0;
69   return isDescribedByReg(*Ranges.back().first);
70 }
72 namespace {
73 // Maps physreg numbers to the variables they describe.
74 typedef std::map<unsigned, SmallVector<const MDNode *, 1>> RegDescribedVarsMap;
75 }
77 // \brief Claim that @Var is not described by @RegNo anymore.
78 static void dropRegDescribedVar(RegDescribedVarsMap &RegVars,
79                                 unsigned RegNo, const MDNode *Var) {
80   const auto &I = RegVars.find(RegNo);
81   assert(RegNo != 0U && I != RegVars.end());
82   auto &VarSet = I->second;
83   const auto &VarPos = std::find(VarSet.begin(), VarSet.end(), Var);
84   assert(VarPos != VarSet.end());
85   VarSet.erase(VarPos);
86   // Don't keep empty sets in a map to keep it as small as possible.
87   if (VarSet.empty())
88     RegVars.erase(I);
89 }
91 // \brief Claim that @Var is now described by @RegNo.
92 static void addRegDescribedVar(RegDescribedVarsMap &RegVars,
93                                unsigned RegNo, const MDNode *Var) {
94   assert(RegNo != 0U);
95   auto &VarSet = RegVars[RegNo];
96   assert(std::find(VarSet.begin(), VarSet.end(), Var) == VarSet.end());
97   VarSet.push_back(Var);
98 }
100 // \brief Terminate the location range for variables described by register
101 // @RegNo by inserting @ClobberingInstr to their history.
102 static void clobberRegisterUses(RegDescribedVarsMap &RegVars, unsigned RegNo,
103                                 DbgValueHistoryMap &HistMap,
104                                 const MachineInstr &ClobberingInstr) {
105   const auto &I = RegVars.find(RegNo);
106   if (I == RegVars.end())
107     return;
108   // Iterate over all variables described by this register and add this
109   // instruction to their history, clobbering it.
110   for (const auto &Var : I->second)
111     HistMap.endInstrRange(Var, ClobberingInstr);
112   RegVars.erase(I);
115 // \brief Collect all registers clobbered by @MI and insert them to @Regs.
116 static void collectClobberedRegisters(const MachineInstr &MI,
117                                       const TargetRegisterInfo *TRI,
118                                       std::set<unsigned> &Regs) {
119   for (const MachineOperand &MO : MI.operands()) {
120     if (!MO.isReg() || !MO.isDef() || !MO.getReg())
121       continue;
122     for (MCRegAliasIterator AI(MO.getReg(), TRI, true); AI.isValid(); ++AI)
123       Regs.insert(*AI);
124   }
127 // \brief Returns the first instruction in @MBB which corresponds to
128 // the function epilogue, or nullptr if @MBB doesn't contain an epilogue.
129 static const MachineInstr *getFirstEpilogueInst(const MachineBasicBlock &MBB) {
130   auto LastMI = MBB.getLastNonDebugInstr();
131   if (LastMI == MBB.end() || !LastMI->isReturn())
132     return nullptr;
133   // Assume that epilogue starts with instruction having the same debug location
134   // as the return instruction.
135   DebugLoc LastLoc = LastMI->getDebugLoc();
136   auto Res = LastMI;
137   for (MachineBasicBlock::const_reverse_iterator I(std::next(LastMI)); I != MBB.rend();
138        ++I) {
139     if (I->getDebugLoc() != LastLoc)
140       return Res;
141     Res = std::prev(I.base());
142   }
143   // If all instructions have the same debug location, assume whole MBB is
144   // an epilogue.
145   return MBB.begin();
148 // \brief Collect registers that are modified in the function body (their
149 // contents is changed only in the prologue and epilogue).
150 static void collectChangingRegs(const MachineFunction *MF,
151                                 const TargetRegisterInfo *TRI,
152                                 std::set<unsigned> &Regs) {
153   for (const auto &MBB : *MF) {
154     auto FirstEpilogueInst = getFirstEpilogueInst(MBB);
155     bool IsInEpilogue = false;
156     for (const auto &MI : MBB) {
157       IsInEpilogue |= &MI == FirstEpilogueInst;
158       if (!MI.getFlag(MachineInstr::FrameSetup) && !IsInEpilogue)
159         collectClobberedRegisters(MI, TRI, Regs);
160     }
161   }
164 void calculateDbgValueHistory(const MachineFunction *MF,
165                               const TargetRegisterInfo *TRI,
166                               DbgValueHistoryMap &Result) {
167   std::set<unsigned> ChangingRegs;
168   collectChangingRegs(MF, TRI, ChangingRegs);
170   RegDescribedVarsMap RegVars;
171   for (const auto &MBB : *MF) {
172     for (const auto &MI : MBB) {
173       if (!MI.isDebugValue()) {
174         // Not a DBG_VALUE instruction. It may clobber registers which describe
175         // some variables.
176         std::set<unsigned> MIClobberedRegs;
177         collectClobberedRegisters(MI, TRI, MIClobberedRegs);
178         for (unsigned RegNo : MIClobberedRegs) {
179           if (ChangingRegs.count(RegNo))
180             clobberRegisterUses(RegVars, RegNo, Result, MI);
181         }
182         continue;
183       }
185       assert(MI.getNumOperands() > 1 && "Invalid DBG_VALUE instruction!");
186       // Use the base variable (without any DW_OP_piece expressions)
187       // as index into History. The full variables including the
188       // piece expressions are attached to the MI.
189       DIVariable Var = getEntireVariable(MI.getDebugVariable());
191       if (unsigned PrevReg = Result.getRegisterForVar(Var))
192         dropRegDescribedVar(RegVars, PrevReg, Var);
194       Result.startInstrRange(Var, MI);
196       if (unsigned NewReg = isDescribedByReg(MI))
197         addRegDescribedVar(RegVars, NewReg, Var);
198     }
200     // Make sure locations for register-described variables are valid only
201     // until the end of the basic block (unless it's the last basic block, in
202     // which case let their liveness run off to the end of the function).
203     if (!MBB.empty() &&  &MBB != &MF->back()) {
204       for (unsigned RegNo : ChangingRegs)
205         clobberRegisterUses(RegVars, RegNo, Result, MBB.back());
206     }
207   }