1 //===-- llvm/CodeGen/AsmPrinter/DbgValueHistoryCalculator.h ----*- C++ -*--===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
10 #ifndef CODEGEN_ASMPRINTER_DBGVALUEHISTORYCALCULATOR_H_
11 #define CODEGEN_ASMPRINTER_DBGVALUEHISTORYCALCULATOR_H_
13 #include "llvm/ADT/MapVector.h"
14 #include "llvm/ADT/SmallVector.h"
16 namespace llvm {
18 class MachineFunction;
19 class MachineInstr;
20 class MDNode;
21 class TargetRegisterInfo;
23 // For each user variable, keep a list of instruction ranges where this variable
24 // is accessible. The variables are listed in order of appearance.
25 class DbgValueHistoryMap {
26 // Each instruction range starts with a DBG_VALUE instruction, specifying the
27 // location of a variable, which is assumed to be valid until the end of the
28 // range. If end is not specified, location is valid until the start
29 // instruction of the next instruction range, or until the end of the
30 // function.
31 public:
32 typedef std::pair<const MachineInstr *, const MachineInstr *> InstrRange;
33 typedef SmallVector<InstrRange, 4> InstrRanges;
34 typedef MapVector<const MDNode *, InstrRanges> InstrRangesMap;
35 private:
36 InstrRangesMap VarInstrRanges;
38 public:
39 void startInstrRange(const MDNode *Var, const MachineInstr &MI);
40 void endInstrRange(const MDNode *Var, const MachineInstr &MI);
41 // Returns register currently describing @Var. If @Var is currently
42 // unaccessible or is not described by a register, returns 0.
43 unsigned getRegisterForVar(const MDNode *Var) const;
45 bool empty() const { return VarInstrRanges.empty(); }
46 void clear() { VarInstrRanges.clear(); }
47 InstrRangesMap::const_iterator begin() const { return VarInstrRanges.begin(); }
48 InstrRangesMap::const_iterator end() const { return VarInstrRanges.end(); }
49 };
51 void calculateDbgValueHistory(const MachineFunction *MF,
52 const TargetRegisterInfo *TRI,
53 DbgValueHistoryMap &Result);
54 }
56 #endif