Remove unused function DebugLocEntry::isEmpty
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DebugLocEntry.h
1 //===-- llvm/CodeGen/DebugLocEntry.h - Entry in debug_loc list -*- C++ -*--===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
10 #ifndef CODEGEN_ASMPRINTER_DEBUGLOCENTRY_H__
11 #define CODEGEN_ASMPRINTER_DEBUGLOCENTRY_H__
12 #include "llvm/IR/Constants.h"
13 #include "llvm/MC/MachineLocation.h"
14 #include "llvm/MC/MCSymbol.h"
16 namespace llvm {
17 class DwarfCompileUnit;
18 class MDNode;
19 /// \brief This struct describes location entries emitted in the .debug_loc
20 /// section.
21 class DebugLocEntry {
22   // Begin and end symbols for the address range that this location is valid.
23   const MCSymbol *Begin;
24   const MCSymbol *End;
26   // Type of entry that this represents.
27   enum EntryType { E_Location, E_Integer, E_ConstantFP, E_ConstantInt };
28   enum EntryType EntryKind;
30   union {
31     int64_t Int;
32     const ConstantFP *CFP;
33     const ConstantInt *CIP;
34   } Constants;
36   // The location in the machine frame.
37   MachineLocation Loc;
39   // The variable to which this location entry corresponds.
40   const MDNode *Variable;
42   // The compile unit to which this location entry is referenced by.
43   const DwarfCompileUnit *Unit;
45   bool hasSameValueOrLocation(const DebugLocEntry &Next) {
46     if (EntryKind != Next.EntryKind)
47       return false;
49     switch (EntryKind) {
50     case E_Location:
51       if (Loc != Next.Loc) return false;
52     case E_Integer:
53       if (Constants.Int != Next.Constants.Int) return false;
54     case E_ConstantFP:
55       if (Constants.CFP != Next.Constants.CFP) return false;
56     case E_ConstantInt:
57       if (Constants.CIP != Next.Constants.CIP) return false;
58     }
60     return true;
61   }
63 public:
64   DebugLocEntry() : Begin(0), End(0), Variable(0), Unit(0) {
65     Constants.Int = 0;
66   }
67   DebugLocEntry(const MCSymbol *B, const MCSymbol *E, MachineLocation &L,
68                 const MDNode *V, const DwarfCompileUnit *U)
69       : Begin(B), End(E), Loc(L), Variable(V), Unit(U) {
70     Constants.Int = 0;
71     EntryKind = E_Location;
72   }
73   DebugLocEntry(const MCSymbol *B, const MCSymbol *E, int64_t i,
74                 const DwarfCompileUnit *U)
75       : Begin(B), End(E), Variable(0), Unit(U) {
76     Constants.Int = i;
77     EntryKind = E_Integer;
78   }
79   DebugLocEntry(const MCSymbol *B, const MCSymbol *E, const ConstantFP *FPtr,
80                 const DwarfCompileUnit *U)
81       : Begin(B), End(E), Variable(0), Unit(U) {
82     Constants.CFP = FPtr;
83     EntryKind = E_ConstantFP;
84   }
85   DebugLocEntry(const MCSymbol *B, const MCSymbol *E, const ConstantInt *IPtr,
86                 const DwarfCompileUnit *U)
87       : Begin(B), End(E), Variable(0), Unit(U) {
88     Constants.CIP = IPtr;
89     EntryKind = E_ConstantInt;
90   }
92   bool Merge(const DebugLocEntry &Next) {
93     return End == Next.Begin && hasSameValueOrLocation(Next);
94   }
95   bool isLocation() const { return EntryKind == E_Location; }
96   bool isInt() const { return EntryKind == E_Integer; }
97   bool isConstantFP() const { return EntryKind == E_ConstantFP; }
98   bool isConstantInt() const { return EntryKind == E_ConstantInt; }
99   int64_t getInt() const { return Constants.Int; }
100   const ConstantFP *getConstantFP() const { return Constants.CFP; }
101   const ConstantInt *getConstantInt() const { return Constants.CIP; }
102   const MDNode *getVariable() const { return Variable; }
103   const MCSymbol *getBeginSym() const { return Begin; }
104   const MCSymbol *getEndSym() const { return End; }
105   const DwarfCompileUnit *getCU() const { return Unit; }
106   MachineLocation getLoc() const { return Loc; }
107 };
110 #endif